1 /*
2 * (C) Copyright 2010
3 * Texas Instruments, <www.ti.com>
4 *
5 * Aneesh V <aneesh@ti.com>
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
25 #include <common.h>
26 #include <spl.h>
27 #include <asm/u-boot.h>
28 #include <nand.h>
29 #include <fat.h>
30 #include <version.h>
31 #include <i2c.h>
32 #include <image.h>
33 #include <malloc.h>
34 #include <linux/compiler.h>
36 DECLARE_GLOBAL_DATA_PTR;
38 #ifndef CONFIG_SYS_UBOOT_START
39 #define CONFIG_SYS_UBOOT_START CONFIG_SYS_TEXT_BASE
40 #endif
41 #ifndef CONFIG_SYS_MONITOR_LEN
42 #define CONFIG_SYS_MONITOR_LEN (200 * 1024)
43 #endif
45 u32 *boot_params_ptr = NULL;
46 struct spl_image_info spl_image;
48 /* Define board data structure */
49 static bd_t bdata __attribute__ ((section(".data")));
51 inline void hang(void)
52 {
53 puts("### ERROR ### Please RESET the board ###\n");
54 for (;;)
55 ;
56 }
58 /*
59 * Default function to determine if u-boot or the OS should
60 * be started. This implementation always returns 1.
61 *
62 * Please implement your own board specific funcion to do this.
63 *
64 * RETURN
65 * 0 to not start u-boot
66 * positive if u-boot should start
67 */
68 #ifdef CONFIG_SPL_OS_BOOT
69 __weak int spl_start_uboot(void)
70 {
71 puts("SPL: Please implement spl_start_uboot() for your board\n");
72 puts("SPL: Direct Linux boot not active!\n");
73 return 1;
74 }
75 #endif
77 void spl_parse_image_header(const struct image_header *header)
78 {
79 u32 header_size = sizeof(struct image_header);
81 if (image_get_magic(header) == IH_MAGIC) {
82 if (spl_image.flags & SPL_COPY_PAYLOAD_ONLY) {
83 /*
84 * On some system (e.g. powerpc), the load-address and
85 * entry-point is located at address 0. We can't load
86 * to 0-0x40. So skip header in this case.
87 */
88 spl_image.load_addr = image_get_load(header);
89 spl_image.entry_point = image_get_ep(header);
90 spl_image.size = image_get_data_size(header);
91 } else {
92 spl_image.entry_point = image_get_load(header);
93 /* Load including the header */
94 spl_image.load_addr = spl_image.entry_point -
95 header_size;
96 spl_image.size = image_get_data_size(header) +
97 header_size;
98 }
99 spl_image.os = image_get_os(header);
100 spl_image.name = image_get_name(header);
101 debug("spl: payload image: %s load addr: 0x%x size: %d\n",
102 spl_image.name, spl_image.load_addr, spl_image.size);
103 } else {
104 /* Signature not found - assume u-boot.bin */
105 debug("mkimage signature not found - ih_magic = %x\n",
106 header->ih_magic);
107 /* Let's assume U-Boot will not be more than 200 KB */
108 spl_image.size = CONFIG_SYS_MONITOR_LEN;
109 spl_image.entry_point = CONFIG_SYS_UBOOT_START;
110 spl_image.load_addr = CONFIG_SYS_TEXT_BASE;
111 spl_image.os = IH_OS_U_BOOT;
112 spl_image.name = "U-Boot";
113 }
114 }
116 __weak void __noreturn jump_to_image_no_args(struct spl_image_info *spl_image)
117 {
118 typedef void __noreturn (*image_entry_noargs_t)(u32 *);
119 image_entry_noargs_t image_entry =
120 (image_entry_noargs_t) spl_image->entry_point;
122 debug("image entry point: 0x%X\n", spl_image->entry_point);
123 /* Pass the saved boot_params from rom code */
124 #if defined(CONFIG_VIRTIO) || defined(CONFIG_ZEBU)
125 image_entry = (image_entry_noargs_t)0x80100000;
126 #endif
127 u32 boot_params_ptr_addr = (u32)&boot_params_ptr;
128 image_entry((u32 *)boot_params_ptr_addr);
129 }
131 #ifdef CONFIG_SPL_RAM_DEVICE
132 static void spl_ram_load_image(void)
133 {
134 const struct image_header *header;
136 /*
137 * Get the header. It will point to an address defined by handoff
138 * which will tell where the image located inside the flash. For
139 * now, it will temporary fixed to address pointed by U-Boot.
140 */
141 header = (struct image_header *)
142 (CONFIG_SYS_TEXT_BASE - sizeof(struct image_header));
144 spl_parse_image_header(header);
145 }
146 #endif
148 void board_init_r(gd_t *dummy1, ulong dummy2)
149 {
150 u32 boot_device;
151 debug(">>spl:board_init_r()\n");
153 #ifdef CONFIG_SYS_SPL_MALLOC_START
154 mem_malloc_init(CONFIG_SYS_SPL_MALLOC_START,
155 CONFIG_SYS_SPL_MALLOC_SIZE);
156 #endif
158 timer_init();
160 #ifdef CONFIG_SPL_BOARD_INIT
161 spl_board_init();
162 #endif
164 boot_device = spl_boot_device();
165 debug("boot device - %d\n", boot_device);
166 switch (boot_device) {
167 #ifdef CONFIG_SPL_RAM_DEVICE
168 case BOOT_DEVICE_RAM:
169 spl_ram_load_image();
170 break;
171 #endif
172 #ifdef CONFIG_SPL_MMC_SUPPORT
173 case BOOT_DEVICE_MMC1:
174 case BOOT_DEVICE_MMC2:
175 case BOOT_DEVICE_MMC2_2:
176 spl_mmc_load_image();
177 break;
178 #endif
179 #ifdef CONFIG_SPL_NAND_SUPPORT
180 case BOOT_DEVICE_NAND:
181 spl_nand_load_image();
182 break;
183 #endif
184 #ifdef CONFIG_SPL_NOR_SUPPORT
185 case BOOT_DEVICE_NOR:
186 spl_nor_load_image();
187 break;
188 #endif
189 #ifdef CONFIG_SPL_YMODEM_SUPPORT
190 case BOOT_DEVICE_UART:
191 spl_ymodem_load_image();
192 break;
193 #endif
194 #ifdef CONFIG_SPL_SPI_SUPPORT
195 case BOOT_DEVICE_SPI:
196 spl_spi_load_image();
197 break;
198 #endif
199 #ifdef CONFIG_SPL_ETH_SUPPORT
200 case BOOT_DEVICE_CPGMAC:
201 #ifdef CONFIG_SPL_ETH_DEVICE
202 spl_net_load_image(CONFIG_SPL_ETH_DEVICE);
203 #else
204 spl_net_load_image(NULL);
205 #endif
206 break;
207 #endif
208 default:
209 debug("SPL: Un-supported Boot Device\n");
210 hang();
211 }
213 switch (spl_image.os) {
214 case IH_OS_U_BOOT:
215 debug("Jumping to U-Boot\n");
216 break;
217 #ifdef CONFIG_SPL_OS_BOOT
218 case IH_OS_LINUX:
219 debug("Jumping to Linux\n");
220 spl_board_prepare_for_linux();
221 jump_to_image_linux((void *)CONFIG_SYS_SPL_ARGS_ADDR);
222 #endif
223 default:
224 debug("Unsupported OS image.. Jumping nevertheless..\n");
225 }
226 jump_to_image_no_args(&spl_image);
227 }
229 /*
230 * This requires UART clocks to be enabled. In order for this to work the
231 * caller must ensure that the gd pointer is valid.
232 */
233 void preloader_console_init(void)
234 {
235 gd->bd = &bdata;
236 gd->baudrate = CONFIG_BAUDRATE;
238 serial_init(); /* serial communications setup */
240 gd->have_console = 1;
242 puts("\nU-Boot SPL " PLAIN_VERSION " (" U_BOOT_DATE " - " \
243 U_BOOT_TIME ")\n");
244 #ifdef CONFIG_SPL_DISPLAY_PRINT
245 spl_display_print();
246 #endif
247 }