]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - config.mk
OMAP4+: Handle sdram init after warm reset
[glsdk/glsdk-u-boot.git] / config.mk
1 #
2 # (C) Copyright 2000-2006
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundation; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 #########################################################################
26 ifeq ($(CURDIR),$(SRCTREE))
27 dir :=
28 else
29 dir := $(subst $(SRCTREE)/,,$(CURDIR))
30 endif
32 ifneq ($(OBJTREE),$(SRCTREE))
33 # Create object files for SPL in a separate directory
34 ifeq ($(CONFIG_SPL_BUILD),y)
35 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
36 else
37 obj := $(if $(dir),$(OBJTREE)/$(dir)/,$(OBJTREE)/)
38 endif
39 src := $(if $(dir),$(SRCTREE)/$(dir)/,$(SRCTREE)/)
41 $(shell mkdir -p $(obj))
42 else
43 # Create object files for SPL in a separate directory
44 ifeq ($(CONFIG_SPL_BUILD),y)
45 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
47 $(shell mkdir -p $(obj))
48 else
49 obj :=
50 endif
51 src :=
52 endif
54 # clean the slate ...
55 PLATFORM_RELFLAGS =
56 PLATFORM_CPPFLAGS =
57 PLATFORM_LDFLAGS =
59 #########################################################################
61 HOSTCFLAGS      = -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer \
62                   $(HOSTCPPFLAGS)
63 HOSTSTRIP       = strip
65 #
66 # Mac OS X / Darwin's C preprocessor is Apple specific.  It
67 # generates numerous errors and warnings.  We want to bypass it
68 # and use GNU C's cpp.  To do this we pass the -traditional-cpp
69 # option to the compiler.  Note that the -traditional-cpp flag
70 # DOES NOT have the same semantics as GNU C's flag, all it does
71 # is invoke the GNU preprocessor in stock ANSI/ISO C fashion.
72 #
73 # Apple's linker is similar, thanks to the new 2 stage linking
74 # multiple symbol definitions are treated as errors, hence the
75 # -multiply_defined suppress option to turn off this error.
76 #
78 ifeq ($(HOSTOS),darwin)
79 # get major and minor product version (e.g. '10' and '6' for Snow Leopard)
80 DARWIN_MAJOR_VERSION    = $(shell sw_vers -productVersion | cut -f 1 -d '.')
81 DARWIN_MINOR_VERSION    = $(shell sw_vers -productVersion | cut -f 2 -d '.')
83 os_x_before     = $(shell if [ $(DARWIN_MAJOR_VERSION) -le $(1) -a \
84         $(DARWIN_MINOR_VERSION) -le $(2) ] ; then echo "$(3)"; else echo "$(4)"; fi ;)
86 # Snow Leopards build environment has no longer restrictions as described above
87 HOSTCC           = $(call os_x_before, 10, 5, "cc", "gcc")
88 HOSTCFLAGS      += $(call os_x_before, 10, 4, "-traditional-cpp")
89 HOSTLDFLAGS     += $(call os_x_before, 10, 5, "-multiply_defined suppress")
90 else
91 HOSTCC          = gcc
92 endif
94 ifeq ($(HOSTOS),cygwin)
95 HOSTCFLAGS      += -ansi
96 endif
98 # We build some files with extra pedantic flags to try to minimize things
99 # that won't build on some weird host compiler -- though there are lots of
100 # exceptions for files that aren't complaint.
102 HOSTCFLAGS_NOPED = $(filter-out -pedantic,$(HOSTCFLAGS))
103 HOSTCFLAGS      += -pedantic
105 #########################################################################
107 # Option checker, gcc version (courtesy linux kernel) to ensure
108 # only supported compiler options are used
110 CC_OPTIONS_CACHE_FILE := $(OBJTREE)/include/generated/cc_options.mk
111 CC_TEST_OFILE := $(OBJTREE)/include/generated/cc_test_file.o
113 -include $(CC_OPTIONS_CACHE_FILE)
115 cc-option-sys = $(shell mkdir -p $(dir $(CC_TEST_OFILE)); \
116                 if $(CC) $(CFLAGS) $(1) -S -xc /dev/null -o $(CC_TEST_OFILE) \
117                 > /dev/null 2>&1; then \
118                 echo 'CC_OPTIONS += $(strip $1)' >> $(CC_OPTIONS_CACHE_FILE); \
119                 echo "$(1)"; fi)
121 ifeq ($(CONFIG_CC_OPT_CACHE_DISABLE),y)
122 cc-option = $(strip $(if $(call cc-option-sys,$1),$1,$2))
123 else
124 cc-option = $(strip $(if $(findstring $1,$(CC_OPTIONS)),$1,\
125                 $(if $(call cc-option-sys,$1),$1,$2)))
126 endif
128 # cc-version
129 # Usage gcc-ver := $(call cc-version)
130 cc-version = $(shell $(SHELL) $(SRCTREE)/tools/gcc-version.sh $(CC))
133 # Include the make variables (CC, etc...)
135 AS      = $(CROSS_COMPILE)as
136 LD      = $(CROSS_COMPILE)ld
137 CC      = $(CROSS_COMPILE)gcc
138 CPP     = $(CC) -E
139 AR      = $(CROSS_COMPILE)ar
140 NM      = $(CROSS_COMPILE)nm
141 LDR     = $(CROSS_COMPILE)ldr
142 STRIP   = $(CROSS_COMPILE)strip
143 OBJCOPY = $(CROSS_COMPILE)objcopy
144 OBJDUMP = $(CROSS_COMPILE)objdump
145 RANLIB  = $(CROSS_COMPILE)RANLIB
146 DTC     = dtc
148 #########################################################################
150 # Load generated board configuration
151 sinclude $(OBJTREE)/include/autoconf.mk
152 sinclude $(OBJTREE)/include/config.mk
154 # Some architecture config.mk files need to know what CPUDIR is set to,
155 # so calculate CPUDIR before including ARCH/SOC/CPU config.mk files.
156 # Check if arch/$ARCH/cpu/$CPU exists, otherwise assume arch/$ARCH/cpu contains
157 # CPU-specific code.
158 CPUDIR=arch/$(ARCH)/cpu/$(CPU)
159 ifneq ($(SRCTREE)/$(CPUDIR),$(wildcard $(SRCTREE)/$(CPUDIR)))
160 CPUDIR=arch/$(ARCH)/cpu
161 endif
163 sinclude $(TOPDIR)/arch/$(ARCH)/config.mk       # include architecture dependend rules
164 sinclude $(TOPDIR)/$(CPUDIR)/config.mk          # include  CPU  specific rules
166 ifdef   SOC
167 sinclude $(TOPDIR)/$(CPUDIR)/$(SOC)/config.mk   # include  SoC  specific rules
168 endif
169 ifdef   VENDOR
170 BOARDDIR = $(VENDOR)/$(BOARD)
171 else
172 BOARDDIR = $(BOARD)
173 endif
174 ifdef   BOARD
175 sinclude $(TOPDIR)/board/$(BOARDDIR)/config.mk  # include board specific rules
176 endif
178 #########################################################################
180 # We don't actually use $(ARFLAGS) anywhere anymore, so catch people
181 # who are porting old code to latest mainline but not updating $(AR).
182 ARFLAGS = $(error update your Makefile to use cmd_link_o_target and not AR)
183 RELFLAGS= $(PLATFORM_RELFLAGS)
184 DBGFLAGS= -g # -DDEBUG
185 OPTFLAGS= -Os #-fomit-frame-pointer
187 OBJCFLAGS += --gap-fill=0xff
189 gccincdir := $(shell $(CC) -print-file-name=include)
191 CPPFLAGS := $(DBGFLAGS) $(OPTFLAGS) $(RELFLAGS)         \
192         -D__KERNEL__
194 # Enable garbage collection of un-used sections for SPL
195 ifeq ($(CONFIG_SPL_BUILD),y)
196 CPPFLAGS += -ffunction-sections -fdata-sections
197 LDFLAGS_FINAL += --gc-sections
198 endif
200 ifneq ($(CONFIG_SYS_TEXT_BASE),)
201 CPPFLAGS += -DCONFIG_SYS_TEXT_BASE=$(CONFIG_SYS_TEXT_BASE)
202 endif
204 ifneq ($(CONFIG_SPL_TEXT_BASE),)
205 CPPFLAGS += -DCONFIG_SPL_TEXT_BASE=$(CONFIG_SPL_TEXT_BASE)
206 endif
208 ifeq ($(CONFIG_SPL_BUILD),y)
209 CPPFLAGS += -DCONFIG_SPL_BUILD
210 endif
212 ifneq ($(RESET_VECTOR_ADDRESS),)
213 CPPFLAGS += -DRESET_VECTOR_ADDRESS=$(RESET_VECTOR_ADDRESS)
214 endif
216 ifneq ($(OBJTREE),$(SRCTREE))
217 CPPFLAGS += -I$(OBJTREE)/include2 -I$(OBJTREE)/include
218 endif
220 CPPFLAGS += -I$(TOPDIR)/include
221 CPPFLAGS += -fno-builtin -ffreestanding -nostdinc       \
222         -isystem $(gccincdir) -pipe $(PLATFORM_CPPFLAGS)
224 ifdef BUILD_TAG
225 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes \
226         -DBUILD_TAG='"$(BUILD_TAG)"'
227 else
228 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes
229 endif
231 CFLAGS_SSP := $(call cc-option,-fno-stack-protector)
232 CFLAGS += $(CFLAGS_SSP)
233 # Some toolchains enable security related warning flags by default,
234 # but they don't make much sense in the u-boot world, so disable them.
235 CFLAGS_WARN := $(call cc-option,-Wno-format-nonliteral) \
236                $(call cc-option,-Wno-format-security)
237 CFLAGS += $(CFLAGS_WARN)
239 # Report stack usage if supported
240 CFLAGS_STACK := $(call cc-option,-fstack-usage)
241 CFLAGS += $(CFLAGS_STACK)
243 # $(CPPFLAGS) sets -g, which causes gcc to pass a suitable -g<format>
244 # option to the assembler.
245 AFLAGS_DEBUG :=
247 # turn jbsr into jsr for m68k
248 ifeq ($(ARCH),m68k)
249 ifeq ($(findstring 3.4,$(shell $(CC) --version)),3.4)
250 AFLAGS_DEBUG := -Wa,-gstabs,-S
251 endif
252 endif
254 AFLAGS := $(AFLAGS_DEBUG) -D__ASSEMBLY__ $(CPPFLAGS)
256 LDFLAGS += $(PLATFORM_LDFLAGS)
257 LDFLAGS_FINAL += -Bstatic
259 LDFLAGS_u-boot += -T $(obj)u-boot.lds $(LDFLAGS_FINAL)
260 ifneq ($(CONFIG_SYS_TEXT_BASE),)
261 LDFLAGS_u-boot += -Ttext $(CONFIG_SYS_TEXT_BASE)
262 endif
264 LDFLAGS_u-boot-spl += -T $(obj)u-boot-spl.lds $(LDFLAGS_FINAL)
265 ifneq ($(CONFIG_SPL_TEXT_BASE),)
266 LDFLAGS_u-boot-spl += -Ttext $(CONFIG_SPL_TEXT_BASE)
267 endif
269 # Location of a usable BFD library, where we define "usable" as
270 # "built for ${HOST}, supports ${TARGET}".  Sensible values are
271 # - When cross-compiling: the root of the cross-environment
272 # - Linux/ppc (native): /usr
273 # - NetBSD/ppc (native): you lose ... (must extract these from the
274 #   binutils build directory, plus the native and U-Boot include
275 #   files don't like each other)
277 # So far, this is used only by tools/gdb/Makefile.
279 ifeq ($(HOSTOS),darwin)
280 BFD_ROOT_DIR =          /usr/local/tools
281 else
282 ifeq ($(HOSTARCH),$(ARCH))
283 # native
284 BFD_ROOT_DIR =          /usr
285 else
286 #BFD_ROOT_DIR =         /LinuxPPC/CDK           # Linux/i386
287 #BFD_ROOT_DIR =         /usr/pkg/cross          # NetBSD/i386
288 BFD_ROOT_DIR =          /opt/powerpc
289 endif
290 endif
292 #########################################################################
294 export  HOSTCC HOSTCFLAGS HOSTLDFLAGS PEDCFLAGS HOSTSTRIP CROSS_COMPILE \
295         AS LD CC CPP AR NM STRIP OBJCOPY OBJDUMP MAKE
296 export  CONFIG_SYS_TEXT_BASE PLATFORM_CPPFLAGS PLATFORM_RELFLAGS CPPFLAGS CFLAGS AFLAGS
298 #########################################################################
300 # Allow boards to use custom optimize flags on a per dir/file basis
301 BCURDIR = $(subst $(SRCTREE)/,,$(CURDIR:$(obj)%=%))
302 ALL_AFLAGS = $(AFLAGS) $(AFLAGS_$(BCURDIR)/$(@F)) $(AFLAGS_$(BCURDIR))
303 ALL_CFLAGS = $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR))
304 EXTRA_CPPFLAGS = $(CPPFLAGS_$(BCURDIR)/$(@F)) $(CPPFLAGS_$(BCURDIR))
305 ALL_CFLAGS += $(EXTRA_CPPFLAGS)
307 # The _DEP version uses the $< file target (for dependency generation)
308 # See rules.mk
309 EXTRA_CPPFLAGS_DEP = $(CPPFLAGS_$(BCURDIR)/$(addsuffix .o,$(basename $<))) \
310                 $(CPPFLAGS_$(BCURDIR))
311 $(obj)%.s:      %.S
312         $(CPP) $(ALL_AFLAGS) -o $@ $<
313 $(obj)%.o:      %.S
314         $(CC)  $(ALL_AFLAGS) -o $@ $< -c
315 $(obj)%.o:      %.c
316         $(CC)  $(ALL_CFLAGS) -o $@ $< -c
317 $(obj)%.i:      %.c
318         $(CPP) $(ALL_CFLAGS) -o $@ $< -c
319 $(obj)%.s:      %.c
320         $(CC)  $(ALL_CFLAGS) -o $@ $< -c -S
322 #########################################################################
324 # If the list of objects to link is empty, just create an empty built-in.o
325 cmd_link_o_target = $(if $(strip $1),\
326                       $(LD) $(LDFLAGS) -r -o $@ $1,\
327                       rm -f $@; $(AR) rcs $@ )
329 #########################################################################