1 #
2 # (C) Copyright 2000-2006
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundation; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 #########################################################################
26 ifeq ($(CURDIR),$(SRCTREE))
27 dir :=
28 else
29 dir := $(subst $(SRCTREE)/,,$(CURDIR))
30 endif
32 ifneq ($(OBJTREE),$(SRCTREE))
33 # Create object files for SPL in a separate directory
34 ifeq ($(CONFIG_SPL_BUILD),y)
35 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
36 else
37 obj := $(if $(dir),$(OBJTREE)/$(dir)/,$(OBJTREE)/)
38 endif
39 src := $(if $(dir),$(SRCTREE)/$(dir)/,$(SRCTREE)/)
41 $(shell mkdir -p $(obj))
42 else
43 # Create object files for SPL in a separate directory
44 ifeq ($(CONFIG_SPL_BUILD),y)
45 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
47 $(shell mkdir -p $(obj))
48 else
49 obj :=
50 endif
51 src :=
52 endif
54 # clean the slate ...
55 PLATFORM_RELFLAGS =
56 PLATFORM_CPPFLAGS =
57 PLATFORM_LDFLAGS =
59 #########################################################################
61 HOSTCFLAGS = -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer \
62 $(HOSTCPPFLAGS)
63 HOSTSTRIP = strip
65 #
66 # Mac OS X / Darwin's C preprocessor is Apple specific. It
67 # generates numerous errors and warnings. We want to bypass it
68 # and use GNU C's cpp. To do this we pass the -traditional-cpp
69 # option to the compiler. Note that the -traditional-cpp flag
70 # DOES NOT have the same semantics as GNU C's flag, all it does
71 # is invoke the GNU preprocessor in stock ANSI/ISO C fashion.
72 #
73 # Apple's linker is similar, thanks to the new 2 stage linking
74 # multiple symbol definitions are treated as errors, hence the
75 # -multiply_defined suppress option to turn off this error.
76 #
78 ifeq ($(HOSTOS),darwin)
79 # get major and minor product version (e.g. '10' and '6' for Snow Leopard)
80 DARWIN_MAJOR_VERSION = $(shell sw_vers -productVersion | cut -f 1 -d '.')
81 DARWIN_MINOR_VERSION = $(shell sw_vers -productVersion | cut -f 2 -d '.')
83 os_x_before = $(shell if [ $(DARWIN_MAJOR_VERSION) -le $(1) -a \
84 $(DARWIN_MINOR_VERSION) -le $(2) ] ; then echo "$(3)"; else echo "$(4)"; fi ;)
86 # Snow Leopards build environment has no longer restrictions as described above
87 HOSTCC = $(call os_x_before, 10, 5, "cc", "gcc")
88 HOSTCFLAGS += $(call os_x_before, 10, 4, "-traditional-cpp")
89 HOSTLDFLAGS += $(call os_x_before, 10, 5, "-multiply_defined suppress")
90 else
91 HOSTCC = gcc
92 endif
94 ifeq ($(HOSTOS),cygwin)
95 HOSTCFLAGS += -ansi
96 endif
98 # We build some files with extra pedantic flags to try to minimize things
99 # that won't build on some weird host compiler -- though there are lots of
100 # exceptions for files that aren't complaint.
102 HOSTCFLAGS_NOPED = $(filter-out -pedantic,$(HOSTCFLAGS))
103 HOSTCFLAGS += -pedantic
105 #########################################################################
106 #
107 # Option checker, gcc version (courtesy linux kernel) to ensure
108 # only supported compiler options are used
109 #
110 CC_OPTIONS_CACHE_FILE := $(OBJTREE)/include/generated/cc_options.mk
111 CC_TEST_OFILE := $(OBJTREE)/include/generated/cc_test_file.o
113 -include $(CC_OPTIONS_CACHE_FILE)
115 cc-option-sys = $(shell mkdir -p $(dir $(CC_TEST_OFILE)); \
116 if $(CC) $(CFLAGS) $(1) -S -xc /dev/null -o $(CC_TEST_OFILE) \
117 > /dev/null 2>&1; then \
118 echo 'CC_OPTIONS += $(strip $1)' >> $(CC_OPTIONS_CACHE_FILE); \
119 echo "$(1)"; fi)
121 ifeq ($(CONFIG_CC_OPT_CACHE_DISABLE),y)
122 cc-option = $(strip $(if $(call cc-option-sys,$1),$1,$2))
123 else
124 cc-option = $(strip $(if $(findstring $1,$(CC_OPTIONS)),$1,\
125 $(if $(call cc-option-sys,$1),$1,$2)))
126 endif
128 # cc-version
129 # Usage gcc-ver := $(call cc-version)
130 cc-version = $(shell $(SHELL) $(SRCTREE)/tools/gcc-version.sh $(CC))
132 #
133 # Include the make variables (CC, etc...)
134 #
135 AS = $(CROSS_COMPILE)as
137 # Always use GNU ld
138 LD = $(shell if $(CROSS_COMPILE)ld.bfd -v > /dev/null 2>&1; \
139 then echo "$(CROSS_COMPILE)ld.bfd"; else echo "$(CROSS_COMPILE)ld"; fi;)
141 CC = $(CROSS_COMPILE)gcc
142 CPP = $(CC) -E
143 AR = $(CROSS_COMPILE)ar
144 NM = $(CROSS_COMPILE)nm
145 LDR = $(CROSS_COMPILE)ldr
146 STRIP = $(CROSS_COMPILE)strip
147 OBJCOPY = $(CROSS_COMPILE)objcopy
148 OBJDUMP = $(CROSS_COMPILE)objdump
149 RANLIB = $(CROSS_COMPILE)RANLIB
150 DTC = dtc
152 #########################################################################
154 # Load generated board configuration
155 sinclude $(OBJTREE)/include/autoconf.mk
156 sinclude $(OBJTREE)/include/config.mk
158 # Some architecture config.mk files need to know what CPUDIR is set to,
159 # so calculate CPUDIR before including ARCH/SOC/CPU config.mk files.
160 # Check if arch/$ARCH/cpu/$CPU exists, otherwise assume arch/$ARCH/cpu contains
161 # CPU-specific code.
162 CPUDIR=arch/$(ARCH)/cpu/$(CPU)
163 ifneq ($(SRCTREE)/$(CPUDIR),$(wildcard $(SRCTREE)/$(CPUDIR)))
164 CPUDIR=arch/$(ARCH)/cpu
165 endif
167 sinclude $(TOPDIR)/arch/$(ARCH)/config.mk # include architecture dependend rules
168 sinclude $(TOPDIR)/$(CPUDIR)/config.mk # include CPU specific rules
170 ifdef SOC
171 sinclude $(TOPDIR)/$(CPUDIR)/$(SOC)/config.mk # include SoC specific rules
172 endif
173 ifdef VENDOR
174 BOARDDIR = $(VENDOR)/$(BOARD)
175 else
176 BOARDDIR = $(BOARD)
177 endif
178 ifdef BOARD
179 sinclude $(TOPDIR)/board/$(BOARDDIR)/config.mk # include board specific rules
180 endif
182 #########################################################################
184 # We don't actually use $(ARFLAGS) anywhere anymore, so catch people
185 # who are porting old code to latest mainline but not updating $(AR).
186 ARFLAGS = $(error update your Makefile to use cmd_link_o_target and not AR)
187 RELFLAGS= $(PLATFORM_RELFLAGS)
188 DBGFLAGS= -g # -DDEBUG
189 OPTFLAGS= -Os #-fomit-frame-pointer
191 OBJCFLAGS += --gap-fill=0xff
193 gccincdir := $(shell $(CC) -print-file-name=include)
195 CPPFLAGS := $(DBGFLAGS) $(OPTFLAGS) $(RELFLAGS) \
196 -D__KERNEL__
198 # Enable garbage collection of un-used sections for SPL
199 ifeq ($(CONFIG_SPL_BUILD),y)
200 CPPFLAGS += -ffunction-sections -fdata-sections
201 LDFLAGS_FINAL += --gc-sections
202 endif
204 ifneq ($(CONFIG_SYS_TEXT_BASE),)
205 CPPFLAGS += -DCONFIG_SYS_TEXT_BASE=$(CONFIG_SYS_TEXT_BASE)
206 endif
208 ifneq ($(CONFIG_SPL_TEXT_BASE),)
209 CPPFLAGS += -DCONFIG_SPL_TEXT_BASE=$(CONFIG_SPL_TEXT_BASE)
210 endif
212 ifneq ($(CONFIG_SPL_PAD_TO),)
213 CPPFLAGS += -DCONFIG_SPL_PAD_TO=$(CONFIG_SPL_PAD_TO)
214 endif
216 ifeq ($(CONFIG_SPL_BUILD),y)
217 CPPFLAGS += -DCONFIG_SPL_BUILD
218 endif
220 ifneq ($(RESET_VECTOR_ADDRESS),)
221 CPPFLAGS += -DRESET_VECTOR_ADDRESS=$(RESET_VECTOR_ADDRESS)
222 endif
224 ifneq ($(OBJTREE),$(SRCTREE))
225 CPPFLAGS += -I$(OBJTREE)/include2 -I$(OBJTREE)/include
226 endif
228 CPPFLAGS += -I$(TOPDIR)/include
229 CPPFLAGS += -fno-builtin -ffreestanding -nostdinc \
230 -isystem $(gccincdir) -pipe $(PLATFORM_CPPFLAGS)
232 ifdef BUILD_TAG
233 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes \
234 -DBUILD_TAG='"$(BUILD_TAG)"'
235 else
236 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes
237 endif
239 CFLAGS_SSP := $(call cc-option,-fno-stack-protector)
240 CFLAGS += $(CFLAGS_SSP)
241 # Some toolchains enable security related warning flags by default,
242 # but they don't make much sense in the u-boot world, so disable them.
243 CFLAGS_WARN := $(call cc-option,-Wno-format-nonliteral) \
244 $(call cc-option,-Wno-format-security)
245 CFLAGS += $(CFLAGS_WARN)
247 # Report stack usage if supported
248 CFLAGS_STACK := $(call cc-option,-fstack-usage)
249 CFLAGS += $(CFLAGS_STACK)
251 # $(CPPFLAGS) sets -g, which causes gcc to pass a suitable -g<format>
252 # option to the assembler.
253 AFLAGS_DEBUG :=
255 # turn jbsr into jsr for m68k
256 ifeq ($(ARCH),m68k)
257 ifeq ($(findstring 3.4,$(shell $(CC) --version)),3.4)
258 AFLAGS_DEBUG := -Wa,-gstabs,-S
259 endif
260 endif
262 AFLAGS := $(AFLAGS_DEBUG) -D__ASSEMBLY__ $(CPPFLAGS)
264 LDFLAGS += $(PLATFORM_LDFLAGS)
265 LDFLAGS_FINAL += -Bstatic
267 LDFLAGS_u-boot += -T $(obj)u-boot.lds $(LDFLAGS_FINAL)
268 ifneq ($(CONFIG_SYS_TEXT_BASE),)
269 LDFLAGS_u-boot += -Ttext $(CONFIG_SYS_TEXT_BASE)
270 endif
272 LDFLAGS_u-boot-spl += -T $(obj)u-boot-spl.lds $(LDFLAGS_FINAL)
273 ifneq ($(CONFIG_SPL_TEXT_BASE),)
274 LDFLAGS_u-boot-spl += -Ttext $(CONFIG_SPL_TEXT_BASE)
275 endif
277 # Location of a usable BFD library, where we define "usable" as
278 # "built for ${HOST}, supports ${TARGET}". Sensible values are
279 # - When cross-compiling: the root of the cross-environment
280 # - Linux/ppc (native): /usr
281 # - NetBSD/ppc (native): you lose ... (must extract these from the
282 # binutils build directory, plus the native and U-Boot include
283 # files don't like each other)
284 #
285 # So far, this is used only by tools/gdb/Makefile.
287 ifeq ($(HOSTOS),darwin)
288 BFD_ROOT_DIR = /usr/local/tools
289 else
290 ifeq ($(HOSTARCH),$(ARCH))
291 # native
292 BFD_ROOT_DIR = /usr
293 else
294 #BFD_ROOT_DIR = /LinuxPPC/CDK # Linux/i386
295 #BFD_ROOT_DIR = /usr/pkg/cross # NetBSD/i386
296 BFD_ROOT_DIR = /opt/powerpc
297 endif
298 endif
300 #########################################################################
302 export HOSTCC HOSTCFLAGS HOSTLDFLAGS PEDCFLAGS HOSTSTRIP CROSS_COMPILE \
303 AS LD CC CPP AR NM STRIP OBJCOPY OBJDUMP MAKE
304 export CONFIG_SYS_TEXT_BASE PLATFORM_CPPFLAGS PLATFORM_RELFLAGS CPPFLAGS CFLAGS AFLAGS
306 #########################################################################
308 # Allow boards to use custom optimize flags on a per dir/file basis
309 BCURDIR = $(subst $(SRCTREE)/,,$(CURDIR:$(obj)%=%))
310 ALL_AFLAGS = $(AFLAGS) $(AFLAGS_$(BCURDIR)/$(@F)) $(AFLAGS_$(BCURDIR))
311 ALL_CFLAGS = $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR))
312 EXTRA_CPPFLAGS = $(CPPFLAGS_$(BCURDIR)/$(@F)) $(CPPFLAGS_$(BCURDIR))
313 ALL_CFLAGS += $(EXTRA_CPPFLAGS)
315 # The _DEP version uses the $< file target (for dependency generation)
316 # See rules.mk
317 EXTRA_CPPFLAGS_DEP = $(CPPFLAGS_$(BCURDIR)/$(addsuffix .o,$(basename $<))) \
318 $(CPPFLAGS_$(BCURDIR))
319 $(obj)%.s: %.S
320 $(CPP) $(ALL_AFLAGS) -o $@ $<
321 $(obj)%.o: %.S
322 $(CC) $(ALL_AFLAGS) -o $@ $< -c
323 $(obj)%.o: %.c
324 $(CC) $(ALL_CFLAGS) -o $@ $< -c
325 $(obj)%.i: %.c
326 $(CPP) $(ALL_CFLAGS) -o $@ $< -c
327 $(obj)%.s: %.c
328 $(CC) $(ALL_CFLAGS) -o $@ $< -c -S
330 #########################################################################
332 # If the list of objects to link is empty, just create an empty built-in.o
333 cmd_link_o_target = $(if $(strip $1),\
334 $(LD) $(LDFLAGS) -r -o $@ $1,\
335 rm -f $@; $(AR) rcs $@ )
337 #########################################################################