]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - config.mk
Makefile: Move SHELL setup to config.mk
[glsdk/glsdk-u-boot.git] / config.mk
1 #
2 # (C) Copyright 2000-2006
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundation; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 #########################################################################
26 # Set shell to bash if possible, otherwise fall back to sh
27 SHELL := $(shell if [ -x "$$BASH" ]; then echo $$BASH; \
28         else if [ -x /bin/bash ]; then echo /bin/bash; \
29         else echo sh; fi; fi)
31 export  SHELL
33 ifeq ($(CURDIR),$(SRCTREE))
34 dir :=
35 else
36 dir := $(subst $(SRCTREE)/,,$(CURDIR))
37 endif
39 ifneq ($(OBJTREE),$(SRCTREE))
40 # Create object files for SPL in a separate directory
41 ifeq ($(CONFIG_SPL_BUILD),y)
42 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
43 else
44 obj := $(if $(dir),$(OBJTREE)/$(dir)/,$(OBJTREE)/)
45 endif
46 src := $(if $(dir),$(SRCTREE)/$(dir)/,$(SRCTREE)/)
48 $(shell mkdir -p $(obj))
49 else
50 # Create object files for SPL in a separate directory
51 ifeq ($(CONFIG_SPL_BUILD),y)
52 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
54 $(shell mkdir -p $(obj))
55 else
56 obj :=
57 endif
58 src :=
59 endif
61 # clean the slate ...
62 PLATFORM_RELFLAGS =
63 PLATFORM_CPPFLAGS =
64 PLATFORM_LDFLAGS =
66 #########################################################################
68 HOSTCFLAGS      = -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer \
69                   $(HOSTCPPFLAGS)
70 HOSTSTRIP       = strip
72 #
73 # Mac OS X / Darwin's C preprocessor is Apple specific.  It
74 # generates numerous errors and warnings.  We want to bypass it
75 # and use GNU C's cpp.  To do this we pass the -traditional-cpp
76 # option to the compiler.  Note that the -traditional-cpp flag
77 # DOES NOT have the same semantics as GNU C's flag, all it does
78 # is invoke the GNU preprocessor in stock ANSI/ISO C fashion.
79 #
80 # Apple's linker is similar, thanks to the new 2 stage linking
81 # multiple symbol definitions are treated as errors, hence the
82 # -multiply_defined suppress option to turn off this error.
83 #
85 ifeq ($(HOSTOS),darwin)
86 # get major and minor product version (e.g. '10' and '6' for Snow Leopard)
87 DARWIN_MAJOR_VERSION    = $(shell sw_vers -productVersion | cut -f 1 -d '.')
88 DARWIN_MINOR_VERSION    = $(shell sw_vers -productVersion | cut -f 2 -d '.')
90 os_x_before     = $(shell if [ $(DARWIN_MAJOR_VERSION) -le $(1) -a \
91         $(DARWIN_MINOR_VERSION) -le $(2) ] ; then echo "$(3)"; else echo "$(4)"; fi ;)
93 # Snow Leopards build environment has no longer restrictions as described above
94 HOSTCC           = $(call os_x_before, 10, 5, "cc", "gcc")
95 HOSTCFLAGS      += $(call os_x_before, 10, 4, "-traditional-cpp")
96 HOSTLDFLAGS     += $(call os_x_before, 10, 5, "-multiply_defined suppress")
97 else
98 HOSTCC          = gcc
99 endif
101 ifeq ($(HOSTOS),cygwin)
102 HOSTCFLAGS      += -ansi
103 endif
105 # We build some files with extra pedantic flags to try to minimize things
106 # that won't build on some weird host compiler -- though there are lots of
107 # exceptions for files that aren't complaint.
109 HOSTCFLAGS_NOPED = $(filter-out -pedantic,$(HOSTCFLAGS))
110 HOSTCFLAGS      += -pedantic
112 #########################################################################
114 # Option checker, gcc version (courtesy linux kernel) to ensure
115 # only supported compiler options are used
117 CC_OPTIONS_CACHE_FILE := $(OBJTREE)/include/generated/cc_options.mk
118 CC_TEST_OFILE := $(OBJTREE)/include/generated/cc_test_file.o
120 -include $(CC_OPTIONS_CACHE_FILE)
122 cc-option-sys = $(shell mkdir -p $(dir $(CC_TEST_OFILE)); \
123                 if $(CC) $(CFLAGS) $(1) -S -xc /dev/null -o $(CC_TEST_OFILE) \
124                 > /dev/null 2>&1; then \
125                 echo 'CC_OPTIONS += $(strip $1)' >> $(CC_OPTIONS_CACHE_FILE); \
126                 echo "$(1)"; fi)
128 ifeq ($(CONFIG_CC_OPT_CACHE_DISABLE),y)
129 cc-option = $(strip $(if $(call cc-option-sys,$1),$1,$2))
130 else
131 cc-option = $(strip $(if $(findstring $1,$(CC_OPTIONS)),$1,\
132                 $(if $(call cc-option-sys,$1),$1,$2)))
133 endif
135 # cc-version
136 # Usage gcc-ver := $(call cc-version)
137 cc-version = $(shell $(SHELL) $(SRCTREE)/tools/gcc-version.sh $(CC))
138 binutils-version = $(shell $(SHELL) $(SRCTREE)/tools/binutils-version.sh $(AS))
141 # Include the make variables (CC, etc...)
143 AS      = $(CROSS_COMPILE)as
145 # Always use GNU ld
146 LD      = $(shell if $(CROSS_COMPILE)ld.bfd -v > /dev/null 2>&1; \
147                 then echo "$(CROSS_COMPILE)ld.bfd"; else echo "$(CROSS_COMPILE)ld"; fi;)
149 CC      = $(CROSS_COMPILE)gcc
150 CPP     = $(CC) -E
151 AR      = $(CROSS_COMPILE)ar
152 NM      = $(CROSS_COMPILE)nm
153 LDR     = $(CROSS_COMPILE)ldr
154 STRIP   = $(CROSS_COMPILE)strip
155 OBJCOPY = $(CROSS_COMPILE)objcopy
156 OBJDUMP = $(CROSS_COMPILE)objdump
157 RANLIB  = $(CROSS_COMPILE)RANLIB
158 DTC     = dtc
159 CHECK   = sparse
161 #########################################################################
163 # Load generated board configuration
164 sinclude $(OBJTREE)/include/autoconf.mk
165 sinclude $(OBJTREE)/include/config.mk
167 # Some architecture config.mk files need to know what CPUDIR is set to,
168 # so calculate CPUDIR before including ARCH/SOC/CPU config.mk files.
169 # Check if arch/$ARCH/cpu/$CPU exists, otherwise assume arch/$ARCH/cpu contains
170 # CPU-specific code.
171 CPUDIR=arch/$(ARCH)/cpu/$(CPU)
172 ifneq ($(SRCTREE)/$(CPUDIR),$(wildcard $(SRCTREE)/$(CPUDIR)))
173 CPUDIR=arch/$(ARCH)/cpu
174 endif
176 sinclude $(TOPDIR)/arch/$(ARCH)/config.mk       # include architecture dependend rules
177 sinclude $(TOPDIR)/$(CPUDIR)/config.mk          # include  CPU  specific rules
179 ifdef   SOC
180 sinclude $(TOPDIR)/$(CPUDIR)/$(SOC)/config.mk   # include  SoC  specific rules
181 endif
182 ifdef   VENDOR
183 BOARDDIR = $(VENDOR)/$(BOARD)
184 else
185 BOARDDIR = $(BOARD)
186 endif
187 ifdef   BOARD
188 sinclude $(TOPDIR)/board/$(BOARDDIR)/config.mk  # include board specific rules
189 endif
191 #########################################################################
193 # We don't actually use $(ARFLAGS) anywhere anymore, so catch people
194 # who are porting old code to latest mainline but not updating $(AR).
195 ARFLAGS = $(error update your Makefile to use cmd_link_o_target and not AR)
196 RELFLAGS= $(PLATFORM_RELFLAGS)
197 DBGFLAGS= -g # -DDEBUG
198 OPTFLAGS= -Os #-fomit-frame-pointer
200 OBJCFLAGS += --gap-fill=0xff
202 gccincdir := $(shell $(CC) -print-file-name=include)
204 CPPFLAGS := $(DBGFLAGS) $(OPTFLAGS) $(RELFLAGS)         \
205         -D__KERNEL__
207 # Enable garbage collection of un-used sections for SPL
208 ifeq ($(CONFIG_SPL_BUILD),y)
209 CPPFLAGS += -ffunction-sections -fdata-sections
210 LDFLAGS_FINAL += --gc-sections
211 endif
213 ifneq ($(CONFIG_SYS_TEXT_BASE),)
214 CPPFLAGS += -DCONFIG_SYS_TEXT_BASE=$(CONFIG_SYS_TEXT_BASE)
215 endif
217 ifneq ($(CONFIG_SPL_TEXT_BASE),)
218 CPPFLAGS += -DCONFIG_SPL_TEXT_BASE=$(CONFIG_SPL_TEXT_BASE)
219 endif
221 ifneq ($(CONFIG_SPL_PAD_TO),)
222 CPPFLAGS += -DCONFIG_SPL_PAD_TO=$(CONFIG_SPL_PAD_TO)
223 endif
225 ifeq ($(CONFIG_SPL_BUILD),y)
226 CPPFLAGS += -DCONFIG_SPL_BUILD
227 endif
229 # Does this architecture support generic board init?
230 ifeq ($(__HAVE_ARCH_GENERIC_BOARD),)
231 ifneq ($(CONFIG_SYS_GENERIC_BOARD),)
232 $(error Your architecture does not support generic board. Please undefined \
233 CONFIG_SYS_GENERIC_BOARD in your board config file)
234 endif
235 endif
237 ifneq ($(RESET_VECTOR_ADDRESS),)
238 CPPFLAGS += -DRESET_VECTOR_ADDRESS=$(RESET_VECTOR_ADDRESS)
239 endif
241 ifneq ($(OBJTREE),$(SRCTREE))
242 CPPFLAGS += -I$(OBJTREE)/include2 -I$(OBJTREE)/include
243 endif
245 CPPFLAGS += -I$(TOPDIR)/include
246 CPPFLAGS += -fno-builtin -ffreestanding -nostdinc       \
247         -isystem $(gccincdir) -pipe $(PLATFORM_CPPFLAGS)
249 ifdef BUILD_TAG
250 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes \
251         -DBUILD_TAG='"$(BUILD_TAG)"'
252 else
253 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes
254 endif
256 CFLAGS_SSP := $(call cc-option,-fno-stack-protector)
257 CFLAGS += $(CFLAGS_SSP)
258 # Some toolchains enable security related warning flags by default,
259 # but they don't make much sense in the u-boot world, so disable them.
260 CFLAGS_WARN := $(call cc-option,-Wno-format-nonliteral) \
261                $(call cc-option,-Wno-format-security)
262 CFLAGS += $(CFLAGS_WARN)
264 # Report stack usage if supported
265 CFLAGS_STACK := $(call cc-option,-fstack-usage)
266 CFLAGS += $(CFLAGS_STACK)
268 # $(CPPFLAGS) sets -g, which causes gcc to pass a suitable -g<format>
269 # option to the assembler.
270 AFLAGS_DEBUG :=
272 # turn jbsr into jsr for m68k
273 ifeq ($(ARCH),m68k)
274 ifeq ($(findstring 3.4,$(shell $(CC) --version)),3.4)
275 AFLAGS_DEBUG := -Wa,-gstabs,-S
276 endif
277 endif
279 AFLAGS := $(AFLAGS_DEBUG) -D__ASSEMBLY__ $(CPPFLAGS)
281 LDFLAGS += $(PLATFORM_LDFLAGS)
282 LDFLAGS_FINAL += -Bstatic
284 LDFLAGS_u-boot += -T $(obj)u-boot.lds $(LDFLAGS_FINAL)
285 ifneq ($(CONFIG_SYS_TEXT_BASE),)
286 LDFLAGS_u-boot += -Ttext $(CONFIG_SYS_TEXT_BASE)
287 endif
289 LDFLAGS_u-boot-spl += -T $(obj)u-boot-spl.lds $(LDFLAGS_FINAL)
290 ifneq ($(CONFIG_SPL_TEXT_BASE),)
291 LDFLAGS_u-boot-spl += -Ttext $(CONFIG_SPL_TEXT_BASE)
292 endif
294 # Linus' kernel sanity checking tool
295 CHECKFLAGS     := -D__linux__ -Dlinux -D__STDC__ -Dunix -D__unix__ \
296                   -Wbitwise -Wno-return-void -D__CHECK_ENDIAN__ $(CF)
298 # Location of a usable BFD library, where we define "usable" as
299 # "built for ${HOST}, supports ${TARGET}".  Sensible values are
300 # - When cross-compiling: the root of the cross-environment
301 # - Linux/ppc (native): /usr
302 # - NetBSD/ppc (native): you lose ... (must extract these from the
303 #   binutils build directory, plus the native and U-Boot include
304 #   files don't like each other)
306 # So far, this is used only by tools/gdb/Makefile.
308 ifeq ($(HOSTOS),darwin)
309 BFD_ROOT_DIR =          /usr/local/tools
310 else
311 ifeq ($(HOSTARCH),$(ARCH))
312 # native
313 BFD_ROOT_DIR =          /usr
314 else
315 #BFD_ROOT_DIR =         /LinuxPPC/CDK           # Linux/i386
316 #BFD_ROOT_DIR =         /usr/pkg/cross          # NetBSD/i386
317 BFD_ROOT_DIR =          /opt/powerpc
318 endif
319 endif
321 #########################################################################
323 export  HOSTCC HOSTCFLAGS HOSTLDFLAGS PEDCFLAGS HOSTSTRIP CROSS_COMPILE \
324         AS LD CC CPP AR NM STRIP OBJCOPY OBJDUMP MAKE
325 export  CONFIG_SYS_TEXT_BASE PLATFORM_CPPFLAGS PLATFORM_RELFLAGS CPPFLAGS CFLAGS AFLAGS
327 #########################################################################
329 # Allow boards to use custom optimize flags on a per dir/file basis
330 BCURDIR = $(subst $(SRCTREE)/,,$(CURDIR:$(obj)%=%))
331 ALL_AFLAGS = $(AFLAGS) $(AFLAGS_$(BCURDIR)/$(@F)) $(AFLAGS_$(BCURDIR))
332 ALL_CFLAGS = $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR))
333 EXTRA_CPPFLAGS = $(CPPFLAGS_$(BCURDIR)/$(@F)) $(CPPFLAGS_$(BCURDIR))
334 ALL_CFLAGS += $(EXTRA_CPPFLAGS)
336 # The _DEP version uses the $< file target (for dependency generation)
337 # See rules.mk
338 EXTRA_CPPFLAGS_DEP = $(CPPFLAGS_$(BCURDIR)/$(addsuffix .o,$(basename $<))) \
339                 $(CPPFLAGS_$(BCURDIR))
340 $(obj)%.s:      %.S
341         $(CPP) $(ALL_AFLAGS) -o $@ $<
342 $(obj)%.o:      %.S
343         $(CC)  $(ALL_AFLAGS) -o $@ $< -c
344 $(obj)%.o:      %.c
345 ifneq ($(CHECKSRC),0)
346         $(CHECK) $(CHECKFLAGS) $(ALL_CFLAGS) $<
347 endif
348         $(CC)  $(ALL_CFLAGS) -o $@ $< -c
349 $(obj)%.i:      %.c
350         $(CPP) $(ALL_CFLAGS) -o $@ $< -c
351 $(obj)%.s:      %.c
352         $(CC)  $(ALL_CFLAGS) -o $@ $< -c -S
354 #########################################################################
356 # If the list of objects to link is empty, just create an empty built-in.o
357 cmd_link_o_target = $(if $(strip $1),\
358                       $(LD) $(LDFLAGS) -r -o $@ $1,\
359                       rm -f $@; $(AR) rcs $@ )
361 #########################################################################