1 #
2 # (C) Copyright 2000-2006
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundation; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 #########################################################################
26 ifeq ($(CURDIR),$(SRCTREE))
27 dir :=
28 else
29 dir := $(subst $(SRCTREE)/,,$(CURDIR))
30 endif
32 ifneq ($(OBJTREE),$(SRCTREE))
33 # Create object files for SPL in a separate directory
34 ifeq ($(CONFIG_SPL_BUILD),y)
35 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
36 else
37 obj := $(if $(dir),$(OBJTREE)/$(dir)/,$(OBJTREE)/)
38 endif
39 src := $(if $(dir),$(SRCTREE)/$(dir)/,$(SRCTREE)/)
41 $(shell mkdir -p $(obj))
42 else
43 # Create object files for SPL in a separate directory
44 ifeq ($(CONFIG_SPL_BUILD),y)
45 obj := $(if $(dir),$(SPLTREE)/$(dir)/,$(SPLTREE)/)
47 $(shell mkdir -p $(obj))
48 else
49 obj :=
50 endif
51 src :=
52 endif
54 # clean the slate ...
55 PLATFORM_RELFLAGS =
56 PLATFORM_CPPFLAGS =
57 PLATFORM_LDFLAGS =
59 #########################################################################
61 HOSTCFLAGS = -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer \
62 $(HOSTCPPFLAGS)
63 HOSTSTRIP = strip
65 #
66 # Mac OS X / Darwin's C preprocessor is Apple specific. It
67 # generates numerous errors and warnings. We want to bypass it
68 # and use GNU C's cpp. To do this we pass the -traditional-cpp
69 # option to the compiler. Note that the -traditional-cpp flag
70 # DOES NOT have the same semantics as GNU C's flag, all it does
71 # is invoke the GNU preprocessor in stock ANSI/ISO C fashion.
72 #
73 # Apple's linker is similar, thanks to the new 2 stage linking
74 # multiple symbol definitions are treated as errors, hence the
75 # -multiply_defined suppress option to turn off this error.
76 #
78 ifeq ($(HOSTOS),darwin)
79 # get major and minor product version (e.g. '10' and '6' for Snow Leopard)
80 DARWIN_MAJOR_VERSION = $(shell sw_vers -productVersion | cut -f 1 -d '.')
81 DARWIN_MINOR_VERSION = $(shell sw_vers -productVersion | cut -f 2 -d '.')
83 os_x_before = $(shell if [ $(DARWIN_MAJOR_VERSION) -le $(1) -a \
84 $(DARWIN_MINOR_VERSION) -le $(2) ] ; then echo "$(3)"; else echo "$(4)"; fi ;)
86 # Snow Leopards build environment has no longer restrictions as described above
87 HOSTCC = $(call os_x_before, 10, 5, "cc", "gcc")
88 HOSTCFLAGS += $(call os_x_before, 10, 4, "-traditional-cpp")
89 HOSTLDFLAGS += $(call os_x_before, 10, 5, "-multiply_defined suppress")
90 else
91 HOSTCC = gcc
92 endif
94 ifeq ($(HOSTOS),cygwin)
95 HOSTCFLAGS += -ansi
96 endif
98 # We build some files with extra pedantic flags to try to minimize things
99 # that won't build on some weird host compiler -- though there are lots of
100 # exceptions for files that aren't complaint.
102 HOSTCFLAGS_NOPED = $(filter-out -pedantic,$(HOSTCFLAGS))
103 HOSTCFLAGS += -pedantic
105 #########################################################################
106 #
107 # Option checker (courtesy linux kernel) to ensure
108 # only supported compiler options are used
109 #
110 cc-option = $(shell if $(CC) $(CFLAGS) $(1) -S -o /dev/null -xc /dev/null \
111 > /dev/null 2>&1; then echo "$(1)"; else echo "$(2)"; fi ;)
113 #
114 # Include the make variables (CC, etc...)
115 #
116 AS = $(CROSS_COMPILE)as
117 LD = $(CROSS_COMPILE)ld
118 CC = $(CROSS_COMPILE)gcc
119 CPP = $(CC) -E
120 AR = $(CROSS_COMPILE)ar
121 NM = $(CROSS_COMPILE)nm
122 LDR = $(CROSS_COMPILE)ldr
123 STRIP = $(CROSS_COMPILE)strip
124 OBJCOPY = $(CROSS_COMPILE)objcopy
125 OBJDUMP = $(CROSS_COMPILE)objdump
126 RANLIB = $(CROSS_COMPILE)RANLIB
128 #########################################################################
130 # Load generated board configuration
131 sinclude $(OBJTREE)/include/autoconf.mk
132 sinclude $(OBJTREE)/include/config.mk
134 # Some architecture config.mk files need to know what CPUDIR is set to,
135 # so calculate CPUDIR before including ARCH/SOC/CPU config.mk files.
136 # Check if arch/$ARCH/cpu/$CPU exists, otherwise assume arch/$ARCH/cpu contains
137 # CPU-specific code.
138 CPUDIR=arch/$(ARCH)/cpu/$(CPU)
139 ifneq ($(SRCTREE)/$(CPUDIR),$(wildcard $(SRCTREE)/$(CPUDIR)))
140 CPUDIR=arch/$(ARCH)/cpu
141 endif
143 sinclude $(TOPDIR)/arch/$(ARCH)/config.mk # include architecture dependend rules
144 sinclude $(TOPDIR)/$(CPUDIR)/config.mk # include CPU specific rules
146 ifdef SOC
147 sinclude $(TOPDIR)/$(CPUDIR)/$(SOC)/config.mk # include SoC specific rules
148 endif
149 ifdef VENDOR
150 BOARDDIR = $(VENDOR)/$(BOARD)
151 else
152 BOARDDIR = $(BOARD)
153 endif
154 ifdef BOARD
155 sinclude $(TOPDIR)/board/$(BOARDDIR)/config.mk # include board specific rules
156 endif
158 #########################################################################
160 ifneq (,$(findstring s,$(MAKEFLAGS)))
161 ARFLAGS = cr
162 else
163 ARFLAGS = crv
164 endif
165 RELFLAGS= $(PLATFORM_RELFLAGS)
166 DBGFLAGS= -g # -DDEBUG
167 OPTFLAGS= -Os #-fomit-frame-pointer
169 OBJCFLAGS += --gap-fill=0xff
171 gccincdir := $(shell $(CC) -print-file-name=include)
173 CPPFLAGS := $(DBGFLAGS) $(OPTFLAGS) $(RELFLAGS) \
174 -D__KERNEL__
176 # Enable garbage collection of un-used sections for SPL
177 ifeq ($(CONFIG_SPL_BUILD),y)
178 CPPFLAGS += -ffunction-sections -fdata-sections
179 LDFLAGS_FINAL += --gc-sections
180 endif
182 ifneq ($(CONFIG_SYS_TEXT_BASE),)
183 CPPFLAGS += -DCONFIG_SYS_TEXT_BASE=$(CONFIG_SYS_TEXT_BASE)
184 endif
186 ifneq ($(CONFIG_SPL_TEXT_BASE),)
187 CPPFLAGS += -DCONFIG_SPL_TEXT_BASE=$(CONFIG_SPL_TEXT_BASE)
188 endif
190 ifeq ($(CONFIG_SPL_BUILD),y)
191 CPPFLAGS += -DCONFIG_SPL_BUILD
192 endif
194 ifneq ($(RESET_VECTOR_ADDRESS),)
195 CPPFLAGS += -DRESET_VECTOR_ADDRESS=$(RESET_VECTOR_ADDRESS)
196 endif
198 ifneq ($(OBJTREE),$(SRCTREE))
199 CPPFLAGS += -I$(OBJTREE)/include2 -I$(OBJTREE)/include
200 endif
202 CPPFLAGS += -I$(TOPDIR)/include
203 CPPFLAGS += -fno-builtin -ffreestanding -nostdinc \
204 -isystem $(gccincdir) -pipe $(PLATFORM_CPPFLAGS)
206 ifdef BUILD_TAG
207 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes \
208 -DBUILD_TAG='"$(BUILD_TAG)"'
209 else
210 CFLAGS := $(CPPFLAGS) -Wall -Wstrict-prototypes
211 endif
213 CFLAGS += $(call cc-option,-fno-stack-protector)
214 # Some toolchains enable security related warning flags by default,
215 # but they don't make much sense in the u-boot world, so disable them.
216 CFLAGS += $(call cc-option,-Wno-format-nonliteral)
217 CFLAGS += $(call cc-option,-Wno-format-security)
219 # $(CPPFLAGS) sets -g, which causes gcc to pass a suitable -g<format>
220 # option to the assembler.
221 AFLAGS_DEBUG :=
223 # turn jbsr into jsr for m68k
224 ifeq ($(ARCH),m68k)
225 ifeq ($(findstring 3.4,$(shell $(CC) --version)),3.4)
226 AFLAGS_DEBUG := -Wa,-gstabs,-S
227 endif
228 endif
230 AFLAGS := $(AFLAGS_DEBUG) -D__ASSEMBLY__ $(CPPFLAGS)
232 LDFLAGS += $(PLATFORM_LDFLAGS)
233 LDFLAGS_FINAL += -Bstatic
235 LDFLAGS_u-boot += -T $(obj)u-boot.lds $(LDFLAGS_FINAL)
236 ifneq ($(CONFIG_SYS_TEXT_BASE),)
237 LDFLAGS_u-boot += -Ttext $(CONFIG_SYS_TEXT_BASE)
238 endif
240 LDFLAGS_u-boot-spl += -T $(obj)u-boot-spl.lds $(LDFLAGS_FINAL)
241 ifneq ($(CONFIG_SPL_TEXT_BASE),)
242 LDFLAGS_u-boot-spl += -Ttext $(CONFIG_SPL_TEXT_BASE)
243 endif
245 # Location of a usable BFD library, where we define "usable" as
246 # "built for ${HOST}, supports ${TARGET}". Sensible values are
247 # - When cross-compiling: the root of the cross-environment
248 # - Linux/ppc (native): /usr
249 # - NetBSD/ppc (native): you lose ... (must extract these from the
250 # binutils build directory, plus the native and U-Boot include
251 # files don't like each other)
252 #
253 # So far, this is used only by tools/gdb/Makefile.
255 ifeq ($(HOSTOS),darwin)
256 BFD_ROOT_DIR = /usr/local/tools
257 else
258 ifeq ($(HOSTARCH),$(ARCH))
259 # native
260 BFD_ROOT_DIR = /usr
261 else
262 #BFD_ROOT_DIR = /LinuxPPC/CDK # Linux/i386
263 #BFD_ROOT_DIR = /usr/pkg/cross # NetBSD/i386
264 BFD_ROOT_DIR = /opt/powerpc
265 endif
266 endif
268 #########################################################################
270 export HOSTCC HOSTCFLAGS HOSTLDFLAGS PEDCFLAGS HOSTSTRIP CROSS_COMPILE \
271 AS LD CC CPP AR NM STRIP OBJCOPY OBJDUMP MAKE
272 export CONFIG_SYS_TEXT_BASE PLATFORM_CPPFLAGS PLATFORM_RELFLAGS CPPFLAGS CFLAGS AFLAGS
274 #########################################################################
276 # Allow boards to use custom optimize flags on a per dir/file basis
277 BCURDIR = $(subst $(SRCTREE)/,,$(CURDIR:$(obj)%=%))
278 ALL_AFLAGS = $(AFLAGS) $(AFLAGS_$(BCURDIR)/$(@F)) $(AFLAGS_$(BCURDIR))
279 ALL_CFLAGS = $(CFLAGS) $(CFLAGS_$(BCURDIR)/$(@F)) $(CFLAGS_$(BCURDIR))
280 $(obj)%.s: %.S
281 $(CPP) $(ALL_AFLAGS) -o $@ $<
282 $(obj)%.o: %.S
283 $(CC) $(ALL_AFLAGS) -o $@ $< -c
284 $(obj)%.o: %.c
285 $(CC) $(ALL_CFLAGS) -o $@ $< -c
286 $(obj)%.i: %.c
287 $(CPP) $(ALL_CFLAGS) -o $@ $< -c
288 $(obj)%.s: %.c
289 $(CC) $(ALL_CFLAGS) -o $@ $< -c -S
291 #########################################################################
293 # If the list of objects to link is empty, just create an empty built-in.o
294 cmd_link_o_target = $(if $(strip $1),\
295 $(LD) $(LDFLAGS) -r -o $@ $1,\
296 rm -f $@; $(AR) rcs $@ )
298 #########################################################################