1 How to configure modem support in U-Boot :
3 1. Define modem initialization strings:
4 ---------------------------------------
6 The modem initialization strings have following format:
8 mdm_init1=<AT-command>
9 mdm_init2=<AT-command>
10 ...
12 Turning off modem verbose responses with ATV0 or ATQ1 is not allowed;
13 U-Boot analyzes only verbose (not numeric) result codes. Modem local
14 command echo can be turned off (ATE0).
16 2. RTS/CTS hardware flow control:
17 ---------------------------------
19 You may wish to enable RTS/CTS hardware flow control, if the board's
20 UART driver supports it (see CONFIG_HWFLOW compile-time flag in
21 config/<board>.h). This is controlled by the 'mdm_flow_control'
22 environment variable:
24 'mdm_flow_control=rts/cts' - to enable RTS/CTS flow control.
25 'mdm_flow_control=none ' - to disable.
28 The following are the examples using a Rockwell OEM modem
29 configuration:
31 SAMSUNG # setenv mdm_init1 ATZ - reset the modem to
32 the factory defaults.
33 SAMSUNG # setenv mdm_init2 ATS0=1 - set modem into
34 answer mode.
35 SAMSUNG # setenv mdm_flow_control rts/cts - enable serial port
36 flow control
37 SAMSUNG # saveenv
39 The example above initializes modem into answer mode to wait for the
40 incoming call. RTS/CTS flow control is enabled for the serial port.
41 (The RTS/CTS flow control is enabled by default on the modem).
44 SAMSUNG # setenv mdm_init1 ATZ
45 SAMSUNG # setenv mdm_init2 ATS39=0+IFC=0,0 - disable modem
46 RTS/CTS flow control
47 SAMSUNG # setenv mdm_init3 ATDT1643973 - dial out the number
48 SAMSUNG # setenv mdm_flow_control none
49 SAMSUNG # saveenv
51 The example above initializes modem to dial-up connection on the
52 number 1643973. Flow control is disabled.
54 Note that flow control must be turned both off or both on for the
55 board serial port and for the modem.
58 If the connection was set up successfully, the U-Boot prompt appears
59 on the terminal console. If not (U-Boot modem was configured for
60 originating the call and connection was not established) - the board
61 should be reset for another dial-up try.
64 Note on the SMDK2400 board:
65 ---------------------------
67 Since the board serial ports does not have DTR signal wired, modem
68 should be told to ignore port DTR setting prior to connection to the
69 SMDK board, and this setting should be stored in modem NVRAM. For the
70 Rockwell OEM modem this can to be done with the following command:
72 AT&D0&W