1 To use SNTP support, add define CONFIG_CMD_SNTP to the
2 configuration file of the board.
4 The "sntp" command gets network time from NTP time server and
5 syncronize RTC of the board. This command needs the command line
6 parameter of server's IP address or environment variable
7 "ntpserverip". The network time is sent as UTC. So if you want to
8 set local time to RTC, set the offset in second from UTC to the
9 environment variable "time offset".
11 If the DHCP server provides time server's IP or time offset, you
12 don't need to set the above environment variables yourself.
14 Current limitations of SNTP support:
15 1. The roundtrip time is ignored.
16 2. Only the 1st NTP server IP, in the option ntp-servers of DHCP, will
17 be used.