923418b1a455a4dc610c4efd4c5f59b5d5da6263
2 Commands are added to U-Boot by creating a new command structure.
3 This is done by first including command.h, then using the U_BOOT_CMD() macro
4 to fill in a cmd_tbl_t struct.
6 U_BOOT_CMD(name,maxargs,repeatable,command,"usage","help")
8 name: is the name of the commad. THIS IS NOT a string.
9 maxargs: the maximum number of arguments this function takes
10 repeatable: either 0 or 1 to indicate if autorepeat is allowed
11 command: Function pointer (*cmd)(struct cmd_tbl_s *, int, int, char *[]);
12 usage: Short description. This is a string
13 help: Long description. This is a string
16 **** Behind the scene ******
18 The structure created is named with a special prefix (__u_boot_list_cmd_)
19 and placed by the linker in a special section.
21 This makes it possible for the final link to extract all commands
22 compiled into any object code and construct a static array so the
23 command can be found in an array starting at _u_boot_list_cmd__start.
25 To ensure that the linker does not discard these symbols when linking
26 full U-Boot we generate a list of all the commands we have built (based
27 on the sections mentioned above) and use that to force the linker to
28 first enter the symbol as undefined in the output object so that there
29 is then a need for the symbol to be kept (this is the UNDEF_SYM logic in
30 the Makefile).
32 If a new board is defined do not forget to define the command section
33 by writing in u-boot.lds ($(TOPDIR)/board/boardname/u-boot.lds) these
34 3 lines:
36 .u_boot_list : {
37 #include "u-boot.lst";
38 }