1 If you are experiencing hangups/data-aborts when trying to display a BMP image,
2 the following might be relevant to your situation...
4 Some architectures cannot handle unaligned memory accesses, and an attempt to
5 perform one will lead to a data abort. On such architectures it is necessary to
6 make sure all data is properly aligned, and in many situations simply choosing
7 a 32 bit aligned address is enough to ensure proper alignment. This is not
8 always the case when dealing with data that has an internal layout such as a
9 BMP image:
11 BMP images have a header that starts with 2 byte-size fields followed by mostly
12 32 bit fields. The packed struct that represents this header can be seen below:
14 typedef struct bmp_header {
15 /* Header */
16 char signature[2];
17 __u32 file_size;
18 __u32 reserved;
19 __u32 data_offset;
20 ... etc
21 } __attribute__ ((packed)) bmp_header_t;
23 When placed in an aligned address such as 0x80a00000, char signature offsets
24 the __u32 fields into unaligned addresses (in our example 0x80a00002,
25 0x80a00006, and so on...). When these fields are accessed by U-Boot, a 32 bit
26 access is generated at a non-32-bit-aligned address, causing a data abort.
27 The proper alignment for BMP images is therefore: 32-bit-aligned-address + 2.