1 Freescale-specific 'hwconfig' options.
3 This file documents Freescale-specific key:value pairs for the 'hwconfig'
4 option. See README.hwconfig for general information about 'hwconfig'.
6 audclk
7 Specific to the P1022DS reference board.
9 This option specifies which of the two oscillator frequencies should be
10 routed to the Wolfson WM8776 codec. The ngPIXIS can be programmed to
11 route either a 11.2896MHz or a 12.288MHz clock. The default is
12 12.288MHz. This option has two effects. First, the MUX on the board
13 will be programmed accordingly. Second, the clock-frequency property
14 in the codec node in the device tree will be updated to the correct
15 value.
17 'audclk:11'
18 Select the 11.2896MHz clock
20 'audclk:12'
21 Select the 12.288MHz clock
23 usb
24 Specific to boards have USB controller
26 This option specifies the following for a USB controller:
28 - which controller mode to use
29 - which USB PHY to use
31 This is used by generic USB device-tree fixup function to update
32 modified values of phy type and controller mode.
34 Also used for configuring multiple USB controllers such that
35 'usbN' (where N is 1, 2, etc. refers to controller no.)
37 'phy_type'
38 Select USB phy type: 'utmi' OR 'ulpi'
40 'dr_mode'
41 Select USB controller mode: 'host', 'peripheral' OR 'otg'
43 Examples:
44 usb1:dr_mode=host;usb2:dr_mode=peripheral'
46 usb1:dr_mode=host,phy_type=utmi;usb2:dr_mode=host'