1 #
2 # Copyright (C) 2012 Samsung Electronics
3 #
4 # Lukasz Majewski <l.majewski@samsung.com>
5 #
6 #
7 # See file CREDITS for list of people who contributed to this
8 # project.
9 #
10 # This program is free software; you can redistribute it and/or
11 # modify it under the terms of the GNU General Public License as
12 # published by the Free Software Foundation; either version 2 of
13 # the License, or (at your option) any later version.
14 #
15 # This program is distributed in the hope that it will be useful,
16 # but WITHOUT ANY WARRANTY; without even the implied warranty of
17 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 # GNU General Public License for more details.
19 #
20 # You should have received a copy of the GNU General Public License
21 # along with this program; if not, write to the Free Software
22 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 # MA 02111-1307 USA
26 Glossary:
27 ========
28 - UUID -(Universally Unique Identifier)
29 - GUID - (Globally Unique ID)
30 - EFI - (Extensible Firmware Interface)
31 - UEFI - (Unified EFI) - EFI evolution
32 - GPT (GUID Partition Table) - it is the EFI standard part
33 - partitions - lists of available partitions (defined at u-boot):
34 ./include/configs/{target}.h
36 Introduction:
37 =============
38 This document describes the GPT partition table format and usage of
39 the gpt command in u-boot.
42 UUID introduction:
43 ====================
45 GPT for marking disks/partitions is using the UUID. It is supposed to be a
46 globally unique value. A UUID is a 16-byte (128-bit) number. The number of
47 theoretically possible UUIDs is therefore about 3 x 10^38.
48 More often UUID is displayed as 32 hexadecimal digits, in 5 groups,
49 separated by hyphens, in the form 8-4-4-4-12 for a total of 36 characters
50 (32 digits and 4 hyphens)
52 For instance, GUID of Linux data partition: EBD0A0A2-B9E5-4433-87C0-68B6B72699C7
54 Historically there are 5 methods to generate this number. The oldest one is
55 combining machine's MAC address and timer (epoch) value.
57 Successive versions are using MD5 hash, random numbers and SHA-1 hash. All major
58 OSes and programming languages are providing libraries to compute UUID (e.g.
59 uuid command line tool).
61 GPT brief explanation:
62 ======================
64 Layout:
65 -------
67 --------------------------------------------------
68 LBA 0 |Protective MBR |
69 ----------------------------------------------------------
70 LBA 1 |Primary GPT Header | Primary
71 -------------------------------------------------- GPT
72 LBA 2 |Entry 1|Entry 2| Entry 3| Entry 4|
73 --------------------------------------------------
74 LBA 3 |Entries 5 - 128 |
75 | |
76 | |
77 ----------------------------------------------------------
78 LBA 34 |Partition 1 |
79 | |
80 -----------------------------------
81 |Partition 2 |
82 | |
83 -----------------------------------
84 |Partition n |
85 | |
86 ----------------------------------------------------------
87 LBA -34 |Entry 1|Entry 2| Entry 3| Entry 4| Secondary
88 -------------------------------------------------- (bkp)
89 LBA -33 |Entries 5 - 128 | GPT
90 | |
91 | |
92 LBA -2 | |
93 --------------------------------------------------
94 LBA -1 |Secondary GPT Header |
95 ----------------------------------------------------------
98 For a legacy reasons, GPT's LBA 0 sector has a MBR structure. It is called
99 "protective MBR".
100 Its first partition entry ID has 0xEE value, and disk software, which is not
101 handling the GPT sees it as a storage device without free space.
103 It is possible to define 128 linearly placed partition entries.
105 "LBA -1" means the last addressable block (in the mmc subsystem:
106 "dev_desc->lba - 1")
108 Primary/Secondary GPT header:
109 ----------------------------
110 Offset Size Description
112 0 8 B Signature ("EFI PART", 45 46 49 20 50 41 52 54)
113 8 4 B Revision (For version 1.0, the value is 00 00 01 00)
114 12 4 B Header size (in bytes, usually 5C 00 00 00 meaning 92 bytes)
115 16 4 B CRC32 of header (0 to header size), with this field zeroed
116 during calculation
117 20 4 B Reserved (ZERO);
118 24 8 B Current LBA (location of this header copy)
119 32 8 B Backup LBA (location of the other header copy)
120 40 8 B First usable LBA for partitions (primary partition table last
121 LBA + 1)
122 48 8 B Last usable LBA (secondary partition table first LBA - 1)
123 56 16 B Disk GUID (also referred as UUID on UNIXes)
124 72 8 B Partition entries starting LBA (always 2 in primary copy)
125 80 4 B Number of partition entries
126 84 4 B Size of a partition entry (usually 128)
127 88 4 B CRC32 of partition array
128 92 * Reserved; must be ZERO (420 bytes for a 512-byte LBA)
130 TOTAL: 512 B
134 IMPORTANT:
136 GPT headers and partition entries are protected by CRC32 (the POSIX CRC32).
138 Primary GPT header and Secondary GPT header have swapped values of "Current LBA"
139 and "Backup LBA" and therefore different CRC32 check-sum.
141 CRC32 for GPT headers (field "CRC of header") are calculated up till
142 "Header size" (92), NOT 512 bytes.
144 CRC32 for partition entries (field "CRC32 of partition array") is calculated for
145 the whole array entry ( Number_of_partition_entries *
146 sizeof(partition_entry_size (usually 128)))
148 Observe, how Secondary GPT is placed in the memory. It is NOT a mirror reflect
149 of the Primary.
152 Partition Entry Format:
153 ----------------------
154 Offset Size Description
156 0 16 B Partition type GUID
157 16 16 B Unique partition GUID
158 32 8 B First LBA (Little Endian)
159 40 8 B Last LBA (inclusive)
160 48 8 B Attribute flags [+]
161 56 72 B Partition name (text)
163 Attribute flags:
164 Bit 0 - System partition
165 Bit 60 - Read-only
166 Bit 62 - Hidden
167 Bit 63 - Not mount
170 Creating GPT partitions in U-Boot:
171 ==============
173 To restore GUID partition table one needs to:
174 1. Define partition layout in the environment.
175 Format of partitions layout:
176 "partitions=uuid_disk=...;name=u-boot,size=60MiB,uuid=...;
177 name=kernel,size=60MiB,uuid=...;"
178 or
179 "partitions=uuid_disk=${uuid_gpt_disk};name=${uboot_name},
180 size=${uboot_size},uuid=${uboot_uuid};"
182 Fields 'name', 'size' and 'uuid' are mandatory for every partition.
183 The field 'start' is optional.
185 2. Define 'CONFIG_EFI_PARTITION' and 'CONFIG_CMD_GPT'
187 2. From u-boot prompt type:
188 gpt write mmc 0 $partitions
191 Useful info:
192 ============
194 Two programs, namely: 'fdisk' and 'parted' are recommended to work with GPT
195 recovery. Parted is able to handle GUID partitions. Unfortunately the 'fdisk'
196 hasn't got such ability.
197 Please, pay attention at -l switch for parted.
199 "uuid" program is recommended to generate UUID string. Moreover it can decode
200 (-d switch) passed in UUID string. It can be used to generate partitions UUID
201 passed to u-boot environment variables.