]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - doc/README.nand
README: qspi usecase and testing documentation.
[glsdk/glsdk-u-boot.git] / doc / README.nand
1 NAND FLASH commands and notes
3 See NOTE below!!!
5 # (C) Copyright 2003
6 # Dave Ellis, SIXNET, dge@sixnetio.com
7 #
8 # See file CREDITS for list of people who contributed to this
9 # project.
10 #
11 # This program is free software; you can redistribute it and/or
12 # modify it under the terms of the GNU General Public License as
13 # published by the Free Software Foundation; either version 2 of
14 # the License, or (at your option) any later version.
15 #
16 # This program is distributed in the hope that it will be useful,
17 # but WITHOUT ANY WARRANTY; without even the implied warranty of
18 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
19 # GNU General Public License for more details.
20 #
21 # You should have received a copy of the GNU General Public License
22 # along with this program; if not, write to the Free Software
23 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 # MA 02111-1307 USA
26 Commands:
28    nand bad
29       Print a list of all of the bad blocks in the current device.
31    nand device
32       Print information about the current NAND device.
34    nand device num
35       Make device `num' the current device and print information about it.
37    nand erase off|partition size
38    nand erase clean [off|partition size]
39       Erase `size' bytes starting at offset `off'. Alternatively partition
40       name can be specified, in this case size will be eventually limited
41       to not exceed partition size (this behaviour applies also to read
42       and write commands). Only complete erase blocks can be erased.
44       If `erase' is specified without an offset or size, the entire flash
45       is erased. If `erase' is specified with partition but without an
46       size, the entire partition is erased.
48       If `clean' is specified, a JFFS2-style clean marker is written to
49       each block after it is erased.
51       This command will not erase blocks that are marked bad. There is
52       a debug option in cmd_nand.c to allow bad blocks to be erased.
53       Please read the warning there before using it, as blocks marked
54       bad by the manufacturer must _NEVER_ be erased.
56    nand info
57       Print information about all of the NAND devices found.
59    nand read addr ofs|partition size
60       Read `size' bytes from `ofs' in NAND flash to `addr'.  Blocks that
61       are marked bad are skipped.  If a page cannot be read because an
62       uncorrectable data error is found, the command stops with an error.
64    nand read.oob addr ofs|partition size
65       Read `size' bytes from the out-of-band data area corresponding to
66       `ofs' in NAND flash to `addr'. This is limited to the 16 bytes of
67       data for one 512-byte page or 2 256-byte pages. There is no check
68       for bad blocks or ECC errors.
70    nand write addr ofs|partition size
71       Write `size' bytes from `addr' to `ofs' in NAND flash.  Blocks that
72       are marked bad are skipped.  If a page cannot be read because an
73       uncorrectable data error is found, the command stops with an error.
75       As JFFS2 skips blocks similarly, this allows writing a JFFS2 image,
76       as long as the image is short enough to fit even after skipping the
77       bad blocks.  Compact images, such as those produced by mkfs.jffs2
78       should work well, but loading an image copied from another flash is
79       going to be trouble if there are any bad blocks.
81    nand write.trimffs addr ofs|partition size
82       Enabled by the CONFIG_CMD_NAND_TRIMFFS macro. This command will write to
83       the NAND flash in a manner identical to the 'nand write' command
84       described above -- with the additional check that all pages at the end
85       of eraseblocks which contain only 0xff data will not be written to the
86       NAND flash. This behaviour is required when flashing UBI images
87       containing UBIFS volumes as per the UBI FAQ[1].
89       [1] http://www.linux-mtd.infradead.org/doc/ubi.html#L_flasher_algo
91    nand write.oob addr ofs|partition size
92       Write `size' bytes from `addr' to the out-of-band data area
93       corresponding to `ofs' in NAND flash. This is limited to the 16 bytes
94       of data for one 512-byte page or 2 256-byte pages. There is no check
95       for bad blocks.
97    nand read.raw addr ofs|partition [count]
98    nand write.raw addr ofs|partition [count]
99       Read or write one or more pages at "ofs" in NAND flash, from or to
100       "addr" in memory.  This is a raw access, so ECC is avoided and the
101       OOB area is transferred as well.  If count is absent, it is assumed
102       to be one page.  As with .yaffs2 accesses, the data is formatted as
103       a packed sequence of "data, oob, data, oob, ..." -- no alignment of
104       individual pages is maintained.
106 Configuration Options:
108    CONFIG_CMD_NAND
109       Enables NAND support and commmands.
111    CONFIG_CMD_NAND_TORTURE
112       Enables the torture command (see description of this command below).
114    CONFIG_MTD_NAND_ECC_JFFS2
115       Define this if you want the Error Correction Code information in
116       the out-of-band data to be formatted to match the JFFS2 file system.
117       CONFIG_MTD_NAND_ECC_YAFFS would be another useful choice for
118       someone to implement.
120    CONFIG_SYS_MAX_NAND_DEVICE
121       The maximum number of NAND devices you want to support.
123    CONFIG_SYS_NAND_MAX_CHIPS
124       The maximum number of NAND chips per device to be supported.
126    CONFIG_SYS_NAND_SELF_INIT
127       Traditionally, glue code in drivers/mtd/nand/nand.c has driven
128       the initialization process -- it provides the mtd and nand
129       structs, calls a board init function for a specific device,
130       calls nand_scan(), and registers with mtd.
132       This arrangement does not provide drivers with the flexibility to
133       run code between nand_scan_ident() and nand_scan_tail(), or other
134       deviations from the "normal" flow.
136       If a board defines CONFIG_SYS_NAND_SELF_INIT, drivers/mtd/nand/nand.c
137       will make one call to board_nand_init(), with no arguments.  That
138       function is responsible for calling a driver init function for
139       each NAND device on the board, that performs all initialization
140       tasks except setting mtd->name, and registering with the rest of
141       U-Boot.  Those last tasks are accomplished by calling  nand_register()
142       on the new mtd device.
144       Example of new init to be added to the end of an existing driver
145       init:
147         /*
148          * devnum is the device number to be used in nand commands
149          * and in mtd->name.  Must be less than
150          * CONFIG_SYS_NAND_MAX_DEVICE.
151          */
152         mtd = &nand_info[devnum];
154         /* chip is struct nand_chip, and is now provided by the driver. */
155         mtd->priv = &chip;
157         /*
158          * Fill in appropriate values if this driver uses these fields,
159          * or uses the standard read_byte/write_buf/etc. functions from
160          * nand_base.c that use these fields.
161          */
162         chip.IO_ADDR_R = ...;
163         chip.IO_ADDR_W = ...;
165         if (nand_scan_ident(mtd, CONFIG_SYS_MAX_NAND_CHIPS, NULL))
166                 error out
168         /*
169          * Insert here any code you wish to run after the chip has been
170          * identified, but before any other I/O is done.
171          */
173         if (nand_scan_tail(mtd))
174                 error out
176         if (nand_register(devnum))
177                 error out
179       In addition to providing more flexibility to the driver, it reduces
180       the difference between a U-Boot driver and its Linux counterpart.
181       nand_init() is now reduced to calling board_nand_init() once, and
182       printing a size summary.  This should also make it easier to
183       transition to delayed NAND initialization.
185       Please convert your driver even if you don't need the extra
186       flexibility, so that one day we can eliminate the old mechanism.
188 NOTE:
189 =====
191 The current NAND implementation is based on what is in recent
192 Linux kernels.  The old legacy implementation has been removed.
194 If you have board code which used CONFIG_NAND_LEGACY, you'll need
195 to convert to the current NAND interface for it to continue to work.
197 The Disk On Chip driver is currently broken and has been for some time.
198 There is a driver in drivers/mtd/nand, taken from Linux, that works with
199 the current NAND system but has not yet been adapted to the u-boot
200 environment.
202 Additional improvements to the NAND subsystem by Guido Classen, 10-10-2006
204 JFFS2 related commands:
206   implement "nand erase clean" and old "nand erase"
207   using both the new code which is able to skip bad blocks
208   "nand erase clean" additionally writes JFFS2-cleanmarkers in the oob.
210 Miscellaneous and testing commands:
211   "markbad [offset]"
212   create an artificial bad block (for testing bad block handling)
214   "scrub [offset length]"
215   like "erase" but don't skip bad block. Instead erase them.
216   DANGEROUS!!! Factory set bad blocks will be lost. Use only
217   to remove artificial bad blocks created with the "markbad" command.
219   "torture offset"
220   Torture block to determine if it is still reliable.
221   Enabled by the CONFIG_CMD_NAND_TORTURE configuration option.
222   This command returns 0 if the block is still reliable, else 1.
223   If the block is detected as unreliable, it is up to the user to decide to
224   mark this block as bad.
225   The analyzed block is put through 3 erase / write cycles (or less if the block
226   is detected as unreliable earlier).
227   This command can be used in scripts, e.g. together with the markbad command to
228   automate retries and handling of possibly newly detected bad blocks if the
229   nand write command fails.
230   It can also be used manually by users having seen some NAND errors in logs to
231   search the root cause of these errors.
232   The underlying nand_torture() function is also useful for code willing to
233   automate actions following a nand->write() error. This would e.g. be required
234   in order to program or update safely firmware to NAND, especially for the UBI
235   part of such firmware.
238 NAND locking command (for chips with active LOCKPRE pin)
240   "nand lock"
241   set NAND chip to lock state (all pages locked)
243   "nand lock tight"
244   set NAND chip to lock tight state (software can't change locking anymore)
246   "nand lock status"
247   displays current locking status of all pages
249   "nand unlock [offset] [size]"
250   unlock consecutive area (can be called multiple times for different areas)
252   "nand unlock.allexcept [offset] [size]"
253   unlock all except specified consecutive area
255 I have tested the code with board containing 128MiB NAND large page chips
256 and 32MiB small page chips.