1 This driver supports NE2000 compatible cards (those based on DP8390,
2 DP83902 and similar). It can be used with PCMCIA/CF cards provided
3 that the CCR is correctly initialized.
5 The code is based on sources from the Linux kernel (pcnet_cs.c,
6 8390.h) and eCOS(if_dp83902a.c, if_dp83902a.h). Both of these 2
7 wonderful world are GPL, so this is, of course, GPL.
9 I developed and tested this driver on a custom PXA255 based system and
10 with a billionton CF network card connected to the PCMCIA interface of
11 the micro (have a look at README.PXA_CF for the support of this port).
13 The options you have to specify in the config file are (with the
14 value for my board as an example):
16 #define CONFIG_DRIVER_NE2000
18 - Enables the driver
20 #define CONFIG_DRIVER_NE2000_BASE (0x20000000+0x300)
22 - Address where the board is mapped
24 #define CONFIG_DRIVER_NE2000_CCR (0x28000000+0x3f8)
26 - Address of the CCR (card configuration register). It could be found
27 by enabling DEBUG in cmd_pcmcia.c. If this is not defined nothing is
28 done as far as PCMCIA support is concerned.
30 #define CONFIG_DRIVER_NE2000_VAL (0x20)
32 - The value to be written in the CCR. It selects among different I/O
33 spaces that could be used by the card.
36 Enjoy!
38 Christian Pellegrin <chri@ascensit.com>