2 Summary
3 =======
5 This README is about U-Boot support for TI's ARM Cortex-A8 based OMAP3 [1]
6 family of SoCs. TI's OMAP3 SoC family contains an ARM Cortex-A8. Additionally,
7 some family members contain a TMS320C64x+ DSP and/or an Imagination SGX 2D/3D
8 graphics processor and various other standard peripherals.
10 Currently the following boards are supported:
12 * OMAP3530 BeagleBoard [2]
14 * Gumstix Overo [3]
16 * TI EVM [4]
18 * OpenPandora Ltd. Pandora [5]
20 * TI/Logic PD Zoom MDK [6]
22 * TI/Logic PD Zoom 2 [7]
24 * CompuLab Ltd. CM-T35 [8]
26 Toolchain
27 =========
29 While ARM Cortex-A8 support ARM v7 instruction set (-march=armv7a) we compile
30 with -march=armv5 to allow more compilers to work. For U-Boot code this has
31 no performance impact.
33 Build
34 =====
36 * BeagleBoard:
38 make omap3_beagle_config
39 make
41 * Gumstix Overo:
43 make omap3_overo_config
44 make
46 * TI EVM:
48 make omap3_evm_config
49 make
51 * Pandora:
53 make omap3_pandora_config
54 make
56 * Zoom MDK:
58 make omap3_zoom1_config
59 make
61 * Zoom 2:
63 make omap3_zoom2_config
64 make
66 * CM-T35:
68 make cm_t35_config
69 make
71 * BlueLYNX-X:
73 make omap3_mvblx_config
74 make
76 Custom commands
77 ===============
79 To make U-Boot for OMAP3 support NAND device SW or HW ECC calculation, U-Boot
80 for OMAP3 supports custom user command
82 nandecc hw/sw
84 To be compatible with NAND drivers using SW ECC (e.g. kernel code)
86 nandecc sw
88 enables SW ECC calculation. HW ECC enabled with
90 nandecc hw
92 is typically used to write 2nd stage bootloader (known as 'x-loader') which is
93 executed by OMAP3's boot rom and therefore has to be written with HW ECC.
95 For all other commands see
97 help
99 Interfaces
100 ==========
102 gpio
103 ----
105 To set a bit :
107 if (!gpio_request(N, "")) {
108 gpio_direction_output(N, 0);
109 gpio_set_value(N, 1);
110 }
112 To clear a bit :
114 if (!gpio_request(N, "")) {
115 gpio_direction_output(N, 0);
116 gpio_set_value(N, 0);
117 }
119 To read a bit :
121 if (!gpio_request(N, "")) {
122 gpio_direction_input(N);
123 val = gpio_get_value(N);
124 gpio_free(N);
125 }
126 if (val)
127 printf("GPIO N is set\n");
128 else
129 printf("GPIO N is clear\n");
131 dma
132 ---
133 void omap3_dma_init(void)
134 Init the DMA module
135 int omap3_dma_get_conf_chan(uint32_t chan, struct dma4_chan *config);
136 Read config of the channel
137 int omap3_dma_conf_chan(uint32_t chan, struct dma4_chan *config);
138 Write config to the channel
139 int omap3_dma_conf_transfer(uint32_t chan, uint32_t *src, uint32_t *dst,
140 uint32_t sze)
141 Config source, destination and size of a transfer
142 int omap3_dma_wait_for_transfer(uint32_t chan)
143 Wait for a transfer to end - this hast to be called before a channel
144 or the data the channel transferd are used.
145 int omap3_dma_get_revision(uint32_t *minor, uint32_t *major)
146 Read silicon Revision of the DMA module
148 NAND
149 ====
151 There are some OMAP3 devices out there with NAND attached. Due to the fact that
152 OMAP3 ROM code can only handle 1-bit hamming ECC for accessing first page
153 (place where SPL lives) we require this setup for u-boot at least when reading
154 the second progam within SPL. A lot of newer NAND chips however require more
155 than 1-bit ECC for the pages, some can live with 1-bit for the first page. To
156 handle this we can switch to another ECC algorithm after reading the payload
157 within SPL.
159 BCH8
160 ----
162 To enable hardware assisted BCH8 (8-bit BCH [Bose, Chaudhuri, Hocquenghem]) on
163 OMAP3 devices we can use the BCH library in lib/bch.c. To do so add CONFIG_BCH
164 to enable the library and CONFIG_NAND_OMAP_BCH8 to to enable hardware assisted
165 syndrom generation to your board config.
166 The NAND OOB layout is the same as in linux kernel, if the linux kernel BCH8
167 implementation for OMAP3 works for you so the u-boot version should also.
168 When you require the SPL to read with BCH8 there are two more configs to
169 change:
171 * CONFIG_SYS_NAND_ECCPOS (must be the same as .eccpos in
172 GPMC_NAND_HW_BCH8_ECC_LAYOUT defined in
173 arch/arm/include/asm/arch-omap3/omap_gpmc.h)
174 * CONFIG_SYS_NAND_ECCSIZE must be 512
175 * CONFIG_SYS_NAND_ECCBYTES must be 13 for this BCH8 setup
177 Acknowledgements
178 ================
180 OMAP3 U-Boot is based on U-Boot tar ball [9] for BeagleBoard and EVM done by
181 several TI employees.
183 Links
184 =====
186 [1] OMAP3:
188 http://www.ti.com/omap3 (high volume) and
189 http://www.ti.com/omap35x (broad market)
191 [2] OMAP3530 BeagleBoard:
193 http://beagleboard.org/
195 [3] Gumstix Overo:
197 http://www.gumstix.net/Overo/
199 [4] TI EVM:
201 http://focus.ti.com/docs/toolsw/folders/print/tmdxevm3503.html
203 [5] OpenPandora Ltd. Pandora:
205 http://openpandora.org/
207 [6] TI/Logic PD Zoom MDK:
209 http://www.logicpd.com/products/devkit/ti/zoom_mobile_development_kit
211 [7] TI/Logic PD Zoom 2
213 http://www.logicpd.com/sites/default/files/1012659A_Zoom_OMAP34x-II_MDP_Brief.pdf
215 [8] CompuLab Ltd. CM-T35:
217 http://www.compulab.co.il/t3530/html/t3530-cm-datasheet.htm
219 [9] TI OMAP3 U-Boot:
221 http://beagleboard.googlecode.com/files/u-boot_beagle_revb.tar.gz