1 PowerPC 440
3 Last Update: September 11, 2002
4 =======================================================================
7 OVERVIEW
8 ============
10 Support for the ppc440 is contained in the cpu/ppc44x directory
11 and enabled via the CONFIG_440 flag. It is largely based on the
12 405gp code. A sample board support implementation is contained
13 in the board/ebony directory.
15 All testing was performed using the AMCC Ebony board using both
16 Rev B and Rev C silicon. However, since the Rev B. silicon has
17 extensive errata, support for Rev B. is minimal (it boots, and
18 features such as i2c, pci, tftpboot, etc. seem to work ok).
19 The expectation is that all new board designs will be using
20 Rev C or later parts -- if not, you may be in for a rough ride ;-)
22 The ppc440 port does a fair job of keeping "board-specific" code
23 out of the "cpu-specific" source. The goal of course was to
24 provide mechanisms for each board to customize without having
25 to clutter the cpu-specific source with a lot of ifdefs. Most
26 of these mechanisms are described in the following sections.
29 MEMORY MANAGEMENT
30 =================
32 The ppc440 doesn't run in "real mode". The MMU must be active
33 at all times. Additionally, the 440 implements a 36-bit physical
34 memory space that gets mapped into the PowerPC 32-bit virtual
35 address space. So things like memory-mapped peripherals, etc must
36 all be mapped in. Once this is done, the 32-bit virtual address
37 space is then viewed as though it were physical memory.
39 However, this means that memory, peripherals, etc can be configured
40 to appear (mostly) anywhere in the virtual address space. Each board
41 must define its own mappings using the tlbtab (see board/ebony/init.S).
42 The actual TLB setup is performed by the cpu-specific code.
44 Although each board is free to define its own mappings, there are
45 several definitions to be aware of. These definitions may be used in
46 the cpu-specific code (vs. board-specific code), so you should
47 at least review these before deciding to make any changes ... it
48 will probably save you some headaches ;-)
50 CONFIG_SYS_SDRAM_BASE - The virtual address where SDRAM is mapped (always 0)
52 CONFIG_SYS_FLASH_BASE - The virtual address where FLASH is mapped.
54 CONFIG_SYS_PCI_MEMBASE - The virtual address where PCI-bus memory is mapped.
55 This mapping provides access to PCI-bus memory.
57 CONFIG_SYS_PERIPHERAL_BASE - The virtual address where the 440 memory-mapped
58 peripherals are mapped. (e.g. -- UART registers, IIC registers, etc).
60 CONFIG_SYS_ISRAM_BASE - The virtual address where the 440 internal SRAM is
61 mapped. The internal SRAM is equivalent to 405gp OCM and is used
62 for the initial stack.
64 CONFIG_SYS_PCI_BASE - The virtual address where the 440 PCI-x bridge config
65 registers are mapped.
67 CONFIG_SYS_PCI_TARGBASE - The PCI address that is mapped to the virtual address
68 defined by CONFIG_SYS_PCI_MEMBASE.
71 UART / SERIAL
72 =================
74 The UART port works fine when an external serial clock is provided
75 (like the one on the Ebony board) and when using internal clocking.
76 This is controlled with the CONFIG_SYS_EXT_SERIAL_CLOCK flag. When using
77 internal clocking, the "ideal baud rate" settings in the 440GP
78 user manual are automatically calculated.
81 I2C
82 =================
84 The i2c utilities have been tested on both Rev B. and Rev C. and
85 look good. The 'i2c probe' command implementation has been updated to
86 allow for 'skipped' addresses. Some i2c slaves are write only and
87 cause problems when a probe (read) is performed (for example the
88 CDCV850 clock controller at address 0x69 on the ebony board).
90 To prevent probing certain addresses you can define the
91 CONFIG_SYS_I2C_NOPROBES macro in your board-specific header file. When
92 defined, all specified addresses are skipped during a probe.
93 The addresses that are skipped will be displayed in the output
94 of the 'i2c probe' command.
96 For example, to prevent probing address 0x69, define the macro as
97 follows:
99 #define CONFIG_SYS_I2C_NOPROBES {0x69}
101 Similarly, to prevent probing addresses 0x69 and 0x70, define the
102 macro a:
104 #define CONFIG_SYS_I2C_NOPROBES {0x69, 0x70}
107 DDR SDRAM CONTROLLER
108 ====================
110 SDRAM controller intialization using Serial Presence Detect (SPD) is
111 now supported (thanks Jun). It is enabled by defining CONFIG_SPD_EEPROM.
112 The i2c eeprom addresses are controlled by the SPD_EEPROM_ADDRESS macro.
114 NOTE: The SPD_EEPROM_ADDRESS macro is defined differently than for other
115 processors. Traditionally, it defined a single address. For the 440 it
116 defines an array of addresses to support multiple banks. Address order
117 is significant: the addresses are used in order to program the BankN
118 registers. For example, two banks with i2c addresses of 0x53 (bank 0)
119 and 0x52 (bank 1) would be defined as follows:
121 #define SPD_EEPROM_ADDRESS {0x53,0x52}
124 PCI-X BRIDGE
125 ====================
127 PCI is an area that requires lots of flexibility since every board has
128 its own set of constraints and configuration. This section describes the
129 440 implementation.
131 CPC0_STRP1[PISE] -- if the PISE strap bit is not asserted, PCI init
132 is aborted and an indication is printed. This is NOT considered an
133 error -- only an indication that PCI shouldn't be initialized. This
134 gives you a chance to edit the i2c bootstrap eeproms using the i2c
135 utilities once you get to the U-Boot command prompt. NOTE: the default
136 440 bootstrap options (not using i2c eeprom) negates this bit.
138 The cpu-specific code sets up a default pci_controller structure
139 that maps in a single PCI I/O space and PCI memory space. The I/O
140 space begins at PCI I/O address 0 and the PCI memory space is
141 256 MB starting at PCI address CONFIG_SYS_PCI_TARGBASE. After the
142 pci_controller structure is initialized, the cpu-specific code will
143 call the routine pci_pre_init(). This routine is implemented by
144 board-specific code & is where the board can over-ride/extend the
145 default pci_controller structure settings and exspecially provide
146 a routine to map the PCI interrupts and do other pre-initialization
147 tasks. If pci_pre_init() returns a value of zero, PCI initialization
148 is aborted; otherwise the controller structure is registered and
149 initialization continues.
151 The default 440GP PCI target configuration is minimal -- it assumes that
152 the strapping registers are set as necessary. Since the strapping bits
153 provide very limited flexibility, you may want to customize the boards
154 target configuration. If CONFIG_SYS_PCI_TARGET_INIT is defined, the cpu-specific
155 code will call the routine pci_target_init() which you must implement
156 in your board-specific code.
158 Target initialization is completed by the cpu-specific code by
159 initializing the subsystem id and subsystem vendor id, and then ensuring
160 that the 'enable host configuration' bit in the PCIX0_BRDGOPT2 is set.
162 The default PCI master initialization maps in 256 MB of pci memory
163 starting at PCI address CONFIG_SYS_PCI_MEMBASE. To customize this, define
164 PCI_MASTER_INIT. This will call the routine pci_master_init() in your
165 board-specific code rather than performing the default master
166 initialization.
168 The decision to perform PCI host configuration must often be determined
169 at run time. The ppc440 port differs from most other implementations in
170 that it requires the board to determine its host configuration at run
171 time rather than by using compile-time flags. This shouldn't create a
172 large impact on the board-specific code since the board only needs to
173 implement a single routine that returns a zero or non-zero value:
174 is_pci_host().
176 Justification for this becomes clear when considering systems running
177 in a cPCI environment:
179 1. Arbiter strapping: Many cPCI boards provide an external arbiter (often
180 part of the PCI-to-PCI bridge). Even though the arbiter is external (the
181 arbiter strapping is negated), the CPU may still be required to perform
182 local PCI bus configuration.
184 2. Host only: PPMC boards must sample the MONARCH# signal at run-time.
185 Depending on the configuration of the carrier boar, the PPMC board must
186 determine if it should configure the PCI bus at run-time. And in most
187 cases, access to the MONARCH# signal is board-specific (e.g. via
188 board-specific FPGA registers, etc).
190 In any event, the is_pci_host() routine gives each board the opportunity
191 to decide at run-time. If your board is always configured a certain way,
192 then just hardcode a return of 1 or 0 as appropriate.
195 Regards,
196 --Scott
197 <smcnutt@artesyncp.com>