1 /***********************************************************************
2 *
3 * Copyright (C) 2004 by FS Forth-Systeme GmbH.
4 * All rights reserved.
5 *
6 * $Id: ns9750_serial.c,v 1.1 2004/02/16 10:37:20 mpietrek Exp $
7 * @Author: Markus Pietrek
8 * @Descr: Serial driver for the NS9750. Only one UART is supported yet.
9 * @References: [1] NS9750 Hardware Reference/December 2003
10 * @TODO: Implement Character GAP Timer when chip is fixed for PLL bypass
11 *
12 * This program is free software; you can redistribute it and/or
13 * modify it under the terms of the GNU General Public License as
14 * published by the Free Software Foundation; either version 2 of
15 * the License, or (at your option) any later version.
16 *
17 * This program is distributed in the hope that it will be useful,
18 * but WITHOUT ANY WARRANTY; without even the implied warranty of
19 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
20 * GNU General Public License for more details.
21 *
22 * You should have received a copy of the GNU General Public License
23 * along with this program; if not, write to the Free Software
24 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
25 * MA 02111-1307 USA
26 *
27 ***********************************************************************/
29 #include <common.h>
31 #include "ns9750_bbus.h" /* for GPIOs */
32 #include "ns9750_ser.h" /* for serial configuration */
34 DECLARE_GLOBAL_DATA_PTR;
36 #if !defined(CONFIG_CONS_INDEX)
37 #error "No console index specified."
38 #endif
40 #define CONSOLE CONFIG_CONS_INDEX
42 static unsigned int calcBitrateRegister( void );
43 static unsigned int calcRxCharGapRegister( void );
45 static char cCharsAvailable; /* Numbers of chars in unCharCache */
46 static unsigned int unCharCache; /* unCharCache is only valid if
47 * cCharsAvailable > 0 */
49 /***********************************************************************
50 * @Function: serial_init
51 * @Return: 0
52 * @Descr: configures GPIOs and UART. Requires BBUS Master Reset turned off
53 ***********************************************************************/
55 static int ns9750_serial_init(void)
56 {
57 unsigned int aunGPIOTxD[] = { 0, 8, 40, 44 };
58 unsigned int aunGPIORxD[] = { 1, 9, 41, 45 };
60 cCharsAvailable = 0;
62 /* configure TxD and RxD pins for their special function */
63 set_gpio_cfg_reg_val( aunGPIOTxD[ CONSOLE ],
64 NS9750_GPIO_CFG_FUNC_0 | NS9750_GPIO_CFG_OUTPUT );
65 set_gpio_cfg_reg_val( aunGPIORxD[ CONSOLE ],
66 NS9750_GPIO_CFG_FUNC_0 | NS9750_GPIO_CFG_INPUT );
68 /* configure serial engine */
69 *get_ser_reg_addr_channel( NS9750_SER_CTRL_A, CONSOLE ) =
70 NS9750_SER_CTRL_A_CE |
71 NS9750_SER_CTRL_A_STOP |
72 NS9750_SER_CTRL_A_WLS_8;
74 serial_setbrg();
76 *get_ser_reg_addr_channel( NS9750_SER_CTRL_B, CONSOLE ) =
77 NS9750_SER_CTRL_B_RCGT;
79 return 0;
80 }
82 /***********************************************************************
83 * @Function: serial_putc
84 * @Return: n/a
85 * @Descr: writes one character to the FIFO. Blocks until FIFO is not full
86 ***********************************************************************/
88 static void ns9750_serial_putc(const char c)
89 {
90 if (c == '\n')
91 serial_putc( '\r' );
93 while (!(*get_ser_reg_addr_channel( NS9750_SER_STAT_A, CONSOLE) &
94 NS9750_SER_STAT_A_TRDY ) ) {
95 /* do nothing, wait for characters in FIFO sent */
96 }
98 *(volatile char*) get_ser_reg_addr_channel( NS9750_SER_FIFO,
99 CONSOLE) = c;
100 }
102 /***********************************************************************
103 * @Function: serial_getc
104 * @Return: the character read
105 * @Descr: performs only 8bit accesses to the FIFO. No error handling
106 ***********************************************************************/
108 static int ns9750_serial_getc(void)
109 {
110 int i;
112 while (!serial_tstc() ) {
113 /* do nothing, wait for incoming characters */
114 }
116 /* at least one character in unCharCache */
117 i = (int) (unCharCache & 0xff);
119 unCharCache >>= 8;
120 cCharsAvailable--;
122 return i;
123 }
125 /***********************************************************************
126 * @Function: serial_tstc
127 * @Return: 0 if no input available, otherwise != 0
128 * @Descr: checks for incoming FIFO not empty. Stores the incoming chars in
129 * unCharCache and the numbers of characters in cCharsAvailable
130 ***********************************************************************/
132 static int ns9750_serial_tstc(void)
133 {
134 unsigned int unRegCache;
136 if ( cCharsAvailable )
137 return 1;
139 unRegCache = *get_ser_reg_addr_channel( NS9750_SER_STAT_A,CONSOLE );
140 if( unRegCache & NS9750_SER_STAT_A_RBC ) {
141 *get_ser_reg_addr_channel( NS9750_SER_STAT_A, CONSOLE ) =
142 NS9750_SER_STAT_A_RBC;
143 unRegCache = *get_ser_reg_addr_channel( NS9750_SER_STAT_A,
144 CONSOLE );
145 }
147 if ( unRegCache & NS9750_SER_STAT_A_RRDY ) {
148 cCharsAvailable = (unRegCache & NS9750_SER_STAT_A_RXFDB_MA)>>20;
149 if ( !cCharsAvailable )
150 cCharsAvailable = 4;
152 unCharCache = *get_ser_reg_addr_channel( NS9750_SER_FIFO,
153 CONSOLE );
154 return 1;
155 }
157 /* no chars available */
158 return 0;
159 }
161 static void ns9750_serial_setbrg(void)
162 {
163 *get_ser_reg_addr_channel( NS9750_SER_BITRATE, CONSOLE ) =
164 calcBitrateRegister();
165 *get_ser_reg_addr_channel( NS9750_SER_RX_CHAR_TIMER, CONSOLE ) =
166 calcRxCharGapRegister();
167 }
169 /***********************************************************************
170 * @Function: calcBitrateRegister
171 * @Return: value for the serial bitrate register
172 * @Descr: register value depends on clock frequency and baudrate
173 ***********************************************************************/
175 static unsigned int calcBitrateRegister( void )
176 {
177 return ( NS9750_SER_BITRATE_EBIT |
178 NS9750_SER_BITRATE_CLKMUX_BCLK |
179 NS9750_SER_BITRATE_TMODE |
180 NS9750_SER_BITRATE_TCDR_16 |
181 NS9750_SER_BITRATE_RCDR_16 |
182 ( ( ( ( CONFIG_SYS_CLK_FREQ / 8 ) / /* BBUS clock,[1] Fig. 38 */
183 ( gd->baudrate * 16 ) ) - 1 ) &
184 NS9750_SER_BITRATE_N_MA ) );
185 }
187 /***********************************************************************
188 * @Function: calcRxCharGapRegister
189 * @Return: value for the character gap timer register
190 * @Descr: register value depends on clock frequency and baudrate. Currently 0
191 * is used as there is a bug with the gap timer in PLL bypass mode.
192 ***********************************************************************/
194 static unsigned int calcRxCharGapRegister( void )
195 {
196 return NS9750_SER_RX_CHAR_TIMER_TRUN;
197 }
199 static struct serial_device ns9750_serial_drv = {
200 .name = "ns9750_serial",
201 .start = ns9750_serial_init,
202 .stop = NULL,
203 .setbrg = ns9750_serial_setbrg,
204 .putc = ns9750_serial_putc,
205 .puts = default_serial_puts,
206 .getc = ns9750_serial_getc,
207 .tstc = ns9750_serial_tstc,
208 };
210 void ns9750_serial_initialize(void)
211 {
212 serial_register(&ns9750_serial_drv);
213 }
215 __weak struct serial_device *default_serial_console(void)
216 {
217 return &ns9750_serial_drv;
218 }