1 /*
2 * Copyright (C) 2012 Samsung Electronics
3 * R. Chandrasekar <rcsekar@samsung.com>
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #include <asm/arch/clk.h>
25 #include <asm/arch/pinmux.h>
26 #include <asm/arch/i2s-regs.h>
27 #include <asm/io.h>
28 #include <common.h>
29 #include <sound.h>
30 #include <i2s.h>
32 #define FIC_TX2COUNT(x) (((x) >> 24) & 0xf)
33 #define FIC_TX1COUNT(x) (((x) >> 16) & 0xf)
34 #define FIC_TXCOUNT(x) (((x) >> 8) & 0xf)
35 #define FIC_RXCOUNT(x) (((x) >> 0) & 0xf)
36 #define FICS_TXCOUNT(x) (((x) >> 8) & 0x7f)
38 #define TIMEOUT_I2S_TX 100 /* i2s transfer timeout */
40 /*
41 * Sets the frame size for I2S LR clock
42 *
43 * @param i2s_reg i2s regiter address
44 * @param rfs Frame Size
45 */
46 static void i2s_set_lr_framesize(struct i2s_reg *i2s_reg, unsigned int rfs)
47 {
48 unsigned int mod = readl(&i2s_reg->mod);
50 mod &= ~MOD_RCLK_MASK;
52 switch (rfs) {
53 case 768:
54 mod |= MOD_RCLK_768FS;
55 break;
56 case 512:
57 mod |= MOD_RCLK_512FS;
58 break;
59 case 384:
60 mod |= MOD_RCLK_384FS;
61 break;
62 default:
63 mod |= MOD_RCLK_256FS;
64 break;
65 }
67 writel(mod, &i2s_reg->mod);
68 }
70 /*
71 * Sets the i2s transfer control
72 *
73 * @param i2s_reg i2s regiter address
74 * @param on 1 enable tx , 0 disable tx transfer
75 */
76 static void i2s_txctrl(struct i2s_reg *i2s_reg, int on)
77 {
78 unsigned int con = readl(&i2s_reg->con);
79 unsigned int mod = readl(&i2s_reg->mod) & ~MOD_MASK;
81 if (on) {
82 con |= CON_ACTIVE;
83 con &= ~CON_TXCH_PAUSE;
85 } else {
87 con |= CON_TXCH_PAUSE;
88 con &= ~CON_ACTIVE;
89 }
91 writel(mod, &i2s_reg->mod);
92 writel(con, &i2s_reg->con);
93 }
95 /*
96 * set the bit clock frame size (in multiples of LRCLK)
97 *
98 * @param i2s_reg i2s regiter address
99 * @param bfs bit Frame Size
100 */
101 static void i2s_set_bitclk_framesize(struct i2s_reg *i2s_reg, unsigned bfs)
102 {
103 unsigned int mod = readl(&i2s_reg->mod);
105 mod &= ~MOD_BCLK_MASK;
107 switch (bfs) {
108 case 48:
109 mod |= MOD_BCLK_48FS;
110 break;
111 case 32:
112 mod |= MOD_BCLK_32FS;
113 break;
114 case 24:
115 mod |= MOD_BCLK_24FS;
116 break;
117 case 16:
118 mod |= MOD_BCLK_16FS;
119 break;
120 default:
121 return;
122 }
123 writel(mod, &i2s_reg->mod);
124 }
126 /*
127 * flushes the i2stx fifo
128 *
129 * @param i2s_reg i2s regiter address
130 * @param flush Tx fifo flush command (0x00 - do not flush
131 * 0x80 - flush tx fifo)
132 */
133 void i2s_fifo(struct i2s_reg *i2s_reg, unsigned int flush)
134 {
135 /* Flush the FIFO */
136 setbits_le32(&i2s_reg->fic, flush);
137 clrbits_le32(&i2s_reg->fic, flush);
138 }
140 /*
141 * Set System Clock direction
142 *
143 * @param i2s_reg i2s regiter address
144 * @param dir Clock direction
145 *
146 * @return int value 0 for success, -1 in case of error
147 */
148 int i2s_set_sysclk_dir(struct i2s_reg *i2s_reg, int dir)
149 {
150 unsigned int mod = readl(&i2s_reg->mod);
152 if (dir == SND_SOC_CLOCK_IN)
153 mod |= MOD_CDCLKCON;
154 else
155 mod &= ~MOD_CDCLKCON;
157 writel(mod, &i2s_reg->mod);
159 return 0;
160 }
162 /*
163 * Sets I2S Clcok format
164 *
165 * @param fmt i2s clock properties
166 * @param i2s_reg i2s regiter address
167 *
168 * @return int value 0 for success, -1 in case of error
169 */
170 int i2s_set_fmt(struct i2s_reg *i2s_reg, unsigned int fmt)
171 {
172 unsigned int mod = readl(&i2s_reg->mod);
173 unsigned int tmp = 0;
174 unsigned int ret = 0;
176 /* Format is priority */
177 switch (fmt & SND_SOC_DAIFMT_FORMAT_MASK) {
178 case SND_SOC_DAIFMT_RIGHT_J:
179 tmp |= MOD_LR_RLOW;
180 tmp |= MOD_SDF_MSB;
181 break;
182 case SND_SOC_DAIFMT_LEFT_J:
183 tmp |= MOD_LR_RLOW;
184 tmp |= MOD_SDF_LSB;
185 break;
186 case SND_SOC_DAIFMT_I2S:
187 tmp |= MOD_SDF_IIS;
188 break;
189 default:
190 debug("%s: Invalid format priority [0x%x]\n", __func__,
191 (fmt & SND_SOC_DAIFMT_FORMAT_MASK));
192 return -1;
193 }
195 /*
196 * INV flag is relative to the FORMAT flag - if set it simply
197 * flips the polarity specified by the Standard
198 */
199 switch (fmt & SND_SOC_DAIFMT_INV_MASK) {
200 case SND_SOC_DAIFMT_NB_NF:
201 break;
202 case SND_SOC_DAIFMT_NB_IF:
203 if (tmp & MOD_LR_RLOW)
204 tmp &= ~MOD_LR_RLOW;
205 else
206 tmp |= MOD_LR_RLOW;
207 break;
208 default:
209 debug("%s: Invalid clock ploarity input [0x%x]\n", __func__,
210 (fmt & SND_SOC_DAIFMT_INV_MASK));
211 return -1;
212 }
214 switch (fmt & SND_SOC_DAIFMT_MASTER_MASK) {
215 case SND_SOC_DAIFMT_CBS_CFS:
216 tmp |= MOD_SLAVE;
217 break;
218 case SND_SOC_DAIFMT_CBM_CFM:
219 /* Set default source clock in Master mode */
220 ret = i2s_set_sysclk_dir(i2s_reg, SND_SOC_CLOCK_OUT);
221 if (ret != 0) {
222 debug("%s:set i2s clock direction failed\n", __func__);
223 return -1;
224 }
225 break;
226 default:
227 debug("%s: Invalid master selection [0x%x]\n", __func__,
228 (fmt & SND_SOC_DAIFMT_MASTER_MASK));
229 return -1;
230 }
232 mod &= ~(MOD_SDF_MASK | MOD_LR_RLOW | MOD_SLAVE);
233 mod |= tmp;
234 writel(mod, &i2s_reg->mod);
236 return 0;
237 }
239 /*
240 * Sets the sample width in bits
241 *
242 * @param blc samplewidth (size of sample in bits)
243 * @param i2s_reg i2s regiter address
244 *
245 * @return int value 0 for success, -1 in case of error
246 */
247 int i2s_set_samplesize(struct i2s_reg *i2s_reg, unsigned int blc)
248 {
249 unsigned int mod = readl(&i2s_reg->mod);
251 mod &= ~MOD_BLCP_MASK;
252 mod &= ~MOD_BLC_MASK;
254 switch (blc) {
255 case 8:
256 mod |= MOD_BLCP_8BIT;
257 mod |= MOD_BLC_8BIT;
258 break;
259 case 16:
260 mod |= MOD_BLCP_16BIT;
261 mod |= MOD_BLC_16BIT;
262 break;
263 case 24:
264 mod |= MOD_BLCP_24BIT;
265 mod |= MOD_BLC_24BIT;
266 break;
267 default:
268 debug("%s: Invalid sample size input [0x%x]\n",
269 __func__, blc);
270 return -1;
271 }
272 writel(mod, &i2s_reg->mod);
274 return 0;
275 }
277 int i2s_transfer_tx_data(struct i2stx_info *pi2s_tx, unsigned int *data,
278 unsigned long data_size)
279 {
280 int i;
281 int start;
282 struct i2s_reg *i2s_reg =
283 (struct i2s_reg *)pi2s_tx->base_address;
285 if (data_size < FIFO_LENGTH) {
286 debug("%s : Invalid data size\n", __func__);
287 return -1; /* invalid pcm data size */
288 }
290 /* fill the tx buffer before stating the tx transmit */
291 for (i = 0; i < FIFO_LENGTH; i++)
292 writel(*data++, &i2s_reg->txd);
294 data_size -= FIFO_LENGTH;
295 i2s_txctrl(i2s_reg, I2S_TX_ON);
297 while (data_size > 0) {
298 start = get_timer(0);
299 if (!(CON_TXFIFO_FULL & (readl(&i2s_reg->con)))) {
300 writel(*data++, &i2s_reg->txd);
301 data_size--;
302 } else {
303 if (get_timer(start) > TIMEOUT_I2S_TX) {
304 i2s_txctrl(i2s_reg, I2S_TX_OFF);
305 debug("%s: I2S Transfer Timeout\n", __func__);
306 return -1;
307 }
308 }
309 }
310 i2s_txctrl(i2s_reg, I2S_TX_OFF);
312 return 0;
313 }
315 int i2s_tx_init(struct i2stx_info *pi2s_tx)
316 {
317 int ret;
318 struct i2s_reg *i2s_reg =
319 (struct i2s_reg *)pi2s_tx->base_address;
321 /* Initialize GPIO for I2s */
322 exynos_pinmux_config(PERIPH_ID_I2S1, 0);
324 /* Set EPLL Clock */
325 ret = set_epll_clk(pi2s_tx->audio_pll_clk);
326 if (ret != 0) {
327 debug("%s: epll clock set rate falied\n", __func__);
328 return -1;
329 }
331 /* Select Clk Source for Audio1 */
332 set_i2s_clk_source();
334 /* Set Prescaler to get MCLK */
335 set_i2s_clk_prescaler(pi2s_tx->audio_pll_clk,
336 (pi2s_tx->samplingrate * (pi2s_tx->rfs)));
338 /* Configure I2s format */
339 ret = i2s_set_fmt(i2s_reg, (SND_SOC_DAIFMT_I2S | SND_SOC_DAIFMT_NB_NF |
340 SND_SOC_DAIFMT_CBM_CFM));
341 if (ret == 0) {
342 i2s_set_lr_framesize(i2s_reg, pi2s_tx->rfs);
343 ret = i2s_set_samplesize(i2s_reg, pi2s_tx->bitspersample);
344 if (ret != 0) {
345 debug("%s:set sample rate failed\n", __func__);
346 return -1;
347 }
349 i2s_set_bitclk_framesize(i2s_reg, pi2s_tx->bfs);
350 /* disable i2s transfer flag and flush the fifo */
351 i2s_txctrl(i2s_reg, I2S_TX_OFF);
352 i2s_fifo(i2s_reg, FIC_TXFLUSH);
353 } else {
354 debug("%s: failed\n", __func__);
355 }
357 return ret;
358 }