1 /*
2 * This file implements recording of each stage of the boot process. It is
3 * intended to implement timing of each stage, reporting this information
4 * to the user and passing it to the OS for logging / further analysis.
5 *
6 * Copyright (c) 2011 The Chromium OS Authors.
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
26 #ifndef _BOOTSTAGE_H
27 #define _BOOTSTAGE_H
29 /* The number of boot stage records available for the user */
30 #ifndef CONFIG_BOOTSTAGE_USER_COUNT
31 #define CONFIG_BOOTSTAGE_USER_COUNT 20
32 #endif
34 /*
35 * A list of boot stages that we know about. Each of these indicates the
36 * state that we are at, and the action that we are about to perform. For
37 * errors, we issue an error for an item when it fails. Therefore the
38 * normal sequence is:
39 *
40 * progress action1
41 * progress action2
42 * progress action3
43 *
44 * and an error condition where action 3 failed would be:
45 *
46 * progress action1
47 * progress action2
48 * progress action3
49 * error on action3
50 */
51 enum bootstage_id {
52 BOOTSTAGE_ID_START = 0,
53 BOOTSTAGE_ID_CHECK_MAGIC, /* Checking image magic */
54 BOOTSTAGE_ID_CHECK_HEADER, /* Checking image header */
55 BOOTSTAGE_ID_CHECK_CHECKSUM, /* Checking image checksum */
56 BOOTSTAGE_ID_CHECK_ARCH, /* Checking architecture */
58 BOOTSTAGE_ID_CHECK_IMAGETYPE = 5,/* Checking image type */
59 BOOTSTAGE_ID_DECOMP_IMAGE, /* Decompressing image */
60 BOOTSTAGE_ID_KERNEL_LOADED, /* Kernel has been loaded */
61 BOOTSTAGE_ID_DECOMP_UNIMPL = 7, /* Odd decompression algorithm */
62 BOOTSTAGE_ID_CHECK_BOOT_OS, /* Calling OS-specific boot function */
63 BOOTSTAGE_ID_BOOT_OS_RETURNED, /* Tried to boot OS, but it returned */
64 BOOTSTAGE_ID_CHECK_RAMDISK = 9, /* Checking ram disk */
66 BOOTSTAGE_ID_RD_MAGIC, /* Checking ram disk magic */
67 BOOTSTAGE_ID_RD_HDR_CHECKSUM, /* Checking ram disk heder checksum */
68 BOOTSTAGE_ID_RD_CHECKSUM, /* Checking ram disk checksum */
69 BOOTSTAGE_ID_COPY_RAMDISK = 12, /* Copying ram disk into place */
70 BOOTSTAGE_ID_RAMDISK, /* Checking for valid ramdisk */
71 BOOTSTAGE_ID_NO_RAMDISK, /* No ram disk found (not an error) */
73 BOOTSTAGE_ID_RUN_OS = 15, /* Exiting U-Boot, entering OS */
75 BOOTSTAGE_ID_NEED_RESET = 30,
76 BOOTSTAGE_ID_POST_FAIL, /* Post failure */
77 BOOTSTAGE_ID_POST_FAIL_R, /* Post failure reported after reloc */
79 /*
80 * This set is reported ony by x86, and the meaning is different. In
81 * this case we are reporting completion of a particular stage.
82 * This should probably change in he x86 code (which doesn't report
83 * errors in any case), but discussion this can perhaps wait until we
84 * have a generic board implementation.
85 */
86 BOOTSTAGE_ID_BOARD_INIT_R, /* We have relocated */
87 BOOTSTAGE_ID_BOARD_GLOBAL_DATA, /* Global data is set up */
89 BOOTSTAGE_ID_BOARD_INIT_SEQ, /* We completed the init sequence */
90 BOOTSTAGE_ID_BOARD_FLASH, /* We have configured flash banks */
91 BOOTSTAGE_ID_BOARD_FLASH_37, /* In case you didn't hear... */
92 BOOTSTAGE_ID_BOARD_ENV, /* Environment is relocated & ready */
93 BOOTSTAGE_ID_BOARD_PCI, /* PCI is up */
95 BOOTSTAGE_ID_BOARD_INTERRUPTS, /* Exceptions / interrupts ready */
96 BOOTSTAGE_ID_BOARD_DONE, /* Board init done, off to main loop */
97 /* ^^^ here ends the x86 sequence */
99 /* Boot stages related to loading a kernel from an IDE device */
100 BOOTSTAGE_ID_IDE_START = 41,
101 BOOTSTAGE_ID_IDE_ADDR,
102 BOOTSTAGE_ID_IDE_BOOT_DEVICE,
103 BOOTSTAGE_ID_IDE_TYPE,
105 BOOTSTAGE_ID_IDE_PART,
106 BOOTSTAGE_ID_IDE_PART_INFO,
107 BOOTSTAGE_ID_IDE_PART_TYPE,
108 BOOTSTAGE_ID_IDE_PART_READ,
109 BOOTSTAGE_ID_IDE_FORMAT,
111 BOOTSTAGE_ID_IDE_CHECKSUM, /* 50 */
112 BOOTSTAGE_ID_IDE_READ,
114 /* Boot stages related to loading a kernel from an NAND device */
115 BOOTSTAGE_ID_NAND_PART,
116 BOOTSTAGE_ID_NAND_SUFFIX,
117 BOOTSTAGE_ID_NAND_BOOT_DEVICE,
118 BOOTSTAGE_ID_NAND_HDR_READ = 55,
119 BOOTSTAGE_ID_NAND_AVAILABLE = 55,
120 BOOTSTAGE_ID_NAND_TYPE = 57,
121 BOOTSTAGE_ID_NAND_READ,
123 /* Boot stages related to loading a kernel from an network device */
124 BOOTSTAGE_ID_NET_CHECKSUM = 60,
125 BOOTSTAGE_ID_NET_ETH_START = 64,
126 BOOTSTAGE_ID_NET_ETH_INIT,
128 BOOTSTAGE_ID_NET_START = 80,
129 BOOTSTAGE_ID_NET_NETLOOP_OK,
130 BOOTSTAGE_ID_NET_LOADED,
131 BOOTSTAGE_ID_NET_DONE_ERR,
132 BOOTSTAGE_ID_NET_DONE,
134 /*
135 * Boot stages related to loading a FIT image. Some of these are a
136 * bit wonky.
137 */
138 BOOTSTAGE_ID_FIT_FORMAT = 100,
139 BOOTSTAGE_ID_FIT_NO_UNIT_NAME,
140 BOOTSTAGE_ID_FIT_UNIT_NAME,
141 BOOTSTAGE_ID_FIT_CONFIG,
142 BOOTSTAGE_ID_FIT_CHECK_SUBIMAGE,
143 BOOTSTAGE_ID_FIT_CHECK_HASH = 104,
145 BOOTSTAGE_ID_FIT_CHECK_ARCH,
146 BOOTSTAGE_ID_FIT_CHECK_KERNEL,
147 BOOTSTAGE_ID_FIT_CHECKED,
149 BOOTSTAGE_ID_FIT_KERNEL_INFO_ERR = 107,
150 BOOTSTAGE_ID_FIT_KERNEL_INFO,
151 BOOTSTAGE_ID_FIT_TYPE,
153 BOOTSTAGE_ID_FIT_COMPRESSION,
154 BOOTSTAGE_ID_FIT_OS,
155 BOOTSTAGE_ID_FIT_LOADADDR,
156 BOOTSTAGE_ID_OVERWRITTEN,
158 BOOTSTAGE_ID_FIT_RD_FORMAT = 120,
159 BOOTSTAGE_ID_FIT_RD_FORMAT_OK,
160 BOOTSTAGE_ID_FIT_RD_NO_UNIT_NAME,
161 BOOTSTAGE_ID_FIT_RD_UNIT_NAME,
162 BOOTSTAGE_ID_FIT_RD_SUBNODE,
164 BOOTSTAGE_ID_FIT_RD_CHECK,
165 BOOTSTAGE_ID_FIT_RD_HASH = 125,
166 BOOTSTAGE_ID_FIT_RD_CHECK_ALL,
167 BOOTSTAGE_ID_FIT_RD_GET_DATA,
168 BOOTSTAGE_ID_FIT_RD_CHECK_ALL_OK = 127,
169 BOOTSTAGE_ID_FIT_RD_GET_DATA_OK,
170 BOOTSTAGE_ID_FIT_RD_LOAD,
172 BOOTSTAGE_ID_IDE_FIT_READ = 140,
173 BOOTSTAGE_ID_IDE_FIT_READ_OK,
175 BOOTSTAGE_ID_NAND_FIT_READ = 150,
176 BOOTSTAGE_ID_NAND_FIT_READ_OK,
178 /*
179 * These boot stages are new, higher level, and not directly related
180 * to the old boot progress numbers. They are useful for recording
181 * rough boot timing information.
182 */
183 BOOTSTAGE_ID_AWAKE,
184 BOOTSTAGE_ID_START_UBOOT_F,
185 BOOTSTAGE_ID_START_UBOOT_R,
186 BOOTSTAGE_ID_USB_START,
187 BOOTSTAGE_ID_ETH_START,
188 BOOTSTAGE_ID_BOOTP_START,
189 BOOTSTAGE_ID_BOOTP_STOP,
190 BOOTSTAGE_ID_BOOTM_START,
191 BOOTSTAGE_ID_BOOTM_HANDOFF,
192 BOOTSTAGE_ID_MAIN_LOOP,
193 BOOTSTAGE_KERNELREAD_START,
194 BOOTSTAGE_KERNELREAD_STOP,
196 BOOTSTAGE_ID_CPU_AWAKE,
197 BOOTSTAGE_ID_MAIN_CPU_AWAKE,
198 BOOTSTAGE_ID_MAIN_CPU_READY,
200 /* a few spare for the user, from here */
201 BOOTSTAGE_ID_USER,
202 BOOTSTAGE_ID_COUNT = BOOTSTAGE_ID_USER + CONFIG_BOOTSTAGE_USER_COUNT,
203 BOOTSTAGE_ID_ALLOC,
204 };
206 /*
207 * Return the time since boot in microseconds, This is needed for bootstage
208 * and should be defined in CPU- or board-specific code. If undefined then
209 * millisecond resolution will be used (the standard get_timer()).
210 */
211 ulong timer_get_boot_us(void);
213 #ifndef CONFIG_SPL_BUILD
214 /*
215 * Board code can implement show_boot_progress() if needed.
216 *
217 * @param val Progress state (enum bootstage_id), or -id if an error
218 * has occurred.
219 */
220 void show_boot_progress(int val);
221 #else
222 #define show_boot_progress(val) do {} while (0)
223 #endif
225 #if defined(CONFIG_BOOTSTAGE) && !defined(CONFIG_SPL_BUILD)
226 /* This is the full bootstage implementation */
228 /*
229 * Mark a time stamp for the current boot stage.
230 */
231 ulong bootstage_mark(enum bootstage_id id);
233 ulong bootstage_error(enum bootstage_id id);
235 ulong bootstage_mark_name(enum bootstage_id id, const char *name);
237 /* Print a report about boot time */
238 void bootstage_report(void);
240 #else
241 /*
242 * This is a dummy implementation which just calls show_boot_progress(),
243 * and won't even do that unless CONFIG_SHOW_BOOT_PROGRESS is defined
244 */
246 static inline ulong bootstage_mark(enum bootstage_id id)
247 {
248 show_boot_progress(id);
249 return 0;
250 }
252 static inline ulong bootstage_error(enum bootstage_id id)
253 {
254 show_boot_progress(-id);
255 return 0;
256 }
258 static inline ulong bootstage_mark_name(enum bootstage_id id, const char *name)
259 {
260 return 0;
261 }
264 #endif /* CONFIG_BOOTSTAGE */
266 #endif