]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/common.h
dra7xx: Enabled UART-boot mode
[glsdk/glsdk-u-boot.git] / include / common.h
1 /*
2  * (C) Copyright 2000-2009
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #ifndef __COMMON_H_
25 #define __COMMON_H_     1
27 #undef  _LINUX_CONFIG_H
28 #define _LINUX_CONFIG_H 1       /* avoid reading Linux autoconf.h file  */
30 #ifndef __ASSEMBLY__            /* put C only stuff in this section */
32 typedef unsigned char           uchar;
33 typedef volatile unsigned long  vu_long;
34 typedef volatile unsigned short vu_short;
35 typedef volatile unsigned char  vu_char;
37 #include <config.h>
38 #include <asm-offsets.h>
39 #include <linux/bitops.h>
40 #include <linux/types.h>
41 #include <linux/string.h>
42 #include <linux/stringify.h>
43 #include <asm/ptrace.h>
44 #include <stdarg.h>
45 #if defined(CONFIG_PCI) && defined(CONFIG_4xx)
46 #include <pci.h>
47 #endif
48 #if defined(CONFIG_8xx)
49 #include <asm/8xx_immap.h>
50 #if defined(CONFIG_MPC852)      || defined(CONFIG_MPC852T)      || \
51     defined(CONFIG_MPC859)      || defined(CONFIG_MPC859T)      || \
52     defined(CONFIG_MPC859DSL)   || \
53     defined(CONFIG_MPC866)      || defined(CONFIG_MPC866T)      || \
54     defined(CONFIG_MPC866P)
55 # define CONFIG_MPC866_FAMILY 1
56 #elif defined(CONFIG_MPC870) \
57    || defined(CONFIG_MPC875) \
58    || defined(CONFIG_MPC880) \
59    || defined(CONFIG_MPC885)
60 # define CONFIG_MPC885_FAMILY   1
61 #endif
62 #if   defined(CONFIG_MPC860)       \
63    || defined(CONFIG_MPC860T)      \
64    || defined(CONFIG_MPC866_FAMILY) \
65    || defined(CONFIG_MPC885_FAMILY)
66 # define CONFIG_MPC86x 1
67 #endif
68 #elif defined(CONFIG_5xx)
69 #include <asm/5xx_immap.h>
70 #elif defined(CONFIG_MPC5xxx)
71 #include <mpc5xxx.h>
72 #elif defined(CONFIG_MPC512X)
73 #include <asm/immap_512x.h>
74 #elif defined(CONFIG_MPC8220)
75 #include <asm/immap_8220.h>
76 #elif defined(CONFIG_8260)
77 #if   defined(CONFIG_MPC8247) \
78    || defined(CONFIG_MPC8248) \
79    || defined(CONFIG_MPC8271) \
80    || defined(CONFIG_MPC8272)
81 #define CONFIG_MPC8272_FAMILY   1
82 #endif
83 #if defined(CONFIG_MPC8272_FAMILY)
84 #define CONFIG_MPC8260  1
85 #endif
86 #include <asm/immap_8260.h>
87 #endif
88 #ifdef CONFIG_MPC86xx
89 #include <mpc86xx.h>
90 #include <asm/immap_86xx.h>
91 #endif
92 #ifdef CONFIG_MPC85xx
93 #include <mpc85xx.h>
94 #include <asm/immap_85xx.h>
95 #endif
96 #ifdef CONFIG_MPC83xx
97 #include <mpc83xx.h>
98 #include <asm/immap_83xx.h>
99 #endif
100 #ifdef  CONFIG_4xx
101 #include <asm/ppc4xx.h>
102 #endif
103 #ifdef CONFIG_HYMOD
104 #include <board/hymod/hymod.h>
105 #endif
106 #ifdef CONFIG_ARM
107 #define asmlinkage      /* nothing */
108 #endif
109 #ifdef CONFIG_BLACKFIN
110 #include <asm/blackfin.h>
111 #endif
112 #ifdef CONFIG_SOC_DA8XX
113 #include <asm/arch/hardware.h>
114 #endif
116 #include <part.h>
117 #include <flash.h>
118 #include <image.h>
120 #ifdef DEBUG
121 #define _DEBUG  1
122 #else
123 #define _DEBUG  0
124 #endif
126 /*
127  * Output a debug text when condition "cond" is met. The "cond" should be
128  * computed by a preprocessor in the best case, allowing for the best
129  * optimization.
130  */
131 #define debug_cond(cond, fmt, args...)          \
132         do {                                    \
133                 if (cond)                       \
134                         printf(fmt, ##args);    \
135         } while (0)
137 #define debug(fmt, args...)                     \
138         debug_cond(_DEBUG, fmt, ##args)
140 /*
141  * An assertion is run-time check done in debug mode only. If DEBUG is not
142  * defined then it is skipped. If DEBUG is defined and the assertion fails,
143  * then it calls panic*( which may or may not reset/halt U-Boot (see
144  * CONFIG_PANIC_HANG), It is hoped that all failing assertions are found
145  * before release, and after release it is hoped that they don't matter. But
146  * in any case these failing assertions cannot be fixed with a reset (which
147  * may just do the same assertion again).
148  */
149 void __assert_fail(const char *assertion, const char *file, unsigned line,
150                    const char *function);
151 #define assert(x) \
152         ({ if (!(x) && _DEBUG) \
153                 __assert_fail(#x, __FILE__, __LINE__, __func__); })
155 #define error(fmt, args...) do {                                        \
156                 printf("ERROR: " fmt "\nat %s:%d/%s()\n",               \
157                         ##args, __FILE__, __LINE__, __func__);          \
158 } while (0)
160 #ifndef BUG
161 #define BUG() do { \
162         printf("BUG: failure at %s:%d/%s()!\n", __FILE__, __LINE__, __FUNCTION__); \
163         panic("BUG!"); \
164 } while (0)
165 #define BUG_ON(condition) do { if (unlikely((condition)!=0)) BUG(); } while(0)
166 #endif /* BUG */
168 /* Force a compilation error if condition is true */
169 #define BUILD_BUG_ON(condition) ((void)sizeof(char[1 - 2*!!(condition)]))
171 typedef void (interrupt_handler_t)(void *);
173 #include <asm/u-boot.h> /* boot information for Linux kernel */
174 #include <asm/global_data.h>    /* global data used for startup functions */
176 /*
177  * enable common handling for all TQM8xxL/M boards:
178  * - CONFIG_TQM8xxM will be defined for all TQM8xxM boards
179  * - CONFIG_TQM8xxL will be defined for all TQM8xxL _and_ TQM8xxM boards
180  *                  and for the TQM885D board
181  */
182 #if defined(CONFIG_TQM823M) || defined(CONFIG_TQM850M) || \
183     defined(CONFIG_TQM855M) || defined(CONFIG_TQM860M) || \
184     defined(CONFIG_TQM862M) || defined(CONFIG_TQM866M)
185 # ifndef CONFIG_TQM8xxM
186 #  define CONFIG_TQM8xxM
187 # endif
188 #endif
189 #if defined(CONFIG_TQM823L) || defined(CONFIG_TQM850L) || \
190     defined(CONFIG_TQM855L) || defined(CONFIG_TQM860L) || \
191     defined(CONFIG_TQM862L) || defined(CONFIG_TQM8xxM) || \
192     defined(CONFIG_TQM885D)
193 # ifndef CONFIG_TQM8xxL
194 #  define CONFIG_TQM8xxL
195 # endif
196 #endif
198 /*
199  * General Purpose Utilities
200  */
201 #define min(X, Y)                               \
202         ({ typeof (X) __x = (X);                \
203                 typeof (Y) __y = (Y);           \
204                 (__x < __y) ? __x : __y; })
206 #define max(X, Y)                               \
207         ({ typeof (X) __x = (X);                \
208                 typeof (Y) __y = (Y);           \
209                 (__x > __y) ? __x : __y; })
211 #define MIN(x, y)  min(x, y)
212 #define MAX(x, y)  max(x, y)
214 /*
215  * Return the absolute value of a number.
216  *
217  * This handles unsigned and signed longs, ints, shorts and chars.  For all
218  * input types abs() returns a signed long.
219  *
220  * For 64-bit types, use abs64()
221  */
222 #define abs(x) ({                                               \
223                 long ret;                                       \
224                 if (sizeof(x) == sizeof(long)) {                \
225                         long __x = (x);                         \
226                         ret = (__x < 0) ? -__x : __x;           \
227                 } else {                                        \
228                         int __x = (x);                          \
229                         ret = (__x < 0) ? -__x : __x;           \
230                 }                                               \
231                 ret;                                            \
232         })
234 #define abs64(x) ({                             \
235                 s64 __x = (x);                  \
236                 (__x < 0) ? -__x : __x;         \
237         })
239 #if defined(CONFIG_ENV_IS_EMBEDDED)
240 #define TOTAL_MALLOC_LEN        CONFIG_SYS_MALLOC_LEN
241 #elif ( ((CONFIG_ENV_ADDR+CONFIG_ENV_SIZE) < CONFIG_SYS_MONITOR_BASE) || \
242         (CONFIG_ENV_ADDR >= (CONFIG_SYS_MONITOR_BASE + CONFIG_SYS_MONITOR_LEN)) ) || \
243       defined(CONFIG_ENV_IS_IN_NVRAM)
244 #define TOTAL_MALLOC_LEN        (CONFIG_SYS_MALLOC_LEN + CONFIG_ENV_SIZE)
245 #else
246 #define TOTAL_MALLOC_LEN        CONFIG_SYS_MALLOC_LEN
247 #endif
249 /**
250  * container_of - cast a member of a structure out to the containing structure
251  * @ptr:        the pointer to the member.
252  * @type:       the type of the container struct this is embedded in.
253  * @member:     the name of the member within the struct.
254  *
255  */
256 #define container_of(ptr, type, member) ({                      \
257         const typeof( ((type *)0)->member ) *__mptr = (ptr);    \
258         (type *)( (char *)__mptr - offsetof(type,member) );})
260 /*
261  * Function Prototypes
262  */
264 void    hang            (void) __attribute__ ((noreturn));
266 int     timer_init(void);
267 int     cpu_init(void);
269 /* */
270 phys_size_t initdram (int);
271 int     display_options (void);
272 void    print_size(unsigned long long, const char *);
273 int print_buffer(ulong addr, const void *data, uint width, uint count,
274                  uint linelen);
276 /* common/main.c */
277 void    main_loop       (void);
278 int run_command(const char *cmd, int flag);
280 /**
281  * Run a list of commands separated by ; or even \0
282  *
283  * Note that if 'len' is not -1, then the command does not need to be nul
284  * terminated, Memory will be allocated for the command in that case.
285  *
286  * @param cmd   List of commands to run, each separated bu semicolon
287  * @param len   Length of commands excluding terminator if known (-1 if not)
288  * @param flag  Execution flags (CMD_FLAG_...)
289  * @return 0 on success, or != 0 on error.
290  */
291 int run_command_list(const char *cmd, int len, int flag);
292 int     readline        (const char *const prompt);
293 int     readline_into_buffer(const char *const prompt, char *buffer,
294                         int timeout);
295 int     parse_line (char *, char *[]);
296 void    init_cmd_timeout(void);
297 void    reset_cmd_timeout(void);
298 #ifdef CONFIG_MENU
299 int     abortboot(int bootdelay);
300 #endif
301 extern char console_buffer[];
303 /* arch/$(ARCH)/lib/board.c */
304 void    board_init_f(ulong);
305 void    board_init_r  (gd_t *, ulong) __attribute__ ((noreturn));
306 int     checkboard    (void);
307 int     checkflash    (void);
308 int     checkdram     (void);
309 int     last_stage_init(void);
310 extern ulong monitor_flash_len;
311 int mac_read_from_eeprom(void);
312 extern u8 _binary_dt_dtb_start[];       /* embedded device tree blob */
313 int set_cpu_clk_info(void);
314 int print_cpuinfo(void);
315 int update_flash_size(int flash_size);
317 /**
318  * Show the DRAM size in a board-specific way
319  *
320  * This is used by boards to display DRAM information in their own way.
321  *
322  * @param size  Size of DRAM (which should be displayed along with other info)
323  */
324 void board_show_dram(ulong size);
326 /* common/flash.c */
327 void flash_perror (int);
329 /* common/cmd_source.c */
330 int     source (ulong addr, const char *fit_uname);
332 extern ulong load_addr;         /* Default Load Address */
333 extern ulong save_addr;         /* Default Save Address */
334 extern ulong save_size;         /* Default Save Size */
336 /* common/cmd_doc.c */
337 void    doc_probe(unsigned long physadr);
339 /* common/cmd_net.c */
340 int do_tftpb(cmd_tbl_t *cmdtp, int flag, int argc, char * const argv[]);
342 /* common/cmd_fat.c */
343 int do_fat_fsload(cmd_tbl_t *, int, int, char * const []);
345 /* common/cmd_ext2.c */
346 int do_ext2load(cmd_tbl_t *, int, int, char * const []);
348 /* common/cmd_nvedit.c */
349 int     env_init     (void);
350 void    env_relocate (void);
351 int     envmatch     (uchar *, int);
352 char    *getenv      (const char *);
353 int     getenv_f     (const char *name, char *buf, unsigned len);
354 ulong getenv_ulong(const char *name, int base, ulong default_val);
355 /*
356  * Read an environment variable as a boolean
357  * Return -1 if variable does not exist (default to true)
358  */
359 int getenv_yesno(const char *var);
360 int     saveenv      (void);
361 int     setenv       (const char *, const char *);
362 int setenv_ulong(const char *varname, ulong value);
363 int setenv_hex(const char *varname, ulong value);
364 /**
365  * setenv_addr - Set an environment variable to an address in hex
366  *
367  * @varname:    Environmet variable to set
368  * @addr:       Value to set it to
369  * @return 0 if ok, 1 on error
370  */
371 static inline int setenv_addr(const char *varname, const void *addr)
373         return setenv_hex(varname, (ulong)addr);
376 #ifdef CONFIG_ARM
377 # include <asm/mach-types.h>
378 # include <asm/setup.h>
379 # include <asm/u-boot-arm.h>    /* ARM version to be fixed! */
380 #endif /* CONFIG_ARM */
381 #ifdef CONFIG_X86               /* x86 version to be fixed! */
382 # include <asm/u-boot-x86.h>
383 #endif /* CONFIG_X86 */
384 #ifdef CONFIG_SANDBOX
385 # include <asm/u-boot-sandbox.h>        /* TODO(sjg) what needs to be fixed? */
386 #endif
387 #ifdef CONFIG_NDS32
388 # include <asm/mach-types.h>
389 # include <asm/u-boot-nds32.h>
390 #endif /* CONFIG_NDS32 */
391 #ifdef CONFIG_MIPS
392 # include <asm/u-boot-mips.h>
393 #endif /* CONFIG_MIPS */
395 #ifdef CONFIG_AUTO_COMPLETE
396 int env_complete(char *var, int maxv, char *cmdv[], int maxsz, char *buf);
397 #endif
398 int get_env_id (void);
400 void    pci_init      (void);
401 void    pci_init_board(void);
402 void    pciinfo       (int, int);
404 #if defined(CONFIG_PCI) && defined(CONFIG_4xx)
405     int    pci_pre_init        (struct pci_controller *);
406     int    is_pci_host         (struct pci_controller *);
407 #endif
409 #if defined(CONFIG_PCI) && (defined(CONFIG_440) || defined(CONFIG_405EX))
410 #   if defined(CONFIG_SYS_PCI_TARGET_INIT)
411         void    pci_target_init      (struct pci_controller *);
412 #   endif
413 #   if defined(CONFIG_SYS_PCI_MASTER_INIT)
414         void    pci_master_init      (struct pci_controller *);
415 #   endif
416 #if defined(CONFIG_440SPE) || \
417     defined(CONFIG_460EX) || defined(CONFIG_460GT) || \
418     defined(CONFIG_405EX)
419    void pcie_setup_hoses(int busno);
420 #endif
421 #endif
423 int     misc_init_f   (void);
424 int     misc_init_r   (void);
426 /* common/exports.c */
427 void    jumptable_init(void);
429 /* common/kallsysm.c */
430 const char *symbol_lookup(unsigned long addr, unsigned long *caddr);
432 /* api/api.c */
433 void    api_init (void);
435 /* common/memsize.c */
436 long    get_ram_size  (long *, long);
438 /* $(BOARD)/$(BOARD).c */
439 void    reset_phy     (void);
440 void    fdc_hw_init   (void);
442 /* $(BOARD)/eeprom.c */
443 void eeprom_init  (void);
444 #ifndef CONFIG_SPI
445 int  eeprom_probe (unsigned dev_addr, unsigned offset);
446 #endif
447 int  eeprom_read  (unsigned dev_addr, unsigned offset, uchar *buffer, unsigned cnt);
448 int  eeprom_write (unsigned dev_addr, unsigned offset, uchar *buffer, unsigned cnt);
449 #ifdef CONFIG_LWMON
450 extern uchar pic_read  (uchar reg);
451 extern void  pic_write (uchar reg, uchar val);
452 #endif
454 /*
455  * Set this up regardless of board
456  * type, to prevent errors.
457  */
458 #if defined(CONFIG_SPI) || !defined(CONFIG_SYS_I2C_EEPROM_ADDR)
459 # define CONFIG_SYS_DEF_EEPROM_ADDR 0
460 #else
461 #if !defined(CONFIG_ENV_EEPROM_IS_ON_I2C)
462 # define CONFIG_SYS_DEF_EEPROM_ADDR CONFIG_SYS_I2C_EEPROM_ADDR
463 #endif
464 #endif /* CONFIG_SPI || !defined(CONFIG_SYS_I2C_EEPROM_ADDR) */
466 #if defined(CONFIG_SPI)
467 extern void spi_init_f (void);
468 extern void spi_init_r (void);
469 extern ssize_t spi_read  (uchar *, int, uchar *, int);
470 extern ssize_t spi_write (uchar *, int, uchar *, int);
471 #endif
473 #ifdef CONFIG_RPXCLASSIC
474 void rpxclassic_init (void);
475 #endif
477 void rpxlite_init (void);
479 #ifdef CONFIG_MBX
480 /* $(BOARD)/mbx8xx.c */
481 void    mbx_init (void);
482 void    board_serial_init (void);
483 void    board_ether_init (void);
484 #endif
486 #ifdef CONFIG_HERMES
487 /* $(BOARD)/hermes.c */
488 void hermes_start_lxt980 (int speed);
489 #endif
491 #ifdef CONFIG_EVB64260
492 void  evb64260_init(void);
493 void  debug_led(int, int);
494 void  display_mem_map(void);
495 void  perform_soft_reset(void);
496 #endif
498 /* $(BOARD)/$(BOARD).c */
499 int board_early_init_f (void);
500 int board_late_init (void);
501 int board_postclk_init (void); /* after clocks/timebase, before env/serial */
502 int board_early_init_r (void);
503 void board_poweroff (void);
505 #if defined(CONFIG_SYS_DRAM_TEST)
506 int testdram(void);
507 #endif /* CONFIG_SYS_DRAM_TEST */
509 /* $(CPU)/start.S */
510 #if defined(CONFIG_5xx) || \
511     defined(CONFIG_8xx)
512 uint    get_immr      (uint);
513 #endif
514 uint    get_pir       (void);
515 #if defined(CONFIG_MPC5xxx)
516 uint    get_svr       (void);
517 #endif
518 uint    get_pvr       (void);
519 uint    get_svr       (void);
520 uint    rd_ic_cst     (void);
521 void    wr_ic_cst     (uint);
522 void    wr_ic_adr     (uint);
523 uint    rd_dc_cst     (void);
524 void    wr_dc_cst     (uint);
525 void    wr_dc_adr     (uint);
526 int     icache_status (void);
527 void    icache_enable (void);
528 void    icache_disable(void);
529 int     dcache_status (void);
530 void    dcache_enable (void);
531 void    dcache_disable(void);
532 void    mmu_disable(void);
533 #if defined(CONFIG_ARM)
534 void    relocate_code(ulong);
535 #else
536 void    relocate_code(ulong, gd_t *, ulong) __attribute__ ((noreturn));
537 #endif
538 ulong   get_endaddr   (void);
539 void    trap_init     (ulong);
540 #if defined (CONFIG_4xx)        || \
541     defined (CONFIG_MPC5xxx)    || \
542     defined (CONFIG_74xx_7xx)   || \
543     defined (CONFIG_74x)        || \
544     defined (CONFIG_75x)        || \
545     defined (CONFIG_74xx)       || \
546     defined (CONFIG_MPC8220)    || \
547     defined (CONFIG_MPC85xx)    || \
548     defined (CONFIG_MPC86xx)    || \
549     defined (CONFIG_MPC83xx)
550 unsigned char   in8(unsigned int);
551 void            out8(unsigned int, unsigned char);
552 unsigned short  in16(unsigned int);
553 unsigned short  in16r(unsigned int);
554 void            out16(unsigned int, unsigned short value);
555 void            out16r(unsigned int, unsigned short value);
556 unsigned long   in32(unsigned int);
557 unsigned long   in32r(unsigned int);
558 void            out32(unsigned int, unsigned long value);
559 void            out32r(unsigned int, unsigned long value);
560 void            ppcDcbf(unsigned long value);
561 void            ppcDcbi(unsigned long value);
562 void            ppcSync(void);
563 void            ppcDcbz(unsigned long value);
564 #endif
565 #if defined (CONFIG_MICROBLAZE)
566 unsigned short  in16(unsigned int);
567 void            out16(unsigned int, unsigned short value);
568 #endif
570 #if defined (CONFIG_MPC83xx)
571 void            ppcDWload(unsigned int *addr, unsigned int *ret);
572 void            ppcDWstore(unsigned int *addr, unsigned int *value);
573 void disable_addr_trans(void);
574 void enable_addr_trans(void);
575 #if defined(CONFIG_DDR_ECC) && !defined(CONFIG_ECC_INIT_VIA_DDRCONTROLLER)
576 void ddr_enable_ecc(unsigned int dram_size);
577 #endif
578 #endif
580 /* $(CPU)/cpu.c */
581 static inline int cpumask_next(int cpu, unsigned int mask)
583         for (cpu++; !((1 << cpu) & mask); cpu++)
584                 ;
586         return cpu;
589 #define for_each_cpu(iter, cpu, num_cpus, mask) \
590         for (iter = 0, cpu = cpumask_next(-1, mask); \
591                 iter < num_cpus; \
592                 iter++, cpu = cpumask_next(cpu, mask)) \
594 int     cpu_numcores  (void);
595 u32     cpu_mask      (void);
596 int     is_core_valid (unsigned int);
597 int     probecpu      (void);
598 int     checkcpu      (void);
599 int     checkicache   (void);
600 int     checkdcache   (void);
601 void    upmconfig     (unsigned int, unsigned int *, unsigned int);
602 ulong   get_tbclk     (void);
603 void    reset_cpu     (ulong addr);
604 #if defined (CONFIG_OF_LIBFDT) && defined (CONFIG_OF_BOARD_SETUP)
605 void ft_cpu_setup(void *blob, bd_t *bd);
606 #ifdef CONFIG_PCI
607 void ft_pci_setup(void *blob, bd_t *bd);
608 #endif
609 #endif
612 /* $(CPU)/serial.c */
613 int     serial_init   (void);
614 void    serial_setbrg (void);
615 void    serial_putc   (const char);
616 void    serial_putc_raw(const char);
617 void    serial_puts   (const char *);
618 int     serial_getc   (void);
619 int     serial_tstc   (void);
621 void    _serial_setbrg (const int);
622 void    _serial_putc   (const char, const int);
623 void    _serial_putc_raw(const char, const int);
624 void    _serial_puts   (const char *, const int);
625 int     _serial_getc   (const int);
626 int     _serial_tstc   (const int);
628 /* $(CPU)/speed.c */
629 int     get_clocks (void);
630 int     get_clocks_866 (void);
631 int     sdram_adjust_866 (void);
632 int     adjust_sdram_tbs_8xx (void);
633 #if defined(CONFIG_8260)
634 int     prt_8260_clks (void);
635 #elif defined(CONFIG_MPC5xxx)
636 int     prt_mpc5xxx_clks (void);
637 #endif
638 #if defined(CONFIG_MPC512X)
639 int     prt_mpc512xxx_clks (void);
640 #endif
641 #if defined(CONFIG_MPC8220)
642 int     prt_mpc8220_clks (void);
643 #endif
644 #ifdef CONFIG_4xx
645 ulong   get_OPB_freq (void);
646 ulong   get_PCI_freq (void);
647 #endif
648 #if defined(CONFIG_S3C24X0) || \
649     defined(CONFIG_LH7A40X) || \
650     defined(CONFIG_EP93XX)
651 ulong   get_FCLK (void);
652 ulong   get_HCLK (void);
653 ulong   get_PCLK (void);
654 ulong   get_UCLK (void);
655 #endif
656 #if defined(CONFIG_LH7A40X)
657 ulong   get_PLLCLK (void);
658 #endif
659 #if defined CONFIG_INCA_IP
660 uint    incaip_get_cpuclk (void);
661 #endif
662 #if defined(CONFIG_IMX)
663 ulong get_systemPLLCLK(void);
664 ulong get_FCLK(void);
665 ulong get_HCLK(void);
666 ulong get_BCLK(void);
667 ulong get_PERCLK1(void);
668 ulong get_PERCLK2(void);
669 ulong get_PERCLK3(void);
670 #endif
671 ulong   get_bus_freq  (ulong);
672 int get_serial_clock(void);
674 #if defined(CONFIG_MPC83xx) || defined(CONFIG_MPC85xx)
675 ulong get_ddr_freq(ulong);
676 #endif
677 #if defined(CONFIG_MPC85xx)
678 typedef MPC85xx_SYS_INFO sys_info_t;
679 void    get_sys_info  ( sys_info_t * );
680 #endif
681 #if defined(CONFIG_MPC86xx)
682 typedef MPC86xx_SYS_INFO sys_info_t;
683 void   get_sys_info  ( sys_info_t * );
684 static inline ulong get_ddr_freq(ulong dummy)
686         return get_bus_freq(dummy);
688 #endif
690 #if defined(CONFIG_4xx)
691 #  if defined(CONFIG_440)
692 #       if defined(CONFIG_440SPE)
693          unsigned long determine_sysper(void);
694          unsigned long determine_pci_clock_per(void);
695 #       endif
696 #  endif
697 typedef PPC4xx_SYS_INFO sys_info_t;
698 int     ppc440spe_revB(void);
699 void    get_sys_info  ( sys_info_t * );
700 #endif
702 /* $(CPU)/cpu_init.c */
703 #if defined(CONFIG_8xx) || defined(CONFIG_8260)
704 void    cpu_init_f    (volatile immap_t *immr);
705 #endif
706 #if defined(CONFIG_4xx) || defined(CONFIG_MPC85xx) || defined(CONFIG_MCF52x2) ||defined(CONFIG_MPC86xx)
707 void    cpu_init_f    (void);
708 #endif
710 int     cpu_init_r    (void);
711 #if defined(CONFIG_8260)
712 int     prt_8260_rsr  (void);
713 #elif defined(CONFIG_MPC83xx)
714 int     prt_83xx_rsr  (void);
715 #endif
717 /* $(CPU)/interrupts.c */
718 int     interrupt_init     (void);
719 void    timer_interrupt    (struct pt_regs *);
720 void    external_interrupt (struct pt_regs *);
721 void    irq_install_handler(int, interrupt_handler_t *, void *);
722 void    irq_free_handler   (int);
723 void    reset_timer        (void);
724 ulong   get_timer          (ulong base);
725 void    enable_interrupts  (void);
726 int     disable_interrupts (void);
728 /* $(CPU)/.../commproc.c */
729 int     dpram_init (void);
730 uint    dpram_base(void);
731 uint    dpram_base_align(uint align);
732 uint    dpram_alloc(uint size);
733 uint    dpram_alloc_align(uint size,uint align);
734 void    bootcount_store (ulong);
735 ulong   bootcount_load (void);
736 #define BOOTCOUNT_MAGIC         0xB001C041
738 /* $(CPU)/.../<eth> */
739 void mii_init (void);
741 /* $(CPU)/.../lcd.c */
742 ulong   lcd_setmem (ulong);
744 /* $(CPU)/.../video.c */
745 ulong   video_setmem (ulong);
747 /* arch/$(ARCH)/lib/cache.c */
748 void    enable_caches(void);
749 void    flush_cache   (unsigned long, unsigned long);
750 void    flush_dcache_all(void);
751 void    flush_dcache_range(unsigned long start, unsigned long stop);
752 void    invalidate_dcache_range(unsigned long start, unsigned long stop);
753 void    invalidate_dcache_all(void);
754 void    invalidate_icache_all(void);
756 /* arch/$(ARCH)/lib/ticks.S */
757 unsigned long long get_ticks(void);
758 void    wait_ticks    (unsigned long);
760 /* arch/$(ARCH)/lib/time.c */
761 void    __udelay      (unsigned long);
762 ulong   usec2ticks    (unsigned long usec);
763 ulong   ticks2usec    (unsigned long ticks);
764 int     init_timebase (void);
766 /* lib/gunzip.c */
767 int gunzip(void *, int, unsigned char *, unsigned long *);
768 int zunzip(void *dst, int dstlen, unsigned char *src, unsigned long *lenp,
769                                                 int stoponerr, int offset);
771 /* lib/qsort.c */
772 void qsort(void *base, size_t nmemb, size_t size,
773            int(*compar)(const void *, const void *));
774 int strcmp_compar(const void *, const void *);
776 /* lib/time.c */
777 void    udelay        (unsigned long);
778 void mdelay(unsigned long);
780 /* lib/uuid.c */
781 void uuid_str_to_bin(const char *uuid, unsigned char *out);
782 int uuid_str_valid(const char *uuid);
784 /* lib/vsprintf.c */
785 #include <vsprintf.h>
787 /* lib/strmhz.c */
788 char *  strmhz(char *buf, unsigned long hz);
790 /* lib/crc32.c */
791 #include <u-boot/crc.h>
793 /* lib/rand.c */
794 #if defined(CONFIG_RANDOM_MACADDR) || \
795         defined(CONFIG_BOOTP_RANDOM_DELAY) || \
796         defined(CONFIG_CMD_LINK_LOCAL)
797 #define RAND_MAX -1U
798 void srand(unsigned int seed);
799 unsigned int rand(void);
800 unsigned int rand_r(unsigned int *seedp);
801 #endif
803 /* common/console.c */
804 int     console_init_f(void);   /* Before relocation; uses the serial  stuff    */
805 int     console_init_r(void);   /* After  relocation; uses the console stuff    */
806 int     console_assign(int file, const char *devname);  /* Assign the console   */
807 int     ctrlc (void);
808 int     had_ctrlc (void);       /* have we had a Control-C since last clear? */
809 void    clear_ctrlc (void);     /* clear the Control-C condition */
810 int     disable_ctrlc (int);    /* 1 to disable, 0 to enable Control-C detect */
812 /*
813  * STDIO based functions (can always be used)
814  */
815 /* serial stuff */
816 int     serial_printf (const char *fmt, ...)
817                 __attribute__ ((format (__printf__, 1, 2)));
818 /* stdin */
819 int     getc(void);
820 int     tstc(void);
822 /* stdout */
823 void    putc(const char c);
824 void    puts(const char *s);
825 int     printf(const char *fmt, ...)
826                 __attribute__ ((format (__printf__, 1, 2)));
827 int     vprintf(const char *fmt, va_list args);
829 /* stderr */
830 #define eputc(c)                fputc(stderr, c)
831 #define eputs(s)                fputs(stderr, s)
832 #define eprintf(fmt,args...)    fprintf(stderr,fmt ,##args)
834 /*
835  * FILE based functions (can only be used AFTER relocation!)
836  */
837 #define stdin           0
838 #define stdout          1
839 #define stderr          2
840 #define MAX_FILES       3
842 int     fprintf(int file, const char *fmt, ...)
843                 __attribute__ ((format (__printf__, 2, 3)));
844 void    fputs(int file, const char *s);
845 void    fputc(int file, const char c);
846 int     ftstc(int file);
847 int     fgetc(int file);
849 /* lib/gzip.c */
850 int gzip(void *dst, unsigned long *lenp,
851                 unsigned char *src, unsigned long srclen);
852 int zzip(void *dst, unsigned long *lenp, unsigned char *src,
853                 unsigned long srclen, int stoponerr,
854                 int (*func)(unsigned long, unsigned long));
856 /* lib/net_utils.c */
857 #include <net.h>
858 static inline IPaddr_t getenv_IPaddr(char *var)
860         return string_to_ip(getenv(var));
863 /*
864  * CONSOLE multiplexing.
865  */
866 #ifdef CONFIG_CONSOLE_MUX
867 #include <iomux.h>
868 #endif
870 int     pcmcia_init (void);
872 #ifdef CONFIG_STATUS_LED
873 # include <status_led.h>
874 #endif
876 #include <bootstage.h>
878 #ifdef CONFIG_SHOW_ACTIVITY
879 void show_activity(int arg);
880 #endif
882 /* Multicore arch functions */
883 #ifdef CONFIG_MP
884 int cpu_status(int nr);
885 int cpu_reset(int nr);
886 int cpu_disable(int nr);
887 int cpu_release(int nr, int argc, char * const argv[]);
888 #endif
890 /* Define a null map_sysmem() if the architecture doesn't use it */
891 # ifndef CONFIG_ARCH_MAP_SYSMEM
892 static inline void *map_sysmem(phys_addr_t paddr, unsigned long len)
894         return (void *)(uintptr_t)paddr;
897 static inline void unmap_sysmem(const void *vaddr)
900 # endif
902 #endif /* __ASSEMBLY__ */
904 #ifdef CONFIG_PPC
905 /*
906  * Has to be included outside of the #ifndef __ASSEMBLY__ section.
907  * Otherwise might lead to compilation errors in assembler files.
908  */
909 #include <asm/cache.h>
910 #endif
912 /* Put only stuff here that the assembler can digest */
914 #ifdef CONFIG_POST
915 #define CONFIG_HAS_POST
916 #ifndef CONFIG_POST_ALT_LIST
917 #define CONFIG_POST_STD_LIST
918 #endif
919 #endif
921 #ifdef CONFIG_INIT_CRITICAL
922 #error CONFIG_INIT_CRITICAL is deprecated!
923 #error Read section CONFIG_SKIP_LOWLEVEL_INIT in README.
924 #endif
926 #define ARRAY_SIZE(x) (sizeof(x) / sizeof((x)[0]))
928 #define ROUND(a,b)              (((a) + (b) - 1) & ~((b) - 1))
929 #define DIV_ROUND(n,d)          (((n) + ((d)/2)) / (d))
930 #define DIV_ROUND_UP(n,d)       (((n) + (d) - 1) / (d))
931 #define roundup(x, y)           ((((x) + ((y) - 1)) / (y)) * (y))
933 #define ALIGN(x,a)              __ALIGN_MASK((x),(typeof(x))(a)-1)
934 #define __ALIGN_MASK(x,mask)    (((x)+(mask))&~(mask))
936 /*
937  * ARCH_DMA_MINALIGN is defined in asm/cache.h for each architecture.  It
938  * is used to align DMA buffers.
939  */
940 #ifndef __ASSEMBLY__
941 #include <asm/cache.h>
942 #endif
944 /*
945  * The ALLOC_CACHE_ALIGN_BUFFER macro is used to allocate a buffer on the
946  * stack that meets the minimum architecture alignment requirements for DMA.
947  * Such a buffer is useful for DMA operations where flushing and invalidating
948  * the cache before and after a read and/or write operation is required for
949  * correct operations.
950  *
951  * When called the macro creates an array on the stack that is sized such
952  * that:
953  *
954  * 1) The beginning of the array can be advanced enough to be aligned.
955  *
956  * 2) The size of the aligned portion of the array is a multiple of the minimum
957  *    architecture alignment required for DMA.
958  *
959  * 3) The aligned portion contains enough space for the original number of
960  *    elements requested.
961  *
962  * The macro then creates a pointer to the aligned portion of this array and
963  * assigns to the pointer the address of the first element in the aligned
964  * portion of the array.
965  *
966  * Calling the macro as:
967  *
968  *     ALLOC_CACHE_ALIGN_BUFFER(uint32_t, buffer, 1024);
969  *
970  * Will result in something similar to saying:
971  *
972  *     uint32_t    buffer[1024];
973  *
974  * The following differences exist:
975  *
976  * 1) The resulting buffer is guaranteed to be aligned to the value of
977  *    ARCH_DMA_MINALIGN.
978  *
979  * 2) The buffer variable created by the macro is a pointer to the specified
980  *    type, and NOT an array of the specified type.  This can be very important
981  *    if you want the address of the buffer, which you probably do, to pass it
982  *    to the DMA hardware.  The value of &buffer is different in the two cases.
983  *    In the macro case it will be the address of the pointer, not the address
984  *    of the space reserved for the buffer.  However, in the second case it
985  *    would be the address of the buffer.  So if you are replacing hard coded
986  *    stack buffers with this macro you need to make sure you remove the & from
987  *    the locations where you are taking the address of the buffer.
988  *
989  * Note that the size parameter is the number of array elements to allocate,
990  * not the number of bytes.
991  *
992  * This macro can not be used outside of function scope, or for the creation
993  * of a function scoped static buffer.  It can not be used to create a cache
994  * line aligned global buffer.
995  */
996 #define ALLOC_ALIGN_BUFFER(type, name, size, align)                     \
997         char __##name[ROUND(size * sizeof(type), align) + (align - 1)]; \
998                                                                         \
999         type *name = (type *) ALIGN((uintptr_t)__##name, align)
1000 #define ALLOC_CACHE_ALIGN_BUFFER(type, name, size)                      \
1001         ALLOC_ALIGN_BUFFER(type, name, size, ARCH_DMA_MINALIGN)
1003 /*
1004  * DEFINE_CACHE_ALIGN_BUFFER() is similar to ALLOC_CACHE_ALIGN_BUFFER, but it's
1005  * purpose is to allow allocating aligned buffers outside of function scope.
1006  * Usage of this macro shall be avoided or used with extreme care!
1007  */
1008 #define DEFINE_ALIGN_BUFFER(type, name, size, align)                    \
1009         static char __##name[roundup(size * sizeof(type), align)]       \
1010                         __attribute__((aligned(align)));                                \
1011                                                                         \
1012         static type *name = (type *)__##name
1013 #define DEFINE_CACHE_ALIGN_BUFFER(type, name, size)                     \
1014         DEFINE_ALIGN_BUFFER(type, name, size, ARCH_DMA_MINALIGN)
1016 /* Pull in stuff for the build system */
1017 #ifdef DO_DEPS_ONLY
1018 # include <environment.h>
1019 #endif
1021 #endif  /* __COMMON_H_ */