1 /*
2 * (C) Copyright 2002,2003 Motorola,Inc.
3 * Xianghua Xiao <X.Xiao@motorola.com>
4 *
5 * (C) Copyright 2004 Wind River Systems Inc <www.windriver.com>.
6 * Added support for Wind River SBC8540 board
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 /*
28 * sbc8540 board configuration file.
29 */
31 #ifndef __CONFIG_H
32 #define __CONFIG_H
34 /*
35 * Top level Makefile configuration choices
36 */
37 #ifdef CONFIG_66
38 #define CONFIG_PCI_66
39 #endif
41 #define TSEC_DEBUG
43 /*
44 * High Level Configuration Options
45 */
46 #define CONFIG_BOOKE 1 /* BOOKE */
47 #define CONFIG_E500 1 /* BOOKE e500 family */
48 #define CONFIG_MPC85xx 1 /* MPC8540/MPC8560 */
49 #define CONFIG_MPC85xx_REV1 1 /* MPC85xx Rev 1.0 chip */
51 #define CONFIG_SYS_TEXT_BASE 0xfffc0000
54 #define CONFIG_CPM2 1 /* has CPM2 */
56 #define CONFIG_SBC8540 1 /* configuration for SBC8560 board */
57 #define CONFIG_MPC8540 1
59 #define CONFIG_MPC8560ADS 1 /* MPC8560ADS board specific (supplement) */
61 #define CONFIG_TSEC_ENET /* tsec ethernet support */
62 #undef CONFIG_PCI /* pci ethernet support */
63 #undef CONFIG_ETHER_ON_FCC /* cpm FCC ethernet support */
65 #define CONFIG_FSL_LAW 1 /* Use common FSL init code */
67 #define CONFIG_ENV_OVERWRITE
69 /* Using Localbus SDRAM to emulate flash before we can program the flash,
70 * normally you need a flash-boot image(u-boot.bin), if so undef this.
71 */
72 #undef CONFIG_RAM_AS_FLASH
74 #if defined(CONFIG_PCI_66) /* some PCI card is 33Mhz only */
75 #define CONFIG_SYS_CLK_FREQ 66000000 /* sysclk for MPC85xx */
76 #else
77 #define CONFIG_SYS_CLK_FREQ 33000000 /* most pci cards are 33Mhz */
78 #endif
80 /* below can be toggled for performance analysis. otherwise use default */
81 #define CONFIG_L2_CACHE /* toggle L2 cache */
82 #undef CONFIG_BTB /* toggle branch predition */
84 #define CONFIG_BOARD_EARLY_INIT_F 1 /* Call board_early_init_f */
85 #define CONFIG_RESET_PHY_R 1 /* Call reset_phy() */
87 #undef CONFIG_SYS_DRAM_TEST /* memory test, takes time */
88 #define CONFIG_SYS_MEMTEST_START 0x00200000 /* memtest region */
89 #define CONFIG_SYS_MEMTEST_END 0x00400000
91 #if (defined(CONFIG_PCI) && defined(CONFIG_TSEC_ENET) || \
92 defined(CONFIG_PCI) && defined(CONFIG_ETHER_ON_FCC) || \
93 defined(CONFIG_TSEC_ENET) && defined(CONFIG_ETHER_ON_FCC))
94 #error "You can only use ONE of PCI Ethernet Card or TSEC Ethernet or CPM FCC."
95 #endif
97 #define CONFIG_SYS_SDRAM_SIZE 512 /* DDR is 512MB */
99 /* DDR Setup */
100 #define CONFIG_FSL_DDR1
101 #undef CONFIG_FSL_DDR_INTERACTIVE
102 #undef CONFIG_DDR_ECC /* only for ECC DDR module */
103 #undef CONFIG_SPD_EEPROM /* Use SPD EEPROM for DDR setup */
104 #undef CONFIG_DDR_SPD
106 #if defined(CONFIG_MPC85xx_REV1)
107 #define CONFIG_SYS_FSL_ERRATUM_DDR_MSYNC_IN /* possible DLL fix needed */
108 #endif
110 #undef CONFIG_DDR_ECC /* only for ECC DDR module */
111 #undef CONFIG_ECC_INIT_VIA_DDRCONTROLLER /* DDR controller or DMA? */
112 #define CONFIG_MEM_INIT_VALUE 0xDeadBeef
114 #define CONFIG_SYS_DDR_SDRAM_BASE 0x00000000
115 #define CONFIG_SYS_SDRAM_BASE CONFIG_SYS_DDR_SDRAM_BASE
116 #define CONFIG_VERY_BIG_RAM
118 #define CONFIG_NUM_DDR_CONTROLLERS 1
119 #define CONFIG_DIMM_SLOTS_PER_CTLR 1
120 #define CONFIG_CHIP_SELECTS_PER_CTRL 2
122 /* I2C addresses of SPD EEPROMs */
123 #define SPD_EEPROM_ADDRESS 0x55 /* CTLR 0 DIMM 0 */
125 #undef CONFIG_CLOCKS_IN_MHZ
127 #if defined(CONFIG_RAM_AS_FLASH)
128 #define CONFIG_SYS_LBC_SDRAM_BASE 0xfc000000 /* Localbus SDRAM */
129 #define CONFIG_SYS_FLASH_BASE 0xf8000000 /* start of FLASH 8M */
130 #define CONFIG_SYS_BR0_PRELIM 0xf8000801 /* port size 8bit */
131 #define CONFIG_SYS_OR0_PRELIM 0xf8000ff7 /* 8MB Flash */
132 #else /* Boot from real Flash */
133 #define CONFIG_SYS_LBC_SDRAM_BASE 0xf8000000 /* Localbus SDRAM */
134 #define CONFIG_SYS_FLASH_BASE 0xff800000 /* start of FLASH 8M */
135 #define CONFIG_SYS_BR0_PRELIM 0xff800801 /* port size 8bit */
136 #define CONFIG_SYS_OR0_PRELIM 0xff800ff7 /* 8MB Flash */
137 #endif
138 #define CONFIG_SYS_LBC_SDRAM_SIZE 64 /* LBC SDRAM is 64MB */
140 /* local bus definitions */
141 #define CONFIG_SYS_BR1_PRELIM 0xe4001801 /* 64M, 32-bit flash */
142 #define CONFIG_SYS_OR1_PRELIM 0xfc000ff7
144 #define CONFIG_SYS_BR2_PRELIM 0x00000000 /* CS2 not used */
145 #define CONFIG_SYS_OR2_PRELIM 0x00000000
147 #define CONFIG_SYS_BR3_PRELIM 0xf0001861 /* 64MB localbus SDRAM */
148 #define CONFIG_SYS_OR3_PRELIM 0xfc000cc1
150 #if defined(CONFIG_RAM_AS_FLASH)
151 #define CONFIG_SYS_BR4_PRELIM 0xf4001861 /* 64M localbus SDRAM */
152 #else
153 #define CONFIG_SYS_BR4_PRELIM 0xf8001861 /* 64M localbus SDRAM */
154 #endif
155 #define CONFIG_SYS_OR4_PRELIM 0xfc000cc1
157 #define CONFIG_SYS_BR5_PRELIM 0xfc000801 /* 16M CS5 misc devices */
158 #if 1
159 #define CONFIG_SYS_OR5_PRELIM 0xff000ff7
160 #else
161 #define CONFIG_SYS_OR5_PRELIM 0xff0000f0
162 #endif
164 #define CONFIG_SYS_BR6_PRELIM 0xe0001801 /* 64M, 32-bit flash */
165 #define CONFIG_SYS_OR6_PRELIM 0xfc000ff7
166 #define CONFIG_SYS_LBC_LCRR 0x00030002 /* local bus freq */
167 #define CONFIG_SYS_LBC_LBCR 0x00000000
168 #define CONFIG_SYS_LBC_LSRT 0x20000000
169 #define CONFIG_SYS_LBC_MRTPR 0x20000000
170 #define CONFIG_SYS_LBC_LSDMR_1 0x2861b723
171 #define CONFIG_SYS_LBC_LSDMR_2 0x0861b723
172 #define CONFIG_SYS_LBC_LSDMR_3 0x0861b723
173 #define CONFIG_SYS_LBC_LSDMR_4 0x1861b723
174 #define CONFIG_SYS_LBC_LSDMR_5 0x4061b723
176 /* just hijack the MOT BCSR def for SBC8560 misc devices */
177 #define CONFIG_SYS_BCSR ((CONFIG_SYS_BR5_PRELIM & 0xff000000)|0x00400000)
178 /* the size of CS5 needs to be >= 16M for TLB and LAW setups */
180 #define CONFIG_SYS_INIT_RAM_LOCK 1
181 #define CONFIG_SYS_INIT_RAM_ADDR 0x70000000 /* Initial RAM address */
182 #define CONFIG_SYS_INIT_RAM_SIZE 0x4000 /* Size of used area in RAM */
184 #define CONFIG_SYS_GBL_DATA_OFFSET (CONFIG_SYS_INIT_RAM_SIZE - GENERATED_GBL_DATA_SIZE)
185 #define CONFIG_SYS_INIT_SP_OFFSET CONFIG_SYS_GBL_DATA_OFFSET
187 #define CONFIG_SYS_MONITOR_LEN (256 * 1024) /* Reserve 256 kB for Mon */
188 #define CONFIG_SYS_MALLOC_LEN (128 * 1024) /* Reserved for malloc */
190 /* Serial Port */
191 #undef CONFIG_CONS_ON_SCC /* define if console on SCC */
192 #undef CONFIG_CONS_NONE /* define if console on something else */
194 #define CONFIG_CONS_INDEX 1
195 #define CONFIG_SYS_NS16550
196 #define CONFIG_SYS_NS16550_SERIAL
197 #define CONFIG_SYS_NS16550_REG_SIZE 1
198 #if 0
199 #define CONFIG_SYS_NS16550_CLK 1843200 /* get_bus_freq(0) */
200 #else
201 #define CONFIG_SYS_NS16550_CLK 264000000 /* get_bus_freq(0) */
202 #endif
204 #define CONFIG_BAUDRATE 9600
206 #define CONFIG_SYS_BAUDRATE_TABLE \
207 {300, 600, 1200, 2400, 4800, 9600, 19200, 38400,115200}
209 #if 0
210 #define CONFIG_SYS_NS16550_COM1 ((CONFIG_SYS_BR5_PRELIM & 0xff000000)+0x00700000)
211 #define CONFIG_SYS_NS16550_COM2 ((CONFIG_SYS_BR5_PRELIM & 0xff000000)+0x00800000)
212 #else
213 /* SBC8540 uses internal COMM controller */
214 #define CONFIG_SYS_NS16550_COM1 ((CONFIG_SYS_CCSRBAR & 0xfff00000)+0x00004500)
215 #define CONFIG_SYS_NS16550_COM2 ((CONFIG_SYS_CCSRBAR & 0xfff00000)+0x00004600)
216 #endif
218 /* Use the HUSH parser */
219 #define CONFIG_SYS_HUSH_PARSER
221 /*
222 * I2C
223 */
224 #define CONFIG_FSL_I2C /* Use FSL common I2C driver */
225 #define CONFIG_HARD_I2C /* I2C with hardware support*/
226 #undef CONFIG_SOFT_I2C /* I2C bit-banged */
227 #define CONFIG_SYS_I2C_SPEED 400000 /* I2C speed and slave address */
228 #define CONFIG_SYS_I2C_SLAVE 0x7F
229 #define CONFIG_SYS_I2C_NOPROBES {0x69} /* Don't probe these addrs */
230 #define CONFIG_SYS_I2C_OFFSET 0x3000
232 #define CONFIG_SYS_PCI_MEM_BASE 0xC0000000
233 #define CONFIG_SYS_PCI_MEM_PHYS 0xC0000000
234 #define CONFIG_SYS_PCI_MEM_SIZE 0x10000000
236 #if defined(CONFIG_TSEC_ENET) /* TSEC Ethernet port */
238 # define CONFIG_MPC85xx_TSEC1
239 # define CONFIG_MPC85xx_TSEC1_NAME "TSEC0"
240 # define CONFIG_MII 1 /* MII PHY management */
241 # define TSEC1_PHY_ADDR 25
242 # define TSEC1_PHYIDX 0
243 /* Options are: TSEC0 */
244 # define CONFIG_ETHPRIME "TSEC0"
247 #elif defined(CONFIG_ETHER_ON_FCC) /* CPM FCC Ethernet */
249 #undef CONFIG_ETHER_NONE /* define if ether on something else */
250 #define CONFIG_ETHER_ON_FCC2 /* cpm FCC ethernet support */
251 #define CONFIG_ETHER_INDEX 2 /* which channel for ether */
253 #if (CONFIG_ETHER_INDEX == 2)
254 /*
255 * - Rx-CLK is CLK13
256 * - Tx-CLK is CLK14
257 * - Select bus for bd/buffers
258 * - Full duplex
259 */
260 #define CONFIG_SYS_CMXFCR_MASK2 (CMXFCR_FC2 | CMXFCR_RF2CS_MSK | CMXFCR_TF2CS_MSK)
261 #define CONFIG_SYS_CMXFCR_VALUE2 (CMXFCR_RF2CS_CLK13 | CMXFCR_TF2CS_CLK14)
262 #define CONFIG_SYS_CPMFCR_RAMTYPE 0
263 #define CONFIG_SYS_FCC_PSMR (FCC_PSMR_FDE)
265 #elif (CONFIG_ETHER_INDEX == 3)
266 /* need more definitions here for FE3 */
267 #endif /* CONFIG_ETHER_INDEX */
269 #define CONFIG_MII /* MII PHY management */
270 #define CONFIG_BITBANGMII /* bit-bang MII PHY management */
271 /*
272 * GPIO pins used for bit-banged MII communications
273 */
274 #define MDIO_PORT 2 /* Port C */
275 #define MDIO_DECLARE volatile ioport_t *iop = ioport_addr ( \
276 (immap_t *) CONFIG_SYS_IMMR, MDIO_PORT )
277 #define MDC_DECLARE MDIO_DECLARE
279 #define MDIO_ACTIVE (iop->pdir |= 0x00400000)
280 #define MDIO_TRISTATE (iop->pdir &= ~0x00400000)
281 #define MDIO_READ ((iop->pdat & 0x00400000) != 0)
283 #define MDIO(bit) if(bit) iop->pdat |= 0x00400000; \
284 else iop->pdat &= ~0x00400000
286 #define MDC(bit) if(bit) iop->pdat |= 0x00200000; \
287 else iop->pdat &= ~0x00200000
289 #define MIIDELAY udelay(1)
291 #endif
293 /*-----------------------------------------------------------------------
294 * FLASH and environment organization
295 */
297 #define CONFIG_SYS_FLASH_CFI 1 /* Flash is CFI conformant */
298 #define CONFIG_FLASH_CFI_DRIVER 1 /* Use the common driver */
299 #if 0
300 #define CONFIG_SYS_FLASH_USE_BUFFER_WRITE 1 /* use buffered writes (20x faster) */
301 #define CONFIG_SYS_FLASH_PROTECTION /* use hardware protection */
302 #endif
303 #define CONFIG_SYS_MAX_FLASH_SECT 64 /* max number of sectors on one chip */
304 #define CONFIG_SYS_MAX_FLASH_BANKS 1 /* max number of memory banks */
306 #undef CONFIG_SYS_FLASH_CHECKSUM
307 #define CONFIG_SYS_FLASH_ERASE_TOUT 200000 /* Timeout for Flash Erase (in ms) */
308 #define CONFIG_SYS_FLASH_WRITE_TOUT 50000 /* Timeout for Flash Write (in ms) */
310 #define CONFIG_SYS_MONITOR_BASE CONFIG_SYS_TEXT_BASE /* start of monitor */
312 #if 0
313 /* XXX This doesn't work and I don't want to fix it */
314 #if (CONFIG_SYS_MONITOR_BASE < CONFIG_SYS_FLASH_BASE)
315 #define CONFIG_SYS_RAMBOOT
316 #else
317 #undef CONFIG_SYS_RAMBOOT
318 #endif
319 #endif
321 /* Environment */
322 #if !defined(CONFIG_SYS_RAMBOOT)
323 #if defined(CONFIG_RAM_AS_FLASH)
324 #define CONFIG_ENV_IS_NOWHERE
325 #define CONFIG_ENV_ADDR (CONFIG_SYS_FLASH_BASE + 0x100000)
326 #define CONFIG_ENV_SIZE 0x2000
327 #else
328 #define CONFIG_ENV_IS_IN_FLASH 1
329 #define CONFIG_ENV_SECT_SIZE 0x20000 /* 128K(one sector) for env */
330 #define CONFIG_ENV_ADDR (CONFIG_SYS_MONITOR_BASE - CONFIG_ENV_SECT_SIZE)
331 #define CONFIG_ENV_SIZE 0x2000 /* CONFIG_ENV_SECT_SIZE */
332 #endif
333 #else
334 #define CONFIG_SYS_NO_FLASH 1 /* Flash is not usable now */
335 #define CONFIG_ENV_IS_NOWHERE 1 /* Store ENV in memory only */
336 #define CONFIG_ENV_ADDR (CONFIG_SYS_MONITOR_BASE - 0x1000)
337 #define CONFIG_ENV_SIZE 0x2000
338 #endif
340 #define CONFIG_BOOTARGS "root=/dev/nfs rw nfsroot=192.168.0.251:/tftpboot ip=192.168.0.105:192.168.0.251::255.255.255.0:sbc8560:eth0:off console=ttyS0,9600"
341 /*#define CONFIG_BOOTARGS "root=/dev/ram rw console=ttyS0,115200"*/
342 #define CONFIG_BOOTCOMMAND "bootm 0xff800000 0xffa00000"
343 #define CONFIG_BOOTDELAY 5 /* -1 disable autoboot */
345 #define CONFIG_LOADS_ECHO 1 /* echo on for serial download */
346 #define CONFIG_SYS_LOADS_BAUD_CHANGE 1 /* allow baudrate change */
349 /*
350 * BOOTP options
351 */
352 #define CONFIG_BOOTP_BOOTFILESIZE
353 #define CONFIG_BOOTP_BOOTPATH
354 #define CONFIG_BOOTP_GATEWAY
355 #define CONFIG_BOOTP_HOSTNAME
358 /*
359 * Command line configuration.
360 */
361 #include <config_cmd_default.h>
363 #define CONFIG_CMD_PING
364 #define CONFIG_CMD_I2C
365 #define CONFIG_CMD_REGINFO
367 #if defined(CONFIG_PCI)
368 #define CONFIG_CMD_PCI
369 #endif
371 #if defined(CONFIG_TSEC_ENET) || defined(CONFIG_ETHER_ON_FCC)
372 #define CONFIG_CMD_MII
373 #endif
375 #if defined(CONFIG_SYS_RAMBOOT)
376 #undef CONFIG_CMD_SAVEENV
377 #undef CONFIG_CMD_LOADS
378 #endif
381 #undef CONFIG_WATCHDOG /* watchdog disabled */
383 /*
384 * Miscellaneous configurable options
385 */
386 #define CONFIG_SYS_LONGHELP /* undef to save memory */
387 #define CONFIG_SYS_PROMPT "SBC8540=> " /* Monitor Command Prompt */
388 #if defined(CONFIG_CMD_KGDB)
389 #define CONFIG_SYS_CBSIZE 1024 /* Console I/O Buffer Size */
390 #else
391 #define CONFIG_SYS_CBSIZE 256 /* Console I/O Buffer Size */
392 #endif
393 #define CONFIG_SYS_PBSIZE (CONFIG_SYS_CBSIZE+sizeof(CONFIG_SYS_PROMPT)+16) /* Print Buffer Size */
394 #define CONFIG_SYS_MAXARGS 16 /* max number of command args */
395 #define CONFIG_SYS_BARGSIZE CONFIG_SYS_CBSIZE /* Boot Argument Buffer Size */
396 #define CONFIG_SYS_LOAD_ADDR 0x1000000 /* default load address */
397 #define CONFIG_SYS_HZ 1000 /* decrementer freq: 1 ms ticks */
399 /*
400 * For booting Linux, the board info and command line data
401 * have to be in the first 8 MB of memory, since this is
402 * the maximum mapped by the Linux kernel during initialization.
403 */
404 #define CONFIG_SYS_BOOTMAPSZ (8 << 20) /* Initial Memory map for Linux */
406 #if defined(CONFIG_CMD_KGDB)
407 #define CONFIG_KGDB_BAUDRATE 230400 /* speed to run kgdb serial port */
408 #define CONFIG_KGDB_SER_INDEX 2 /* which serial port to use */
409 #endif
411 /*Note: change below for your network setting!!! */
412 #if defined(CONFIG_TSEC_ENET) || defined(CONFIG_ETHER_ON_FCC)
413 # define CONFIG_ETHADDR 00:vv:ww:xx:yy:8a
414 # define CONFIG_HAS_ETH1
415 # define CONFIG_ETH1ADDR 00:vv:ww:xx:yy:8b
416 # define CONFIG_HAS_ETH2
417 # define CONFIG_ETH2ADDR 00:vv:ww:xx:yy:8c
418 #endif
420 #define CONFIG_SERVERIP YourServerIP
421 #define CONFIG_IPADDR YourTargetIP
422 #define CONFIG_GATEWAYIP YourGatewayIP
423 #define CONFIG_NETMASK 255.255.255.0
424 #define CONFIG_HOSTNAME SBC8560
425 #define CONFIG_ROOTPATH "YourRootPath"
426 #define CONFIG_BOOTFILE "YourImageName"
428 #endif /* __CONFIG_H */