1 /*
2 * (C) Copyright 2007-2008
3 * Stelian Pop <stelian@popies.net>
4 * Lead Tech Design <www.leadtechdesign.com>
5 *
6 * Configuation settings for the AT91SAM9RLEK board.
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 #ifndef __CONFIG_H
28 #define __CONFIG_H
30 #include <asm/hardware.h>
32 #define CONFIG_SYS_TEXT_BASE 0x21F00000
34 /* ARM asynchronous clock */
35 #define CONFIG_SYS_AT91_SLOW_CLOCK 32768 /* slow clock xtal */
36 #define CONFIG_SYS_AT91_MAIN_CLOCK 12000000 /* main clock xtal */
37 #define CONFIG_SYS_HZ 1000
39 #define CONFIG_AT91SAM9RLEK 1 /* It's an AT91SAM9RLEK Board */
41 #define CONFIG_ARCH_CPU_INIT
42 #define CONFIG_SKIP_LOWLEVEL_INIT
43 #define CONFIG_BOARD_EARLY_INIT_F
45 #define CONFIG_CMDLINE_TAG 1 /* enable passing of ATAGs */
46 #define CONFIG_SETUP_MEMORY_TAGS 1
47 #define CONFIG_INITRD_TAG 1
49 #define CONFIG_DISPLAY_CPUINFO
51 #define CONFIG_ATMEL_LEGACY
52 #define CONFIG_AT91_GPIO 1
53 #define CONFIG_AT91_GPIO_PULLUP 1
55 /*
56 * Hardware drivers
57 */
59 /* serial console */
60 #define CONFIG_ATMEL_USART
61 #define CONFIG_USART_BASE ATMEL_BASE_DBGU
62 #define CONFIG_USART_ID ATMEL_ID_SYS
63 #define CONFIG_BAUDRATE 115200
65 /* LCD */
66 #define CONFIG_LCD 1
67 #define LCD_BPP LCD_COLOR8
68 #define CONFIG_LCD_LOGO 1
69 #undef LCD_TEST_PATTERN
70 #define CONFIG_LCD_INFO 1
71 #define CONFIG_LCD_INFO_BELOW_LOGO 1
72 #define CONFIG_SYS_WHITE_ON_BLACK 1
73 #define CONFIG_ATMEL_LCD 1
74 #define CONFIG_ATMEL_LCD_RGB565 1
75 /* Let board_init_f handle the framebuffer allocation */
76 #undef CONFIG_FB_ADDR
77 #define CONFIG_SYS_CONSOLE_IS_IN_ENV 1
80 /* LED */
81 #define CONFIG_AT91_LED
82 #define CONFIG_RED_LED AT91_PIN_PD14 /* this is the power led */
83 #define CONFIG_GREEN_LED AT91_PIN_PD15 /* this is the user1 led */
84 #define CONFIG_YELLOW_LED AT91_PIN_PD16 /* this is the user2 led */
86 #define CONFIG_BOOTDELAY 3
88 /*
89 * Command line configuration.
90 */
91 #include <config_cmd_default.h>
92 #undef CONFIG_CMD_BDI
93 #undef CONFIG_CMD_FPGA
94 #undef CONFIG_CMD_IMI
95 #undef CONFIG_CMD_IMLS
96 #undef CONFIG_CMD_LOADS
97 #undef CONFIG_CMD_NET
98 #undef CONFIG_CMD_NFS
99 #undef CONFIG_CMD_SOURCE
100 #undef CONFIG_CMD_USB
102 #define CONFIG_CMD_NAND 1
104 /* SDRAM */
105 #define CONFIG_NR_DRAM_BANKS 1
106 #define CONFIG_SYS_SDRAM_BASE ATMEL_BASE_CS1
107 #define CONFIG_SYS_SDRAM_SIZE 0x04000000
109 #define CONFIG_SYS_INIT_SP_ADDR \
110 (ATMEL_BASE_SRAM + 0x1000 - GENERATED_GBL_DATA_SIZE)
112 /* DataFlash */
113 #define CONFIG_ATMEL_DATAFLASH_SPI
114 #define CONFIG_HAS_DATAFLASH 1
115 #define CONFIG_SYS_SPI_WRITE_TOUT (5*CONFIG_SYS_HZ)
116 #define CONFIG_SYS_MAX_DATAFLASH_BANKS 1
117 #define CONFIG_SYS_DATAFLASH_LOGIC_ADDR_CS0 0xC0000000 /* CS0 */
118 #define AT91_SPI_CLK 15000000
119 #define DATAFLASH_TCSS (0x1a << 16)
120 #define DATAFLASH_TCHS (0x1 << 24)
122 /* NOR flash - not present */
123 #define CONFIG_SYS_NO_FLASH 1
125 /* NAND flash */
126 #ifdef CONFIG_CMD_NAND
127 #define CONFIG_NAND_ATMEL
128 #define CONFIG_SYS_MAX_NAND_DEVICE 1
129 #define CONFIG_SYS_NAND_BASE ATMEL_BASE_CS3
130 #define CONFIG_SYS_NAND_DBW_8 1
131 /* our ALE is AD21 */
132 #define CONFIG_SYS_NAND_MASK_ALE (1 << 21)
133 /* our CLE is AD22 */
134 #define CONFIG_SYS_NAND_MASK_CLE (1 << 22)
135 #define CONFIG_SYS_NAND_ENABLE_PIN AT91_PIN_PB6
136 #define CONFIG_SYS_NAND_READY_PIN AT91_PIN_PD17
138 #endif
140 /* Ethernet - not present */
142 /* USB - not supported */
144 #define CONFIG_SYS_LOAD_ADDR 0x22000000 /* load address */
146 #define CONFIG_SYS_MEMTEST_START CONFIG_SYS_SDRAM_BASE
147 #define CONFIG_SYS_MEMTEST_END 0x23e00000
149 #ifdef CONFIG_SYS_USE_DATAFLASH
151 /* bootstrap + u-boot + env + linux in dataflash on CS0 */
152 #define CONFIG_ENV_IS_IN_DATAFLASH 1
153 #define CONFIG_SYS_MONITOR_BASE (CONFIG_SYS_DATAFLASH_LOGIC_ADDR_CS0 + 0x8400)
154 #define CONFIG_ENV_OFFSET 0x4200
155 #define CONFIG_ENV_ADDR (CONFIG_SYS_DATAFLASH_LOGIC_ADDR_CS0 + CONFIG_ENV_OFFSET)
156 #define CONFIG_ENV_SIZE 0x4200
157 #define CONFIG_BOOTCOMMAND "cp.b 0xC0084000 0x22000000 0x210000; bootm"
158 #define CONFIG_BOOTARGS "console=ttyS0,115200 " \
159 "root=/dev/mtdblock0 " \
160 "mtdparts=atmel_nand:-(root) "\
161 "rw rootfstype=jffs2"
163 #else /* CONFIG_SYS_USE_NANDFLASH */
165 /* bootstrap + u-boot + env + linux in nandflash */
166 #define CONFIG_ENV_IS_IN_NAND 1
167 #define CONFIG_ENV_OFFSET 0x60000
168 #define CONFIG_ENV_OFFSET_REDUND 0x80000
169 #define CONFIG_ENV_SIZE 0x20000 /* 1 sector = 128 kB */
170 #define CONFIG_BOOTCOMMAND "nand read 0x22000000 0xA0000 0x200000; bootm"
171 #define CONFIG_BOOTARGS "console=ttyS0,115200 " \
172 "root=/dev/mtdblock5 " \
173 "mtdparts=atmel_nand:128k(bootstrap)ro,256k(uboot)ro,128k(env1)ro,128k(env2)ro,2M(linux),-(root) " \
174 "rw rootfstype=jffs2"
176 #endif
178 #define CONFIG_SYS_PROMPT "U-Boot> "
179 #define CONFIG_SYS_CBSIZE 256
180 #define CONFIG_SYS_MAXARGS 16
181 #define CONFIG_SYS_PBSIZE (CONFIG_SYS_CBSIZE + sizeof(CONFIG_SYS_PROMPT) + 16)
182 #define CONFIG_SYS_LONGHELP 1
183 #define CONFIG_CMDLINE_EDITING 1
184 #define CONFIG_AUTO_COMPLETE
186 /*
187 * Size of malloc() pool
188 */
189 #define CONFIG_SYS_MALLOC_LEN ROUND(3 * CONFIG_ENV_SIZE + 128*1024, 0x1000)
191 #endif