arm: dra7xx: Add dra7xx_evm build support
[glsdk/glsdk-u-boot.git] / include / configs / omap5_common.h
1 /*
2  * (C) Copyright 2013
3  * Texas Instruments Incorporated.
4  * Sricharan R    <r.sricharan@ti.com>
5  *
6  * Derived from OMAP4 done by:
7  *      Aneesh V <aneesh@ti.com>
8  *
9  * TI OMAP5 AND DRA7XX common configuration settings
10  *
11  * See file CREDITS for list of people who contributed to this
12  * project.
13  *
14  * This program is free software; you can redistribute it and/or
15  * modify it under the terms of the GNU General Public License as
16  * published by the Free Software Foundation; either version 2 of
17  * the License, or (at your option) any later version.
18  *
19  * This program is distributed in the hope that it will be useful,
20  * but WITHOUT ANY WARRANTY; without even the implied warranty of
21  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
22  * GNU General Public License for more details.
23  *
24  * You should have received a copy of the GNU General Public License
25  * along with this program; if not, write to the Free Software
26  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
27  * MA 02111-1307 USA
28  */
30 #ifndef __CONFIG_OMAP5_COMMON_H
31 #define __CONFIG_OMAP5_COMMON_H
33 /*
34  * High Level Configuration Options
35  */
36 #define CONFIG_OMAP     /* in a TI OMAP core */
37 #define CONFIG_OMAP54XX /* which is a 54XX */
38 #define CONFIG_OMAP_GPIO
40 /* Get CPU defs */
41 #include <asm/arch/cpu.h>
42 #include <asm/arch/omap.h>
44 /* Display CPU and Board Info */
45 #define CONFIG_DISPLAY_CPUINFO
46 #define CONFIG_DISPLAY_BOARDINFO
48 /* Clock Defines */
49 #define V_OSCK                  19200000        /* Clock output from T2 */
50 #define V_SCLK  V_OSCK
52 #define CONFIG_MISC_INIT_R
54 #define CONFIG_OF_LIBFDT
55 #define CONFIG_CMD_BOOTZ
57 #define CONFIG_CMDLINE_TAG /* enable passing of ATAGs */
58 #define CONFIG_SETUP_MEMORY_TAGS
59 #define CONFIG_INITRD_TAG
61 /*
62  * Size of malloc() pool
63  * Total Size Environment - 128k
64  * Malloc - add 256k
65  */
66 #define CONFIG_ENV_SIZE                 (128 << 10)
67 #define CONFIG_SYS_MALLOC_LEN           (CONFIG_ENV_SIZE + (256 << 10))
68 /* Vector Base */
69 #define CONFIG_SYS_CA9_VECTOR_BASE      SRAM_ROM_VECT_BASE
71 /*
72  * Hardware drivers
73  */
75 /*
76  * serial port - NS16550 compatible
77  */
78 #define V_NS16550_CLK                   48000000
80 #define CONFIG_SYS_NS16550
81 #define CONFIG_SYS_NS16550_SERIAL
82 #define CONFIG_SYS_NS16550_REG_SIZE     (-4)
83 #define CONFIG_SYS_NS16550_CLK          V_NS16550_CLK
84 #define CONFIG_CONS_INDEX               3
85 #define CONFIG_SYS_NS16550_COM3         UART3_BASE
87 #define CONFIG_BAUDRATE                 115200
88 #define CONFIG_SYS_BAUDRATE_TABLE       {4800, 9600, 19200, 38400, 57600,\
89                                         115200}
90 /* I2C  */
91 #define CONFIG_HARD_I2C
92 #define CONFIG_SYS_I2C_SPEED            100000
93 #define CONFIG_SYS_I2C_SLAVE            1
94 #define CONFIG_DRIVER_OMAP34XX_I2C
95 #define CONFIG_I2C_MULTI_BUS
98 /* MMC */
99 #define CONFIG_GENERIC_MMC
100 #define CONFIG_MMC
101 #define CONFIG_OMAP_HSMMC
102 #define CONFIG_DOS_PARTITION
104 /* MMC ENV related defines */
105 #define CONFIG_ENV_IS_IN_MMC
106 #define CONFIG_SYS_MMC_ENV_DEV          1       /* SLOT2: eMMC(1) */
107 #define CONFIG_ENV_OFFSET               0xE0000
108 #define CONFIG_CMD_SAVEENV
110 #define CONFIG_SYS_CONSOLE_IS_IN_ENV
112 /* Flash */
113 #define CONFIG_SYS_NO_FLASH
115 /* Cache */
116 #define CONFIG_SYS_CACHELINE_SIZE       64
117 #define CONFIG_SYS_CACHELINE_SHIFT      6
119 /* commands to include */
120 #include <config_cmd_default.h>
122 /* Enabled commands */
123 #define CONFIG_CMD_EXT2         /* EXT2 Support                 */
124 #define CONFIG_CMD_FAT          /* FAT support                  */
125 #define CONFIG_CMD_I2C          /* I2C serial bus support       */
126 #define CONFIG_CMD_MMC          /* MMC support                  */
127 #define CONFIG_CMD_SAVEENV
129 /* Disabled commands */
130 #undef CONFIG_CMD_NET
131 #undef CONFIG_CMD_NFS
132 #undef CONFIG_CMD_FPGA          /* FPGA configuration Support   */
133 #undef CONFIG_CMD_IMLS          /* List all found images        */
135 /*
136  * Environment setup
137  */
139 #define CONFIG_BOOTDELAY        3
141 #define CONFIG_ENV_OVERWRITE
143 #define CONFIG_EXTRA_ENV_SETTINGS \
144         "loadaddr=0x82000000\0" \
145         "console=ttyO2,115200n8\0" \
146         "usbtty=cdc_acm\0" \
147         "vram=16M\0" \
148         "mmcdev=0\0" \
149         "mmcroot=/dev/mmcblk0p2 rw\0" \
150         "mmcrootfstype=ext3 rootwait\0" \
151         "mmcargs=setenv bootargs console=${console} " \
152                 "vram=${vram} " \
153                 "root=${mmcroot} " \
154                 "rootfstype=${mmcrootfstype}\0" \
155         "loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr\0" \
156         "bootscript=echo Running bootscript from mmc${mmcdev} ...; " \
157                 "source ${loadaddr}\0" \
158         "loaduimage=fatload mmc ${mmcdev} ${loadaddr} uImage\0" \
159         "mmcboot=echo Booting from mmc${mmcdev} ...; " \
160                 "run mmcargs; " \
161                 "bootm ${loadaddr}\0" \
163 #define CONFIG_BOOTCOMMAND \
164         "mmc dev ${mmcdev}; if mmc rescan; then " \
165                 "if run loadbootscript; then " \
166                         "run bootscript; " \
167                 "else " \
168                         "if run loaduimage; then " \
169                                 "run mmcboot; " \
170                         "fi; " \
171                 "fi; " \
172         "fi"
174 #define CONFIG_AUTO_COMPLETE            1
176 /*
177  * Miscellaneous configurable options
178  */
180 #define CONFIG_SYS_LONGHELP     /* undef to save memory */
181 #define CONFIG_SYS_HUSH_PARSER  /* use "hush" command parser */
182 #define CONFIG_SYS_CBSIZE               256
183 /* Print Buffer Size */
184 #define CONFIG_SYS_PBSIZE               (CONFIG_SYS_CBSIZE + \
185                                         sizeof(CONFIG_SYS_PROMPT) + 16)
186 #define CONFIG_SYS_MAXARGS              16
187 /* Boot Argument Buffer Size */
188 #define CONFIG_SYS_BARGSIZE             (CONFIG_SYS_CBSIZE)
190 /*
191  * memtest setup
192  */
193 #define CONFIG_SYS_MEMTEST_START        0x80000000
194 #define CONFIG_SYS_MEMTEST_END          (CONFIG_SYS_MEMTEST_START + (32 << 20))
196 /* Default load address */
197 #define CONFIG_SYS_LOAD_ADDR            0x80000000
199 /* Use General purpose timer 1 */
200 #define CONFIG_SYS_TIMERBASE            GPT2_BASE
201 #define CONFIG_SYS_PTV                  2       /* Divisor: 2^(PTV+1) => 8 */
202 #define CONFIG_SYS_HZ                   1000
204 /*
205  * SDRAM Memory Map
206  * Even though we use two CS all the memory
207  * is mapped to one contiguous block
208  */
209 #define CONFIG_NR_DRAM_BANKS    1
211 #define CONFIG_SYS_SDRAM_BASE           0x80000000
212 #define CONFIG_SYS_INIT_SP_ADDR         (NON_SECURE_SRAM_END - \
213                                          GENERATED_GBL_DATA_SIZE)
215 #define CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS
217 /* Defines for SDRAM init */
218 #ifndef CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGS
219 #define CONFIG_SYS_AUTOMATIC_SDRAM_DETECTION
220 #define CONFIG_SYS_DEFAULT_LPDDR2_TIMINGS
221 #endif
223 /* Defines for SPL */
224 #define CONFIG_SPL
225 #define CONFIG_SPL_FRAMEWORK
226 #define CONFIG_SPL_TEXT_BASE            0x40300350
227 #define CONFIG_SPL_MAX_SIZE             0x19000 /* 100K */
228 #define CONFIG_SPL_STACK                CONFIG_SYS_INIT_SP_ADDR
229 #define CONFIG_SPL_DISPLAY_PRINT
231 #define CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR 0x300 /* address 0x60000 */
232 #define CONFIG_SYS_U_BOOT_MAX_SIZE_SECTORS      0x200 /* 256 KB */
233 #define CONFIG_SYS_MMC_SD_FAT_BOOT_PARTITION    1
234 #define CONFIG_SPL_FAT_LOAD_PAYLOAD_NAME        "u-boot.img"
236 #define CONFIG_SPL_LIBCOMMON_SUPPORT
237 #define CONFIG_SPL_LIBDISK_SUPPORT
238 #define CONFIG_SPL_I2C_SUPPORT
239 #define CONFIG_SPL_MMC_SUPPORT
240 #define CONFIG_SPL_FAT_SUPPORT
241 #define CONFIG_SPL_LIBGENERIC_SUPPORT
242 #define CONFIG_SPL_SERIAL_SUPPORT
243 #define CONFIG_SPL_LDSCRIPT "$(CPUDIR)/omap-common/u-boot-spl.lds"
245 /*
246  * 64 bytes before this address should be set aside for u-boot.img's
247  * header. That is 80E7FFC0--0x80E80000 should not be used for any
248  * other needs.
249  */
250 #define CONFIG_SYS_TEXT_BASE            0x80E80000
252 /*
253  * BSS and malloc area 64MB into memory to allow enough
254  * space for the kernel at the beginning of memory
255  */
256 #define CONFIG_SPL_BSS_START_ADDR       0x84000000
257 #define CONFIG_SPL_BSS_MAX_SIZE         0x100000        /* 1 MB */
258 #define CONFIG_SYS_SPL_MALLOC_START     0x84100000
259 #define CONFIG_SYS_SPL_MALLOC_SIZE      0x100000        /* 1 MB */
260 #define CONFIG_SPL_GPIO_SUPPORT
262 #endif /* __CONFIG_OMAP5_COMMON_H */