1 /*
2 * (C) Copyright 2002
3 * Kyle Harris, Nexus Technologies, Inc. kharris@nexus-tech.net
4 *
5 * (C) Copyright 2002
6 * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
7 * Marius Groeger <mgroeger@sysgo.de>
8 *
9 * Copied from lubbock.h
10 *
11 * (C) Copyright 2004
12 * BEC Systems <http://bec-systems.com>
13 * Cliff Brake <cliff.brake@gmail.com>
14 * Configuation settings for the Accelent/Vibren PXA255 IDP
15 *
16 * See file CREDITS for list of people who contributed to this
17 * project.
18 *
19 * This program is free software; you can redistribute it and/or
20 * modify it under the terms of the GNU General Public License as
21 * published by the Free Software Foundation; either version 2 of
22 * the License, or (at your option) any later version.
23 *
24 * This program is distributed in the hope that it will be useful,
25 * but WITHOUT ANY WARRANTY; without even the implied warranty of
26 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
27 * GNU General Public License for more details.
28 *
29 * You should have received a copy of the GNU General Public License
30 * along with this program; if not, write to the Free Software
31 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
32 * MA 02111-1307 USA
33 */
35 #ifndef __CONFIG_H
36 #define __CONFIG_H
38 #include <asm/arch/pxa-regs.h>
40 /*
41 * If we are developing, we might want to start U-Boot from RAM
42 * so we MUST NOT initialize critical regs like mem-timing ...
43 */
44 #undef CONFIG_SKIP_LOWLEVEL_INIT /* define for developing */
45 #define CONFIG_SYS_TEXT_BASE 0x0
47 /*
48 * define the following to enable debug blinks. A debug blink function
49 * must be defined in memsetup.S
50 */
51 #undef DEBUG_BLINK_ENABLE
52 #undef DEBUG_BLINKC_ENABLE
54 /*
55 * High Level Configuration Options
56 * (easy to change)
57 */
58 #define CONFIG_CPU_PXA25X 1 /* This is an PXA250 CPU */
60 #undef CONFIG_LCD
61 #ifdef CONFIG_LCD
62 #define CONFIG_SHARP_LM8V31
63 #endif
65 #define CONFIG_MMC 1
66 #define CONFIG_DOS_PARTITION 1
67 #define CONFIG_BOARD_LATE_INIT
69 /* we will never enable dcache, because we have to setup MMU first */
70 #define CONFIG_SYS_DCACHE_OFF
72 /*
73 * Size of malloc() pool
74 */
75 #define CONFIG_SYS_MALLOC_LEN (CONFIG_ENV_SIZE + 128*1024)
77 /*
78 * PXA250 IDP memory map information
79 */
81 #define IDP_CS5_ETH_OFFSET 0x03400000
84 /*
85 * Hardware drivers
86 */
87 #define CONFIG_SMC91111
88 #define CONFIG_SMC91111_BASE (PXA_CS5_PHYS + IDP_CS5_ETH_OFFSET + 0x300)
89 #define CONFIG_SMC_USE_32_BIT 1
90 /* #define CONFIG_SMC_USE_IOFUNCS */
92 /* the following has to be set high -- suspect something is wrong with
93 * with the tftp timeout routines. FIXME!!!
94 */
95 #define CONFIG_NET_RETRY_COUNT 100
97 /*
98 * select serial console configuration
99 */
100 #define CONFIG_PXA_SERIAL
101 #define CONFIG_FFUART 1 /* we use FFUART on LUBBOCK */
102 #define CONFIG_CONS_INDEX 3
104 /* allow to overwrite serial and ethaddr */
105 #define CONFIG_ENV_OVERWRITE
107 #define CONFIG_BAUDRATE 115200
110 /*
111 * BOOTP options
112 */
113 #define CONFIG_BOOTP_BOOTFILESIZE
114 #define CONFIG_BOOTP_BOOTPATH
115 #define CONFIG_BOOTP_GATEWAY
116 #define CONFIG_BOOTP_HOSTNAME
119 /*
120 * Command line configuration.
121 */
122 #include <config_cmd_default.h>
124 #define CONFIG_CMD_FAT
125 #define CONFIG_CMD_DHCP
127 #define CONFIG_BOOTDELAY 3
128 #define CONFIG_BOOTCOMMAND "bootm 40000"
129 #define CONFIG_BOOTARGS "root=/dev/mtdblock2 rootfstype=cramfs console=ttyS0,115200"
131 #define CONFIG_CMDLINE_TAG 1 /* enable passing of ATAGs */
132 #define CONFIG_SETUP_MEMORY_TAGS 1
133 /* #define CONFIG_INITRD_TAG 1 */
135 /*
136 * Current memory map for Vibren supplied Linux images:
137 *
138 * Flash:
139 * 0 - 0x3ffff (size = 0x40000): bootloader
140 * 0x40000 - 0x13ffff (size = 0x100000): kernel
141 * 0x140000 - 0x1f3ffff (size = 0x1e00000): jffs
142 *
143 * RAM:
144 * 0xa0008000 - kernel is loaded
145 * 0xa3000000 - Uboot runs (48MB into RAM)
146 *
147 */
149 #define CONFIG_EXTRA_ENV_SETTINGS \
150 "prog_boot_mmc=" \
151 "mw.b 0xa0000000 0xff 0x40000; " \
152 "if mmcinit && " \
153 "fatload mmc 0 0xa0000000 u-boot.bin; " \
154 "then " \
155 "protect off 0x0 0x3ffff; " \
156 "erase 0x0 0x3ffff; " \
157 "cp.b 0xa0000000 0x0 0x40000; " \
158 "reset;" \
159 "fi\0" \
160 "prog_uzImage_mmc=" \
161 "mw.b 0xa0000000 0xff 0x100000; " \
162 "if mmcinit && " \
163 "fatload mmc 0 0xa0000000 uzImage; " \
164 "then " \
165 "protect off 0x40000 0xfffff; " \
166 "erase 0x40000 0xfffff; " \
167 "cp.b 0xa0000000 0x40000 0x100000; " \
168 "fi\0" \
169 "prog_jffs_mmc=" \
170 "mw.b 0xa0000000 0xff 0x1e00000; " \
171 "if mmcinit && " \
172 "fatload mmc 0 0xa0000000 root.jffs; " \
173 "then " \
174 "protect off 0x140000 0x1f3ffff; " \
175 "erase 0x140000 0x1f3ffff; " \
176 "cp.b 0xa0000000 0x140000 0x1e00000; " \
177 "fi\0" \
178 "boot_mmc=" \
179 "if mmcinit && " \
180 "fatload mmc 0 0xa1000000 uzImage && " \
181 "then " \
182 "bootm 0xa1000000; " \
183 "fi\0" \
184 "prog_boot_net=" \
185 "mw.b 0xa0000000 0xff 0x100000; " \
186 "if bootp 0xa0000000 u-boot.bin; " \
187 "then " \
188 "protect off 0x0 0x3ffff; " \
189 "erase 0x0 0x3ffff; " \
190 "cp.b 0xa0000000 0x0 0x40000; " \
191 "reset; " \
192 "fi\0" \
193 "prog_uzImage_net=" \
194 "mw.b 0xa0000000 0xff 0x100000; " \
195 "if bootp 0xa0000000 uzImage; " \
196 "then " \
197 "protect off 0x40000 0xfffff; " \
198 "erase 0x40000 0xfffff; " \
199 "cp.b 0xa0000000 0x40000 0x100000; " \
200 "fi\0" \
201 "prog_jffs_net=" \
202 "mw.b 0xa0000000 0xff 0x1e00000; " \
203 "if bootp 0xa0000000 root.jffs; " \
204 "then " \
205 "protect off 0x140000 0x1f3ffff; " \
206 "erase 0x140000 0x1f3ffff; " \
207 "cp.b 0xa0000000 0x140000 0x1e00000; " \
208 "fi\0"
211 /* "erase_env=" */
212 /* "protect off" */
215 #if defined(CONFIG_CMD_KGDB)
216 #define CONFIG_KGDB_BAUDRATE 115200 /* speed to run kgdb serial port */
217 #define CONFIG_KGDB_SER_INDEX 2 /* which serial port to use */
218 #endif
220 /*
221 * Miscellaneous configurable options
222 */
223 #define CONFIG_SYS_HUSH_PARSER 1
225 #define CONFIG_SYS_LONGHELP /* undef to save memory */
226 #ifdef CONFIG_SYS_HUSH_PARSER
227 #define CONFIG_SYS_PROMPT "$ " /* Monitor Command Prompt */
228 #else
229 #define CONFIG_SYS_PROMPT "=> " /* Monitor Command Prompt */
230 #endif
231 #define CONFIG_SYS_CBSIZE 256 /* Console I/O Buffer Size */
232 #define CONFIG_SYS_PBSIZE (CONFIG_SYS_CBSIZE+sizeof(CONFIG_SYS_PROMPT)+16) /* Print Buffer Size */
233 #define CONFIG_SYS_MAXARGS 16 /* max number of command args */
234 #define CONFIG_SYS_BARGSIZE CONFIG_SYS_CBSIZE /* Boot Argument Buffer Size */
235 #define CONFIG_SYS_DEVICE_NULLDEV 1
237 #define CONFIG_SYS_MEMTEST_START 0xa0400000 /* memtest works on */
238 #define CONFIG_SYS_MEMTEST_END 0xa0800000 /* 4 ... 8 MB in DRAM */
240 #define CONFIG_SYS_LOAD_ADDR 0xa0800000 /* default load address */
242 #define CONFIG_SYS_HZ 1000
243 #define CONFIG_SYS_CPUSPEED 0x161 /* set core clock to 400/200/100 MHz */
245 #define RTC 1 /* enable 32KHz osc */
247 #ifdef CONFIG_MMC
248 #define CONFIG_GENERIC_MMC
249 #define CONFIG_PXA_MMC_GENERIC
250 #define CONFIG_CMD_MMC
251 #define CONFIG_SYS_MMC_BASE 0xF0000000
252 #endif
254 /*
255 * Physical Memory Map
256 */
257 #define CONFIG_NR_DRAM_BANKS 1 /* we have 1 bank of DRAM */
258 #define PHYS_SDRAM_1 0xa0000000 /* SDRAM Bank #1 */
259 #define PHYS_SDRAM_1_SIZE 0x04000000 /* 64 MB */
260 #define PHYS_SDRAM_2 0xa4000000 /* SDRAM Bank #2 */
261 #define PHYS_SDRAM_2_SIZE 0x00000000 /* 0 MB */
262 #define PHYS_SDRAM_3 0xa8000000 /* SDRAM Bank #3 */
263 #define PHYS_SDRAM_3_SIZE 0x00000000 /* 0 MB */
264 #define PHYS_SDRAM_4 0xac000000 /* SDRAM Bank #4 */
265 #define PHYS_SDRAM_4_SIZE 0x00000000 /* 0 MB */
267 #define PHYS_FLASH_1 0x00000000 /* Flash Bank #1 */
268 #define PHYS_FLASH_2 0x04000000 /* Flash Bank #2 */
269 #define PHYS_FLASH_SIZE 0x02000000 /* 32 MB */
270 #define PHYS_FLASH_BANK_SIZE 0x02000000 /* 32 MB Banks */
271 #define PHYS_FLASH_SECT_SIZE 0x00040000 /* 256 KB sectors (x2) */
273 #define CONFIG_SYS_DRAM_BASE 0xa0000000
274 #define CONFIG_SYS_DRAM_SIZE 0x04000000
276 #define CONFIG_SYS_FLASH_BASE PHYS_FLASH_1
278 #define CONFIG_SYS_SDRAM_BASE PHYS_SDRAM_1
279 #define CONFIG_SYS_INIT_SP_ADDR 0xfffff800
281 /*
282 * GPIO settings
283 */
285 #define CONFIG_SYS_GAFR0_L_VAL 0x80001005
286 #define CONFIG_SYS_GAFR0_U_VAL 0xa5128012
287 #define CONFIG_SYS_GAFR1_L_VAL 0x699a9558
288 #define CONFIG_SYS_GAFR1_U_VAL 0xaaa5aa6a
289 #define CONFIG_SYS_GAFR2_L_VAL 0xaaaaaaaa
290 #define CONFIG_SYS_GAFR2_U_VAL 0x2
291 #define CONFIG_SYS_GPCR0_VAL 0x1800400
292 #define CONFIG_SYS_GPCR1_VAL 0x0
293 #define CONFIG_SYS_GPCR2_VAL 0x0
294 #define CONFIG_SYS_GPDR0_VAL 0xc1818440
295 #define CONFIG_SYS_GPDR1_VAL 0xfcffab82
296 #define CONFIG_SYS_GPDR2_VAL 0x1ffff
297 #define CONFIG_SYS_GPSR0_VAL 0x8000
298 #define CONFIG_SYS_GPSR1_VAL 0x3f0002
299 #define CONFIG_SYS_GPSR2_VAL 0x1c000
301 #define CONFIG_SYS_PSSR_VAL 0x20
303 #define CONFIG_SYS_CCCR CCCR_L27|CCCR_M2|CCCR_N10
304 #define CONFIG_SYS_CKEN 0x0
306 /*
307 * Memory settings
308 */
309 #define CONFIG_SYS_MSC0_VAL 0x29DCA4D2
310 #define CONFIG_SYS_MSC1_VAL 0x43AC494C
311 #define CONFIG_SYS_MSC2_VAL 0x39D449D4
312 #define CONFIG_SYS_MDCNFG_VAL 0x090009C9
313 #define CONFIG_SYS_MDREFR_VAL 0x0085C017
314 #define CONFIG_SYS_MDMRS_VAL 0x00220022
315 #define CONFIG_SYS_FLYCNFG_VAL 0x00000000
316 #define CONFIG_SYS_SXCNFG_VAL 0x00000000
318 /*
319 * PCMCIA and CF Interfaces
320 */
321 #define CONFIG_SYS_MECR_VAL 0x00000003
322 #define CONFIG_SYS_MCMEM0_VAL 0x00014405
323 #define CONFIG_SYS_MCMEM1_VAL 0x00014405
324 #define CONFIG_SYS_MCATT0_VAL 0x00014405
325 #define CONFIG_SYS_MCATT1_VAL 0x00014405
326 #define CONFIG_SYS_MCIO0_VAL 0x00014405
327 #define CONFIG_SYS_MCIO1_VAL 0x00014405
329 /*
330 * FLASH and environment organization
331 */
332 #define CONFIG_SYS_FLASH_CFI
333 #define CONFIG_FLASH_CFI_DRIVER 1
335 #define CONFIG_SYS_MONITOR_BASE 0
336 #define CONFIG_SYS_MONITOR_LEN PHYS_FLASH_SECT_SIZE
338 #define CONFIG_SYS_MAX_FLASH_BANKS 1 /* max number of memory banks */
339 #define CONFIG_SYS_MAX_FLASH_SECT 128 /* max number of sectors on one chip */
341 #define CONFIG_SYS_FLASH_USE_BUFFER_WRITE 1
343 /* timeout values are in ticks */
344 #define CONFIG_SYS_FLASH_ERASE_TOUT (25*CONFIG_SYS_HZ) /* Timeout for Flash Erase */
345 #define CONFIG_SYS_FLASH_WRITE_TOUT (25*CONFIG_SYS_HZ) /* Timeout for Flash Write */
347 /* put cfg at end of flash for now */
348 #define CONFIG_ENV_IS_IN_FLASH 1
349 /* Addr of Environment Sector */
350 #define CONFIG_ENV_ADDR (PHYS_FLASH_1 + PHYS_FLASH_SIZE - 0x40000)
351 #define CONFIG_ENV_SIZE PHYS_FLASH_SECT_SIZE /* Total Size of Environment Sector */
352 #define CONFIG_ENV_SECT_SIZE (PHYS_FLASH_SECT_SIZE / 16)
354 #endif /* __CONFIG_H */