1 /*
2 * (C) Copyright 2003
3 * Data Flash Atmel Description File
4 * Author : Hamid Ikdoumi (Atmel)
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 */
25 /* File Name : dataflash.h */
26 /* Object : Data Flash Atmel Description File */
27 /* Translator : */
28 /* */
29 /* 1.0 03/04/01 HI : Creation */
30 /* 1.2 20/10/02 FB : Adapatation Service and Lib v3 */
31 /*----------------------------------------------------------------------*/
33 #ifndef _DataFlash_h
34 #define _DataFlash_h
37 #include "config.h"
39 /*number of protected area*/
40 #define NB_DATAFLASH_AREA 5
42 #ifdef CONFIG_SYS_NO_FLASH
44 /*-----------------------------------------------------------------------
45 * return codes from flash_write():
46 */
47 # define ERR_OK 0
48 # define ERR_TIMOUT 1
49 # define ERR_NOT_ERASED 2
50 # define ERR_PROTECTED 4
51 # define ERR_INVAL 8
52 # define ERR_ALIGN 16
53 # define ERR_UNKNOWN_FLASH_VENDOR 32
54 # define ERR_UNKNOWN_FLASH_TYPE 64
55 # define ERR_PROG_ERROR 128
57 /*-----------------------------------------------------------------------
58 * Protection Flags for flash_protect():
59 */
60 # define FLAG_PROTECT_SET 0x01
61 # define FLAG_PROTECT_CLEAR 0x02
62 # define FLAG_PROTECT_INVALID 0x03
64 /*-----------------------------------------------------------------------
65 * Set Environment according to label:
66 */
67 # define FLAG_SETENV 0x80
68 #endif /* CONFIG_SYS_NO_FLASH */
70 /*define the area structure*/
71 typedef struct {
72 unsigned long start;
73 unsigned long end;
74 unsigned char protected;
75 unsigned char setenv;
76 unsigned char label[20];
77 } dataflash_protect_t;
79 typedef unsigned int AT91S_DataFlashStatus;
81 /*----------------------------------------------------------------------*/
82 /* DataFlash Structures */
83 /*----------------------------------------------------------------------*/
85 /*---------------------------------------------*/
86 /* DataFlash Descriptor Structure Definition */
87 /*---------------------------------------------*/
88 typedef struct _AT91S_DataflashDesc {
89 unsigned char *tx_cmd_pt;
90 unsigned int tx_cmd_size;
91 unsigned char *rx_cmd_pt;
92 unsigned int rx_cmd_size;
93 unsigned char *tx_data_pt;
94 unsigned int tx_data_size;
95 unsigned char *rx_data_pt;
96 unsigned int rx_data_size;
97 volatile unsigned char state;
98 volatile unsigned char DataFlash_state;
99 unsigned char command[8];
100 } AT91S_DataflashDesc, *AT91PS_DataflashDesc;
102 /*---------------------------------------------*/
103 /* DataFlash device definition structure */
104 /*---------------------------------------------*/
105 typedef struct _AT91S_Dataflash {
106 int pages_number; /* dataflash page number */
107 int pages_size; /* dataflash page size */
108 int page_offset; /* page offset in command */
109 int byte_mask; /* byte mask in command */
110 int cs;
111 dataflash_protect_t area_list[NB_DATAFLASH_AREA]; /* area protection status */
112 } AT91S_DataflashFeatures, *AT91PS_DataflashFeatures;
114 /*---------------------------------------------*/
115 /* DataFlash Structure Definition */
116 /*---------------------------------------------*/
117 typedef struct _AT91S_DataFlash {
118 AT91PS_DataflashDesc pDataFlashDesc; /* dataflash descriptor */
119 AT91PS_DataflashFeatures pDevice; /* Pointer on a dataflash features array */
120 } AT91S_DataFlash, *AT91PS_DataFlash;
123 typedef struct _AT91S_DATAFLASH_INFO {
125 AT91S_DataflashDesc Desc;
126 AT91S_DataflashFeatures Device; /* Pointer on a dataflash features array */
127 unsigned long logical_address;
128 unsigned long end_address;
129 unsigned int id; /* device id */
130 } AT91S_DATAFLASH_INFO, *AT91PS_DATAFLASH_INFO;
132 struct dataflash_addr {
133 unsigned long addr;
134 int cs;
135 };
136 /*-------------------------------------------------------------------------------------------------*/
137 #define AT45DB161 0x2c
138 #define AT45DB021 0x14
139 #define AT45DB081 0x24
140 #define AT45DB321 0x34
141 #define AT45DB642 0x3c
142 #define AT45DB128 0x10
143 #define PAGES_PER_BLOCK 8
145 #define AT91C_DATAFLASH_TIMEOUT 10000 /* For AT91F_DataFlashWaitReady */
147 /* DataFlash return value */
148 #define DATAFLASH_BUSY 0x00
149 #define DATAFLASH_OK 0x01
150 #define DATAFLASH_ERROR 0x02
151 #define DATAFLASH_MEMORY_OVERFLOW 0x03
152 #define DATAFLASH_BAD_COMMAND 0x04
153 #define DATAFLASH_BAD_ADDRESS 0x05
156 /* Driver State */
157 #define IDLE 0x0
158 #define BUSY 0x1
159 #define ERROR 0x2
161 /* DataFlash Driver State */
162 #define GET_STATUS 0x0F
164 /*-------------------------------------------------------------------------------------------------*/
165 /* Command Definition */
166 /*-------------------------------------------------------------------------------------------------*/
168 /* READ COMMANDS */
169 #define DB_CONTINUOUS_ARRAY_READ 0xE8 /* Continuous array read */
170 #define DB_BURST_ARRAY_READ 0xE8 /* Burst array read */
171 #define DB_PAGE_READ 0xD2 /* Main memory page read */
172 #define DB_BUF1_READ 0xD4 /* Buffer 1 read */
173 #define DB_BUF2_READ 0xD6 /* Buffer 2 read */
174 #define DB_STATUS 0xD7 /* Status Register */
176 /* PROGRAM and ERASE COMMANDS */
177 #define DB_BUF1_WRITE 0x84 /* Buffer 1 write */
178 #define DB_BUF2_WRITE 0x87 /* Buffer 2 write */
179 #define DB_BUF1_PAGE_ERASE_PGM 0x83 /* Buffer 1 to main memory page program with built-In erase */
180 #define DB_BUF1_PAGE_ERASE_FASTPGM 0x93 /* Buffer 1 to main memory page program with built-In erase, Fast program */
181 #define DB_BUF2_PAGE_ERASE_PGM 0x86 /* Buffer 2 to main memory page program with built-In erase */
182 #define DB_BUF2_PAGE_ERASE_FASTPGM 0x96 /* Buffer 1 to main memory page program with built-In erase, Fast program */
183 #define DB_BUF1_PAGE_PGM 0x88 /* Buffer 1 to main memory page program without built-In erase */
184 #define DB_BUF1_PAGE_FASTPGM 0x98 /* Buffer 1 to main memory page program without built-In erase, Fast program */
185 #define DB_BUF2_PAGE_PGM 0x89 /* Buffer 2 to main memory page program without built-In erase */
186 #define DB_BUF2_PAGE_FASTPGM 0x99 /* Buffer 1 to main memory page program without built-In erase, Fast program */
187 #define DB_PAGE_ERASE 0x81 /* Page Erase */
188 #define DB_BLOCK_ERASE 0x50 /* Block Erase */
189 #define DB_PAGE_PGM_BUF1 0x82 /* Main memory page through buffer 1 */
190 #define DB_PAGE_FASTPGM_BUF1 0x92 /* Main memory page through buffer 1, Fast program */
191 #define DB_PAGE_PGM_BUF2 0x85 /* Main memory page through buffer 2 */
192 #define DB_PAGE_FastPGM_BUF2 0x95 /* Main memory page through buffer 2, Fast program */
194 /* ADDITIONAL COMMANDS */
195 #define DB_PAGE_2_BUF1_TRF 0x53 /* Main memory page to buffer 1 transfert */
196 #define DB_PAGE_2_BUF2_TRF 0x55 /* Main memory page to buffer 2 transfert */
197 #define DB_PAGE_2_BUF1_CMP 0x60 /* Main memory page to buffer 1 compare */
198 #define DB_PAGE_2_BUF2_CMP 0x61 /* Main memory page to buffer 2 compare */
199 #define DB_AUTO_PAGE_PGM_BUF1 0x58 /* Auto page rewrite throught buffer 1 */
200 #define DB_AUTO_PAGE_PGM_BUF2 0x59 /* Auto page rewrite throught buffer 2 */
202 /*-------------------------------------------------------------------------------------------------*/
204 extern int size_dataflash (AT91PS_DataFlash pdataFlash, unsigned long addr, unsigned long size);
205 extern int prot_dataflash (AT91PS_DataFlash pdataFlash, unsigned long addr);
206 extern int addr2ram(ulong addr);
207 extern int dataflash_real_protect (int flag, unsigned long start_addr, unsigned long end_addr);
208 extern int addr_dataflash (unsigned long addr);
209 extern int read_dataflash (unsigned long addr, unsigned long size, char *result);
210 extern int write_dataflash(unsigned long addr_dest, unsigned long addr_src,
211 unsigned long size);
212 extern int AT91F_DataflashInit(void);
214 extern void dataflash_print_info (void);
215 extern void dataflash_perror (int err);
216 extern void AT91F_DataflashSetEnv (void);
218 extern struct dataflash_addr cs[CONFIG_SYS_MAX_DATAFLASH_BANKS];
219 extern dataflash_protect_t area_list[NB_DATAFLASH_AREA];
220 extern AT91S_DATAFLASH_INFO dataflash_info[];
221 #endif