]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/fdc.h
dra7xx: Enabled UART-boot mode
[glsdk/glsdk-u-boot.git] / include / fdc.h
1 /*
2  * (C) Copyright 2002
3  * Stäubli Faverges - <www.staubli.com>
4  * Pierre AUBERT  p.aubert@staubli.com
5  *
6  * See file CREDITS for list of people who contributed to this
7  * project.
8  *
9  * This program is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU General Public License as
11  * published by the Free Software Foundation; either version 2 of
12  * the License, or (at your option) any later version.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
17  * GNU General Public License for more details.
18  *
19  * You should have received a copy of the GNU General Public License
20  * along with this program; if not, write to the Free Software
21  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22  * MA 02111-1307 USA
23  */
25 #ifndef _FDC_H_
26 #define _FDC_H_
28 /* Functions prototype                                                       */
29 int fdc_fdos_init (int drive);
30 int fdc_fdos_seek (int where);
31 int fdc_fdos_read (void *buffer, int len);
33 int dos_open(char *name);
34 int dos_read (ulong addr);
35 int dos_dir (void);
37 #endif