568bcbfaa730f19763512088da1ae9ad50dea109
1 /*
2 * (C) Copyright 2007
3 * Gerald Van Baren, Custom IDEAS, vanbaren@cideas.com
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #ifndef __FDT_SUPPORT_H
25 #define __FDT_SUPPORT_H
27 #ifdef CONFIG_OF_LIBFDT
29 #include <libfdt_env.h>
30 #include <fdt.h>
32 u32 fdt_getprop_u32_default(const void *fdt, const char *path,
33 const char *prop, const u32 dflt);
34 int fdt_chosen(void *fdt, int force);
35 int fdt_initrd(void *fdt, ulong initrd_start, ulong initrd_end, int force);
36 void do_fixup_by_path(void *fdt, const char *path, const char *prop,
37 const void *val, int len, int create);
38 void do_fixup_by_path_u32(void *fdt, const char *path, const char *prop,
39 u32 val, int create);
41 static inline void do_fixup_by_path_string(void *fdt, const char *path,
42 const char *prop, const char *status)
43 {
44 do_fixup_by_path(fdt, path, prop, status, strlen(status) + 1, 1);
45 }
47 void do_fixup_by_prop(void *fdt,
48 const char *pname, const void *pval, int plen,
49 const char *prop, const void *val, int len,
50 int create);
51 void do_fixup_by_prop_u32(void *fdt,
52 const char *pname, const void *pval, int plen,
53 const char *prop, u32 val, int create);
54 void do_fixup_by_compat(void *fdt, const char *compat,
55 const char *prop, const void *val, int len, int create);
56 void do_fixup_by_compat_u32(void *fdt, const char *compat,
57 const char *prop, u32 val, int create);
58 int fdt_fixup_memory(void *blob, u64 start, u64 size);
59 int fdt_fixup_memory_banks(void *blob, u64 start[], u64 size[], int banks);
60 void fdt_fixup_ethernet(void *fdt);
61 int fdt_find_and_setprop(void *fdt, const char *node, const char *prop,
62 const void *val, int len, int create);
63 void fdt_fixup_qe_firmware(void *fdt);
65 #if defined(CONFIG_HAS_FSL_DR_USB) || defined(CONFIG_HAS_FSL_MPH_USB)
66 void fdt_fixup_dr_usb(void *blob, bd_t *bd);
67 #else
68 static inline void fdt_fixup_dr_usb(void *blob, bd_t *bd) {}
69 #endif /* defined(CONFIG_HAS_FSL_DR_USB) || defined(CONFIG_HAS_FSL_MPH_USB) */
71 #if defined(CONFIG_SYS_FSL_SEC_COMPAT)
72 void fdt_fixup_crypto_node(void *blob, int sec_rev);
73 #else
74 static inline void fdt_fixup_crypto_node(void *blob, int sec_rev) {}
75 #endif
77 #ifdef CONFIG_PCI
78 #include <pci.h>
79 int fdt_pci_dma_ranges(void *blob, int phb_off, struct pci_controller *hose);
80 #endif
82 #ifdef CONFIG_OF_BOARD_SETUP
83 void ft_board_setup(void *blob, bd_t *bd);
84 void ft_cpu_setup(void *blob, bd_t *bd);
85 void ft_pci_setup(void *blob, bd_t *bd);
86 #endif
88 void set_working_fdt_addr(void *addr);
89 int fdt_resize(void *blob);
90 int fdt_increase_size(void *fdt, int add_len);
92 int fdt_fixup_nor_flash_size(void *blob);
94 void fdt_fixup_mtdparts(void *fdt, void *node_info, int node_info_size);
95 void fdt_del_node_and_alias(void *blob, const char *alias);
96 u64 fdt_translate_address(void *blob, int node_offset, const __be32 *in_addr);
97 int fdt_node_offset_by_compat_reg(void *blob, const char *compat,
98 phys_addr_t compat_off);
99 int fdt_alloc_phandle(void *blob);
100 int fdt_set_phandle(void *fdt, int nodeoffset, uint32_t phandle);
101 unsigned int fdt_create_phandle(void *fdt, int nodeoffset);
102 int fdt_add_edid(void *blob, const char *compat, unsigned char *buf);
104 int fdt_verify_alias_address(void *fdt, int anode, const char *alias,
105 u64 addr);
106 u64 fdt_get_base_address(void *fdt, int node);
108 enum fdt_status {
109 FDT_STATUS_OKAY,
110 FDT_STATUS_DISABLED,
111 FDT_STATUS_FAIL,
112 FDT_STATUS_FAIL_ERROR_CODE,
113 };
114 int fdt_set_node_status(void *fdt, int nodeoffset,
115 enum fdt_status status, unsigned int error_code);
116 static inline int fdt_status_okay(void *fdt, int nodeoffset)
117 {
118 return fdt_set_node_status(fdt, nodeoffset, FDT_STATUS_OKAY, 0);
119 }
120 static inline int fdt_status_disabled(void *fdt, int nodeoffset)
121 {
122 return fdt_set_node_status(fdt, nodeoffset, FDT_STATUS_DISABLED, 0);
123 }
125 int fdt_set_status_by_alias(void *fdt, const char* alias,
126 enum fdt_status status, unsigned int error_code);
127 static inline int fdt_status_okay_by_alias(void *fdt, const char* alias)
128 {
129 return fdt_set_status_by_alias(fdt, alias, FDT_STATUS_OKAY, 0);
130 }
131 static inline int fdt_status_disabled_by_alias(void *fdt, const char* alias)
132 {
133 return fdt_set_status_by_alias(fdt, alias, FDT_STATUS_DISABLED, 0);
134 }
136 #endif /* ifdef CONFIG_OF_LIBFDT */
137 #endif /* ifndef __FDT_SUPPORT_H */