]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/fdtdec.h
Merge branch 'master' of git://git.denx.de/u-boot
[glsdk/glsdk-u-boot.git] / include / fdtdec.h
1 /*
2  * Copyright (c) 2011 The Chromium OS Authors.
3  * See file CREDITS for list of people who contributed to this
4  * project.
5  *
6  * This program is free software; you can redistribute it and/or
7  * modify it under the terms of the GNU General Public License as
8  * published by the Free Software Foundation; either version 2 of
9  * the License, or (at your option) any later version.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19  * MA 02111-1307 USA
20  */
22 #ifndef __fdtdec_h
23 #define __fdtdec_h
25 /*
26  * This file contains convenience functions for decoding useful and
27  * enlightening information from FDTs. It is intended to be used by device
28  * drivers and board-specific code within U-Boot. It aims to reduce the
29  * amount of FDT munging required within U-Boot itself, so that driver code
30  * changes to support FDT are minimized.
31  */
33 #include <libfdt.h>
35 /*
36  * A typedef for a physical address. Note that fdt data is always big
37  * endian even on a litle endian machine.
38  */
39 #ifdef CONFIG_PHYS_64BIT
40 typedef u64 fdt_addr_t;
41 #define FDT_ADDR_T_NONE (-1ULL)
42 #define fdt_addr_to_cpu(reg) be64_to_cpu(reg)
43 #define fdt_size_to_cpu(reg) be64_to_cpu(reg)
44 #else
45 typedef u32 fdt_addr_t;
46 #define FDT_ADDR_T_NONE (-1U)
47 #define fdt_addr_to_cpu(reg) be32_to_cpu(reg)
48 #define fdt_size_to_cpu(reg) be32_to_cpu(reg)
49 #endif
51 /* Information obtained about memory from the FDT */
52 struct fdt_memory {
53         fdt_addr_t start;
54         fdt_addr_t end;
55 };
57 /**
58  * Compat types that we know about and for which we might have drivers.
59  * Each is named COMPAT_<dir>_<filename> where <dir> is the directory
60  * within drivers.
61  */
62 enum fdt_compat_id {
63         COMPAT_UNKNOWN,
64         COMPAT_NVIDIA_TEGRA20_USB,      /* Tegra20 USB port */
65         COMPAT_NVIDIA_TEGRA20_I2C,      /* Tegra20 i2c */
66         COMPAT_NVIDIA_TEGRA20_DVC,      /* Tegra20 dvc (really just i2c) */
67         COMPAT_NVIDIA_TEGRA20_EMC,      /* Tegra20 memory controller */
68         COMPAT_NVIDIA_TEGRA20_EMC_TABLE, /* Tegra20 memory timing table */
69         COMPAT_NVIDIA_TEGRA20_KBC,      /* Tegra20 Keyboard */
70         COMPAT_NVIDIA_TEGRA20_NAND,     /* Tegra2 NAND controller */
71         COMPAT_NVIDIA_TEGRA20_PWM,      /* Tegra 2 PWM controller */
72         COMPAT_NVIDIA_TEGRA20_DC,       /* Tegra 2 Display controller */
73         COMPAT_NVIDIA_TEGRA20_SFLASH,   /* Tegra 2 SPI flash controller */
74         COMPAT_NVIDIA_TEGRA20_SLINK,    /* Tegra 2 SPI SLINK controller */
75         COMPAT_SMSC_LAN9215,            /* SMSC 10/100 Ethernet LAN9215 */
76         COMPAT_SAMSUNG_EXYNOS5_SROMC,   /* Exynos5 SROMC */
77         COMPAT_SAMSUNG_S3C2440_I2C,     /* Exynos I2C Controller */
78         COMPAT_SAMSUNG_EXYNOS5_SOUND,   /* Exynos Sound */
79         COMPAT_WOLFSON_WM8994_CODEC,    /* Wolfson WM8994 Sound Codec */
80         COMPAT_SAMSUNG_EXYNOS_SPI,      /* Exynos SPI */
81         COMPAT_SAMSUNG_EXYNOS_EHCI,     /* Exynos EHCI controller */
82         COMPAT_SAMSUNG_EXYNOS_USB_PHY,  /* Exynos phy controller for usb2.0 */
83         COMPAT_MAXIM_MAX77686_PMIC,     /* MAX77686 PMIC */
85         COMPAT_COUNT,
86 };
88 /* GPIOs are numbered from 0 */
89 enum {
90         FDT_GPIO_NONE = -1U,    /* an invalid GPIO used to end our list */
92         FDT_GPIO_ACTIVE_LOW = 1 << 0,   /* input is active low (else high) */
93 };
95 /* This is the state of a GPIO pin as defined by the fdt */
96 struct fdt_gpio_state {
97         const char *name;       /* name of the fdt property defining this */
98         uint gpio;              /* GPIO number, or FDT_GPIO_NONE if none */
99         u8 flags;               /* FDT_GPIO_... flags */
100 };
102 /* This tells us whether a fdt_gpio_state record is valid or not */
103 #define fdt_gpio_isvalid(x) ((x)->gpio != FDT_GPIO_NONE)
105 /**
106  * Read the GPIO taking into account the polarity of the pin.
107  *
108  * @param gpio          pointer to the decoded gpio
109  * @return value of the gpio if successful, < 0 if unsuccessful
110  */
111 int fdtdec_get_gpio(struct fdt_gpio_state *gpio);
113 /**
114  * Write the GPIO taking into account the polarity of the pin.
115  *
116  * @param gpio          pointer to the decoded gpio
117  * @return 0 if successful
118  */
119 int fdtdec_set_gpio(struct fdt_gpio_state *gpio, int val);
121 /**
122  * Find the next numbered alias for a peripheral. This is used to enumerate
123  * all the peripherals of a certain type.
124  *
125  * Do the first call with *upto = 0. Assuming /aliases/<name>0 exists then
126  * this function will return a pointer to the node the alias points to, and
127  * then update *upto to 1. Next time you call this function, the next node
128  * will be returned.
129  *
130  * All nodes returned will match the compatible ID, as it is assumed that
131  * all peripherals use the same driver.
132  *
133  * @param blob          FDT blob to use
134  * @param name          Root name of alias to search for
135  * @param id            Compatible ID to look for
136  * @return offset of next compatible node, or -FDT_ERR_NOTFOUND if no more
137  */
138 int fdtdec_next_alias(const void *blob, const char *name,
139                 enum fdt_compat_id id, int *upto);
141 /**
142  * Find the compatible ID for a given node.
143  *
144  * Generally each node has at least one compatible string attached to it.
145  * This function looks through our list of known compatible strings and
146  * returns the corresponding ID which matches the compatible string.
147  *
148  * @param blob          FDT blob to use
149  * @param node          Node containing compatible string to find
150  * @return compatible ID, or COMPAT_UNKNOWN if we cannot find a match
151  */
152 enum fdt_compat_id fdtdec_lookup(const void *blob, int node);
154 /**
155  * Find the next compatible node for a peripheral.
156  *
157  * Do the first call with node = 0. This function will return a pointer to
158  * the next compatible node. Next time you call this function, pass the
159  * value returned, and the next node will be provided.
160  *
161  * @param blob          FDT blob to use
162  * @param node          Start node for search
163  * @param id            Compatible ID to look for (enum fdt_compat_id)
164  * @return offset of next compatible node, or -FDT_ERR_NOTFOUND if no more
165  */
166 int fdtdec_next_compatible(const void *blob, int node,
167                 enum fdt_compat_id id);
169 /**
170  * Find the next compatible subnode for a peripheral.
171  *
172  * Do the first call with node set to the parent and depth = 0. This
173  * function will return the offset of the next compatible node. Next time
174  * you call this function, pass the node value returned last time, with
175  * depth unchanged, and the next node will be provided.
176  *
177  * @param blob          FDT blob to use
178  * @param node          Start node for search
179  * @param id            Compatible ID to look for (enum fdt_compat_id)
180  * @param depthp        Current depth (set to 0 before first call)
181  * @return offset of next compatible node, or -FDT_ERR_NOTFOUND if no more
182  */
183 int fdtdec_next_compatible_subnode(const void *blob, int node,
184                 enum fdt_compat_id id, int *depthp);
186 /**
187  * Look up an address property in a node and return it as an address.
188  * The property must hold either one address with no trailing data or
189  * one address with a length. This is only tested on 32-bit machines.
190  *
191  * @param blob  FDT blob
192  * @param node  node to examine
193  * @param prop_name     name of property to find
194  * @return address, if found, or FDT_ADDR_T_NONE if not
195  */
196 fdt_addr_t fdtdec_get_addr(const void *blob, int node,
197                 const char *prop_name);
199 /**
200  * Look up a 32-bit integer property in a node and return it. The property
201  * must have at least 4 bytes of data. The value of the first cell is
202  * returned.
203  *
204  * @param blob  FDT blob
205  * @param node  node to examine
206  * @param prop_name     name of property to find
207  * @param default_val   default value to return if the property is not found
208  * @return integer value, if found, or default_val if not
209  */
210 s32 fdtdec_get_int(const void *blob, int node, const char *prop_name,
211                 s32 default_val);
213 /**
214  * Look up a 64-bit integer property in a node and return it. The property
215  * must have at least 8 bytes of data (2 cells). The first two cells are
216  * concatenated to form a 8 bytes value, where the first cell is top half and
217  * the second cell is bottom half.
218  *
219  * @param blob  FDT blob
220  * @param node  node to examine
221  * @param prop_name     name of property to find
222  * @param default_val   default value to return if the property is not found
223  * @return integer value, if found, or default_val if not
224  */
225 uint64_t fdtdec_get_uint64(const void *blob, int node, const char *prop_name,
226                 uint64_t default_val);
228 /**
229  * Checks whether a node is enabled.
230  * This looks for a 'status' property. If this exists, then returns 1 if
231  * the status is 'ok' and 0 otherwise. If there is no status property,
232  * it returns 1 on the assumption that anything mentioned should be enabled
233  * by default.
234  *
235  * @param blob  FDT blob
236  * @param node  node to examine
237  * @return integer value 0 (not enabled) or 1 (enabled)
238  */
239 int fdtdec_get_is_enabled(const void *blob, int node);
241 /**
242  * Make sure we have a valid fdt available to control U-Boot.
243  *
244  * If not, a message is printed to the console if the console is ready.
245  *
246  * @return 0 if all ok, -1 if not
247  */
248 int fdtdec_prepare_fdt(void);
250 /**
251  * Checks that we have a valid fdt available to control U-Boot.
253  * However, if not then for the moment nothing is done, since this function
254  * is called too early to panic().
255  *
256  * @returns 0
257  */
258 int fdtdec_check_fdt(void);
260 /**
261  * Find the nodes for a peripheral and return a list of them in the correct
262  * order. This is used to enumerate all the peripherals of a certain type.
263  *
264  * To use this, optionally set up a /aliases node with alias properties for
265  * a peripheral. For example, for usb you could have:
266  *
267  * aliases {
268  *              usb0 = "/ehci@c5008000";
269  *              usb1 = "/ehci@c5000000";
270  * };
271  *
272  * Pass "usb" as the name to this function and will return a list of two
273  * nodes offsets: /ehci@c5008000 and ehci@c5000000.
274  *
275  * All nodes returned will match the compatible ID, as it is assumed that
276  * all peripherals use the same driver.
277  *
278  * If no alias node is found, then the node list will be returned in the
279  * order found in the fdt. If the aliases mention a node which doesn't
280  * exist, then this will be ignored. If nodes are found with no aliases,
281  * they will be added in any order.
282  *
283  * If there is a gap in the aliases, then this function return a 0 node at
284  * that position. The return value will also count these gaps.
285  *
286  * This function checks node properties and will not return nodes which are
287  * marked disabled (status = "disabled").
288  *
289  * @param blob          FDT blob to use
290  * @param name          Root name of alias to search for
291  * @param id            Compatible ID to look for
292  * @param node_list     Place to put list of found nodes
293  * @param maxcount      Maximum number of nodes to find
294  * @return number of nodes found on success, FTD_ERR_... on error
295  */
296 int fdtdec_find_aliases_for_id(const void *blob, const char *name,
297                         enum fdt_compat_id id, int *node_list, int maxcount);
299 /*
300  * This function is similar to fdtdec_find_aliases_for_id() except that it
301  * adds to the node_list that is passed in. Any 0 elements are considered
302  * available for allocation - others are considered already used and are
303  * skipped.
304  *
305  * You can use this by calling fdtdec_find_aliases_for_id() with an
306  * uninitialised array, then setting the elements that are returned to -1,
307  * say, then calling this function, perhaps with a different compat id.
308  * Any elements you get back that are >0 are new nodes added by the call
309  * to this function.
310  *
311  * Note that if you have some nodes with aliases and some without, you are
312  * sailing close to the wind. The call to fdtdec_find_aliases_for_id() with
313  * one compat_id may fill in positions for which you have aliases defined
314  * for another compat_id. When you later call *this* function with the second
315  * compat_id, the alias positions may already be used. A debug warning may
316  * be generated in this case, but it is safest to define aliases for all
317  * nodes when you care about the ordering.
318  */
319 int fdtdec_add_aliases_for_id(const void *blob, const char *name,
320                         enum fdt_compat_id id, int *node_list, int maxcount);
322 /*
323  * Get the name for a compatible ID
324  *
325  * @param id            Compatible ID to look for
326  * @return compatible string for that id
327  */
328 const char *fdtdec_get_compatible(enum fdt_compat_id id);
330 /* Look up a phandle and follow it to its node. Then return the offset
331  * of that node.
332  *
333  * @param blob          FDT blob
334  * @param node          node to examine
335  * @param prop_name     name of property to find
336  * @return node offset if found, -ve error code on error
337  */
338 int fdtdec_lookup_phandle(const void *blob, int node, const char *prop_name);
340 /**
341  * Look up a property in a node and return its contents in an integer
342  * array of given length. The property must have at least enough data for
343  * the array (4*count bytes). It may have more, but this will be ignored.
344  *
345  * @param blob          FDT blob
346  * @param node          node to examine
347  * @param prop_name     name of property to find
348  * @param array         array to fill with data
349  * @param count         number of array elements
350  * @return 0 if ok, or -FDT_ERR_NOTFOUND if the property is not found,
351  *              or -FDT_ERR_BADLAYOUT if not enough data
352  */
353 int fdtdec_get_int_array(const void *blob, int node, const char *prop_name,
354                 u32 *array, int count);
356 /**
357  * Look up a property in a node and return a pointer to its contents as a
358  * unsigned int array of given length. The property must have at least enough
359  * data for the array ('count' cells). It may have more, but this will be
360  * ignored. The data is not copied.
361  *
362  * Note that you must access elements of the array with fdt32_to_cpu(),
363  * since the elements will be big endian even on a little endian machine.
364  *
365  * @param blob          FDT blob
366  * @param node          node to examine
367  * @param prop_name     name of property to find
368  * @param count         number of array elements
369  * @return pointer to array if found, or NULL if the property is not
370  *              found or there is not enough data
371  */
372 const u32 *fdtdec_locate_array(const void *blob, int node,
373                                const char *prop_name, int count);
375 /**
376  * Look up a boolean property in a node and return it.
377  *
378  * A boolean properly is true if present in the device tree and false if not
379  * present, regardless of its value.
380  *
381  * @param blob  FDT blob
382  * @param node  node to examine
383  * @param prop_name     name of property to find
384  * @return 1 if the properly is present; 0 if it isn't present
385  */
386 int fdtdec_get_bool(const void *blob, int node, const char *prop_name);
388 /**
389  * Decode a single GPIOs from an FDT.
390  *
391  * If the property is not found, then the GPIO structure will still be
392  * initialised, with gpio set to FDT_GPIO_NONE. This makes it easy to
393  * provide optional GPIOs.
394  *
395  * @param blob          FDT blob to use
396  * @param node          Node to look at
397  * @param prop_name     Node property name
398  * @param gpio          gpio elements to fill from FDT
399  * @return 0 if ok, -FDT_ERR_NOTFOUND if the property is missing.
400  */
401 int fdtdec_decode_gpio(const void *blob, int node, const char *prop_name,
402                 struct fdt_gpio_state *gpio);
404 /**
405  * Decode a list of GPIOs from an FDT. This creates a list of GPIOs with no
406  * terminating item.
407  *
408  * @param blob         FDT blob to use
409  * @param node         Node to look at
410  * @param prop_name    Node property name
411  * @param gpio         Array of gpio elements to fill from FDT. This will be
412  *                     untouched if either 0 or an error is returned
413  * @param max_count    Maximum number of elements allowed
414  * @return number of GPIOs read if ok, -FDT_ERR_BADLAYOUT if max_count would
415  * be exceeded, or -FDT_ERR_NOTFOUND if the property is missing.
416  */
417 int fdtdec_decode_gpios(const void *blob, int node, const char *prop_name,
418                 struct fdt_gpio_state *gpio, int max_count);
420 /**
421  * Set up a GPIO pin according to the provided gpio information. At present this
422  * just requests the GPIO.
423  *
424  * If the gpio is FDT_GPIO_NONE, no action is taken. This makes it easy to
425  * deal with optional GPIOs.
426  *
427  * @param gpio          GPIO info to use for set up
428  * @return 0 if all ok or gpio was FDT_GPIO_NONE; -1 on error
429  */
430 int fdtdec_setup_gpio(struct fdt_gpio_state *gpio);
432 /**
433  * Look in the FDT for a config item with the given name and return its value
434  * as a 32-bit integer. The property must have at least 4 bytes of data. The
435  * value of the first cell is returned.
436  *
437  * @param blob          FDT blob to use
438  * @param prop_name     Node property name
439  * @param default_val   default value to return if the property is not found
440  * @return integer value, if found, or default_val if not
441  */
442 int fdtdec_get_config_int(const void *blob, const char *prop_name,
443                 int default_val);
445 /**
446  * Look in the FDT for a config item with the given name
447  * and return whether it exists.
448  *
449  * @param blob          FDT blob
450  * @param prop_name     property name to look up
451  * @return 1, if it exists, or 0 if not
452  */
453 int fdtdec_get_config_bool(const void *blob, const char *prop_name);
455 /**
456  * Look in the FDT for a config item with the given name and return its value
457  * as a string.
458  *
459  * @param blob          FDT blob
460  * @param prop_name     property name to look up
461  * @returns property string, NULL on error.
462  */
463 char *fdtdec_get_config_string(const void *blob, const char *prop_name);
465 /*
466  * Look up a property in a node and return its contents in a byte
467  * array of given length. The property must have at least enough data for
468  * the array (count bytes). It may have more, but this will be ignored.
469  *
470  * @param blob          FDT blob
471  * @param node          node to examine
472  * @param prop_name     name of property to find
473  * @param array         array to fill with data
474  * @param count         number of array elements
475  * @return 0 if ok, or -FDT_ERR_MISSING if the property is not found,
476  *              or -FDT_ERR_BADLAYOUT if not enough data
477  */
478 int fdtdec_get_byte_array(const void *blob, int node, const char *prop_name,
479                 u8 *array, int count);
481 /**
482  * Look up a property in a node and return a pointer to its contents as a
483  * byte array of given length. The property must have at least enough data
484  * for the array (count bytes). It may have more, but this will be ignored.
485  * The data is not copied.
486  *
487  * @param blob          FDT blob
488  * @param node          node to examine
489  * @param prop_name     name of property to find
490  * @param count         number of array elements
491  * @return pointer to byte array if found, or NULL if the property is not
492  *              found or there is not enough data
493  */
494 const u8 *fdtdec_locate_byte_array(const void *blob, int node,
495                              const char *prop_name, int count);
497 /**
498  * Look up a property in a node which contains a memory region address and
499  * size. Then return a pointer to this address.
500  *
501  * The property must hold one address with a length. This is only tested on
502  * 32-bit machines.
503  *
504  * @param blob          FDT blob
505  * @param node          node to examine
506  * @param prop_name     name of property to find
507  * @param ptrp          returns pointer to region, or NULL if no address
508  * @param size          returns size of region
509  * @return 0 if ok, -1 on error (propery not found)
510  */
511 int fdtdec_decode_region(const void *blob, int node,
512                 const char *prop_name, void **ptrp, size_t *size);
513 #endif