1 /*
2 * (C) Copyright 2001
3 * Gerald Van Baren, Custom IDEAS, vanbaren@cideas.com.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 *
23 * The original I2C interface was
24 * (C) 2000 by Paolo Scaffardi (arsenio@tin.it)
25 * AIRVENT SAM s.p.a - RIMINI(ITALY)
26 * but has been changed substantially.
27 */
29 #ifndef _I2C_H_
30 #define _I2C_H_
32 /*
33 * WARNING WARNING WARNING WARNING WARNING WARNING WARNING WARNING
34 *
35 * The implementation MUST NOT use static or global variables if the
36 * I2C routines are used to read SDRAM configuration information
37 * because this is done before the memories are initialized. Limited
38 * use of stack-based variables are OK (the initial stack size is
39 * limited).
40 *
41 * WARNING WARNING WARNING WARNING WARNING WARNING WARNING WARNING
42 */
44 /*
45 * Configuration items.
46 */
47 #define I2C_RXTX_LEN 128 /* maximum tx/rx buffer length */
49 #ifdef CONFIG_I2C_MULTI_BUS
50 #define MAX_I2C_BUS 2
51 #define I2C_MULTI_BUS 1
52 #else
53 #define MAX_I2C_BUS 1
54 #define I2C_MULTI_BUS 0
55 #endif
57 #if !defined(CONFIG_SYS_MAX_I2C_BUS)
58 #define CONFIG_SYS_MAX_I2C_BUS MAX_I2C_BUS
59 #endif
61 /* define the I2C bus number for RTC and DTT if not already done */
62 #if !defined(CONFIG_SYS_RTC_BUS_NUM)
63 #define CONFIG_SYS_RTC_BUS_NUM 0
64 #endif
65 #if !defined(CONFIG_SYS_DTT_BUS_NUM)
66 #define CONFIG_SYS_DTT_BUS_NUM 0
67 #endif
68 #if !defined(CONFIG_SYS_SPD_BUS_NUM)
69 #define CONFIG_SYS_SPD_BUS_NUM 0
70 #endif
72 #ifndef I2C_SOFT_DECLARATIONS
73 # if defined(CONFIG_MPC8260)
74 # define I2C_SOFT_DECLARATIONS volatile ioport_t *iop = ioport_addr((immap_t *)CONFIG_SYS_IMMR, I2C_PORT);
75 # elif defined(CONFIG_8xx)
76 # define I2C_SOFT_DECLARATIONS volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
78 # elif (defined(CONFIG_AT91RM9200) || \
79 defined(CONFIG_AT91SAM9260) || defined(CONFIG_AT91SAM9261) || \
80 defined(CONFIG_AT91SAM9263)) && !defined(CONFIG_AT91_LEGACY)
81 # define I2C_SOFT_DECLARATIONS at91_pio_t *pio = (at91_pio_t *) ATMEL_BASE_PIOA;
82 # else
83 # define I2C_SOFT_DECLARATIONS
84 # endif
85 #endif
87 #ifdef CONFIG_8xx
88 /* Set default value for the I2C bus speed on 8xx. In the
89 * future, we'll define these in all 8xx board config files.
90 */
91 #ifndef CONFIG_SYS_I2C_SPEED
92 #define CONFIG_SYS_I2C_SPEED 50000
93 #endif
94 #endif
96 /*
97 * Many boards/controllers/drivers don't support an I2C slave interface so
98 * provide a default slave address for them for use in common code. A real
99 * value for CONFIG_SYS_I2C_SLAVE should be defined for any board which does
100 * support a slave interface.
101 */
102 #ifndef CONFIG_SYS_I2C_SLAVE
103 #define CONFIG_SYS_I2C_SLAVE 0xfe
104 #endif
106 /*
107 * Initialization, must be called once on start up, may be called
108 * repeatedly to change the speed and slave addresses.
109 */
110 void i2c_init(int speed, int slaveaddr);
111 void i2c_init_board(void);
112 #ifdef CONFIG_SYS_I2C_BOARD_LATE_INIT
113 void i2c_board_late_init(void);
114 #endif
116 #if defined(CONFIG_I2C_MUX)
118 typedef struct _mux {
119 uchar chip;
120 uchar channel;
121 char *name;
122 struct _mux *next;
123 } I2C_MUX;
125 typedef struct _mux_device {
126 int busid;
127 I2C_MUX *mux; /* List of muxes, to reach the device */
128 struct _mux_device *next;
129 } I2C_MUX_DEVICE;
131 I2C_MUX_DEVICE *i2c_mux_search_device(int id);
132 I2C_MUX_DEVICE *i2c_mux_ident_muxstring (uchar *buf);
133 int i2x_mux_select_mux(int bus);
134 int i2c_mux_ident_muxstring_f (uchar *buf);
135 #endif
137 /*
138 * Probe the given I2C chip address. Returns 0 if a chip responded,
139 * not 0 on failure.
140 */
141 int i2c_probe(uchar chip);
143 /*
144 * Read/Write interface:
145 * chip: I2C chip address, range 0..127
146 * addr: Memory (register) address within the chip
147 * alen: Number of bytes to use for addr (typically 1, 2 for larger
148 * memories, 0 for register type devices with only one
149 * register)
150 * buffer: Where to read/write the data
151 * len: How many bytes to read/write
152 *
153 * Returns: 0 on success, not 0 on failure
154 */
155 int i2c_read(uchar chip, uint addr, int alen, uchar *buffer, int len);
156 int i2c_write(uchar chip, uint addr, int alen, uchar *buffer, int len);
158 /*
159 * Utility routines to read/write registers.
160 */
161 static inline u8 i2c_reg_read(u8 addr, u8 reg)
162 {
163 u8 buf;
165 #ifdef CONFIG_8xx
166 /* MPC8xx needs this. Maybe one day we can get rid of it. */
167 i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
168 #endif
170 #ifdef DEBUG
171 printf("%s: addr=0x%02x, reg=0x%02x\n", __func__, addr, reg);
172 #endif
174 i2c_read(addr, reg, 1, &buf, 1);
176 return buf;
177 }
179 static inline void i2c_reg_write(u8 addr, u8 reg, u8 val)
180 {
181 #ifdef CONFIG_8xx
182 /* MPC8xx needs this. Maybe one day we can get rid of it. */
183 i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
184 #endif
186 #ifdef DEBUG
187 printf("%s: addr=0x%02x, reg=0x%02x, val=0x%02x\n",
188 __func__, addr, reg, val);
189 #endif
191 i2c_write(addr, reg, 1, &val, 1);
192 }
194 /*
195 * Functions for setting the current I2C bus and its speed
196 */
198 /*
199 * i2c_set_bus_num:
200 *
201 * Change the active I2C bus. Subsequent read/write calls will
202 * go to this one.
203 *
204 * bus - bus index, zero based
205 *
206 * Returns: 0 on success, not 0 on failure
207 *
208 */
209 int i2c_set_bus_num(unsigned int bus);
211 /*
212 * i2c_get_bus_num:
213 *
214 * Returns index of currently active I2C bus. Zero-based.
215 */
217 unsigned int i2c_get_bus_num(void);
219 /*
220 * i2c_set_bus_speed:
221 *
222 * Change the speed of the active I2C bus
223 *
224 * speed - bus speed in Hz
225 *
226 * Returns: 0 on success, not 0 on failure
227 *
228 */
229 int i2c_set_bus_speed(unsigned int);
231 /*
232 * i2c_get_bus_speed:
233 *
234 * Returns speed of currently active I2C bus in Hz
235 */
237 unsigned int i2c_get_bus_speed(void);
239 /* NOTE: These two functions MUST be always_inline to avoid code growth! */
240 static inline unsigned int I2C_GET_BUS(void) __attribute__((always_inline));
241 static inline unsigned int I2C_GET_BUS(void)
242 {
243 return I2C_MULTI_BUS ? i2c_get_bus_num() : 0;
244 }
246 static inline void I2C_SET_BUS(unsigned int bus) __attribute__((always_inline));
247 static inline void I2C_SET_BUS(unsigned int bus)
248 {
249 if (I2C_MULTI_BUS)
250 i2c_set_bus_num(bus);
251 }
253 /* Multi I2C definitions */
254 enum {
255 I2C_0, I2C_1, I2C_2, I2C_3, I2C_4, I2C_5, I2C_6, I2C_7,
256 I2C_8, I2C_9, I2C_10,
257 };
259 /* Multi I2C busses handling */
260 #ifdef CONFIG_SOFT_I2C_MULTI_BUS
261 extern int get_multi_scl_pin(void);
262 extern int get_multi_sda_pin(void);
263 extern int multi_i2c_init(void);
264 #endif
266 /**
267 * Get FDT values for i2c bus.
268 *
269 * @param blob Device tree blbo
270 * @return the number of I2C bus
271 */
272 void board_i2c_init(const void *blob);
274 /**
275 * Find the I2C bus number by given a FDT I2C node.
276 *
277 * @param blob Device tree blbo
278 * @param node FDT I2C node to find
279 * @return the number of I2C bus (zero based), or -1 on error
280 */
281 int i2c_get_bus_num_fdt(int node);
283 /**
284 * Reset the I2C bus represented by the given a FDT I2C node.
285 *
286 * @param blob Device tree blbo
287 * @param node FDT I2C node to find
288 * @return 0 if port was reset, -1 if not found
289 */
290 int i2c_reset_port_fdt(const void *blob, int node);
291 #endif /* _I2C_H_ */