]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/ide.h
Merge remote-tracking branch 'u-boot-atmel/master'
[glsdk/glsdk-u-boot.git] / include / ide.h
1 /*
2  * (C) Copyright 2000
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #ifndef _IDE_H
25 #define _IDE_H
27 #define IDE_BUS(dev)    (dev / (CONFIG_SYS_IDE_MAXDEVICE / CONFIG_SYS_IDE_MAXBUS))
29 #define ATA_CURR_BASE(dev)      (CONFIG_SYS_ATA_BASE_ADDR+ide_bus_offset[IDE_BUS(dev)])
30 extern ulong ide_bus_offset[];
32 #ifdef CONFIG_IDE_LED
34 /*
35  * LED Port
36  */
37 #define LED_PORT        ((uchar *)(PER8_BASE + 0x3000))
38 #define LED_IDE1        0x01
39 #define LED_IDE2        0x02
40 #define DEVICE_LED(d)   ((d & 2) | ((d & 2) == 0)) /* depends on bit positions! */
42 #endif /* CONFIG_IDE_LED */
44 #ifdef CONFIG_SYS_64BIT_LBA
45 typedef uint64_t lbaint_t;
46 #define LBAF "%llx"
47 #else
48 typedef ulong lbaint_t;
49 #define LBAF "%lx"
50 #endif
52 /*
53  * Function Prototypes
54  */
56 void ide_init(void);
57 ulong ide_read(int device, ulong blknr, lbaint_t blkcnt, void *buffer);
58 ulong ide_write(int device, ulong blknr, lbaint_t blkcnt, const void *buffer);
60 #ifdef CONFIG_IDE_PREINIT
61 int ide_preinit(void);
62 #endif
64 #ifdef CONFIG_IDE_INIT_POSTRESET
65 int ide_init_postreset(void);
66 #endif
68 #if defined(CONFIG_OF_IDE_FIXUP)
69 int ide_device_present(int dev);
70 #endif
72 #if defined(CONFIG_IDE_AHB)
73 unsigned char ide_read_register(int dev, unsigned int port);
74 void ide_write_register(int dev, unsigned int port, unsigned char val);
75 void ide_read_data(int dev, ulong *sect_buf, int words);
76 void ide_write_data(int dev, ulong *sect_buf, int words);
77 #endif
79 /*
80  * I/O function overrides
81  */
82 void ide_input_swap_data(int dev, ulong *sect_buf, int words);
83 void ide_input_data(int dev, ulong *sect_buf, int words);
84 void ide_output_data(int dev, const ulong *sect_buf, int words);
85 void ide_input_data_shorts(int dev, ushort *sect_buf, int shorts);
86 void ide_output_data_shorts(int dev, ushort *sect_buf, int shorts);
88 #endif /* _IDE_H */