1 /*
2 * (C) Copyright 2008 Semihalf
3 *
4 * (C) Copyright 2000-2005
5 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 *
25 ********************************************************************
26 * NOTE: This header file defines an interface to U-Boot. Including
27 * this (unmodified) header file in another file is considered normal
28 * use of U-Boot, and does *not* fall under the heading of "derived
29 * work".
30 ********************************************************************
31 */
33 #ifndef __IMAGE_H__
34 #define __IMAGE_H__
36 #include "compiler.h"
37 #include <asm/byteorder.h>
39 #ifdef USE_HOSTCC
41 /* new uImage format support enabled on host */
42 #define CONFIG_FIT 1
43 #define CONFIG_OF_LIBFDT 1
44 #define CONFIG_FIT_VERBOSE 1 /* enable fit_format_{error,warning}() */
46 #else
48 #include <lmb.h>
49 #include <asm/u-boot.h>
50 #include <command.h>
52 #endif /* USE_HOSTCC */
54 #if defined(CONFIG_FIT)
55 #include <libfdt.h>
56 #include <fdt_support.h>
57 #define CONFIG_MD5 /* FIT images need MD5 support */
58 #define CONFIG_SHA1 /* and SHA1 */
59 #endif
61 /*
62 * Operating System Codes
63 */
64 #define IH_OS_INVALID 0 /* Invalid OS */
65 #define IH_OS_OPENBSD 1 /* OpenBSD */
66 #define IH_OS_NETBSD 2 /* NetBSD */
67 #define IH_OS_FREEBSD 3 /* FreeBSD */
68 #define IH_OS_4_4BSD 4 /* 4.4BSD */
69 #define IH_OS_LINUX 5 /* Linux */
70 #define IH_OS_SVR4 6 /* SVR4 */
71 #define IH_OS_ESIX 7 /* Esix */
72 #define IH_OS_SOLARIS 8 /* Solaris */
73 #define IH_OS_IRIX 9 /* Irix */
74 #define IH_OS_SCO 10 /* SCO */
75 #define IH_OS_DELL 11 /* Dell */
76 #define IH_OS_NCR 12 /* NCR */
77 #define IH_OS_LYNXOS 13 /* LynxOS */
78 #define IH_OS_VXWORKS 14 /* VxWorks */
79 #define IH_OS_PSOS 15 /* pSOS */
80 #define IH_OS_QNX 16 /* QNX */
81 #define IH_OS_U_BOOT 17 /* Firmware */
82 #define IH_OS_RTEMS 18 /* RTEMS */
83 #define IH_OS_ARTOS 19 /* ARTOS */
84 #define IH_OS_UNITY 20 /* Unity OS */
85 #define IH_OS_INTEGRITY 21 /* INTEGRITY */
86 #define IH_OS_OSE 22 /* OSE */
87 #define IH_OS_PLAN9 23 /* Plan 9 */
89 /*
90 * CPU Architecture Codes (supported by Linux)
91 */
92 #define IH_ARCH_INVALID 0 /* Invalid CPU */
93 #define IH_ARCH_ALPHA 1 /* Alpha */
94 #define IH_ARCH_ARM 2 /* ARM */
95 #define IH_ARCH_I386 3 /* Intel x86 */
96 #define IH_ARCH_IA64 4 /* IA64 */
97 #define IH_ARCH_MIPS 5 /* MIPS */
98 #define IH_ARCH_MIPS64 6 /* MIPS 64 Bit */
99 #define IH_ARCH_PPC 7 /* PowerPC */
100 #define IH_ARCH_S390 8 /* IBM S390 */
101 #define IH_ARCH_SH 9 /* SuperH */
102 #define IH_ARCH_SPARC 10 /* Sparc */
103 #define IH_ARCH_SPARC64 11 /* Sparc 64 Bit */
104 #define IH_ARCH_M68K 12 /* M68K */
105 #define IH_ARCH_MICROBLAZE 14 /* MicroBlaze */
106 #define IH_ARCH_NIOS2 15 /* Nios-II */
107 #define IH_ARCH_BLACKFIN 16 /* Blackfin */
108 #define IH_ARCH_AVR32 17 /* AVR32 */
109 #define IH_ARCH_ST200 18 /* STMicroelectronics ST200 */
110 #define IH_ARCH_SANDBOX 19 /* Sandbox architecture (test only) */
111 #define IH_ARCH_NDS32 20 /* ANDES Technology - NDS32 */
112 #define IH_ARCH_OPENRISC 21 /* OpenRISC 1000 */
114 /*
115 * Image Types
116 *
117 * "Standalone Programs" are directly runnable in the environment
118 * provided by U-Boot; it is expected that (if they behave
119 * well) you can continue to work in U-Boot after return from
120 * the Standalone Program.
121 * "OS Kernel Images" are usually images of some Embedded OS which
122 * will take over control completely. Usually these programs
123 * will install their own set of exception handlers, device
124 * drivers, set up the MMU, etc. - this means, that you cannot
125 * expect to re-enter U-Boot except by resetting the CPU.
126 * "RAMDisk Images" are more or less just data blocks, and their
127 * parameters (address, size) are passed to an OS kernel that is
128 * being started.
129 * "Multi-File Images" contain several images, typically an OS
130 * (Linux) kernel image and one or more data images like
131 * RAMDisks. This construct is useful for instance when you want
132 * to boot over the network using BOOTP etc., where the boot
133 * server provides just a single image file, but you want to get
134 * for instance an OS kernel and a RAMDisk image.
135 *
136 * "Multi-File Images" start with a list of image sizes, each
137 * image size (in bytes) specified by an "uint32_t" in network
138 * byte order. This list is terminated by an "(uint32_t)0".
139 * Immediately after the terminating 0 follow the images, one by
140 * one, all aligned on "uint32_t" boundaries (size rounded up to
141 * a multiple of 4 bytes - except for the last file).
142 *
143 * "Firmware Images" are binary images containing firmware (like
144 * U-Boot or FPGA images) which usually will be programmed to
145 * flash memory.
146 *
147 * "Script files" are command sequences that will be executed by
148 * U-Boot's command interpreter; this feature is especially
149 * useful when you configure U-Boot to use a real shell (hush)
150 * as command interpreter (=> Shell Scripts).
151 */
153 #define IH_TYPE_INVALID 0 /* Invalid Image */
154 #define IH_TYPE_STANDALONE 1 /* Standalone Program */
155 #define IH_TYPE_KERNEL 2 /* OS Kernel Image */
156 #define IH_TYPE_RAMDISK 3 /* RAMDisk Image */
157 #define IH_TYPE_MULTI 4 /* Multi-File Image */
158 #define IH_TYPE_FIRMWARE 5 /* Firmware Image */
159 #define IH_TYPE_SCRIPT 6 /* Script file */
160 #define IH_TYPE_FILESYSTEM 7 /* Filesystem Image (any type) */
161 #define IH_TYPE_FLATDT 8 /* Binary Flat Device Tree Blob */
162 #define IH_TYPE_KWBIMAGE 9 /* Kirkwood Boot Image */
163 #define IH_TYPE_IMXIMAGE 10 /* Freescale IMXBoot Image */
164 #define IH_TYPE_UBLIMAGE 11 /* Davinci UBL Image */
165 #define IH_TYPE_OMAPIMAGE 12 /* TI OMAP Config Header Image */
166 #define IH_TYPE_AISIMAGE 13 /* TI Davinci AIS Image */
167 #define IH_TYPE_KERNEL_NOLOAD 14 /* OS Kernel Image, can run from any load address */
168 #define IH_TYPE_PBLIMAGE 15 /* Freescale PBL Boot Image */
170 /*
171 * Compression Types
172 */
173 #define IH_COMP_NONE 0 /* No Compression Used */
174 #define IH_COMP_GZIP 1 /* gzip Compression Used */
175 #define IH_COMP_BZIP2 2 /* bzip2 Compression Used */
176 #define IH_COMP_LZMA 3 /* lzma Compression Used */
177 #define IH_COMP_LZO 4 /* lzo Compression Used */
179 #define IH_MAGIC 0x27051956 /* Image Magic Number */
180 #define IH_NMLEN 32 /* Image Name Length */
182 /* Reused from common.h */
183 #define ROUND(a, b) (((a) + (b) - 1) & ~((b) - 1))
185 /*
186 * Legacy format image header,
187 * all data in network byte order (aka natural aka bigendian).
188 */
189 typedef struct image_header {
190 __be32 ih_magic; /* Image Header Magic Number */
191 __be32 ih_hcrc; /* Image Header CRC Checksum */
192 __be32 ih_time; /* Image Creation Timestamp */
193 __be32 ih_size; /* Image Data Size */
194 __be32 ih_load; /* Data Load Address */
195 __be32 ih_ep; /* Entry Point Address */
196 __be32 ih_dcrc; /* Image Data CRC Checksum */
197 uint8_t ih_os; /* Operating System */
198 uint8_t ih_arch; /* CPU architecture */
199 uint8_t ih_type; /* Image Type */
200 uint8_t ih_comp; /* Compression Type */
201 uint8_t ih_name[IH_NMLEN]; /* Image Name */
202 } image_header_t;
204 typedef struct image_info {
205 ulong start, end; /* start/end of blob */
206 ulong image_start, image_len; /* start of image within blob, len of image */
207 ulong load; /* load addr for the image */
208 uint8_t comp, type, os; /* compression, type of image, os type */
209 } image_info_t;
211 /*
212 * Legacy and FIT format headers used by do_bootm() and do_bootm_<os>()
213 * routines.
214 */
215 typedef struct bootm_headers {
216 /*
217 * Legacy os image header, if it is a multi component image
218 * then boot_get_ramdisk() and get_fdt() will attempt to get
219 * data from second and third component accordingly.
220 */
221 image_header_t *legacy_hdr_os; /* image header pointer */
222 image_header_t legacy_hdr_os_copy; /* header copy */
223 ulong legacy_hdr_valid;
225 #if defined(CONFIG_FIT)
226 const char *fit_uname_cfg; /* configuration node unit name */
228 void *fit_hdr_os; /* os FIT image header */
229 const char *fit_uname_os; /* os subimage node unit name */
230 int fit_noffset_os; /* os subimage node offset */
232 void *fit_hdr_rd; /* init ramdisk FIT image header */
233 const char *fit_uname_rd; /* init ramdisk subimage node unit name */
234 int fit_noffset_rd; /* init ramdisk subimage node offset */
236 void *fit_hdr_fdt; /* FDT blob FIT image header */
237 const char *fit_uname_fdt; /* FDT blob subimage node unit name */
238 int fit_noffset_fdt;/* FDT blob subimage node offset */
239 #endif
241 #ifndef USE_HOSTCC
242 image_info_t os; /* os image info */
243 ulong ep; /* entry point of OS */
245 ulong rd_start, rd_end;/* ramdisk start/end */
247 #ifdef CONFIG_OF_LIBFDT
248 char *ft_addr; /* flat dev tree address */
249 #endif
250 ulong ft_len; /* length of flat device tree */
252 ulong initrd_start;
253 ulong initrd_end;
254 ulong cmdline_start;
255 ulong cmdline_end;
256 bd_t *kbd;
257 #endif
259 int verify; /* getenv("verify")[0] != 'n' */
261 #define BOOTM_STATE_START (0x00000001)
262 #define BOOTM_STATE_LOADOS (0x00000002)
263 #define BOOTM_STATE_RAMDISK (0x00000004)
264 #define BOOTM_STATE_FDT (0x00000008)
265 #define BOOTM_STATE_OS_CMDLINE (0x00000010)
266 #define BOOTM_STATE_OS_BD_T (0x00000020)
267 #define BOOTM_STATE_OS_PREP (0x00000040)
268 #define BOOTM_STATE_OS_GO (0x00000080)
269 int state;
271 #ifdef CONFIG_LMB
272 struct lmb lmb; /* for memory mgmt */
273 #endif
274 } bootm_headers_t;
276 extern bootm_headers_t images;
278 /*
279 * Some systems (for example LWMON) have very short watchdog periods;
280 * we must make sure to split long operations like memmove() or
281 * checksum calculations into reasonable chunks.
282 */
283 #ifndef CHUNKSZ
284 #define CHUNKSZ (64 * 1024)
285 #endif
287 #ifndef CHUNKSZ_CRC32
288 #define CHUNKSZ_CRC32 (64 * 1024)
289 #endif
291 #ifndef CHUNKSZ_MD5
292 #define CHUNKSZ_MD5 (64 * 1024)
293 #endif
295 #ifndef CHUNKSZ_SHA1
296 #define CHUNKSZ_SHA1 (64 * 1024)
297 #endif
299 #define uimage_to_cpu(x) be32_to_cpu(x)
300 #define cpu_to_uimage(x) cpu_to_be32(x)
302 /*
303 * Translation table for entries of a specific type; used by
304 * get_table_entry_id() and get_table_entry_name().
305 */
306 typedef struct table_entry {
307 int id;
308 char *sname; /* short (input) name to find table entry */
309 char *lname; /* long (output) name to print for messages */
310 } table_entry_t;
312 /*
313 * get_table_entry_id() scans the translation table trying to find an
314 * entry that matches the given short name. If a matching entry is
315 * found, it's id is returned to the caller.
316 */
317 int get_table_entry_id(const table_entry_t *table,
318 const char *table_name, const char *name);
319 /*
320 * get_table_entry_name() scans the translation table trying to find
321 * an entry that matches the given id. If a matching entry is found,
322 * its long name is returned to the caller.
323 */
324 char *get_table_entry_name(const table_entry_t *table, char *msg, int id);
326 const char *genimg_get_os_name(uint8_t os);
327 const char *genimg_get_arch_name(uint8_t arch);
328 const char *genimg_get_type_name(uint8_t type);
329 const char *genimg_get_comp_name(uint8_t comp);
330 int genimg_get_os_id(const char *name);
331 int genimg_get_arch_id(const char *name);
332 int genimg_get_type_id(const char *name);
333 int genimg_get_comp_id(const char *name);
334 void genimg_print_size(uint32_t size);
336 #ifndef USE_HOSTCC
337 /* Image format types, returned by _get_format() routine */
338 #define IMAGE_FORMAT_INVALID 0x00
339 #define IMAGE_FORMAT_LEGACY 0x01 /* legacy image_header based format */
340 #define IMAGE_FORMAT_FIT 0x02 /* new, libfdt based format */
342 int genimg_get_format(void *img_addr);
343 int genimg_has_config(bootm_headers_t *images);
344 ulong genimg_get_image(ulong img_addr);
346 int boot_get_ramdisk(int argc, char * const argv[], bootm_headers_t *images,
347 uint8_t arch, ulong *rd_start, ulong *rd_end);
350 #ifdef CONFIG_OF_LIBFDT
351 int boot_get_fdt(int flag, int argc, char * const argv[],
352 bootm_headers_t *images, char **of_flat_tree, ulong *of_size);
353 void boot_fdt_add_mem_rsv_regions(struct lmb *lmb, void *fdt_blob);
354 int boot_relocate_fdt(struct lmb *lmb, char **of_flat_tree, ulong *of_size);
355 #endif
357 #ifdef CONFIG_SYS_BOOT_RAMDISK_HIGH
358 int boot_ramdisk_high(struct lmb *lmb, ulong rd_data, ulong rd_len,
359 ulong *initrd_start, ulong *initrd_end);
360 #endif /* CONFIG_SYS_BOOT_RAMDISK_HIGH */
361 #ifdef CONFIG_SYS_BOOT_GET_CMDLINE
362 int boot_get_cmdline(struct lmb *lmb, ulong *cmd_start, ulong *cmd_end);
363 #endif /* CONFIG_SYS_BOOT_GET_CMDLINE */
364 #ifdef CONFIG_SYS_BOOT_GET_KBD
365 int boot_get_kbd(struct lmb *lmb, bd_t **kbd);
366 #endif /* CONFIG_SYS_BOOT_GET_KBD */
367 #endif /* !USE_HOSTCC */
369 /*******************************************************************/
370 /* Legacy format specific code (prefixed with image_) */
371 /*******************************************************************/
372 static inline uint32_t image_get_header_size(void)
373 {
374 return (sizeof(image_header_t));
375 }
377 #define image_get_hdr_l(f) \
378 static inline uint32_t image_get_##f(const image_header_t *hdr) \
379 { \
380 return uimage_to_cpu(hdr->ih_##f); \
381 }
382 image_get_hdr_l(magic) /* image_get_magic */
383 image_get_hdr_l(hcrc) /* image_get_hcrc */
384 image_get_hdr_l(time) /* image_get_time */
385 image_get_hdr_l(size) /* image_get_size */
386 image_get_hdr_l(load) /* image_get_load */
387 image_get_hdr_l(ep) /* image_get_ep */
388 image_get_hdr_l(dcrc) /* image_get_dcrc */
390 #define image_get_hdr_b(f) \
391 static inline uint8_t image_get_##f(const image_header_t *hdr) \
392 { \
393 return hdr->ih_##f; \
394 }
395 image_get_hdr_b(os) /* image_get_os */
396 image_get_hdr_b(arch) /* image_get_arch */
397 image_get_hdr_b(type) /* image_get_type */
398 image_get_hdr_b(comp) /* image_get_comp */
400 static inline char *image_get_name(const image_header_t *hdr)
401 {
402 return (char *)hdr->ih_name;
403 }
405 static inline uint32_t image_get_data_size(const image_header_t *hdr)
406 {
407 return image_get_size(hdr);
408 }
410 /**
411 * image_get_data - get image payload start address
412 * @hdr: image header
413 *
414 * image_get_data() returns address of the image payload. For single
415 * component images it is image data start. For multi component
416 * images it points to the null terminated table of sub-images sizes.
417 *
418 * returns:
419 * image payload data start address
420 */
421 static inline ulong image_get_data(const image_header_t *hdr)
422 {
423 return ((ulong)hdr + image_get_header_size());
424 }
426 static inline uint32_t image_get_image_size(const image_header_t *hdr)
427 {
428 return (image_get_size(hdr) + image_get_header_size());
429 }
430 static inline ulong image_get_image_end(const image_header_t *hdr)
431 {
432 return ((ulong)hdr + image_get_image_size(hdr));
433 }
435 #define image_set_hdr_l(f) \
436 static inline void image_set_##f(image_header_t *hdr, uint32_t val) \
437 { \
438 hdr->ih_##f = cpu_to_uimage(val); \
439 }
440 image_set_hdr_l(magic) /* image_set_magic */
441 image_set_hdr_l(hcrc) /* image_set_hcrc */
442 image_set_hdr_l(time) /* image_set_time */
443 image_set_hdr_l(size) /* image_set_size */
444 image_set_hdr_l(load) /* image_set_load */
445 image_set_hdr_l(ep) /* image_set_ep */
446 image_set_hdr_l(dcrc) /* image_set_dcrc */
448 #define image_set_hdr_b(f) \
449 static inline void image_set_##f(image_header_t *hdr, uint8_t val) \
450 { \
451 hdr->ih_##f = val; \
452 }
453 image_set_hdr_b(os) /* image_set_os */
454 image_set_hdr_b(arch) /* image_set_arch */
455 image_set_hdr_b(type) /* image_set_type */
456 image_set_hdr_b(comp) /* image_set_comp */
458 static inline void image_set_name(image_header_t *hdr, const char *name)
459 {
460 strncpy(image_get_name(hdr), name, IH_NMLEN);
461 }
463 int image_check_hcrc(const image_header_t *hdr);
464 int image_check_dcrc(const image_header_t *hdr);
465 #ifndef USE_HOSTCC
466 ulong getenv_bootm_low(void);
467 phys_size_t getenv_bootm_size(void);
468 phys_size_t getenv_bootm_mapsize(void);
469 void memmove_wd(void *to, void *from, size_t len, ulong chunksz);
470 #endif
472 static inline int image_check_magic(const image_header_t *hdr)
473 {
474 return (image_get_magic(hdr) == IH_MAGIC);
475 }
476 static inline int image_check_type(const image_header_t *hdr, uint8_t type)
477 {
478 return (image_get_type(hdr) == type);
479 }
480 static inline int image_check_arch(const image_header_t *hdr, uint8_t arch)
481 {
482 return (image_get_arch(hdr) == arch);
483 }
484 static inline int image_check_os(const image_header_t *hdr, uint8_t os)
485 {
486 return (image_get_os(hdr) == os);
487 }
489 ulong image_multi_count(const image_header_t *hdr);
490 void image_multi_getimg(const image_header_t *hdr, ulong idx,
491 ulong *data, ulong *len);
493 void image_print_contents(const void *hdr);
495 #ifndef USE_HOSTCC
496 static inline int image_check_target_arch(const image_header_t *hdr)
497 {
498 #ifndef IH_ARCH_DEFAULT
499 # error "please define IH_ARCH_DEFAULT in your arch asm/u-boot.h"
500 #endif
501 return image_check_arch(hdr, IH_ARCH_DEFAULT);
502 }
503 #endif /* USE_HOSTCC */
505 /*******************************************************************/
506 /* New uImage format specific code (prefixed with fit_) */
507 /*******************************************************************/
508 #if defined(CONFIG_FIT)
510 #define FIT_IMAGES_PATH "/images"
511 #define FIT_CONFS_PATH "/configurations"
513 /* hash node */
514 #define FIT_HASH_NODENAME "hash"
515 #define FIT_ALGO_PROP "algo"
516 #define FIT_VALUE_PROP "value"
517 #define FIT_IGNORE_PROP "uboot-ignore"
519 /* image node */
520 #define FIT_DATA_PROP "data"
521 #define FIT_TIMESTAMP_PROP "timestamp"
522 #define FIT_DESC_PROP "description"
523 #define FIT_ARCH_PROP "arch"
524 #define FIT_TYPE_PROP "type"
525 #define FIT_OS_PROP "os"
526 #define FIT_COMP_PROP "compression"
527 #define FIT_ENTRY_PROP "entry"
528 #define FIT_LOAD_PROP "load"
530 /* configuration node */
531 #define FIT_KERNEL_PROP "kernel"
532 #define FIT_RAMDISK_PROP "ramdisk"
533 #define FIT_FDT_PROP "fdt"
534 #define FIT_DEFAULT_PROP "default"
536 #define FIT_MAX_HASH_LEN 20 /* max(crc32_len(4), sha1_len(20)) */
538 /* cmdline argument format parsing */
539 int fit_parse_conf(const char *spec, ulong addr_curr,
540 ulong *addr, const char **conf_name);
541 int fit_parse_subimage(const char *spec, ulong addr_curr,
542 ulong *addr, const char **image_name);
544 void fit_print_contents(const void *fit);
545 void fit_image_print(const void *fit, int noffset, const char *p);
546 void fit_image_print_hash(const void *fit, int noffset, const char *p);
548 /**
549 * fit_get_end - get FIT image size
550 * @fit: pointer to the FIT format image header
551 *
552 * returns:
553 * size of the FIT image (blob) in memory
554 */
555 static inline ulong fit_get_size(const void *fit)
556 {
557 return fdt_totalsize(fit);
558 }
560 /**
561 * fit_get_end - get FIT image end
562 * @fit: pointer to the FIT format image header
563 *
564 * returns:
565 * end address of the FIT image (blob) in memory
566 */
567 static inline ulong fit_get_end(const void *fit)
568 {
569 return (ulong)fit + fdt_totalsize(fit);
570 }
572 /**
573 * fit_get_name - get FIT node name
574 * @fit: pointer to the FIT format image header
575 *
576 * returns:
577 * NULL, on error
578 * pointer to node name, on success
579 */
580 static inline const char *fit_get_name(const void *fit_hdr,
581 int noffset, int *len)
582 {
583 return fdt_get_name(fit_hdr, noffset, len);
584 }
586 int fit_get_desc(const void *fit, int noffset, char **desc);
587 int fit_get_timestamp(const void *fit, int noffset, time_t *timestamp);
589 int fit_image_get_node(const void *fit, const char *image_uname);
590 int fit_image_get_os(const void *fit, int noffset, uint8_t *os);
591 int fit_image_get_arch(const void *fit, int noffset, uint8_t *arch);
592 int fit_image_get_type(const void *fit, int noffset, uint8_t *type);
593 int fit_image_get_comp(const void *fit, int noffset, uint8_t *comp);
594 int fit_image_get_load(const void *fit, int noffset, ulong *load);
595 int fit_image_get_entry(const void *fit, int noffset, ulong *entry);
596 int fit_image_get_data(const void *fit, int noffset,
597 const void **data, size_t *size);
599 int fit_image_hash_get_algo(const void *fit, int noffset, char **algo);
600 int fit_image_hash_get_value(const void *fit, int noffset, uint8_t **value,
601 int *value_len);
602 #ifndef USE_HOSTCC
603 int fit_image_hash_get_ignore(const void *fit, int noffset, int *ignore);
604 #endif
606 int fit_set_timestamp(void *fit, int noffset, time_t timestamp);
607 int fit_set_hashes(void *fit);
608 int fit_image_set_hashes(void *fit, int image_noffset);
609 int fit_image_hash_set_value(void *fit, int noffset, uint8_t *value,
610 int value_len);
612 int fit_image_check_hashes(const void *fit, int noffset);
613 int fit_all_image_check_hashes(const void *fit);
614 int fit_image_check_os(const void *fit, int noffset, uint8_t os);
615 int fit_image_check_arch(const void *fit, int noffset, uint8_t arch);
616 int fit_image_check_type(const void *fit, int noffset, uint8_t type);
617 int fit_image_check_comp(const void *fit, int noffset, uint8_t comp);
618 int fit_check_format(const void *fit);
620 int fit_conf_find_compat(const void *fit, const void *fdt);
621 int fit_conf_get_node(const void *fit, const char *conf_uname);
622 int fit_conf_get_kernel_node(const void *fit, int noffset);
623 int fit_conf_get_ramdisk_node(const void *fit, int noffset);
624 int fit_conf_get_fdt_node(const void *fit, int noffset);
626 void fit_conf_print(const void *fit, int noffset, const char *p);
628 #ifndef USE_HOSTCC
629 static inline int fit_image_check_target_arch(const void *fdt, int node)
630 {
631 return fit_image_check_arch(fdt, node, IH_ARCH_DEFAULT);
632 }
633 #endif /* USE_HOSTCC */
635 #ifdef CONFIG_FIT_VERBOSE
636 #define fit_unsupported(msg) printf("! %s:%d " \
637 "FIT images not supported for '%s'\n", \
638 __FILE__, __LINE__, (msg))
640 #define fit_unsupported_reset(msg) printf("! %s:%d " \
641 "FIT images not supported for '%s' " \
642 "- must reset board to recover!\n", \
643 __FILE__, __LINE__, (msg))
644 #else
645 #define fit_unsupported(msg)
646 #define fit_unsupported_reset(msg)
647 #endif /* CONFIG_FIT_VERBOSE */
648 #endif /* CONFIG_FIT */
650 #endif /* __IMAGE_H__ */