1 /*
2 * (C) Copyright 2008 Semihalf
3 *
4 * (C) Copyright 2000-2005
5 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 *
25 ********************************************************************
26 * NOTE: This header file defines an interface to U-Boot. Including
27 * this (unmodified) header file in another file is considered normal
28 * use of U-Boot, and does *not* fall under the heading of "derived
29 * work".
30 ********************************************************************
31 */
33 #ifndef __IMAGE_H__
34 #define __IMAGE_H__
36 #include "compiler.h"
38 #ifdef USE_HOSTCC
40 /* new uImage format support enabled on host */
41 #define CONFIG_FIT 1
42 #define CONFIG_OF_LIBFDT 1
43 #define CONFIG_FIT_VERBOSE 1 /* enable fit_format_{error,warning}() */
45 #else
47 #include <lmb.h>
48 #include <asm/u-boot.h>
49 #include <command.h>
51 #endif /* USE_HOSTCC */
53 #if defined(CONFIG_FIT)
54 #include <fdt.h>
55 #include <libfdt.h>
56 #include <fdt_support.h>
57 #define CONFIG_MD5 /* FIT images need MD5 support */
58 #define CONFIG_SHA1 /* and SHA1 */
59 #endif
61 /*
62 * Operating System Codes
63 */
64 #define IH_OS_INVALID 0 /* Invalid OS */
65 #define IH_OS_OPENBSD 1 /* OpenBSD */
66 #define IH_OS_NETBSD 2 /* NetBSD */
67 #define IH_OS_FREEBSD 3 /* FreeBSD */
68 #define IH_OS_4_4BSD 4 /* 4.4BSD */
69 #define IH_OS_LINUX 5 /* Linux */
70 #define IH_OS_SVR4 6 /* SVR4 */
71 #define IH_OS_ESIX 7 /* Esix */
72 #define IH_OS_SOLARIS 8 /* Solaris */
73 #define IH_OS_IRIX 9 /* Irix */
74 #define IH_OS_SCO 10 /* SCO */
75 #define IH_OS_DELL 11 /* Dell */
76 #define IH_OS_NCR 12 /* NCR */
77 #define IH_OS_LYNXOS 13 /* LynxOS */
78 #define IH_OS_VXWORKS 14 /* VxWorks */
79 #define IH_OS_PSOS 15 /* pSOS */
80 #define IH_OS_QNX 16 /* QNX */
81 #define IH_OS_U_BOOT 17 /* Firmware */
82 #define IH_OS_RTEMS 18 /* RTEMS */
83 #define IH_OS_ARTOS 19 /* ARTOS */
84 #define IH_OS_UNITY 20 /* Unity OS */
85 #define IH_OS_INTEGRITY 21 /* INTEGRITY */
86 #define IH_OS_OSE 22 /* OSE */
88 /*
89 * CPU Architecture Codes (supported by Linux)
90 */
91 #define IH_ARCH_INVALID 0 /* Invalid CPU */
92 #define IH_ARCH_ALPHA 1 /* Alpha */
93 #define IH_ARCH_ARM 2 /* ARM */
94 #define IH_ARCH_I386 3 /* Intel x86 */
95 #define IH_ARCH_IA64 4 /* IA64 */
96 #define IH_ARCH_MIPS 5 /* MIPS */
97 #define IH_ARCH_MIPS64 6 /* MIPS 64 Bit */
98 #define IH_ARCH_PPC 7 /* PowerPC */
99 #define IH_ARCH_S390 8 /* IBM S390 */
100 #define IH_ARCH_SH 9 /* SuperH */
101 #define IH_ARCH_SPARC 10 /* Sparc */
102 #define IH_ARCH_SPARC64 11 /* Sparc 64 Bit */
103 #define IH_ARCH_M68K 12 /* M68K */
104 #define IH_ARCH_MICROBLAZE 14 /* MicroBlaze */
105 #define IH_ARCH_NIOS2 15 /* Nios-II */
106 #define IH_ARCH_BLACKFIN 16 /* Blackfin */
107 #define IH_ARCH_AVR32 17 /* AVR32 */
108 #define IH_ARCH_ST200 18 /* STMicroelectronics ST200 */
109 #define IH_ARCH_SANDBOX 19 /* Sandbox architecture (test only) */
110 #define IH_ARCH_NDS32 20 /* ANDES Technology - NDS32 */
111 #define IH_ARCH_OPENRISC 21 /* OpenRISC 1000 */
113 /*
114 * Image Types
115 *
116 * "Standalone Programs" are directly runnable in the environment
117 * provided by U-Boot; it is expected that (if they behave
118 * well) you can continue to work in U-Boot after return from
119 * the Standalone Program.
120 * "OS Kernel Images" are usually images of some Embedded OS which
121 * will take over control completely. Usually these programs
122 * will install their own set of exception handlers, device
123 * drivers, set up the MMU, etc. - this means, that you cannot
124 * expect to re-enter U-Boot except by resetting the CPU.
125 * "RAMDisk Images" are more or less just data blocks, and their
126 * parameters (address, size) are passed to an OS kernel that is
127 * being started.
128 * "Multi-File Images" contain several images, typically an OS
129 * (Linux) kernel image and one or more data images like
130 * RAMDisks. This construct is useful for instance when you want
131 * to boot over the network using BOOTP etc., where the boot
132 * server provides just a single image file, but you want to get
133 * for instance an OS kernel and a RAMDisk image.
134 *
135 * "Multi-File Images" start with a list of image sizes, each
136 * image size (in bytes) specified by an "uint32_t" in network
137 * byte order. This list is terminated by an "(uint32_t)0".
138 * Immediately after the terminating 0 follow the images, one by
139 * one, all aligned on "uint32_t" boundaries (size rounded up to
140 * a multiple of 4 bytes - except for the last file).
141 *
142 * "Firmware Images" are binary images containing firmware (like
143 * U-Boot or FPGA images) which usually will be programmed to
144 * flash memory.
145 *
146 * "Script files" are command sequences that will be executed by
147 * U-Boot's command interpreter; this feature is especially
148 * useful when you configure U-Boot to use a real shell (hush)
149 * as command interpreter (=> Shell Scripts).
150 */
152 #define IH_TYPE_INVALID 0 /* Invalid Image */
153 #define IH_TYPE_STANDALONE 1 /* Standalone Program */
154 #define IH_TYPE_KERNEL 2 /* OS Kernel Image */
155 #define IH_TYPE_RAMDISK 3 /* RAMDisk Image */
156 #define IH_TYPE_MULTI 4 /* Multi-File Image */
157 #define IH_TYPE_FIRMWARE 5 /* Firmware Image */
158 #define IH_TYPE_SCRIPT 6 /* Script file */
159 #define IH_TYPE_FILESYSTEM 7 /* Filesystem Image (any type) */
160 #define IH_TYPE_FLATDT 8 /* Binary Flat Device Tree Blob */
161 #define IH_TYPE_KWBIMAGE 9 /* Kirkwood Boot Image */
162 #define IH_TYPE_IMXIMAGE 10 /* Freescale IMXBoot Image */
163 #define IH_TYPE_UBLIMAGE 11 /* Davinci UBL Image */
164 #define IH_TYPE_OMAPIMAGE 12 /* TI OMAP Config Header Image */
165 #define IH_TYPE_AISIMAGE 13 /* TI Davinci AIS Image */
166 #define IH_TYPE_KERNEL_NOLOAD 14 /* OS Kernel Image, can run from any load address */
167 #define IH_TYPE_PBLIMAGE 15 /* Freescale PBL Boot Image */
169 /*
170 * Compression Types
171 */
172 #define IH_COMP_NONE 0 /* No Compression Used */
173 #define IH_COMP_GZIP 1 /* gzip Compression Used */
174 #define IH_COMP_BZIP2 2 /* bzip2 Compression Used */
175 #define IH_COMP_LZMA 3 /* lzma Compression Used */
176 #define IH_COMP_LZO 4 /* lzo Compression Used */
178 #define IH_MAGIC 0x27051956 /* Image Magic Number */
179 #define IH_NMLEN 32 /* Image Name Length */
181 /*
182 * Legacy format image header,
183 * all data in network byte order (aka natural aka bigendian).
184 */
185 typedef struct image_header {
186 uint32_t ih_magic; /* Image Header Magic Number */
187 uint32_t ih_hcrc; /* Image Header CRC Checksum */
188 uint32_t ih_time; /* Image Creation Timestamp */
189 uint32_t ih_size; /* Image Data Size */
190 uint32_t ih_load; /* Data Load Address */
191 uint32_t ih_ep; /* Entry Point Address */
192 uint32_t ih_dcrc; /* Image Data CRC Checksum */
193 uint8_t ih_os; /* Operating System */
194 uint8_t ih_arch; /* CPU architecture */
195 uint8_t ih_type; /* Image Type */
196 uint8_t ih_comp; /* Compression Type */
197 uint8_t ih_name[IH_NMLEN]; /* Image Name */
198 } image_header_t;
200 typedef struct image_info {
201 ulong start, end; /* start/end of blob */
202 ulong image_start, image_len; /* start of image within blob, len of image */
203 ulong load; /* load addr for the image */
204 uint8_t comp, type, os; /* compression, type of image, os type */
205 } image_info_t;
207 /*
208 * Legacy and FIT format headers used by do_bootm() and do_bootm_<os>()
209 * routines.
210 */
211 typedef struct bootm_headers {
212 /*
213 * Legacy os image header, if it is a multi component image
214 * then boot_get_ramdisk() and get_fdt() will attempt to get
215 * data from second and third component accordingly.
216 */
217 image_header_t *legacy_hdr_os; /* image header pointer */
218 image_header_t legacy_hdr_os_copy; /* header copy */
219 ulong legacy_hdr_valid;
221 #if defined(CONFIG_FIT)
222 const char *fit_uname_cfg; /* configuration node unit name */
224 void *fit_hdr_os; /* os FIT image header */
225 const char *fit_uname_os; /* os subimage node unit name */
226 int fit_noffset_os; /* os subimage node offset */
228 void *fit_hdr_rd; /* init ramdisk FIT image header */
229 const char *fit_uname_rd; /* init ramdisk subimage node unit name */
230 int fit_noffset_rd; /* init ramdisk subimage node offset */
232 void *fit_hdr_fdt; /* FDT blob FIT image header */
233 const char *fit_uname_fdt; /* FDT blob subimage node unit name */
234 int fit_noffset_fdt;/* FDT blob subimage node offset */
235 #endif
237 #ifndef USE_HOSTCC
238 image_info_t os; /* os image info */
239 ulong ep; /* entry point of OS */
241 ulong rd_start, rd_end;/* ramdisk start/end */
243 #ifdef CONFIG_OF_LIBFDT
244 char *ft_addr; /* flat dev tree address */
245 #endif
246 ulong ft_len; /* length of flat device tree */
248 ulong initrd_start;
249 ulong initrd_end;
250 ulong cmdline_start;
251 ulong cmdline_end;
252 bd_t *kbd;
253 #endif
255 int verify; /* getenv("verify")[0] != 'n' */
257 #define BOOTM_STATE_START (0x00000001)
258 #define BOOTM_STATE_LOADOS (0x00000002)
259 #define BOOTM_STATE_RAMDISK (0x00000004)
260 #define BOOTM_STATE_FDT (0x00000008)
261 #define BOOTM_STATE_OS_CMDLINE (0x00000010)
262 #define BOOTM_STATE_OS_BD_T (0x00000020)
263 #define BOOTM_STATE_OS_PREP (0x00000040)
264 #define BOOTM_STATE_OS_GO (0x00000080)
265 int state;
267 #ifdef CONFIG_LMB
268 struct lmb lmb; /* for memory mgmt */
269 #endif
270 } bootm_headers_t;
272 extern bootm_headers_t images;
274 /*
275 * Some systems (for example LWMON) have very short watchdog periods;
276 * we must make sure to split long operations like memmove() or
277 * checksum calculations into reasonable chunks.
278 */
279 #ifndef CHUNKSZ
280 #define CHUNKSZ (64 * 1024)
281 #endif
283 #ifndef CHUNKSZ_CRC32
284 #define CHUNKSZ_CRC32 (64 * 1024)
285 #endif
287 #ifndef CHUNKSZ_MD5
288 #define CHUNKSZ_MD5 (64 * 1024)
289 #endif
291 #ifndef CHUNKSZ_SHA1
292 #define CHUNKSZ_SHA1 (64 * 1024)
293 #endif
295 #define uimage_to_cpu(x) be32_to_cpu(x)
296 #define cpu_to_uimage(x) cpu_to_be32(x)
298 /*
299 * Translation table for entries of a specific type; used by
300 * get_table_entry_id() and get_table_entry_name().
301 */
302 typedef struct table_entry {
303 int id;
304 char *sname; /* short (input) name to find table entry */
305 char *lname; /* long (output) name to print for messages */
306 } table_entry_t;
308 /*
309 * get_table_entry_id() scans the translation table trying to find an
310 * entry that matches the given short name. If a matching entry is
311 * found, it's id is returned to the caller.
312 */
313 int get_table_entry_id(const table_entry_t *table,
314 const char *table_name, const char *name);
315 /*
316 * get_table_entry_name() scans the translation table trying to find
317 * an entry that matches the given id. If a matching entry is found,
318 * its long name is returned to the caller.
319 */
320 char *get_table_entry_name(const table_entry_t *table, char *msg, int id);
322 const char *genimg_get_os_name(uint8_t os);
323 const char *genimg_get_arch_name(uint8_t arch);
324 const char *genimg_get_type_name(uint8_t type);
325 const char *genimg_get_comp_name(uint8_t comp);
326 int genimg_get_os_id(const char *name);
327 int genimg_get_arch_id(const char *name);
328 int genimg_get_type_id(const char *name);
329 int genimg_get_comp_id(const char *name);
330 void genimg_print_size(uint32_t size);
332 #ifndef USE_HOSTCC
333 /* Image format types, returned by _get_format() routine */
334 #define IMAGE_FORMAT_INVALID 0x00
335 #define IMAGE_FORMAT_LEGACY 0x01 /* legacy image_header based format */
336 #define IMAGE_FORMAT_FIT 0x02 /* new, libfdt based format */
338 int genimg_get_format(void *img_addr);
339 int genimg_has_config(bootm_headers_t *images);
340 ulong genimg_get_image(ulong img_addr);
342 int boot_get_ramdisk(int argc, char * const argv[], bootm_headers_t *images,
343 uint8_t arch, ulong *rd_start, ulong *rd_end);
346 #ifdef CONFIG_OF_LIBFDT
347 int boot_get_fdt(int flag, int argc, char * const argv[],
348 bootm_headers_t *images, char **of_flat_tree, ulong *of_size);
349 void boot_fdt_add_mem_rsv_regions(struct lmb *lmb, void *fdt_blob);
350 int boot_relocate_fdt(struct lmb *lmb, char **of_flat_tree, ulong *of_size);
351 #endif
353 #ifdef CONFIG_SYS_BOOT_RAMDISK_HIGH
354 int boot_ramdisk_high(struct lmb *lmb, ulong rd_data, ulong rd_len,
355 ulong *initrd_start, ulong *initrd_end);
356 #endif /* CONFIG_SYS_BOOT_RAMDISK_HIGH */
357 #ifdef CONFIG_SYS_BOOT_GET_CMDLINE
358 int boot_get_cmdline(struct lmb *lmb, ulong *cmd_start, ulong *cmd_end);
359 #endif /* CONFIG_SYS_BOOT_GET_CMDLINE */
360 #ifdef CONFIG_SYS_BOOT_GET_KBD
361 int boot_get_kbd(struct lmb *lmb, bd_t **kbd);
362 #endif /* CONFIG_SYS_BOOT_GET_KBD */
363 #endif /* !USE_HOSTCC */
365 /*******************************************************************/
366 /* Legacy format specific code (prefixed with image_) */
367 /*******************************************************************/
368 static inline uint32_t image_get_header_size(void)
369 {
370 return (sizeof(image_header_t));
371 }
373 #define image_get_hdr_l(f) \
374 static inline uint32_t image_get_##f(const image_header_t *hdr) \
375 { \
376 return uimage_to_cpu(hdr->ih_##f); \
377 }
378 image_get_hdr_l(magic) /* image_get_magic */
379 image_get_hdr_l(hcrc) /* image_get_hcrc */
380 image_get_hdr_l(time) /* image_get_time */
381 image_get_hdr_l(size) /* image_get_size */
382 image_get_hdr_l(load) /* image_get_load */
383 image_get_hdr_l(ep) /* image_get_ep */
384 image_get_hdr_l(dcrc) /* image_get_dcrc */
386 #define image_get_hdr_b(f) \
387 static inline uint8_t image_get_##f(const image_header_t *hdr) \
388 { \
389 return hdr->ih_##f; \
390 }
391 image_get_hdr_b(os) /* image_get_os */
392 image_get_hdr_b(arch) /* image_get_arch */
393 image_get_hdr_b(type) /* image_get_type */
394 image_get_hdr_b(comp) /* image_get_comp */
396 static inline char *image_get_name(const image_header_t *hdr)
397 {
398 return (char *)hdr->ih_name;
399 }
401 static inline uint32_t image_get_data_size(const image_header_t *hdr)
402 {
403 return image_get_size(hdr);
404 }
406 /**
407 * image_get_data - get image payload start address
408 * @hdr: image header
409 *
410 * image_get_data() returns address of the image payload. For single
411 * component images it is image data start. For multi component
412 * images it points to the null terminated table of sub-images sizes.
413 *
414 * returns:
415 * image payload data start address
416 */
417 static inline ulong image_get_data(const image_header_t *hdr)
418 {
419 return ((ulong)hdr + image_get_header_size());
420 }
422 static inline uint32_t image_get_image_size(const image_header_t *hdr)
423 {
424 return (image_get_size(hdr) + image_get_header_size());
425 }
426 static inline ulong image_get_image_end(const image_header_t *hdr)
427 {
428 return ((ulong)hdr + image_get_image_size(hdr));
429 }
431 #define image_set_hdr_l(f) \
432 static inline void image_set_##f(image_header_t *hdr, uint32_t val) \
433 { \
434 hdr->ih_##f = cpu_to_uimage(val); \
435 }
436 image_set_hdr_l(magic) /* image_set_magic */
437 image_set_hdr_l(hcrc) /* image_set_hcrc */
438 image_set_hdr_l(time) /* image_set_time */
439 image_set_hdr_l(size) /* image_set_size */
440 image_set_hdr_l(load) /* image_set_load */
441 image_set_hdr_l(ep) /* image_set_ep */
442 image_set_hdr_l(dcrc) /* image_set_dcrc */
444 #define image_set_hdr_b(f) \
445 static inline void image_set_##f(image_header_t *hdr, uint8_t val) \
446 { \
447 hdr->ih_##f = val; \
448 }
449 image_set_hdr_b(os) /* image_set_os */
450 image_set_hdr_b(arch) /* image_set_arch */
451 image_set_hdr_b(type) /* image_set_type */
452 image_set_hdr_b(comp) /* image_set_comp */
454 static inline void image_set_name(image_header_t *hdr, const char *name)
455 {
456 strncpy(image_get_name(hdr), name, IH_NMLEN);
457 }
459 int image_check_hcrc(const image_header_t *hdr);
460 int image_check_dcrc(const image_header_t *hdr);
461 #ifndef USE_HOSTCC
462 int getenv_yesno(char *var);
463 ulong getenv_bootm_low(void);
464 phys_size_t getenv_bootm_size(void);
465 phys_size_t getenv_bootm_mapsize(void);
466 void memmove_wd(void *to, void *from, size_t len, ulong chunksz);
467 #endif
469 static inline int image_check_magic(const image_header_t *hdr)
470 {
471 return (image_get_magic(hdr) == IH_MAGIC);
472 }
473 static inline int image_check_type(const image_header_t *hdr, uint8_t type)
474 {
475 return (image_get_type(hdr) == type);
476 }
477 static inline int image_check_arch(const image_header_t *hdr, uint8_t arch)
478 {
479 return (image_get_arch(hdr) == arch);
480 }
481 static inline int image_check_os(const image_header_t *hdr, uint8_t os)
482 {
483 return (image_get_os(hdr) == os);
484 }
486 ulong image_multi_count(const image_header_t *hdr);
487 void image_multi_getimg(const image_header_t *hdr, ulong idx,
488 ulong *data, ulong *len);
490 void image_print_contents(const void *hdr);
492 #ifndef USE_HOSTCC
493 static inline int image_check_target_arch(const image_header_t *hdr)
494 {
495 #ifndef IH_ARCH_DEFAULT
496 # error "please define IH_ARCH_DEFAULT in your arch asm/u-boot.h"
497 #endif
498 return image_check_arch(hdr, IH_ARCH_DEFAULT);
499 }
500 #endif /* USE_HOSTCC */
502 /*******************************************************************/
503 /* New uImage format specific code (prefixed with fit_) */
504 /*******************************************************************/
505 #if defined(CONFIG_FIT)
507 #define FIT_IMAGES_PATH "/images"
508 #define FIT_CONFS_PATH "/configurations"
510 /* hash node */
511 #define FIT_HASH_NODENAME "hash"
512 #define FIT_ALGO_PROP "algo"
513 #define FIT_VALUE_PROP "value"
515 /* image node */
516 #define FIT_DATA_PROP "data"
517 #define FIT_TIMESTAMP_PROP "timestamp"
518 #define FIT_DESC_PROP "description"
519 #define FIT_ARCH_PROP "arch"
520 #define FIT_TYPE_PROP "type"
521 #define FIT_OS_PROP "os"
522 #define FIT_COMP_PROP "compression"
523 #define FIT_ENTRY_PROP "entry"
524 #define FIT_LOAD_PROP "load"
526 /* configuration node */
527 #define FIT_KERNEL_PROP "kernel"
528 #define FIT_RAMDISK_PROP "ramdisk"
529 #define FIT_FDT_PROP "fdt"
530 #define FIT_DEFAULT_PROP "default"
532 #define FIT_MAX_HASH_LEN 20 /* max(crc32_len(4), sha1_len(20)) */
534 /* cmdline argument format parsing */
535 int fit_parse_conf(const char *spec, ulong addr_curr,
536 ulong *addr, const char **conf_name);
537 int fit_parse_subimage(const char *spec, ulong addr_curr,
538 ulong *addr, const char **image_name);
540 void fit_print_contents(const void *fit);
541 void fit_image_print(const void *fit, int noffset, const char *p);
542 void fit_image_print_hash(const void *fit, int noffset, const char *p);
544 /**
545 * fit_get_end - get FIT image size
546 * @fit: pointer to the FIT format image header
547 *
548 * returns:
549 * size of the FIT image (blob) in memory
550 */
551 static inline ulong fit_get_size(const void *fit)
552 {
553 return fdt_totalsize(fit);
554 }
556 /**
557 * fit_get_end - get FIT image end
558 * @fit: pointer to the FIT format image header
559 *
560 * returns:
561 * end address of the FIT image (blob) in memory
562 */
563 static inline ulong fit_get_end(const void *fit)
564 {
565 return (ulong)fit + fdt_totalsize(fit);
566 }
568 /**
569 * fit_get_name - get FIT node name
570 * @fit: pointer to the FIT format image header
571 *
572 * returns:
573 * NULL, on error
574 * pointer to node name, on success
575 */
576 static inline const char *fit_get_name(const void *fit_hdr,
577 int noffset, int *len)
578 {
579 return fdt_get_name(fit_hdr, noffset, len);
580 }
582 int fit_get_desc(const void *fit, int noffset, char **desc);
583 int fit_get_timestamp(const void *fit, int noffset, time_t *timestamp);
585 int fit_image_get_node(const void *fit, const char *image_uname);
586 int fit_image_get_os(const void *fit, int noffset, uint8_t *os);
587 int fit_image_get_arch(const void *fit, int noffset, uint8_t *arch);
588 int fit_image_get_type(const void *fit, int noffset, uint8_t *type);
589 int fit_image_get_comp(const void *fit, int noffset, uint8_t *comp);
590 int fit_image_get_load(const void *fit, int noffset, ulong *load);
591 int fit_image_get_entry(const void *fit, int noffset, ulong *entry);
592 int fit_image_get_data(const void *fit, int noffset,
593 const void **data, size_t *size);
595 int fit_image_hash_get_algo(const void *fit, int noffset, char **algo);
596 int fit_image_hash_get_value(const void *fit, int noffset, uint8_t **value,
597 int *value_len);
599 int fit_set_timestamp(void *fit, int noffset, time_t timestamp);
600 int fit_set_hashes(void *fit);
601 int fit_image_set_hashes(void *fit, int image_noffset);
602 int fit_image_hash_set_value(void *fit, int noffset, uint8_t *value,
603 int value_len);
605 int fit_image_check_hashes(const void *fit, int noffset);
606 int fit_all_image_check_hashes(const void *fit);
607 int fit_image_check_os(const void *fit, int noffset, uint8_t os);
608 int fit_image_check_arch(const void *fit, int noffset, uint8_t arch);
609 int fit_image_check_type(const void *fit, int noffset, uint8_t type);
610 int fit_image_check_comp(const void *fit, int noffset, uint8_t comp);
611 int fit_check_format(const void *fit);
613 int fit_conf_get_node(const void *fit, const char *conf_uname);
614 int fit_conf_get_kernel_node(const void *fit, int noffset);
615 int fit_conf_get_ramdisk_node(const void *fit, int noffset);
616 int fit_conf_get_fdt_node(const void *fit, int noffset);
618 void fit_conf_print(const void *fit, int noffset, const char *p);
620 #ifndef USE_HOSTCC
621 static inline int fit_image_check_target_arch(const void *fdt, int node)
622 {
623 return fit_image_check_arch(fdt, node, IH_ARCH_DEFAULT);
624 }
625 #endif /* USE_HOSTCC */
627 #ifdef CONFIG_FIT_VERBOSE
628 #define fit_unsupported(msg) printf("! %s:%d " \
629 "FIT images not supported for '%s'\n", \
630 __FILE__, __LINE__, (msg))
632 #define fit_unsupported_reset(msg) printf("! %s:%d " \
633 "FIT images not supported for '%s' " \
634 "- must reset board to recover!\n", \
635 __FILE__, __LINE__, (msg))
636 #else
637 #define fit_unsupported(msg)
638 #define fit_unsupported_reset(msg)
639 #endif /* CONFIG_FIT_VERBOSE */
640 #endif /* CONFIG_FIT */
642 #endif /* __IMAGE_H__ */