]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/lattice.h
HACK: ARM: DRA7xx: Add Ethernet crossbar setting
[glsdk/glsdk-u-boot.git] / include / lattice.h
1 /*
2  * Porting to U-Boot:
3  *
4  * (C) Copyright 2010
5  * Stefano Babic, DENX Software Engineering, sbabic@denx.de.
6  *
7  * Lattice's ispVME Embedded Tool to load Lattice's FPGA:
8  *
9  * Lattice Semiconductor Corp. Copyright 2009
10  *
11  * See file CREDITS for list of people who contributed to this
12  * project.
13  *
14  * This program is free software; you can redistribute it and/or
15  * modify it under the terms of the GNU General Public License as
16  * published by the Free Software Foundation; either version 2 of
17  * the License, or (at your option) any later version.
18  *
19  * This program is distributed in the hope that it will be useful,
20  * but WITHOUT ANY WARRANTY; without even the implied warranty of
21  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
22  * GNU General Public License for more details.
23  *
24  * You should have received a copy of the GNU General Public License
25  * along with this program; if not, write to the Free Software
26  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
27  * MA 02111-1307 USA
28  *
29  */
31 #ifndef _VME_OPCODE_H
32 #define _VME_OPCODE_H
34 #define VME_VERSION_NUMBER "12.1"
36 /* Maximum declarations. */
38 #define VMEHEXMAX       60000L  /* The hex file is split 60K per file. */
39 #define SCANMAX         64000L  /* The maximum SDR/SIR burst. */
41 /*
42  *
43  * Supported JTAG state transitions.
44  *
45  */
47 #define RESET           0x00
48 #define IDLE            0x01
49 #define IRPAUSE         0x02
50 #define DRPAUSE         0x03
51 #define SHIFTIR         0x04
52 #define SHIFTDR         0x05
53 /* 11/15/05 Nguyen changed to support DRCAPTURE*/
54 #define DRCAPTURE       0x06
56 /*
57  * Flow control register bit definitions.  A set bit indicates
58  * that the register currently exhibits the corresponding mode.
59  */
61 #define INTEL_PRGM      0x0001  /* Intelligent programming is in effect. */
62 #define CASCADE         0x0002  /* Currently splitting large SDR. */
63 #define REPEATLOOP      0x0008  /* Currently executing a repeat loop. */
64 #define SHIFTRIGHT      0x0080  /* The next data stream needs a right shift. */
65 #define SHIFTLEFT       0x0100  /* The next data stream needs a left shift. */
66 #define VERIFYUES       0x0200  /* Continue if fail is in effect. */
68 /*
69  * DataType register bit definitions.  A set bit indicates
70  * that the register currently holds the corresponding type of data.
71  */
73 #define EXPRESS         0x0001    /* Simultaneous program and verify. */
74 #define SIR_DATA        0x0002    /* SIR is the active SVF command. */
75 #define SDR_DATA        0x0004    /* SDR is the active SVF command. */
76 #define COMPRESS        0x0008    /* Data is compressed. */
77 #define TDI_DATA        0x0010    /* TDI data is present. */
78 #define TDO_DATA        0x0020    /* TDO data is present. */
79 #define MASK_DATA       0x0040    /* MASK data is present. */
80 #define HEAP_IN         0x0080    /* Data is from the heap. */
81 #define LHEAP_IN        0x0200    /* Data is from intel data buffer. */
82 #define VARIABLE        0x0400    /* Data is from a declared variable. */
83 #define CRC_DATA        0x0800   /* CRC data is pressent. */
84 #define CMASK_DATA      0x1000    /* CMASK data is pressent. */
85 #define RMASK_DATA      0x2000   /* RMASK data is pressent. */
86 #define READ_DATA       0x4000    /* READ data is pressent. */
87 #define DMASK_DATA      0x8000   /* DMASK data is pressent. */
89 /*
90  *
91  * Pin opcodes.
92  *
93  */
95 #define signalENABLE    0x1C    /* ispENABLE pin. */
96 #define signalTMS       0x1D    /* TMS pin. */
97 #define signalTCK       0x1E    /* TCK pin. */
98 #define signalTDI       0x1F    /* TDI pin. */
99 #define signalTRST      0x20    /* TRST pin. */
101 /*
102  *
103  * Supported vendors.
104  *
105  */
107 #define VENDOR          0x56
108 #define LATTICE         0x01
109 #define ALTERA          0x02
110 #define XILINX          0x03
112 /*
113  * Opcode definitions.
114  *
115  * Note: opcodes must be unique.
116  */
118 #define ENDDATA         0x00    /* The end of the current SDR data stream. */
119 #define RUNTEST         0x01    /* The duration to stay at the stable state. */
120 #define ENDDR           0x02    /* The stable state after SDR. */
121 #define ENDIR           0x03    /* The stable state after SIR. */
122 #define ENDSTATE        0x04    /* The stable state after RUNTEST. */
123 #define TRST            0x05    /* Assert the TRST pin. */
124 #define HIR             0x06    /*
125                                  * The sum of the IR bits of the
126                                  * leading devices.
127                                  */
128 #define TIR             0x07    /*
129                                  * The sum of the IR bits of the trailing
130                                  * devices.
131                                  */
132 #define HDR             0x08    /* The number of leading devices. */
133 #define TDR             0x09    /* The number of trailing devices. */
134 #define ispEN           0x0A    /* Assert the ispEN pin. */
135 #define FREQUENCY       0x0B    /*
136                                  * The maximum clock rate to run the JTAG state
137                                  * machine.
138                                  */
139 #define STATE           0x10    /* Move to the next stable state. */
140 #define SIR             0x11    /* The instruction stream follows. */
141 #define SDR             0x12    /* The data stream follows. */
142 #define TDI             0x13    /* The following data stream feeds into
143                                         the device. */
144 #define TDO             0x14    /*
145                                  * The following data stream is compared against
146                                  * the device.
147                                  */
148 #define MASK            0x15    /* The following data stream is used as mask. */
149 #define XSDR            0x16    /*
150                                  * The following data stream is for simultaneous
151                                  * program and verify.
152                                  */
153 #define XTDI            0x17    /* The following data stream is for shift in
154                                  * only. It must be stored for the next
155                                  * XSDR.
156                                  */
157 #define XTDO            0x18    /*
158                                  * There is not data stream.  The data stream
159                                  * was stored from the previous XTDI.
160                                  */
161 #define MEM             0x19    /*
162                                  * The maximum memory needed to allocate in
163                                  * order hold one row of data.
164                                  */
165 #define WAIT            0x1A    /* The duration of delay to observe. */
166 #define TCK             0x1B    /* The number of TCK pulses. */
167 #define SHR             0x23    /*
168                                  * Set the flow control register for
169                                  * right shift
170                                  */
171 #define SHL             0x24    /*
172                                  * Set the flow control register for left shift.
173                                  */
174 #define HEAP            0x32    /* The memory size needed to hold one loop. */
175 #define REPEAT          0x33    /* The beginning of the loop. */
176 #define LEFTPAREN       0x35    /* The beginning of data following the loop. */
177 #define VAR             0x55    /* Plac holder for loop data. */
178 #define SEC             0x1C    /*
179                                  * The delay time in seconds that must be
180                                  * observed.
181                                  */
182 #define SMASK           0x1D    /* The mask for TDI data. */
183 #define MAX_WAIT        0x1E    /* The absolute maximum wait time. */
184 #define ON              0x1F    /* Assert the targeted pin. */
185 #define OFF             0x20    /* Dis-assert the targeted pin. */
186 #define SETFLOW         0x30    /* Change the flow control register. */
187 #define RESETFLOW       0x31    /* Clear the flow control register. */
189 #define CRC             0x47    /*
190                                  * The following data stream is used for CRC
191                                  * calculation.
192                                  */
193 #define CMASK           0x48    /*
194                                  * The following data stream is used as mask
195                                  * for CRC calculation.
196                                  */
197 #define RMASK           0x49    /*
198                                  * The following data stream is used as mask
199                                  * for read and save.
200                                  */
201 #define READ            0x50    /*
202                                  * The following data stream is used for read
203                                  * and save.
204                                  */
205 #define ENDLOOP         0x59    /* The end of the repeat loop. */
206 #define SECUREHEAP      0x60    /* Used to secure the HEAP opcode. */
207 #define VUES            0x61    /* Support continue if fail. */
208 #define DMASK           0x62    /*
209                                  * The following data stream is used for dynamic
210                                  * I/O.
211                                  */
212 #define COMMENT         0x63    /* Support SVF comments in the VME file. */
213 #define HEADER          0x64    /* Support header in VME file. */
214 #define FILE_CRC        0x65    /* Support crc-protected VME file. */
215 #define LCOUNT          0x66    /* Support intelligent programming. */
216 #define LDELAY          0x67    /* Support intelligent programming. */
217 #define LSDR            0x68    /* Support intelligent programming. */
218 #define LHEAP           0x69    /*
219                                  * Memory needed to hold intelligent data
220                                  * buffer
221                                  */
222 #define CONTINUE        0x70    /* Allow continuation. */
223 #define LVDS            0x71    /* Support LVDS. */
224 #define ENDVME          0x7F    /* End of the VME file. */
225 #define ENDFILE         0xFF    /* End of file. */
227 /*
228  *
229  * ispVM Embedded Return Codes.
230  *
231  */
233 #define VME_VERIFICATION_FAILURE        -1
234 #define VME_FILE_READ_FAILURE           -2
235 #define VME_VERSION_FAILURE             -3
236 #define VME_INVALID_FILE                -4
237 #define VME_ARGUMENT_FAILURE            -5
238 #define VME_CRC_FAILURE                 -6
240 #define g_ucPinTDI      0x01
241 #define g_ucPinTCK      0x02
242 #define g_ucPinTMS      0x04
243 #define g_ucPinENABLE   0x08
244 #define g_ucPinTRST     0x10
246 /*
247  *
248  * Type definitions.
249  *
250  */
252 /* Support LVDS */
253 typedef struct {
254         unsigned short usPositiveIndex;
255         unsigned short usNegativeIndex;
256         unsigned char  ucUpdate;
257 } LVDSPair;
259 typedef enum {
260         min_lattice_iface_type,         /* insert all new types after this */
261         lattice_jtag_mode,              /* jtag/tap  */
262         max_lattice_iface_type          /* insert all new types before this */
263 } Lattice_iface;
265 typedef enum {
266         min_lattice_type,
267         Lattice_XP2,                    /* Lattice XP2 Family */
268         max_lattice_type                /* insert all new types before this */
269 } Lattice_Family;
271 typedef struct {
272         Lattice_Family  family; /* part type */
273         Lattice_iface   iface;  /* interface type */
274         size_t          size;   /* bytes of data part can accept */
275         void            *iface_fns; /* interface function table */
276         void            *base;  /* base interface address */
277         int             cookie; /* implementation specific cookie */
278         char            *desc;  /* description string */
279 } Lattice_desc;                 /* end, typedef Altera_desc */
281 /* Lattice Model Type */
282 #define CONFIG_SYS_XP2          CONFIG_SYS_FPGA_DEV(0x1)
284 /* Board specific implementation specific function types */
285 typedef void (*Lattice_jtag_init)(void);
286 typedef void (*Lattice_jtag_set_tdi)(int v);
287 typedef void (*Lattice_jtag_set_tms)(int v);
288 typedef void (*Lattice_jtag_set_tck)(int v);
289 typedef int (*Lattice_jtag_get_tdo)(void);
291 typedef struct {
292         Lattice_jtag_init       jtag_init;
293         Lattice_jtag_set_tdi    jtag_set_tdi;
294         Lattice_jtag_set_tms    jtag_set_tms;
295         Lattice_jtag_set_tck    jtag_set_tck;
296         Lattice_jtag_get_tdo    jtag_get_tdo;
297 } lattice_board_specific_func;
299 void writePort(unsigned char pins, unsigned char value);
300 unsigned char readPort(void);
301 void sclock(void);
302 void ispVMDelay(unsigned short int a_usMicroSecondDelay);
303 void calibration(void);
305 int lattice_load(Lattice_desc *desc, const void *buf, size_t bsize);
306 int lattice_dump(Lattice_desc *desc, const void *buf, size_t bsize);
307 int lattice_info(Lattice_desc *desc);
309 void ispVMStart(void);
310 void ispVMEnd(void);
311 extern void ispVMFreeMem(void);
312 signed char ispVMCode(void);
313 void ispVMDelay(unsigned short int a_usMicroSecondDelay);
314 void ispVMCalculateCRC32(unsigned char a_ucData);
315 unsigned char GetByte(void);
316 void writePort(unsigned char pins, unsigned char value);
317 unsigned char readPort(void);
318 void sclock(void);
319 #endif