1 /*
2 * (C) Copyright 2003
3 * Orbacom Systems, Inc.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #ifndef __LYNXKDI_H__
25 #define __LYNXKDI_H__
28 /* Boot parameter struct passed to kernel
29 */
30 typedef struct lynxos_bootparms_t {
31 uint8_t rsvd1[2]; /* Reserved */
32 uint8_t ethaddr[6]; /* Ethernet address */
33 uint16_t flags; /* Boot flags */
34 uint32_t rate; /* System frequency */
35 uint32_t clock_ref; /* Time reference */
36 uint32_t dramsz; /* DRAM size */
37 uint32_t rsvd2; /* Reserved */
38 } lynxos_bootparms_t;
41 #endif /* __LYNXKDI_H__ */