]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/lynxkdi.h
HACK: ARM: DRA7xx: Add VPE crossbar setting
[glsdk/glsdk-u-boot.git] / include / lynxkdi.h
1 /*
2  * (C) Copyright 2003
3  * Orbacom Systems, Inc.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #ifndef __LYNXKDI_H__
25 #define __LYNXKDI_H__
28 /* Boot parameter struct passed to kernel
29  */
30 typedef struct lynxos_bootparms_t {
31         uint8_t         rsvd1[2];       /* Reserved                     */
32         uint8_t         ethaddr[6];     /* Ethernet address             */
33         uint16_t        flags;          /* Boot flags                   */
34         uint32_t        rate;           /* System frequency             */
35         uint32_t        clock_ref;      /* Time reference               */
36         uint32_t        dramsz;         /* DRAM size                    */
37         uint32_t        rsvd2;          /* Reserved                     */
38 } lynxos_bootparms_t;
41 #endif  /* __LYNXKDI_H__ */