]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/net.h
HACK: ARM: DRA7xx: Add Ethernet crossbar setting
[glsdk/glsdk-u-boot.git] / include / net.h
1 /*
2  *      LiMon Monitor (LiMon) - Network.
3  *
4  *      Copyright 1994 - 2000 Neil Russell.
5  *      (See License)
6  *
7  *
8  * History
9  *      9/16/00   bor  adapted to TQM823L/STK8xxL board, RARP/TFTP boot added
10  */
12 #ifndef __NET_H__
13 #define __NET_H__
15 #if defined(CONFIG_8xx)
16 #include <commproc.h>
17 #endif  /* CONFIG_8xx */
19 #include <asm/cache.h>
20 #include <asm/byteorder.h>      /* for nton* / ntoh* stuff */
22 #define DEBUG_LL_STATE 0        /* Link local state machine changes */
23 #define DEBUG_DEV_PKT 0         /* Packets or info directed to the device */
24 #define DEBUG_NET_PKT 0         /* Packets on info on the network at large */
25 #define DEBUG_INT_STATE 0       /* Internal network state changes */
27 /*
28  *      The number of receive packet buffers, and the required packet buffer
29  *      alignment in memory.
30  *
31  */
33 #ifdef CONFIG_SYS_RX_ETH_BUFFER
34 # define PKTBUFSRX      CONFIG_SYS_RX_ETH_BUFFER
35 #else
36 # define PKTBUFSRX      4
37 #endif
39 #define PKTALIGN        ARCH_DMA_MINALIGN
41 /* IPv4 addresses are always 32 bits in size */
42 typedef u32             IPaddr_t;
45 /**
46  * An incoming packet handler.
47  * @param pkt    pointer to the application packet
48  * @param dport  destination UDP port
49  * @param sip    source IP address
50  * @param sport  source UDP port
51  * @param len    packet length
52  */
53 typedef void rxhand_f(uchar *pkt, unsigned dport,
54                       IPaddr_t sip, unsigned sport,
55                       unsigned len);
57 /**
58  * An incoming ICMP packet handler.
59  * @param type  ICMP type
60  * @param code  ICMP code
61  * @param dport destination UDP port
62  * @param sip   source IP address
63  * @param sport source UDP port
64  * @param pkt   pointer to the ICMP packet data
65  * @param len   packet length
66  */
67 typedef void rxhand_icmp_f(unsigned type, unsigned code, unsigned dport,
68                 IPaddr_t sip, unsigned sport, uchar *pkt, unsigned len);
70 /*
71  *      A timeout handler.  Called after time interval has expired.
72  */
73 typedef void    thand_f(void);
75 enum eth_state_t {
76         ETH_STATE_INIT,
77         ETH_STATE_PASSIVE,
78         ETH_STATE_ACTIVE
79 };
81 struct eth_device {
82         char name[16];
83         unsigned char enetaddr[6];
84         int iobase;
85         int state;
87         int  (*init) (struct eth_device *, bd_t *);
88         int  (*send) (struct eth_device *, void *packet, int length);
89         int  (*recv) (struct eth_device *);
90         void (*halt) (struct eth_device *);
91 #ifdef CONFIG_MCAST_TFTP
92         int (*mcast) (struct eth_device *, u32 ip, u8 set);
93 #endif
94         int  (*write_hwaddr) (struct eth_device *);
95         struct eth_device *next;
96         int index;
97         void *priv;
98 };
100 extern int eth_initialize(bd_t *bis);   /* Initialize network subsystem */
101 extern int eth_register(struct eth_device* dev);/* Register network device */
102 extern int eth_unregister(struct eth_device *dev);/* Remove network device */
103 extern void eth_try_another(int first_restart); /* Change the device */
104 extern void eth_set_current(void);              /* set nterface to ethcur var */
106 /* get the current device MAC */
107 extern struct eth_device *eth_current;
109 static inline __attribute__((always_inline))
110 struct eth_device *eth_get_dev(void)
112         return eth_current;
114 extern struct eth_device *eth_get_dev_by_name(const char *devname);
115 extern struct eth_device *eth_get_dev_by_index(int index); /* get dev @ index */
116 extern int eth_get_dev_index(void);             /* get the device index */
117 extern void eth_parse_enetaddr(const char *addr, uchar *enetaddr);
118 extern int eth_getenv_enetaddr(char *name, uchar *enetaddr);
119 extern int eth_setenv_enetaddr(char *name, const uchar *enetaddr);
121 /*
122  * Get the hardware address for an ethernet interface .
123  * Args:
124  *      base_name - base name for device (normally "eth")
125  *      index - device index number (0 for first)
126  *      enetaddr - returns 6 byte hardware address
127  * Returns:
128  *      Return true if the address is valid.
129  */
130 extern int eth_getenv_enetaddr_by_index(const char *base_name, int index,
131                                         uchar *enetaddr);
133 #ifdef CONFIG_RANDOM_MACADDR
134 /*
135  * The u-boot policy does not allow hardcoded ethernet addresses. Under the
136  * following circumstances a random generated address is allowed:
137  *  - in emergency cases, where you need a working network connection to set
138  *    the ethernet address.
139  *    Eg. you want a rescue boot and don't have a serial port to access the
140  *    CLI to set environment variables.
141  *
142  * In these cases, we generate a random locally administered ethernet address.
143  *
144  * Args:
145  *  enetaddr - returns 6 byte hardware address
146  */
147 extern void eth_random_enetaddr(uchar *enetaddr);
148 #endif
150 extern int usb_eth_initialize(bd_t *bi);
151 extern int eth_init(bd_t *bis);                 /* Initialize the device */
152 extern int eth_send(void *packet, int length);     /* Send a packet */
154 #ifdef CONFIG_API
155 extern int eth_receive(void *packet, int length); /* Receive a packet*/
156 extern void (*push_packet)(void *packet, int length);
157 #endif
158 extern int eth_rx(void);                        /* Check for received packets */
159 extern void eth_halt(void);                     /* stop SCC */
160 extern char *eth_get_name(void);                /* get name of current device */
162 /* Set active state */
163 static inline __attribute__((always_inline)) int eth_init_state_only(bd_t *bis)
165         eth_get_dev()->state = ETH_STATE_ACTIVE;
167         return 0;
169 /* Set passive state */
170 static inline __attribute__((always_inline)) void eth_halt_state_only(void)
172         eth_get_dev()->state = ETH_STATE_PASSIVE;
175 /*
176  * Set the hardware address for an ethernet interface based on 'eth%daddr'
177  * environment variable (or just 'ethaddr' if eth_number is 0).
178  * Args:
179  *      base_name - base name for device (normally "eth")
180  *      eth_number - value of %d (0 for first device of this type)
181  * Returns:
182  *      0 is success, non-zero is error status from driver.
183  */
184 int eth_write_hwaddr(struct eth_device *dev, const char *base_name,
185                      int eth_number);
187 #ifdef CONFIG_MCAST_TFTP
188 int eth_mcast_join(IPaddr_t mcast_addr, u8 join);
189 u32 ether_crc(size_t len, unsigned char const *p);
190 #endif
193 /**********************************************************************/
194 /*
195  *      Protocol headers.
196  */
198 /*
199  *      Ethernet header
200  */
202 struct ethernet_hdr {
203         uchar           et_dest[6];     /* Destination node             */
204         uchar           et_src[6];      /* Source node                  */
205         ushort          et_protlen;     /* Protocol or length           */
206 };
208 /* Ethernet header size */
209 #define ETHER_HDR_SIZE  (sizeof(struct ethernet_hdr))
211 struct e802_hdr {
212         uchar           et_dest[6];     /* Destination node             */
213         uchar           et_src[6];      /* Source node                  */
214         ushort          et_protlen;     /* Protocol or length           */
215         uchar           et_dsap;        /* 802 DSAP                     */
216         uchar           et_ssap;        /* 802 SSAP                     */
217         uchar           et_ctl;         /* 802 control                  */
218         uchar           et_snap1;       /* SNAP                         */
219         uchar           et_snap2;
220         uchar           et_snap3;
221         ushort          et_prot;        /* 802 protocol                 */
222 };
224 /* 802 + SNAP + ethernet header size */
225 #define E802_HDR_SIZE   (sizeof(struct e802_hdr))
227 /*
228  *      Virtual LAN Ethernet header
229  */
230 struct vlan_ethernet_hdr {
231         uchar           vet_dest[6];    /* Destination node             */
232         uchar           vet_src[6];     /* Source node                  */
233         ushort          vet_vlan_type;  /* PROT_VLAN                    */
234         ushort          vet_tag;        /* TAG of VLAN                  */
235         ushort          vet_type;       /* protocol type                */
236 };
238 /* VLAN Ethernet header size */
239 #define VLAN_ETHER_HDR_SIZE     (sizeof(struct vlan_ethernet_hdr))
241 #define PROT_IP         0x0800          /* IP protocol                  */
242 #define PROT_ARP        0x0806          /* IP ARP protocol              */
243 #define PROT_RARP       0x8035          /* IP ARP protocol              */
244 #define PROT_VLAN       0x8100          /* IEEE 802.1q protocol         */
246 #define IPPROTO_ICMP     1      /* Internet Control Message Protocol    */
247 #define IPPROTO_UDP     17      /* User Datagram Protocol               */
249 /*
250  *      Internet Protocol (IP) header.
251  */
252 struct ip_hdr {
253         uchar           ip_hl_v;        /* header length and version    */
254         uchar           ip_tos;         /* type of service              */
255         ushort          ip_len;         /* total length                 */
256         ushort          ip_id;          /* identification               */
257         ushort          ip_off;         /* fragment offset field        */
258         uchar           ip_ttl;         /* time to live                 */
259         uchar           ip_p;           /* protocol                     */
260         ushort          ip_sum;         /* checksum                     */
261         IPaddr_t        ip_src;         /* Source IP address            */
262         IPaddr_t        ip_dst;         /* Destination IP address       */
263 };
265 #define IP_OFFS         0x1fff /* ip offset *= 8 */
266 #define IP_FLAGS        0xe000 /* first 3 bits */
267 #define IP_FLAGS_RES    0x8000 /* reserved */
268 #define IP_FLAGS_DFRAG  0x4000 /* don't fragments */
269 #define IP_FLAGS_MFRAG  0x2000 /* more fragments */
271 #define IP_HDR_SIZE             (sizeof(struct ip_hdr))
273 /*
274  *      Internet Protocol (IP) + UDP header.
275  */
276 struct ip_udp_hdr {
277         uchar           ip_hl_v;        /* header length and version    */
278         uchar           ip_tos;         /* type of service              */
279         ushort          ip_len;         /* total length                 */
280         ushort          ip_id;          /* identification               */
281         ushort          ip_off;         /* fragment offset field        */
282         uchar           ip_ttl;         /* time to live                 */
283         uchar           ip_p;           /* protocol                     */
284         ushort          ip_sum;         /* checksum                     */
285         IPaddr_t        ip_src;         /* Source IP address            */
286         IPaddr_t        ip_dst;         /* Destination IP address       */
287         ushort          udp_src;        /* UDP source port              */
288         ushort          udp_dst;        /* UDP destination port         */
289         ushort          udp_len;        /* Length of UDP packet         */
290         ushort          udp_xsum;       /* Checksum                     */
291 };
293 #define IP_UDP_HDR_SIZE         (sizeof(struct ip_udp_hdr))
294 #define UDP_HDR_SIZE            (IP_UDP_HDR_SIZE - IP_HDR_SIZE)
296 /*
297  *      Address Resolution Protocol (ARP) header.
298  */
299 struct arp_hdr {
300         ushort          ar_hrd;         /* Format of hardware address   */
301 #   define ARP_ETHER        1           /* Ethernet  hardware address   */
302         ushort          ar_pro;         /* Format of protocol address   */
303         uchar           ar_hln;         /* Length of hardware address   */
304 #   define ARP_HLEN     6
305         uchar           ar_pln;         /* Length of protocol address   */
306 #   define ARP_PLEN     4
307         ushort          ar_op;          /* Operation                    */
308 #   define ARPOP_REQUEST    1           /* Request  to resolve  address */
309 #   define ARPOP_REPLY      2           /* Response to previous request */
311 #   define RARPOP_REQUEST   3           /* Request  to resolve  address */
312 #   define RARPOP_REPLY     4           /* Response to previous request */
314         /*
315          * The remaining fields are variable in size, according to
316          * the sizes above, and are defined as appropriate for
317          * specific hardware/protocol combinations.
318          */
319         uchar           ar_data[0];
320 #define ar_sha          ar_data[0]
321 #define ar_spa          ar_data[ARP_HLEN]
322 #define ar_tha          ar_data[ARP_HLEN + ARP_PLEN]
323 #define ar_tpa          ar_data[ARP_HLEN + ARP_PLEN + ARP_HLEN]
324 #if 0
325         uchar           ar_sha[];       /* Sender hardware address      */
326         uchar           ar_spa[];       /* Sender protocol address      */
327         uchar           ar_tha[];       /* Target hardware address      */
328         uchar           ar_tpa[];       /* Target protocol address      */
329 #endif /* 0 */
330 };
332 #define ARP_HDR_SIZE    (8+20)          /* Size assuming ethernet       */
334 /*
335  * ICMP stuff (just enough to handle (host) redirect messages)
336  */
337 #define ICMP_ECHO_REPLY         0       /* Echo reply                   */
338 #define ICMP_NOT_REACH          3       /* Detination unreachable       */
339 #define ICMP_REDIRECT           5       /* Redirect (change route)      */
340 #define ICMP_ECHO_REQUEST       8       /* Echo request                 */
342 /* Codes for REDIRECT. */
343 #define ICMP_REDIR_NET          0       /* Redirect Net                 */
344 #define ICMP_REDIR_HOST         1       /* Redirect Host                */
346 /* Codes for NOT_REACH */
347 #define ICMP_NOT_REACH_PORT     3       /* Port unreachable             */
349 struct icmp_hdr {
350         uchar           type;
351         uchar           code;
352         ushort          checksum;
353         union {
354                 struct {
355                         ushort  id;
356                         ushort  sequence;
357                 } echo;
358                 ulong   gateway;
359                 struct {
360                         ushort  __unused;
361                         ushort  mtu;
362                 } frag;
363                 uchar data[0];
364         } un;
365 };
367 #define ICMP_HDR_SIZE           (sizeof(struct icmp_hdr))
368 #define IP_ICMP_HDR_SIZE        (IP_HDR_SIZE + ICMP_HDR_SIZE)
370 /*
371  * Maximum packet size; used to allocate packet storage.
372  * TFTP packets can be 524 bytes + IP header + ethernet header.
373  * Lets be conservative, and go for 38 * 16.  (Must also be
374  * a multiple of 32 bytes).
375  */
376 /*
377  * AS.HARNOIS : Better to set PKTSIZE to maximum size because
378  * traffic type is not always controlled
379  * maximum packet size =  1518
380  * maximum packet size and multiple of 32 bytes =  1536
381  */
382 #define PKTSIZE                 1518
383 #define PKTSIZE_ALIGN           1536
384 /*#define PKTSIZE               608*/
386 /*
387  * Maximum receive ring size; that is, the number of packets
388  * we can buffer before overflow happens. Basically, this just
389  * needs to be enough to prevent a packet being discarded while
390  * we are processing the previous one.
391  */
392 #define RINGSZ          4
393 #define RINGSZ_LOG2     2
395 /**********************************************************************/
396 /*
397  *      Globals.
398  *
399  * Note:
400  *
401  * All variables of type IPaddr_t are stored in NETWORK byte order
402  * (big endian).
403  */
405 /* net.c */
406 /** BOOTP EXTENTIONS **/
407 extern IPaddr_t NetOurGatewayIP;        /* Our gateway IP address */
408 extern IPaddr_t NetOurSubnetMask;       /* Our subnet mask (0 = unknown) */
409 extern IPaddr_t NetOurDNSIP;    /* Our Domain Name Server (0 = unknown) */
410 #if defined(CONFIG_BOOTP_DNS2)
411 extern IPaddr_t NetOurDNS2IP;   /* Our 2nd Domain Name Server (0 = unknown) */
412 #endif
413 extern char     NetOurNISDomain[32];    /* Our NIS domain */
414 extern char     NetOurHostName[32];     /* Our hostname */
415 extern char     NetOurRootPath[64];     /* Our root path */
416 extern ushort   NetBootFileSize;        /* Our boot file size in blocks */
417 /** END OF BOOTP EXTENTIONS **/
418 extern ulong            NetBootFileXferSize;    /* size of bootfile in bytes */
419 extern uchar            NetOurEther[6];         /* Our ethernet address */
420 extern uchar            NetServerEther[6];      /* Boot server enet address */
421 extern IPaddr_t         NetOurIP;       /* Our    IP addr (0 = unknown) */
422 extern IPaddr_t         NetServerIP;    /* Server IP addr (0 = unknown) */
423 extern uchar            *NetTxPacket;           /* THE transmit packet */
424 extern uchar            *NetRxPackets[PKTBUFSRX]; /* Receive packets */
425 extern uchar            *NetRxPacket;           /* Current receive packet */
426 extern int              NetRxPacketLen;         /* Current rx packet length */
427 extern unsigned         NetIPID;                /* IP ID (counting) */
428 extern uchar            NetBcastAddr[6];        /* Ethernet boardcast address */
429 extern uchar            NetEtherNullAddr[6];
431 #define VLAN_NONE       4095                    /* untagged */
432 #define VLAN_IDMASK     0x0fff                  /* mask of valid vlan id */
433 extern ushort           NetOurVLAN;             /* Our VLAN */
434 extern ushort           NetOurNativeVLAN;       /* Our Native VLAN */
436 extern int              NetRestartWrap;         /* Tried all network devices */
438 enum proto_t {
439         BOOTP, RARP, ARP, TFTPGET, DHCP, PING, DNS, NFS, CDP, NETCONS, SNTP,
440         TFTPSRV, TFTPPUT, LINKLOCAL
441 };
443 /* from net/net.c */
444 extern char     BootFile[128];                  /* Boot File name */
446 #if defined(CONFIG_CMD_DNS)
447 extern char *NetDNSResolve;             /* The host to resolve  */
448 extern char *NetDNSenvvar;              /* the env var to put the ip into */
449 #endif
451 #if defined(CONFIG_CMD_PING)
452 extern IPaddr_t NetPingIP;                      /* the ip address to ping */
453 #endif
455 #if defined(CONFIG_CMD_CDP)
456 /* when CDP completes these hold the return values */
457 extern ushort CDPNativeVLAN;            /* CDP returned native VLAN */
458 extern ushort CDPApplianceVLAN;         /* CDP returned appliance VLAN */
460 /*
461  * Check for a CDP packet by examining the received MAC address field
462  */
463 static inline int is_cdp_packet(const uchar *et_addr)
465         extern const uchar NetCDPAddr[6];
467         return memcmp(et_addr, NetCDPAddr, 6) == 0;
469 #endif
471 #if defined(CONFIG_CMD_SNTP)
472 extern IPaddr_t NetNtpServerIP;                 /* the ip address to NTP */
473 extern int NetTimeOffset;                       /* offset time from UTC */
474 #endif
476 #if defined(CONFIG_MCAST_TFTP)
477 extern IPaddr_t Mcast_addr;
478 #endif
480 /* Initialize the network adapter */
481 extern void net_init(void);
482 extern int NetLoop(enum proto_t);
484 /* Shutdown adapters and cleanup */
485 extern void     NetStop(void);
487 /* Load failed.  Start again. */
488 extern void     NetStartAgain(void);
490 /* Get size of the ethernet header when we send */
491 extern int      NetEthHdrSize(void);
493 /* Set ethernet header; returns the size of the header */
494 extern int NetSetEther(uchar *, uchar *, uint);
495 extern int net_update_ether(struct ethernet_hdr *et, uchar *addr, uint prot);
497 /* Set IP header */
498 extern void net_set_ip_header(uchar *pkt, IPaddr_t dest, IPaddr_t source);
499 extern void net_set_udp_header(uchar *pkt, IPaddr_t dest, int dport,
500                                 int sport, int len);
502 /* Checksum */
503 extern int      NetCksumOk(uchar *, int);       /* Return true if cksum OK */
504 extern uint     NetCksum(uchar *, int);         /* Calculate the checksum */
506 /* Callbacks */
507 extern rxhand_f *net_get_udp_handler(void);     /* Get UDP RX packet handler */
508 extern void net_set_udp_handler(rxhand_f *);    /* Set UDP RX packet handler */
509 extern rxhand_f *net_get_arp_handler(void);     /* Get ARP RX packet handler */
510 extern void net_set_arp_handler(rxhand_f *);    /* Set ARP RX packet handler */
511 extern void net_set_icmp_handler(rxhand_icmp_f *f); /* Set ICMP RX handler */
512 extern void     NetSetTimeout(ulong, thand_f *);/* Set timeout handler */
514 /* Network loop state */
515 enum net_loop_state {
516         NETLOOP_CONTINUE,
517         NETLOOP_RESTART,
518         NETLOOP_SUCCESS,
519         NETLOOP_FAIL
520 };
521 extern enum net_loop_state net_state;
523 static inline void net_set_state(enum net_loop_state state)
525         debug_cond(DEBUG_INT_STATE, "--- NetState set to %d\n", state);
526         net_state = state;
529 /* Transmit a packet */
530 static inline void NetSendPacket(uchar *pkt, int len)
532         (void) eth_send(pkt, len);
535 /*
536  * Transmit "NetTxPacket" as UDP packet, performing ARP request if needed
537  *  (ether will be populated)
538  *
539  * @param ether Raw packet buffer
540  * @param dest IP address to send the datagram to
541  * @param dport Destination UDP port
542  * @param sport Source UDP port
543  * @param payload_len Length of data after the UDP header
544  */
545 extern int NetSendUDPPacket(uchar *ether, IPaddr_t dest, int dport,
546                         int sport, int payload_len);
548 /* Processes a received packet */
549 extern void NetReceive(uchar *, int);
551 #ifdef CONFIG_NETCONSOLE
552 void NcStart(void);
553 int nc_input_packet(uchar *pkt, IPaddr_t src_ip, unsigned dest_port,
554         unsigned src_port, unsigned len);
555 #endif
557 static inline __attribute__((always_inline)) int eth_is_on_demand_init(void)
559 #ifdef CONFIG_NETCONSOLE
560         extern enum proto_t net_loop_last_protocol;
562         return net_loop_last_protocol != NETCONS;
563 #else
564         return 1;
565 #endif
568 static inline void eth_set_last_protocol(int protocol)
570 #ifdef CONFIG_NETCONSOLE
571         extern enum proto_t net_loop_last_protocol;
573         net_loop_last_protocol = protocol;
574 #endif
577 /*
578  * Check if autoload is enabled. If so, use either NFS or TFTP to download
579  * the boot file.
580  */
581 void net_auto_load(void);
583 /*
584  * The following functions are a bit ugly, but necessary to deal with
585  * alignment restrictions on ARM.
586  *
587  * We're using inline functions, which had the smallest memory
588  * footprint in our tests.
589  */
590 /* return IP *in network byteorder* */
591 static inline IPaddr_t NetReadIP(void *from)
593         IPaddr_t ip;
595         memcpy((void *)&ip, (void *)from, sizeof(ip));
596         return ip;
599 /* return ulong *in network byteorder* */
600 static inline ulong NetReadLong(ulong *from)
602         ulong l;
604         memcpy((void *)&l, (void *)from, sizeof(l));
605         return l;
608 /* write IP *in network byteorder* */
609 static inline void NetWriteIP(void *to, IPaddr_t ip)
611         memcpy(to, (void *)&ip, sizeof(ip));
614 /* copy IP */
615 static inline void NetCopyIP(void *to, void *from)
617         memcpy((void *)to, from, sizeof(IPaddr_t));
620 /* copy ulong */
621 static inline void NetCopyLong(ulong *to, ulong *from)
623         memcpy((void *)to, (void *)from, sizeof(ulong));
626 /**
627  * is_zero_ether_addr - Determine if give Ethernet address is all zeros.
628  * @addr: Pointer to a six-byte array containing the Ethernet address
629  *
630  * Return true if the address is all zeroes.
631  */
632 static inline int is_zero_ether_addr(const u8 *addr)
634         return !(addr[0] | addr[1] | addr[2] | addr[3] | addr[4] | addr[5]);
637 /**
638  * is_multicast_ether_addr - Determine if the Ethernet address is a multicast.
639  * @addr: Pointer to a six-byte array containing the Ethernet address
640  *
641  * Return true if the address is a multicast address.
642  * By definition the broadcast address is also a multicast address.
643  */
644 static inline int is_multicast_ether_addr(const u8 *addr)
646         return 0x01 & addr[0];
649 /*
650  * is_broadcast_ether_addr - Determine if the Ethernet address is broadcast
651  * @addr: Pointer to a six-byte array containing the Ethernet address
652  *
653  * Return true if the address is the broadcast address.
654  */
655 static inline int is_broadcast_ether_addr(const u8 *addr)
657         return (addr[0] & addr[1] & addr[2] & addr[3] & addr[4] & addr[5]) ==
658                 0xff;
661 /*
662  * is_valid_ether_addr - Determine if the given Ethernet address is valid
663  * @addr: Pointer to a six-byte array containing the Ethernet address
664  *
665  * Check that the Ethernet address (MAC) is not 00:00:00:00:00:00, is not
666  * a multicast address, and is not FF:FF:FF:FF:FF:FF.
667  *
668  * Return true if the address is valid.
669  */
670 static inline int is_valid_ether_addr(const u8 *addr)
672         /* FF:FF:FF:FF:FF:FF is a multicast address so we don't need to
673          * explicitly check for it here. */
674         return !is_multicast_ether_addr(addr) && !is_zero_ether_addr(addr);
677 /* Convert an IP address to a string */
678 extern void ip_to_string(IPaddr_t x, char *s);
680 /* Convert a string to ip address */
681 extern IPaddr_t string_to_ip(const char *s);
683 /* Convert a VLAN id to a string */
684 extern void VLAN_to_string(ushort x, char *s);
686 /* Convert a string to a vlan id */
687 extern ushort string_to_VLAN(const char *s);
689 /* read a VLAN id from an environment variable */
690 extern ushort getenv_VLAN(char *);
692 /* copy a filename (allow for "..." notation, limit length) */
693 extern void copy_filename(char *dst, const char *src, int size);
695 /* get a random source port */
696 extern unsigned int random_port(void);
698 /**********************************************************************/
700 #endif /* __NET_H__ */