1 /*
2 * LiMon Monitor (LiMon) - Network.
3 *
4 * Copyright 1994 - 2000 Neil Russell.
5 * (See License)
6 *
7 *
8 * History
9 * 9/16/00 bor adapted to TQM823L/STK8xxL board, RARP/TFTP boot added
10 */
12 #ifndef __NET_H__
13 #define __NET_H__
15 #if defined(CONFIG_8xx)
16 #include <commproc.h>
17 #endif /* CONFIG_8xx */
19 #include <asm/cache.h>
20 #include <asm/byteorder.h> /* for nton* / ntoh* stuff */
22 #define DEBUG_LL_STATE 0 /* Link local state machine changes */
23 #define DEBUG_DEV_PKT 0 /* Packets or info directed to the device */
24 #define DEBUG_NET_PKT 0 /* Packets on info on the network at large */
25 #define DEBUG_INT_STATE 0 /* Internal network state changes */
27 /*
28 * The number of receive packet buffers, and the required packet buffer
29 * alignment in memory.
30 *
31 */
33 #ifdef CONFIG_SYS_RX_ETH_BUFFER
34 # define PKTBUFSRX CONFIG_SYS_RX_ETH_BUFFER
35 #else
36 # define PKTBUFSRX 4
37 #endif
39 #define PKTALIGN ARCH_DMA_MINALIGN
41 /* IPv4 addresses are always 32 bits in size */
42 typedef u32 IPaddr_t;
45 /**
46 * An incoming packet handler.
47 * @param pkt pointer to the application packet
48 * @param dport destination UDP port
49 * @param sip source IP address
50 * @param sport source UDP port
51 * @param len packet length
52 */
53 typedef void rxhand_f(uchar *pkt, unsigned dport,
54 IPaddr_t sip, unsigned sport,
55 unsigned len);
57 /**
58 * An incoming ICMP packet handler.
59 * @param type ICMP type
60 * @param code ICMP code
61 * @param dport destination UDP port
62 * @param sip source IP address
63 * @param sport source UDP port
64 * @param pkt pointer to the ICMP packet data
65 * @param len packet length
66 */
67 typedef void rxhand_icmp_f(unsigned type, unsigned code, unsigned dport,
68 IPaddr_t sip, unsigned sport, uchar *pkt, unsigned len);
70 /*
71 * A timeout handler. Called after time interval has expired.
72 */
73 typedef void thand_f(void);
75 enum eth_state_t {
76 ETH_STATE_INIT,
77 ETH_STATE_PASSIVE,
78 ETH_STATE_ACTIVE
79 };
81 struct eth_device {
82 char name[16];
83 unsigned char enetaddr[6];
84 int iobase;
85 int state;
87 int (*init) (struct eth_device *, bd_t *);
88 int (*send) (struct eth_device *, void *packet, int length);
89 int (*recv) (struct eth_device *);
90 void (*halt) (struct eth_device *);
91 #ifdef CONFIG_MCAST_TFTP
92 int (*mcast) (struct eth_device *, u32 ip, u8 set);
93 #endif
94 int (*write_hwaddr) (struct eth_device *);
95 struct eth_device *next;
96 int index;
97 void *priv;
98 };
100 extern int eth_initialize(bd_t *bis); /* Initialize network subsystem */
101 extern int eth_register(struct eth_device* dev);/* Register network device */
102 extern int eth_unregister(struct eth_device *dev);/* Remove network device */
103 extern void eth_try_another(int first_restart); /* Change the device */
104 extern void eth_set_current(void); /* set nterface to ethcur var */
106 /* get the current device MAC */
107 extern struct eth_device *eth_current;
109 static inline __attribute__((always_inline))
110 struct eth_device *eth_get_dev(void)
111 {
112 return eth_current;
113 }
114 extern struct eth_device *eth_get_dev_by_name(const char *devname);
115 extern struct eth_device *eth_get_dev_by_index(int index); /* get dev @ index */
116 extern int eth_get_dev_index(void); /* get the device index */
117 extern void eth_parse_enetaddr(const char *addr, uchar *enetaddr);
118 extern int eth_getenv_enetaddr(char *name, uchar *enetaddr);
119 extern int eth_setenv_enetaddr(char *name, const uchar *enetaddr);
121 /*
122 * Get the hardware address for an ethernet interface .
123 * Args:
124 * base_name - base name for device (normally "eth")
125 * index - device index number (0 for first)
126 * enetaddr - returns 6 byte hardware address
127 * Returns:
128 * Return true if the address is valid.
129 */
130 extern int eth_getenv_enetaddr_by_index(const char *base_name, int index,
131 uchar *enetaddr);
133 #ifdef CONFIG_RANDOM_MACADDR
134 /*
135 * The u-boot policy does not allow hardcoded ethernet addresses. Under the
136 * following circumstances a random generated address is allowed:
137 * - in emergency cases, where you need a working network connection to set
138 * the ethernet address.
139 * Eg. you want a rescue boot and don't have a serial port to access the
140 * CLI to set environment variables.
141 *
142 * In these cases, we generate a random locally administered ethernet address.
143 *
144 * Args:
145 * enetaddr - returns 6 byte hardware address
146 */
147 extern void eth_random_enetaddr(uchar *enetaddr);
148 #endif
150 extern int usb_eth_initialize(bd_t *bi);
151 extern int eth_init(bd_t *bis); /* Initialize the device */
152 extern int eth_send(void *packet, int length); /* Send a packet */
154 #ifdef CONFIG_API
155 extern int eth_receive(void *packet, int length); /* Receive a packet*/
156 extern void (*push_packet)(void *packet, int length);
157 #endif
158 extern int eth_rx(void); /* Check for received packets */
159 extern void eth_halt(void); /* stop SCC */
160 extern char *eth_get_name(void); /* get name of current device */
162 /* Set active state */
163 static inline __attribute__((always_inline)) int eth_init_state_only(bd_t *bis)
164 {
165 eth_get_dev()->state = ETH_STATE_ACTIVE;
167 return 0;
168 }
169 /* Set passive state */
170 static inline __attribute__((always_inline)) void eth_halt_state_only(void)
171 {
172 eth_get_dev()->state = ETH_STATE_PASSIVE;
173 }
175 /*
176 * Set the hardware address for an ethernet interface based on 'eth%daddr'
177 * environment variable (or just 'ethaddr' if eth_number is 0).
178 * Args:
179 * base_name - base name for device (normally "eth")
180 * eth_number - value of %d (0 for first device of this type)
181 * Returns:
182 * 0 is success, non-zero is error status from driver.
183 */
184 int eth_write_hwaddr(struct eth_device *dev, const char *base_name,
185 int eth_number);
187 #ifdef CONFIG_MCAST_TFTP
188 int eth_mcast_join(IPaddr_t mcast_addr, u8 join);
189 u32 ether_crc(size_t len, unsigned char const *p);
190 #endif
193 /**********************************************************************/
194 /*
195 * Protocol headers.
196 */
198 /*
199 * Ethernet header
200 */
202 struct ethernet_hdr {
203 uchar et_dest[6]; /* Destination node */
204 uchar et_src[6]; /* Source node */
205 ushort et_protlen; /* Protocol or length */
206 };
208 /* Ethernet header size */
209 #define ETHER_HDR_SIZE (sizeof(struct ethernet_hdr))
211 struct e802_hdr {
212 uchar et_dest[6]; /* Destination node */
213 uchar et_src[6]; /* Source node */
214 ushort et_protlen; /* Protocol or length */
215 uchar et_dsap; /* 802 DSAP */
216 uchar et_ssap; /* 802 SSAP */
217 uchar et_ctl; /* 802 control */
218 uchar et_snap1; /* SNAP */
219 uchar et_snap2;
220 uchar et_snap3;
221 ushort et_prot; /* 802 protocol */
222 };
224 /* 802 + SNAP + ethernet header size */
225 #define E802_HDR_SIZE (sizeof(struct e802_hdr))
227 /*
228 * Virtual LAN Ethernet header
229 */
230 struct vlan_ethernet_hdr {
231 uchar vet_dest[6]; /* Destination node */
232 uchar vet_src[6]; /* Source node */
233 ushort vet_vlan_type; /* PROT_VLAN */
234 ushort vet_tag; /* TAG of VLAN */
235 ushort vet_type; /* protocol type */
236 };
238 /* VLAN Ethernet header size */
239 #define VLAN_ETHER_HDR_SIZE (sizeof(struct vlan_ethernet_hdr))
241 #define PROT_IP 0x0800 /* IP protocol */
242 #define PROT_ARP 0x0806 /* IP ARP protocol */
243 #define PROT_RARP 0x8035 /* IP ARP protocol */
244 #define PROT_VLAN 0x8100 /* IEEE 802.1q protocol */
246 #define IPPROTO_ICMP 1 /* Internet Control Message Protocol */
247 #define IPPROTO_UDP 17 /* User Datagram Protocol */
249 /*
250 * Internet Protocol (IP) header.
251 */
252 struct ip_hdr {
253 uchar ip_hl_v; /* header length and version */
254 uchar ip_tos; /* type of service */
255 ushort ip_len; /* total length */
256 ushort ip_id; /* identification */
257 ushort ip_off; /* fragment offset field */
258 uchar ip_ttl; /* time to live */
259 uchar ip_p; /* protocol */
260 ushort ip_sum; /* checksum */
261 IPaddr_t ip_src; /* Source IP address */
262 IPaddr_t ip_dst; /* Destination IP address */
263 };
265 #define IP_OFFS 0x1fff /* ip offset *= 8 */
266 #define IP_FLAGS 0xe000 /* first 3 bits */
267 #define IP_FLAGS_RES 0x8000 /* reserved */
268 #define IP_FLAGS_DFRAG 0x4000 /* don't fragments */
269 #define IP_FLAGS_MFRAG 0x2000 /* more fragments */
271 #define IP_HDR_SIZE (sizeof(struct ip_hdr))
273 /*
274 * Internet Protocol (IP) + UDP header.
275 */
276 struct ip_udp_hdr {
277 uchar ip_hl_v; /* header length and version */
278 uchar ip_tos; /* type of service */
279 ushort ip_len; /* total length */
280 ushort ip_id; /* identification */
281 ushort ip_off; /* fragment offset field */
282 uchar ip_ttl; /* time to live */
283 uchar ip_p; /* protocol */
284 ushort ip_sum; /* checksum */
285 IPaddr_t ip_src; /* Source IP address */
286 IPaddr_t ip_dst; /* Destination IP address */
287 ushort udp_src; /* UDP source port */
288 ushort udp_dst; /* UDP destination port */
289 ushort udp_len; /* Length of UDP packet */
290 ushort udp_xsum; /* Checksum */
291 };
293 #define IP_UDP_HDR_SIZE (sizeof(struct ip_udp_hdr))
294 #define UDP_HDR_SIZE (IP_UDP_HDR_SIZE - IP_HDR_SIZE)
296 /*
297 * Address Resolution Protocol (ARP) header.
298 */
299 struct arp_hdr {
300 ushort ar_hrd; /* Format of hardware address */
301 # define ARP_ETHER 1 /* Ethernet hardware address */
302 ushort ar_pro; /* Format of protocol address */
303 uchar ar_hln; /* Length of hardware address */
304 # define ARP_HLEN 6
305 uchar ar_pln; /* Length of protocol address */
306 # define ARP_PLEN 4
307 ushort ar_op; /* Operation */
308 # define ARPOP_REQUEST 1 /* Request to resolve address */
309 # define ARPOP_REPLY 2 /* Response to previous request */
311 # define RARPOP_REQUEST 3 /* Request to resolve address */
312 # define RARPOP_REPLY 4 /* Response to previous request */
314 /*
315 * The remaining fields are variable in size, according to
316 * the sizes above, and are defined as appropriate for
317 * specific hardware/protocol combinations.
318 */
319 uchar ar_data[0];
320 #define ar_sha ar_data[0]
321 #define ar_spa ar_data[ARP_HLEN]
322 #define ar_tha ar_data[ARP_HLEN + ARP_PLEN]
323 #define ar_tpa ar_data[ARP_HLEN + ARP_PLEN + ARP_HLEN]
324 #if 0
325 uchar ar_sha[]; /* Sender hardware address */
326 uchar ar_spa[]; /* Sender protocol address */
327 uchar ar_tha[]; /* Target hardware address */
328 uchar ar_tpa[]; /* Target protocol address */
329 #endif /* 0 */
330 };
332 #define ARP_HDR_SIZE (8+20) /* Size assuming ethernet */
334 /*
335 * ICMP stuff (just enough to handle (host) redirect messages)
336 */
337 #define ICMP_ECHO_REPLY 0 /* Echo reply */
338 #define ICMP_NOT_REACH 3 /* Detination unreachable */
339 #define ICMP_REDIRECT 5 /* Redirect (change route) */
340 #define ICMP_ECHO_REQUEST 8 /* Echo request */
342 /* Codes for REDIRECT. */
343 #define ICMP_REDIR_NET 0 /* Redirect Net */
344 #define ICMP_REDIR_HOST 1 /* Redirect Host */
346 /* Codes for NOT_REACH */
347 #define ICMP_NOT_REACH_PORT 3 /* Port unreachable */
349 struct icmp_hdr {
350 uchar type;
351 uchar code;
352 ushort checksum;
353 union {
354 struct {
355 ushort id;
356 ushort sequence;
357 } echo;
358 ulong gateway;
359 struct {
360 ushort __unused;
361 ushort mtu;
362 } frag;
363 uchar data[0];
364 } un;
365 };
367 #define ICMP_HDR_SIZE (sizeof(struct icmp_hdr))
368 #define IP_ICMP_HDR_SIZE (IP_HDR_SIZE + ICMP_HDR_SIZE)
370 /*
371 * Maximum packet size; used to allocate packet storage.
372 * TFTP packets can be 524 bytes + IP header + ethernet header.
373 * Lets be conservative, and go for 38 * 16. (Must also be
374 * a multiple of 32 bytes).
375 */
376 /*
377 * AS.HARNOIS : Better to set PKTSIZE to maximum size because
378 * traffic type is not always controlled
379 * maximum packet size = 1518
380 * maximum packet size and multiple of 32 bytes = 1536
381 */
382 #define PKTSIZE 1518
383 #define PKTSIZE_ALIGN 1536
384 /*#define PKTSIZE 608*/
386 /*
387 * Maximum receive ring size; that is, the number of packets
388 * we can buffer before overflow happens. Basically, this just
389 * needs to be enough to prevent a packet being discarded while
390 * we are processing the previous one.
391 */
392 #define RINGSZ 4
393 #define RINGSZ_LOG2 2
395 /**********************************************************************/
396 /*
397 * Globals.
398 *
399 * Note:
400 *
401 * All variables of type IPaddr_t are stored in NETWORK byte order
402 * (big endian).
403 */
405 /* net.c */
406 /** BOOTP EXTENTIONS **/
407 extern IPaddr_t NetOurGatewayIP; /* Our gateway IP address */
408 extern IPaddr_t NetOurSubnetMask; /* Our subnet mask (0 = unknown) */
409 extern IPaddr_t NetOurDNSIP; /* Our Domain Name Server (0 = unknown) */
410 #if defined(CONFIG_BOOTP_DNS2)
411 extern IPaddr_t NetOurDNS2IP; /* Our 2nd Domain Name Server (0 = unknown) */
412 #endif
413 extern char NetOurNISDomain[32]; /* Our NIS domain */
414 extern char NetOurHostName[32]; /* Our hostname */
415 extern char NetOurRootPath[64]; /* Our root path */
416 extern ushort NetBootFileSize; /* Our boot file size in blocks */
417 /** END OF BOOTP EXTENTIONS **/
418 extern ulong NetBootFileXferSize; /* size of bootfile in bytes */
419 extern uchar NetOurEther[6]; /* Our ethernet address */
420 extern uchar NetServerEther[6]; /* Boot server enet address */
421 extern IPaddr_t NetOurIP; /* Our IP addr (0 = unknown) */
422 extern IPaddr_t NetServerIP; /* Server IP addr (0 = unknown) */
423 extern uchar *NetTxPacket; /* THE transmit packet */
424 extern uchar *NetRxPackets[PKTBUFSRX]; /* Receive packets */
425 extern uchar *NetRxPacket; /* Current receive packet */
426 extern int NetRxPacketLen; /* Current rx packet length */
427 extern unsigned NetIPID; /* IP ID (counting) */
428 extern uchar NetBcastAddr[6]; /* Ethernet boardcast address */
429 extern uchar NetEtherNullAddr[6];
431 #define VLAN_NONE 4095 /* untagged */
432 #define VLAN_IDMASK 0x0fff /* mask of valid vlan id */
433 extern ushort NetOurVLAN; /* Our VLAN */
434 extern ushort NetOurNativeVLAN; /* Our Native VLAN */
436 extern int NetRestartWrap; /* Tried all network devices */
438 enum proto_t {
439 BOOTP, RARP, ARP, TFTPGET, DHCP, PING, DNS, NFS, CDP, NETCONS, SNTP,
440 TFTPSRV, TFTPPUT, LINKLOCAL
441 };
443 /* from net/net.c */
444 extern char BootFile[128]; /* Boot File name */
446 #if defined(CONFIG_CMD_DNS)
447 extern char *NetDNSResolve; /* The host to resolve */
448 extern char *NetDNSenvvar; /* the env var to put the ip into */
449 #endif
451 #if defined(CONFIG_CMD_PING)
452 extern IPaddr_t NetPingIP; /* the ip address to ping */
453 #endif
455 #if defined(CONFIG_CMD_CDP)
456 /* when CDP completes these hold the return values */
457 extern ushort CDPNativeVLAN; /* CDP returned native VLAN */
458 extern ushort CDPApplianceVLAN; /* CDP returned appliance VLAN */
460 /*
461 * Check for a CDP packet by examining the received MAC address field
462 */
463 static inline int is_cdp_packet(const uchar *et_addr)
464 {
465 extern const uchar NetCDPAddr[6];
467 return memcmp(et_addr, NetCDPAddr, 6) == 0;
468 }
469 #endif
471 #if defined(CONFIG_CMD_SNTP)
472 extern IPaddr_t NetNtpServerIP; /* the ip address to NTP */
473 extern int NetTimeOffset; /* offset time from UTC */
474 #endif
476 #if defined(CONFIG_MCAST_TFTP)
477 extern IPaddr_t Mcast_addr;
478 #endif
480 /* Initialize the network adapter */
481 extern void net_init(void);
482 extern int NetLoop(enum proto_t);
484 /* Shutdown adapters and cleanup */
485 extern void NetStop(void);
487 /* Load failed. Start again. */
488 extern void NetStartAgain(void);
490 /* Get size of the ethernet header when we send */
491 extern int NetEthHdrSize(void);
493 /* Set ethernet header; returns the size of the header */
494 extern int NetSetEther(uchar *, uchar *, uint);
495 extern int net_update_ether(struct ethernet_hdr *et, uchar *addr, uint prot);
497 /* Set IP header */
498 extern void net_set_ip_header(uchar *pkt, IPaddr_t dest, IPaddr_t source);
499 extern void net_set_udp_header(uchar *pkt, IPaddr_t dest, int dport,
500 int sport, int len);
502 /* Checksum */
503 extern int NetCksumOk(uchar *, int); /* Return true if cksum OK */
504 extern uint NetCksum(uchar *, int); /* Calculate the checksum */
506 /* Callbacks */
507 extern rxhand_f *net_get_udp_handler(void); /* Get UDP RX packet handler */
508 extern void net_set_udp_handler(rxhand_f *); /* Set UDP RX packet handler */
509 extern rxhand_f *net_get_arp_handler(void); /* Get ARP RX packet handler */
510 extern void net_set_arp_handler(rxhand_f *); /* Set ARP RX packet handler */
511 extern void net_set_icmp_handler(rxhand_icmp_f *f); /* Set ICMP RX handler */
512 extern void NetSetTimeout(ulong, thand_f *);/* Set timeout handler */
514 /* Network loop state */
515 enum net_loop_state {
516 NETLOOP_CONTINUE,
517 NETLOOP_RESTART,
518 NETLOOP_SUCCESS,
519 NETLOOP_FAIL
520 };
521 extern enum net_loop_state net_state;
523 static inline void net_set_state(enum net_loop_state state)
524 {
525 debug_cond(DEBUG_INT_STATE, "--- NetState set to %d\n", state);
526 net_state = state;
527 }
529 /* Transmit a packet */
530 static inline void NetSendPacket(uchar *pkt, int len)
531 {
532 (void) eth_send(pkt, len);
533 }
535 /*
536 * Transmit "NetTxPacket" as UDP packet, performing ARP request if needed
537 * (ether will be populated)
538 *
539 * @param ether Raw packet buffer
540 * @param dest IP address to send the datagram to
541 * @param dport Destination UDP port
542 * @param sport Source UDP port
543 * @param payload_len Length of data after the UDP header
544 */
545 extern int NetSendUDPPacket(uchar *ether, IPaddr_t dest, int dport,
546 int sport, int payload_len);
548 /* Processes a received packet */
549 extern void NetReceive(uchar *, int);
551 #ifdef CONFIG_NETCONSOLE
552 void NcStart(void);
553 int nc_input_packet(uchar *pkt, IPaddr_t src_ip, unsigned dest_port,
554 unsigned src_port, unsigned len);
555 #endif
557 static inline __attribute__((always_inline)) int eth_is_on_demand_init(void)
558 {
559 #ifdef CONFIG_NETCONSOLE
560 extern enum proto_t net_loop_last_protocol;
562 return net_loop_last_protocol != NETCONS;
563 #else
564 return 1;
565 #endif
566 }
568 static inline void eth_set_last_protocol(int protocol)
569 {
570 #ifdef CONFIG_NETCONSOLE
571 extern enum proto_t net_loop_last_protocol;
573 net_loop_last_protocol = protocol;
574 #endif
575 }
577 /*
578 * Check if autoload is enabled. If so, use either NFS or TFTP to download
579 * the boot file.
580 */
581 void net_auto_load(void);
583 /*
584 * The following functions are a bit ugly, but necessary to deal with
585 * alignment restrictions on ARM.
586 *
587 * We're using inline functions, which had the smallest memory
588 * footprint in our tests.
589 */
590 /* return IP *in network byteorder* */
591 static inline IPaddr_t NetReadIP(void *from)
592 {
593 IPaddr_t ip;
595 memcpy((void *)&ip, (void *)from, sizeof(ip));
596 return ip;
597 }
599 /* return ulong *in network byteorder* */
600 static inline ulong NetReadLong(ulong *from)
601 {
602 ulong l;
604 memcpy((void *)&l, (void *)from, sizeof(l));
605 return l;
606 }
608 /* write IP *in network byteorder* */
609 static inline void NetWriteIP(void *to, IPaddr_t ip)
610 {
611 memcpy(to, (void *)&ip, sizeof(ip));
612 }
614 /* copy IP */
615 static inline void NetCopyIP(void *to, void *from)
616 {
617 memcpy((void *)to, from, sizeof(IPaddr_t));
618 }
620 /* copy ulong */
621 static inline void NetCopyLong(ulong *to, ulong *from)
622 {
623 memcpy((void *)to, (void *)from, sizeof(ulong));
624 }
626 /**
627 * is_zero_ether_addr - Determine if give Ethernet address is all zeros.
628 * @addr: Pointer to a six-byte array containing the Ethernet address
629 *
630 * Return true if the address is all zeroes.
631 */
632 static inline int is_zero_ether_addr(const u8 *addr)
633 {
634 return !(addr[0] | addr[1] | addr[2] | addr[3] | addr[4] | addr[5]);
635 }
637 /**
638 * is_multicast_ether_addr - Determine if the Ethernet address is a multicast.
639 * @addr: Pointer to a six-byte array containing the Ethernet address
640 *
641 * Return true if the address is a multicast address.
642 * By definition the broadcast address is also a multicast address.
643 */
644 static inline int is_multicast_ether_addr(const u8 *addr)
645 {
646 return 0x01 & addr[0];
647 }
649 /*
650 * is_broadcast_ether_addr - Determine if the Ethernet address is broadcast
651 * @addr: Pointer to a six-byte array containing the Ethernet address
652 *
653 * Return true if the address is the broadcast address.
654 */
655 static inline int is_broadcast_ether_addr(const u8 *addr)
656 {
657 return (addr[0] & addr[1] & addr[2] & addr[3] & addr[4] & addr[5]) ==
658 0xff;
659 }
661 /*
662 * is_valid_ether_addr - Determine if the given Ethernet address is valid
663 * @addr: Pointer to a six-byte array containing the Ethernet address
664 *
665 * Check that the Ethernet address (MAC) is not 00:00:00:00:00:00, is not
666 * a multicast address, and is not FF:FF:FF:FF:FF:FF.
667 *
668 * Return true if the address is valid.
669 */
670 static inline int is_valid_ether_addr(const u8 *addr)
671 {
672 /* FF:FF:FF:FF:FF:FF is a multicast address so we don't need to
673 * explicitly check for it here. */
674 return !is_multicast_ether_addr(addr) && !is_zero_ether_addr(addr);
675 }
677 /* Convert an IP address to a string */
678 extern void ip_to_string(IPaddr_t x, char *s);
680 /* Convert a string to ip address */
681 extern IPaddr_t string_to_ip(const char *s);
683 /* Convert a VLAN id to a string */
684 extern void VLAN_to_string(ushort x, char *s);
686 /* Convert a string to a vlan id */
687 extern ushort string_to_VLAN(const char *s);
689 /* read a VLAN id from an environment variable */
690 extern ushort getenv_VLAN(char *);
692 /* copy a filename (allow for "..." notation, limit length) */
693 extern void copy_filename(char *dst, const char *src, int size);
695 /* get a random source port */
696 extern unsigned int random_port(void);
698 /**********************************************************************/
700 #endif /* __NET_H__ */