]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/phy.h
Merge 'u-boot-microblaze/mainline/arm' into 'u-boot-arm/master'
[glsdk/glsdk-u-boot.git] / include / phy.h
1 /*
2  * Copyright 2011 Freescale Semiconductor, Inc.
3  *      Andy Fleming <afleming@freescale.com>
4  *
5  * This program is free software; you can redistribute it and/or
6  * modify it under the terms of the GNU General Public License as
7  * published by the Free Software Foundation; either version 2 of
8  * the License, or (at your option) any later version.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
13  * GNU General Public License for more details.
14  *
15  * You should have received a copy of the GNU General Public License
16  * along with this program; if not, write to the Free Software
17  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18  * MA 02111-1307 USA
19  *
20  * This file pretty much stolen from Linux's mii.h/ethtool.h/phy.h
21  */
23 #ifndef _PHY_H
24 #define _PHY_H
26 #include <linux/list.h>
27 #include <linux/mii.h>
28 #include <linux/ethtool.h>
29 #include <linux/mdio.h>
31 #define PHY_MAX_ADDR 32
33 #define PHY_BASIC_FEATURES      (SUPPORTED_10baseT_Half | \
34                                  SUPPORTED_10baseT_Full | \
35                                  SUPPORTED_100baseT_Half | \
36                                  SUPPORTED_100baseT_Full | \
37                                  SUPPORTED_Autoneg | \
38                                  SUPPORTED_TP | \
39                                  SUPPORTED_MII)
41 #define PHY_GBIT_FEATURES       (PHY_BASIC_FEATURES | \
42                                  SUPPORTED_1000baseT_Half | \
43                                  SUPPORTED_1000baseT_Full)
45 #define PHY_10G_FEATURES        (PHY_GBIT_FEATURES | \
46                                 SUPPORTED_10000baseT_Full)
48 #define PHY_ANEG_TIMEOUT        4000
51 typedef enum {
52         PHY_INTERFACE_MODE_MII,
53         PHY_INTERFACE_MODE_GMII,
54         PHY_INTERFACE_MODE_SGMII,
55         PHY_INTERFACE_MODE_TBI,
56         PHY_INTERFACE_MODE_RMII,
57         PHY_INTERFACE_MODE_RGMII,
58         PHY_INTERFACE_MODE_RGMII_ID,
59         PHY_INTERFACE_MODE_RGMII_RXID,
60         PHY_INTERFACE_MODE_RGMII_TXID,
61         PHY_INTERFACE_MODE_RTBI,
62         PHY_INTERFACE_MODE_XGMII,
63         PHY_INTERFACE_MODE_NONE /* Must be last */
64 } phy_interface_t;
66 static const char *phy_interface_strings[] = {
67         [PHY_INTERFACE_MODE_MII]                = "mii",
68         [PHY_INTERFACE_MODE_GMII]               = "gmii",
69         [PHY_INTERFACE_MODE_SGMII]              = "sgmii",
70         [PHY_INTERFACE_MODE_TBI]                = "tbi",
71         [PHY_INTERFACE_MODE_RMII]               = "rmii",
72         [PHY_INTERFACE_MODE_RGMII]              = "rgmii",
73         [PHY_INTERFACE_MODE_RGMII_ID]           = "rgmii-id",
74         [PHY_INTERFACE_MODE_RGMII_RXID]         = "rgmii-rxid",
75         [PHY_INTERFACE_MODE_RGMII_TXID]         = "rgmii-txid",
76         [PHY_INTERFACE_MODE_RTBI]               = "rtbi",
77         [PHY_INTERFACE_MODE_XGMII]              = "xgmii",
78         [PHY_INTERFACE_MODE_NONE]               = "",
79 };
81 static inline const char *phy_string_for_interface(phy_interface_t i)
82 {
83         /* Default to unknown */
84         if (i > PHY_INTERFACE_MODE_NONE)
85                 i = PHY_INTERFACE_MODE_NONE;
87         return phy_interface_strings[i];
88 }
91 struct phy_device;
93 #define MDIO_NAME_LEN 32
95 struct mii_dev {
96         struct list_head link;
97         char name[MDIO_NAME_LEN];
98         void *priv;
99         int (*read)(struct mii_dev *bus, int addr, int devad, int reg);
100         int (*write)(struct mii_dev *bus, int addr, int devad, int reg,
101                         u16 val);
102         int (*reset)(struct mii_dev *bus);
103         struct phy_device *phymap[PHY_MAX_ADDR];
104         u32 phy_mask;
105 };
107 /* struct phy_driver: a structure which defines PHY behavior
108  *
109  * uid will contain a number which represents the PHY.  During
110  * startup, the driver will poll the PHY to find out what its
111  * UID--as defined by registers 2 and 3--is.  The 32-bit result
112  * gotten from the PHY will be masked to
113  * discard any bits which may change based on revision numbers
114  * unimportant to functionality
115  *
116  */
117 struct phy_driver {
118         char *name;
119         unsigned int uid;
120         unsigned int mask;
121         unsigned int mmds;
123         u32 features;
125         /* Called to do any driver startup necessities */
126         /* Will be called during phy_connect */
127         int (*probe)(struct phy_device *phydev);
129         /* Called to configure the PHY, and modify the controller
130          * based on the results.  Should be called after phy_connect */
131         int (*config)(struct phy_device *phydev);
133         /* Called when starting up the controller */
134         int (*startup)(struct phy_device *phydev);
136         /* Called when bringing down the controller */
137         int (*shutdown)(struct phy_device *phydev);
139         struct list_head list;
140 };
142 struct phy_device {
143         /* Information about the PHY type */
144         /* And management functions */
145         struct mii_dev *bus;
146         struct phy_driver *drv;
147         void *priv;
149         struct eth_device *dev;
151         /* forced speed & duplex (no autoneg)
152          * partner speed & duplex & pause (autoneg)
153          */
154         int speed;
155         int duplex;
157         /* The most recently read link state */
158         int link;
159         int port;
160         phy_interface_t interface;
162         u32 advertising;
163         u32 supported;
164         u32 mmds;
166         int autoneg;
167         int addr;
168         int pause;
169         int asym_pause;
170         u32 phy_id;
171         u32 flags;
172 };
174 static inline int phy_read(struct phy_device *phydev, int devad, int regnum)
176         struct mii_dev *bus = phydev->bus;
178         return bus->read(bus, phydev->addr, devad, regnum);
181 static inline int phy_write(struct phy_device *phydev, int devad, int regnum,
182                         u16 val)
184         struct mii_dev *bus = phydev->bus;
186         return bus->write(bus, phydev->addr, devad, regnum, val);
189 #ifdef CONFIG_PHYLIB_10G
190 extern struct phy_driver gen10g_driver;
192 /* For now, XGMII is the only 10G interface */
193 static inline int is_10g_interface(phy_interface_t interface)
195         return interface == PHY_INTERFACE_MODE_XGMII;
198 #endif
200 int phy_init(void);
201 int phy_reset(struct phy_device *phydev);
202 struct phy_device *phy_find_by_mask(struct mii_dev *bus, unsigned phy_mask,
203                 phy_interface_t interface);
204 void phy_connect_dev(struct phy_device *phydev, struct eth_device *dev);
205 struct phy_device *phy_connect(struct mii_dev *bus, int addr,
206                                 struct eth_device *dev,
207                                 phy_interface_t interface);
208 int phy_startup(struct phy_device *phydev);
209 int phy_config(struct phy_device *phydev);
210 int phy_shutdown(struct phy_device *phydev);
211 int phy_register(struct phy_driver *drv);
212 int genphy_config_aneg(struct phy_device *phydev);
213 int genphy_restart_aneg(struct phy_device *phydev);
214 int genphy_update_link(struct phy_device *phydev);
215 int genphy_config(struct phy_device *phydev);
216 int genphy_startup(struct phy_device *phydev);
217 int genphy_shutdown(struct phy_device *phydev);
218 int gen10g_config(struct phy_device *phydev);
219 int gen10g_startup(struct phy_device *phydev);
220 int gen10g_shutdown(struct phy_device *phydev);
221 int gen10g_discover_mmds(struct phy_device *phydev);
223 int phy_atheros_init(void);
224 int phy_broadcom_init(void);
225 int phy_davicom_init(void);
226 int phy_lxt_init(void);
227 int phy_marvell_init(void);
228 int phy_micrel_init(void);
229 int phy_natsemi_init(void);
230 int phy_realtek_init(void);
231 int phy_smsc_init(void);
232 int phy_teranetics_init(void);
233 int phy_vitesse_init(void);
235 /* PHY UIDs for various PHYs that are referenced in external code */
236 #define PHY_UID_TN2020  0x00a19410
238 #endif