1 /*
2 * Copyright 2011 Freescale Semiconductor, Inc.
3 * Andy Fleming <afleming@freescale.com>
4 *
5 * This program is free software; you can redistribute it and/or
6 * modify it under the terms of the GNU General Public License as
7 * published by the Free Software Foundation; either version 2 of
8 * the License, or (at your option) any later version.
9 *
10 * This program is distributed in the hope that it will be useful,
11 * but WITHOUT ANY WARRANTY; without even the implied warranty of
12 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
13 * GNU General Public License for more details.
14 *
15 * You should have received a copy of the GNU General Public License
16 * along with this program; if not, write to the Free Software
17 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
18 * MA 02111-1307 USA
19 *
20 * This file pretty much stolen from Linux's mii.h/ethtool.h/phy.h
21 */
23 #ifndef _PHY_H
24 #define _PHY_H
26 #include <linux/list.h>
27 #include <linux/mii.h>
28 #include <linux/ethtool.h>
29 #include <linux/mdio.h>
31 #define PHY_MAX_ADDR 32
33 #define PHY_BASIC_FEATURES (SUPPORTED_10baseT_Half | \
34 SUPPORTED_10baseT_Full | \
35 SUPPORTED_100baseT_Half | \
36 SUPPORTED_100baseT_Full | \
37 SUPPORTED_Autoneg | \
38 SUPPORTED_TP | \
39 SUPPORTED_MII)
41 #define PHY_GBIT_FEATURES (PHY_BASIC_FEATURES | \
42 SUPPORTED_1000baseT_Half | \
43 SUPPORTED_1000baseT_Full)
45 #define PHY_10G_FEATURES (PHY_GBIT_FEATURES | \
46 SUPPORTED_10000baseT_Full)
48 #define PHY_ANEG_TIMEOUT 4000
51 typedef enum {
52 PHY_INTERFACE_MODE_MII,
53 PHY_INTERFACE_MODE_GMII,
54 PHY_INTERFACE_MODE_SGMII,
55 PHY_INTERFACE_MODE_TBI,
56 PHY_INTERFACE_MODE_RMII,
57 PHY_INTERFACE_MODE_RGMII,
58 PHY_INTERFACE_MODE_RGMII_ID,
59 PHY_INTERFACE_MODE_RGMII_RXID,
60 PHY_INTERFACE_MODE_RGMII_TXID,
61 PHY_INTERFACE_MODE_RTBI,
62 PHY_INTERFACE_MODE_XGMII,
63 PHY_INTERFACE_MODE_NONE /* Must be last */
64 } phy_interface_t;
66 static const char *phy_interface_strings[] = {
67 [PHY_INTERFACE_MODE_MII] = "mii",
68 [PHY_INTERFACE_MODE_GMII] = "gmii",
69 [PHY_INTERFACE_MODE_SGMII] = "sgmii",
70 [PHY_INTERFACE_MODE_TBI] = "tbi",
71 [PHY_INTERFACE_MODE_RMII] = "rmii",
72 [PHY_INTERFACE_MODE_RGMII] = "rgmii",
73 [PHY_INTERFACE_MODE_RGMII_ID] = "rgmii-id",
74 [PHY_INTERFACE_MODE_RGMII_RXID] = "rgmii-rxid",
75 [PHY_INTERFACE_MODE_RGMII_TXID] = "rgmii-txid",
76 [PHY_INTERFACE_MODE_RTBI] = "rtbi",
77 [PHY_INTERFACE_MODE_XGMII] = "xgmii",
78 [PHY_INTERFACE_MODE_NONE] = "",
79 };
81 static inline const char *phy_string_for_interface(phy_interface_t i)
82 {
83 /* Default to unknown */
84 if (i > PHY_INTERFACE_MODE_NONE)
85 i = PHY_INTERFACE_MODE_NONE;
87 return phy_interface_strings[i];
88 }
91 struct phy_device;
93 #define MDIO_NAME_LEN 32
95 struct mii_dev {
96 struct list_head link;
97 char name[MDIO_NAME_LEN];
98 void *priv;
99 int (*read)(struct mii_dev *bus, int addr, int devad, int reg);
100 int (*write)(struct mii_dev *bus, int addr, int devad, int reg,
101 u16 val);
102 int (*reset)(struct mii_dev *bus);
103 struct phy_device *phymap[PHY_MAX_ADDR];
104 u32 phy_mask;
105 };
107 /* struct phy_driver: a structure which defines PHY behavior
108 *
109 * uid will contain a number which represents the PHY. During
110 * startup, the driver will poll the PHY to find out what its
111 * UID--as defined by registers 2 and 3--is. The 32-bit result
112 * gotten from the PHY will be masked to
113 * discard any bits which may change based on revision numbers
114 * unimportant to functionality
115 *
116 */
117 struct phy_driver {
118 char *name;
119 unsigned int uid;
120 unsigned int mask;
121 unsigned int mmds;
123 u32 features;
125 /* Called to do any driver startup necessities */
126 /* Will be called during phy_connect */
127 int (*probe)(struct phy_device *phydev);
129 /* Called to configure the PHY, and modify the controller
130 * based on the results. Should be called after phy_connect */
131 int (*config)(struct phy_device *phydev);
133 /* Called when starting up the controller */
134 int (*startup)(struct phy_device *phydev);
136 /* Called when bringing down the controller */
137 int (*shutdown)(struct phy_device *phydev);
139 struct list_head list;
140 };
142 struct phy_device {
143 /* Information about the PHY type */
144 /* And management functions */
145 struct mii_dev *bus;
146 struct phy_driver *drv;
147 void *priv;
149 struct eth_device *dev;
151 /* forced speed & duplex (no autoneg)
152 * partner speed & duplex & pause (autoneg)
153 */
154 int speed;
155 int duplex;
157 /* The most recently read link state */
158 int link;
159 int port;
160 phy_interface_t interface;
162 u32 advertising;
163 u32 supported;
164 u32 mmds;
166 int autoneg;
167 int addr;
168 int pause;
169 int asym_pause;
170 u32 phy_id;
171 u32 flags;
172 };
174 static inline int phy_read(struct phy_device *phydev, int devad, int regnum)
175 {
176 struct mii_dev *bus = phydev->bus;
178 return bus->read(bus, phydev->addr, devad, regnum);
179 }
181 static inline int phy_write(struct phy_device *phydev, int devad, int regnum,
182 u16 val)
183 {
184 struct mii_dev *bus = phydev->bus;
186 return bus->write(bus, phydev->addr, devad, regnum, val);
187 }
189 #ifdef CONFIG_PHYLIB_10G
190 extern struct phy_driver gen10g_driver;
192 /* For now, XGMII is the only 10G interface */
193 static inline int is_10g_interface(phy_interface_t interface)
194 {
195 return interface == PHY_INTERFACE_MODE_XGMII;
196 }
198 #endif
200 int phy_init(void);
201 int phy_reset(struct phy_device *phydev);
202 struct phy_device *phy_find_by_mask(struct mii_dev *bus, unsigned phy_mask,
203 phy_interface_t interface);
204 void phy_connect_dev(struct phy_device *phydev, struct eth_device *dev);
205 struct phy_device *phy_connect(struct mii_dev *bus, int addr,
206 struct eth_device *dev,
207 phy_interface_t interface);
208 int phy_startup(struct phy_device *phydev);
209 int phy_config(struct phy_device *phydev);
210 int phy_shutdown(struct phy_device *phydev);
211 int phy_register(struct phy_driver *drv);
212 int genphy_config_aneg(struct phy_device *phydev);
213 int genphy_restart_aneg(struct phy_device *phydev);
214 int genphy_update_link(struct phy_device *phydev);
215 int genphy_config(struct phy_device *phydev);
216 int genphy_startup(struct phy_device *phydev);
217 int genphy_shutdown(struct phy_device *phydev);
218 int gen10g_config(struct phy_device *phydev);
219 int gen10g_startup(struct phy_device *phydev);
220 int gen10g_shutdown(struct phy_device *phydev);
221 int gen10g_discover_mmds(struct phy_device *phydev);
223 int phy_atheros_init(void);
224 int phy_broadcom_init(void);
225 int phy_davicom_init(void);
226 int phy_lxt_init(void);
227 int phy_marvell_init(void);
228 int phy_micrel_init(void);
229 int phy_natsemi_init(void);
230 int phy_realtek_init(void);
231 int phy_smsc_init(void);
232 int phy_teranetics_init(void);
233 int phy_vitesse_init(void);
235 /* PHY UIDs for various PHYs that are referenced in external code */
236 #define PHY_UID_TN2020 0x00a19410
238 #endif