]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/s_record.h
ARM: DRA7xx: Lock DPLL_GMAC
[glsdk/glsdk-u-boot.git] / include / s_record.h
1 /*
2  * (C) Copyright 2000
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 /*--------------------------------------------------------------------------
25  *
26  * Motorola S-Record Format:
27  *
28  * Motorola S-Records are an industry-standard format for
29  * transmitting binary files to target systems and PROM
30  * programmers. LSI Logic have extended this standard to include
31  * an S4-record containing an address and a symbol.
32  *
33  * The extended S-record standard is as follows:
34  *
35  * S<type><length><address><data....><checksum>
36  * S4<length><address><name>,<checksum>
37  *
38  * Where:
39  *
40  * type
41  *     is the record type. Where:
42  *
43  *     0  starting record (optional)
44  *     1  data record with 16-bit address
45  *     2  data record with 24-bit address
46  *     3  data record with 32-bit address
47  *     4  symbol record (LSI extension)
48  *     5  number of data records in preceeding block
49  *     6  unused
50  *     7  ending record for S3 records
51  *     8  ending record for S2 records
52  *     9  ending record for S1 records
53  *
54  * length
55  *     is two hex characters. This defines the length of the
56  *     record in bytes (not characters). It includes the address
57  *     field, the data field, and the checksum field.
58  *
59  * address
60  *     is 4, 6, or 8 characters. Corresponding to a 16-, 24-, or
61  *     32-bit address. The address field for S4 records is
62  *     always 32 bits.
63  *
64  * data
65  *
66  *     Are the data bytes. Each pair of hex characters represent
67  *     one byte in memory.
68  *
69  * name
70  *     Is the symbol name. The symbol is terminated by a ','.
71  *
72  * checksum
73  *     Is the one's complement of the 8-bit checksum.
74  *
75  * Example
76  *
77  * S0030000FC
78  * .
79  * .
80  * S325000004403C0880018D08DD900000000011000026000000003C0880012508DC50C50000B401
81  * S32500000460C50100B8C50200BCC50300C0C50400C4C50500C8C50600CCC50700D0C50800D4FA
82  * S32500000480C50900D8C50A00DCC50B00E0C50C00E4C50D00E8C50E00ECC50F00F0C51000F49A
83  * S325000004A0C51100F8C51200FCC5130100C5140104C5150108C516010CC5170110C518011434
84  * .
85  * .
86  * S70500000000FA
87  *
88  * The S0 record starts the file. The S3 records contain the
89  * data. The S7 record contains the entry address and terminates
90  * the download.
91  *
92  *--------------------------------------------------------------------------
93  */
95 #define SREC_START      0       /* Start Record (module name)               */
96 #define SREC_DATA2      1       /* Data  Record with 2 byte address         */
97 #define SREC_DATA3      2       /* Data  Record with 3 byte address         */
98 #define SREC_DATA4      3       /* Data  Record with 4 byte address         */
99 #define SREC_COUNT      5       /* Count Record (previously transmitted)    */
100 #define SREC_END4       7       /* End   Record with 4 byte start address   */
101 #define SREC_END3       8       /* End   Record with 3 byte start address   */
102 #define SREC_END2       9       /* End   Record with 2 byte start address   */
103 #define SREC_EMPTY      10      /* Empty Record without any data            */
105 #define SREC_REC_OK  SREC_EMPTY /* last code without error condition        */
107 #define SREC_E_BADTYPE  -1      /* no valid S-Record                        */
108 #define SREC_E_NOSREC   -2      /* line format differs from s-record        */
109 #define SREC_E_BADCHKS  -3      /* checksum error in an s-record line       */
111 #define SREC_MAXRECLEN  (512 + 4)   /* max ASCII record length              */
112 #define SREC_MAXBINLEN  255         /* resulting binary length              */
114 int srec_decode (char *input, int *count, ulong *addr, char *data);