]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/search.h
Merge branch 'u-boot-imx/master' into 'u-boot-arm/master'
[glsdk/glsdk-u-boot.git] / include / search.h
1 /*
2  * Declarations for System V style searching functions.
3  * Copyright (C) 1995-1999, 2000 Free Software Foundation, Inc.
4  * This file is part of the GNU C Library.
5  *
6  * The GNU C Library is free software; you can redistribute it and/or
7  * modify it under the terms of the GNU Lesser General Public
8  * License as published by the Free Software Foundation; either
9  * version 2.1 of the License, or (at your option) any later version.
10  *
11  * The GNU C Library is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
14  * Lesser General Public License for more details.
15  *
16  * You should have received a copy of the GNU Lesser General Public
17  * License along with the GNU C Library; if not, write to the Free
18  * Software Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA
19  * 02111-1307 USA.
20  */
22 /*
23  * Based on code from uClibc-0.9.30.3
24  * Extensions for use within U-Boot
25  * Copyright (C) 2010 Wolfgang Denk <wd@denx.de>
26  */
28 #ifndef _SEARCH_H
29 #define _SEARCH_H 1
31 #include <stddef.h>
33 #define __set_errno(val) do { errno = val; } while (0)
35 enum env_op {
36         env_op_create,
37         env_op_delete,
38         env_op_overwrite,
39 };
41 /* Action which shall be performed in the call the hsearch.  */
42 typedef enum {
43         FIND,
44         ENTER
45 } ACTION;
47 typedef struct entry {
48         const char *key;
49         char *data;
50         int (*callback)(const char *name, const char *value, enum env_op op,
51                 int flags);
52         int flags;
53 } ENTRY;
55 /* Opaque type for internal use.  */
56 struct _ENTRY;
58 /*
59  * Family of hash table handling functions.  The functions also
60  * have reentrant counterparts ending with _r.  The non-reentrant
61  * functions all work on a signle internal hashing table.
62  */
64 /* Data type for reentrant functions.  */
65 struct hsearch_data {
66         struct _ENTRY *table;
67         unsigned int size;
68         unsigned int filled;
69 /*
70  * Callback function which will check whether the given change for variable
71  * "item" to "newval" may be applied or not, and possibly apply such change.
72  * When (flag & H_FORCE) is set, it shall not print out any error message and
73  * shall force overwriting of write-once variables.
74 .* Must return 0 for approval, 1 for denial.
75  */
76         int (*change_ok)(const ENTRY *__item, const char *newval, enum env_op,
77                 int flag);
78 };
80 /* Create a new hashing table which will at most contain NEL elements.  */
81 extern int hcreate_r(size_t __nel, struct hsearch_data *__htab);
83 /* Destroy current internal hashing table.  */
84 extern void hdestroy_r(struct hsearch_data *__htab);
86 /*
87  * Search for entry matching ITEM.key in internal hash table.  If
88  * ACTION is `FIND' return found entry or signal error by returning
89  * NULL.  If ACTION is `ENTER' replace existing data (if any) with
90  * ITEM.data.
91  * */
92 extern int hsearch_r(ENTRY __item, ACTION __action, ENTRY ** __retval,
93                      struct hsearch_data *__htab, int __flag);
95 /*
96  * Search for an entry matching `MATCH'.  Otherwise, Same semantics
97  * as hsearch_r().
98  */
99 extern int hmatch_r(const char *__match, int __last_idx, ENTRY ** __retval,
100                     struct hsearch_data *__htab);
101 /*
102  * Search for an entry whose key or data contains `MATCH'.  Otherwise,
103  * Same semantics as hsearch_r().
104  */
105 extern int hstrstr_r(const char *__match, int __last_idx, ENTRY ** __retval,
106                     struct hsearch_data *__htab);
108 /* Search and delete entry matching ITEM.key in internal hash table. */
109 extern int hdelete_r(const char *__key, struct hsearch_data *__htab,
110                      int __flag);
112 extern ssize_t hexport_r(struct hsearch_data *__htab,
113                      const char __sep, int __flag, char **__resp, size_t __size,
114                      int argc, char * const argv[]);
116 /*
117  * nvars: length of vars array
118  * vars: array of strings (variable names) to import (nvars == 0 means all)
119  * do_apply: whether to call callback function to check the new argument,
120  * and possibly apply changes (false means accept everything)
121  */
122 extern int himport_r(struct hsearch_data *__htab,
123                      const char *__env, size_t __size, const char __sep,
124                      int __flag, int nvars, char * const vars[]);
126 /* Walk the whole table calling the callback on each element */
127 extern int hwalk_r(struct hsearch_data *__htab, int (*callback)(ENTRY *));
129 /* Flags for himport_r(), hexport_r(), hdelete_r(), and hsearch_r() */
130 #define H_NOCLEAR       (1 << 0) /* do not clear hash table before importing */
131 #define H_FORCE         (1 << 1) /* overwrite read-only/write-once variables */
132 #define H_INTERACTIVE   (1 << 2) /* indicate that an import is user directed */
133 #define H_HIDE_DOT      (1 << 3) /* don't print env vars that begin with '.' */
135 #endif /* search.h */