]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - include/status_led.h
HACK: ARM: DRA7xx: Add VPE crossbar setting
[glsdk/glsdk-u-boot.git] / include / status_led.h
1 /*
2  * (C) Copyright 2000-2004
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 /*
25  * The purpose of this code is to signal the operational status of a
26  * target which usually boots over the network; while running in
27  * PCBoot, a status LED is blinking. As soon as a valid BOOTP reply
28  * message has been received, the LED is turned off. The Linux
29  * kernel, once it is running, will start blinking the LED again,
30  * with another frequency.
31  */
33 #ifndef _STATUS_LED_H_
34 #define _STATUS_LED_H_
36 #ifdef CONFIG_STATUS_LED
38 #define STATUS_LED_OFF          0
39 #define STATUS_LED_BLINKING     1
40 #define STATUS_LED_ON           2
42 void status_led_tick (unsigned long timestamp);
43 void status_led_set  (int led, int state);
45 /*****  TQM8xxL  ********************************************************/
46 #if defined(CONFIG_TQM8xxL)
47 # define STATUS_LED_PAR         im_cpm.cp_pbpar
48 # define STATUS_LED_DIR         im_cpm.cp_pbdir
49 # define STATUS_LED_ODR         im_cpm.cp_pbodr
50 # define STATUS_LED_DAT         im_cpm.cp_pbdat
52 # define STATUS_LED_BIT         0x00000001
53 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
54 # define STATUS_LED_STATE       STATUS_LED_BLINKING
56 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
58 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
60 /*****  MVS v1  **********************************************************/
61 #elif (defined(CONFIG_MVS) && CONFIG_MVS < 2)
62 # define STATUS_LED_PAR         im_ioport.iop_pdpar
63 # define STATUS_LED_DIR         im_ioport.iop_pddir
64 # undef  STATUS_LED_ODR
65 # define STATUS_LED_DAT         im_ioport.iop_pddat
67 # define STATUS_LED_BIT         0x00000001
68 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
69 # define STATUS_LED_STATE       STATUS_LED_BLINKING
71 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
73 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
75 /*****  GEN860T  *********************************************************/
76 #elif defined(CONFIG_GEN860T)
78 # define STATUS_LED_PAR                 im_ioport.iop_papar
79 # define STATUS_LED_DIR                 im_ioport.iop_padir
80 # define STATUS_LED_ODR                 im_ioport.iop_paodr
81 # define STATUS_LED_DAT                 im_ioport.iop_padat
83 # define STATUS_LED_BIT                 0x0800  /* Red LED 0 is on PA.4 */
84 # define STATUS_LED_PERIOD              (CONFIG_SYS_HZ / 4)
85 # define STATUS_LED_STATE               STATUS_LED_OFF
86 # define STATUS_LED_BIT1                0x0400  /* Grn LED 1 is on PA.5 */
87 # define STATUS_LED_PERIOD1             (CONFIG_SYS_HZ / 8)
88 # define STATUS_LED_STATE1              STATUS_LED_BLINKING
89 # define STATUS_LED_BIT2                0x0080  /* Red LED 2 is on PA.8 */
90 # define STATUS_LED_PERIOD2             (CONFIG_SYS_HZ / 4)
91 # define STATUS_LED_STATE2              STATUS_LED_OFF
92 # define STATUS_LED_BIT3                0x0040  /* Grn LED 3 is on PA.9 */
93 # define STATUS_LED_PERIOD3             (CONFIG_SYS_HZ / 4)
94 # define STATUS_LED_STATE3              STATUS_LED_OFF
96 # define STATUS_LED_ACTIVE              1       /* LED on for bit == 1  */
97 # define STATUS_LED_BOOT                1       /* Boot status on LED 1 */
99 /*****  IVMS8  **********************************************************/
100 #elif defined(CONFIG_IVMS8)
102 # define STATUS_LED_PAR         im_cpm.cp_pbpar
103 # define STATUS_LED_DIR         im_cpm.cp_pbdir
104 # define STATUS_LED_ODR         im_cpm.cp_pbodr
105 # define STATUS_LED_DAT         im_cpm.cp_pbdat
107 # define STATUS_LED_BIT         0x00000010      /* LED 0 is on PB.27    */
108 # define STATUS_LED_PERIOD      (1 * CONFIG_SYS_HZ)
109 # define STATUS_LED_STATE       STATUS_LED_OFF
110 # define STATUS_LED_BIT1        0x00000020      /* LED 1 is on PB.26    */
111 # define STATUS_LED_PERIOD1     (1 * CONFIG_SYS_HZ)
112 # define STATUS_LED_STATE1      STATUS_LED_OFF
113 /* IDE LED usable for other purposes, too */
114 # define STATUS_LED_BIT2        0x00000008      /* LED 2 is on PB.28    */
115 # define STATUS_LED_PERIOD2     (1 * CONFIG_SYS_HZ)
116 # define STATUS_LED_STATE2      STATUS_LED_OFF
118 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
120 # define STATUS_ILOCK_SWITCH    0x00800000      /* ILOCK switch in IRQ4 */
122 # define STATUS_ILOCK_PERIOD    (CONFIG_SYS_HZ / 10)    /* about every 100 ms   */
124 # define STATUS_LED_YELLOW      0
125 # define STATUS_LED_GREEN       1
126 # define STATUS_LED_BOOT        2               /* IDE LED used for boot status */
128 /*****  IVML24  *********************************************************/
129 #elif defined(CONFIG_IVML24)
131 # define STATUS_LED_PAR         im_cpm.cp_pbpar
132 # define STATUS_LED_DIR         im_cpm.cp_pbdir
133 # define STATUS_LED_ODR         im_cpm.cp_pbodr
134 # define STATUS_LED_DAT         im_cpm.cp_pbdat
136 # define STATUS_LED_BIT         0x00000010      /* LED 0 is on PB.27    */
137 # define STATUS_LED_PERIOD      (1 * CONFIG_SYS_HZ)
138 # define STATUS_LED_STATE       STATUS_LED_OFF
139 # define STATUS_LED_BIT1        0x00000020      /* LED 1 is on PB.26    */
140 # define STATUS_LED_PERIOD1     (1 * CONFIG_SYS_HZ)
141 # define STATUS_LED_STATE1      STATUS_LED_OFF
142 /* IDE LED usable for other purposes, too */
143 # define STATUS_LED_BIT2        0x00000008      /* LED 2 is on PB.28    */
144 # define STATUS_LED_PERIOD2     (1 * CONFIG_SYS_HZ)
145 # define STATUS_LED_STATE2      STATUS_LED_OFF
147 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
149 # define STATUS_ILOCK_SWITCH    0x00004000      /* ILOCK is on PB.17    */
151 # define STATUS_ILOCK_PERIOD    (CONFIG_SYS_HZ / 10)    /* about every 100 ms   */
153 # define STATUS_LED_YELLOW      0
154 # define STATUS_LED_GREEN       1
155 # define STATUS_LED_BOOT        2               /* IDE LED used for boot status */
157 /*****  ICU862   ********************************************************/
158 #elif defined(CONFIG_ICU862)
160 # define STATUS_LED_PAR         im_ioport.iop_papar
161 # define STATUS_LED_DIR         im_ioport.iop_padir
162 # define STATUS_LED_ODR         im_ioport.iop_paodr
163 # define STATUS_LED_DAT         im_ioport.iop_padat
165 # define STATUS_LED_BIT         0x4000          /* LED 0 is on PA.1 */
166 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
167 # define STATUS_LED_STATE       STATUS_LED_BLINKING
168 # define STATUS_LED_BIT1        0x1000          /* LED 1 is on PA.3 */
169 # define STATUS_LED_PERIOD1     (CONFIG_SYS_HZ)
170 # define STATUS_LED_STATE1      STATUS_LED_OFF
172 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
174 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
176 /*****  Someone else defines these  *************************************/
177 #elif defined(STATUS_LED_PAR)
179   /*
180    * ADVICE: Define in your board configuration file rather than
181    * filling this file up with lots of custom board stuff.
182    */
184 /*****  NetVia   ********************************************************/
185 #elif defined(CONFIG_NETVIA)
187 #if !defined(CONFIG_NETVIA_VERSION) || CONFIG_NETVIA_VERSION == 1
189 #define STATUS_LED_PAR          im_ioport.iop_pdpar
190 #define STATUS_LED_DIR          im_ioport.iop_pddir
191 #undef  STATUS_LED_ODR
192 #define STATUS_LED_DAT          im_ioport.iop_pddat
194 # define STATUS_LED_BIT         0x0080                  /* PD.8 */
195 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
196 # define STATUS_LED_STATE       STATUS_LED_BLINKING
198 # define STATUS_LED_BIT1        0x0040                  /* PD.9 */
199 # define STATUS_LED_PERIOD1     (CONFIG_SYS_HZ / 2)
200 # define STATUS_LED_STATE1      STATUS_LED_OFF
202 # define STATUS_LED_ACTIVE      0               /* LED on for bit == 0  */
203 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
205 #endif
207 /*****  CMI   ********************************************************/
208 #elif defined(CONFIG_CMI)
209 # define STATUS_LED_DIR         im_mios.mios_mpiosm32ddr
210 # define STATUS_LED_DAT         im_mios.mios_mpiosm32dr
212 # define STATUS_LED_BIT         0x2000          /* Select one of the 16 possible*/
213                                                 /* MIOS outputs */
214 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)     /* Blinking periode is 500 ms */
215 # define STATUS_LED_STATE       STATUS_LED_BLINKING
217 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 0  */
218 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
220 /*****  KUP4K, KUP4X  ****************************************************/
221 #elif defined(CONFIG_KUP4K) || defined(CONFIG_KUP4X)
223 # define STATUS_LED_PAR         im_ioport.iop_papar
224 # define STATUS_LED_DIR         im_ioport.iop_padir
225 # define STATUS_LED_ODR         im_ioport.iop_paodr
226 # define STATUS_LED_DAT         im_ioport.iop_padat
228 # define STATUS_LED_BIT         0x00000300  /*  green + red    PA[8]=yellow,  PA[7]=red,  PA[6]=green */
229 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
230 # define STATUS_LED_STATE       STATUS_LED_BLINKING
232 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
234 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
236 #elif defined(CONFIG_SVM_SC8xx)
237 # define STATUS_LED_PAR         im_cpm.cp_pbpar
238 # define STATUS_LED_DIR         im_cpm.cp_pbdir
239 # define STATUS_LED_ODR         im_cpm.cp_pbodr
240 # define STATUS_LED_DAT         im_cpm.cp_pbdat
242 # define STATUS_LED_BIT         0x00000001
243 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
244 # define STATUS_LED_STATE       STATUS_LED_BLINKING
246 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
248 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
250 /*****  RBC823    ********************************************************/
251 #elif defined(CONFIG_RBC823)
253 # define STATUS_LED_PAR         im_ioport.iop_pcpar
254 # define STATUS_LED_DIR         im_ioport.iop_pcdir
255 #  undef STATUS_LED_ODR
256 # define STATUS_LED_DAT         im_ioport.iop_pcdat
258 # define STATUS_LED_BIT         0x0002          /* LED 0 is on PC.14 */
259 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
260 # define STATUS_LED_STATE       STATUS_LED_BLINKING
261 # define STATUS_LED_BIT1        0x0004          /* LED 1 is on PC.13 */
262 # define STATUS_LED_PERIOD1     (CONFIG_SYS_HZ)
263 # define STATUS_LED_STATE1      STATUS_LED_OFF
265 # define STATUS_LED_ACTIVE      1               /* LED on for bit == 1  */
267 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
269 /*****  NetPhone   ********************************************************/
270 #elif defined(CONFIG_NETPHONE) || defined(CONFIG_NETTA2)
271 /* XXX empty just to avoid the error */
272 /*****  STx XTc    ********************************************************/
273 #elif defined(CONFIG_STXXTC)
274 /* XXX empty just to avoid the error */
275 /************************************************************************/
276 #elif defined(CONFIG_V38B)
278 # define STATUS_LED_BIT         0x0010                  /* Timer7 GPIO */
279 # define STATUS_LED_PERIOD      (CONFIG_SYS_HZ / 2)
280 # define STATUS_LED_STATE       STATUS_LED_BLINKING
282 # define STATUS_LED_ACTIVE      0               /* LED on for bit == 0 */
283 # define STATUS_LED_BOOT        0               /* LED 0 used for boot status */
285 #elif defined(CONFIG_MOTIONPRO)
287 #define STATUS_LED_BIT          ((vu_long *) MPC5XXX_GPT6_ENABLE)
288 #define STATUS_LED_PERIOD       (CONFIG_SYS_HZ / 10)
289 #define STATUS_LED_STATE        STATUS_LED_BLINKING
291 #define STATUS_LED_BIT1         ((vu_long *) MPC5XXX_GPT7_ENABLE)
292 #define STATUS_LED_PERIOD1      (CONFIG_SYS_HZ / 10)
293 #define STATUS_LED_STATE1       STATUS_LED_OFF
295 #define STATUS_LED_BOOT         0       /* LED 0 used for boot status */
297 #elif defined(CONFIG_BOARD_SPECIFIC_LED)
298 /* led_id_t is unsigned long mask */
299 typedef unsigned long led_id_t;
301 extern void __led_toggle (led_id_t mask);
302 extern void __led_init (led_id_t mask, int state);
303 extern void __led_set (led_id_t mask, int state);
304 #else
305 # error Status LED configuration missing
306 #endif
307 /************************************************************************/
309 #ifndef CONFIG_BOARD_SPECIFIC_LED
310 # include <asm/status_led.h>
311 #endif
313 /*
314  * Coloured LEDs API
315  */
316 #ifndef __ASSEMBLY__
317 extern void     coloured_LED_init (void);
318 extern void     red_led_on(void);
319 extern void     red_led_off(void);
320 extern void     green_led_on(void);
321 extern void     green_led_off(void);
322 extern void     yellow_led_on(void);
323 extern void     yellow_led_off(void);
324 extern void     blue_led_on(void);
325 extern void     blue_led_off(void);
326 #else
327         .extern LED_init
328         .extern red_led_on
329         .extern red_led_off
330         .extern yellow_led_on
331         .extern yellow_led_off
332         .extern green_led_on
333         .extern green_led_off
334         .extern blue_led_on
335         .extern blue_led_off
336 #endif
338 #endif  /* CONFIG_STATUS_LED    */
340 #endif  /* _STATUS_LED_H_       */