1 /*
2 * Copyright (c) 2013 The Chromium OS Authors.
3 *
4 * See file CREDITS for list of people who contributed to this
5 * project.
6 *
7 * This program is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU General Public License as
9 * published by the Free Software Foundation; either version 2 of
10 * the License, or (at your option) any later version.
11 *
12 * This program is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15 * GNU General Public License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with this program; if not, write to the Free Software
19 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20 * MA 02111-1307 USA
21 */
23 #ifndef __TPM_H
24 #define __TPM_H
26 #include <tis.h>
28 /*
29 * Here is a partial implementation of TPM commands. Please consult TCG Main
30 * Specification for definitions of TPM commands.
31 */
33 enum tpm_startup_type {
34 TPM_ST_CLEAR = 0x0001,
35 TPM_ST_STATE = 0x0002,
36 TPM_ST_DEACTIVATED = 0x0003,
37 };
39 enum tpm_physical_presence {
40 TPM_PHYSICAL_PRESENCE_HW_DISABLE = 0x0200,
41 TPM_PHYSICAL_PRESENCE_CMD_DISABLE = 0x0100,
42 TPM_PHYSICAL_PRESENCE_LIFETIME_LOCK = 0x0080,
43 TPM_PHYSICAL_PRESENCE_HW_ENABLE = 0x0040,
44 TPM_PHYSICAL_PRESENCE_CMD_ENABLE = 0x0020,
45 TPM_PHYSICAL_PRESENCE_NOTPRESENT = 0x0010,
46 TPM_PHYSICAL_PRESENCE_PRESENT = 0x0008,
47 TPM_PHYSICAL_PRESENCE_LOCK = 0x0004,
48 };
50 enum tpm_nv_index {
51 TPM_NV_INDEX_LOCK = 0xffffffff,
52 TPM_NV_INDEX_0 = 0x00000000,
53 TPM_NV_INDEX_DIR = 0x10000001,
54 };
56 /**
57 * Initialize TPM device. It must be called before any TPM commands.
58 *
59 * @return 0 on success, non-0 on error.
60 */
61 uint32_t tpm_init(void);
63 /**
64 * Issue a TPM_Startup command.
65 *
66 * @param mode TPM startup mode
67 * @return return code of the operation
68 */
69 uint32_t tpm_startup(enum tpm_startup_type mode);
71 /**
72 * Issue a TPM_SelfTestFull command.
73 *
74 * @return return code of the operation
75 */
76 uint32_t tpm_self_test_full(void);
78 /**
79 * Issue a TPM_ContinueSelfTest command.
80 *
81 * @return return code of the operation
82 */
83 uint32_t tpm_continue_self_test(void);
85 /**
86 * Issue a TPM_NV_DefineSpace command. The implementation is limited
87 * to specify TPM_NV_ATTRIBUTES and size of the area. The area index
88 * could be one of the special value listed in enum tpm_nv_index.
89 *
90 * @param index index of the area
91 * @param perm TPM_NV_ATTRIBUTES of the area
92 * @param size size of the area
93 * @return return code of the operation
94 */
95 uint32_t tpm_nv_define_space(uint32_t index, uint32_t perm, uint32_t size);
97 /**
98 * Issue a TPM_NV_ReadValue command. This implementation is limited
99 * to read the area from offset 0. The area index could be one of
100 * the special value listed in enum tpm_nv_index.
101 *
102 * @param index index of the area
103 * @param data output buffer of the area contents
104 * @param count size of output buffer
105 * @return return code of the operation
106 */
107 uint32_t tpm_nv_read_value(uint32_t index, void *data, uint32_t count);
109 /**
110 * Issue a TPM_NV_WriteValue command. This implementation is limited
111 * to write the area from offset 0. The area index could be one of
112 * the special value listed in enum tpm_nv_index.
113 *
114 * @param index index of the area
115 * @param data input buffer to be wrote to the area
116 * @param length length of data bytes of input buffer
117 * @return return code of the operation
118 */
119 uint32_t tpm_nv_write_value(uint32_t index, const void *data, uint32_t length);
121 /**
122 * Issue a TPM_Extend command.
123 *
124 * @param index index of the PCR
125 * @param in_digest 160-bit value representing the event to be
126 * recorded
127 * @param out_digest 160-bit PCR value after execution of the
128 * command
129 * @return return code of the operation
130 */
131 uint32_t tpm_extend(uint32_t index, const void *in_digest, void *out_digest);
133 /**
134 * Issue a TPM_PCRRead command.
135 *
136 * @param index index of the PCR
137 * @param data output buffer for contents of the named PCR
138 * @param count size of output buffer
139 * @return return code of the operation
140 */
141 uint32_t tpm_pcr_read(uint32_t index, void *data, size_t count);
143 /**
144 * Issue a TSC_PhysicalPresence command. TPM physical presence flag
145 * is bit-wise OR'ed of flags listed in enum tpm_physical_presence.
146 *
147 * @param presence TPM physical presence flag
148 * @return return code of the operation
149 */
150 uint32_t tpm_tsc_physical_presence(uint16_t presence);
152 /**
153 * Issue a TPM_ReadPubek command.
154 *
155 * @param data output buffer for the public endorsement key
156 * @param count size of ouput buffer
157 * @return return code of the operation
158 */
159 uint32_t tpm_read_pubek(void *data, size_t count);
161 /**
162 * Issue a TPM_ForceClear command.
163 *
164 * @return return code of the operation
165 */
166 uint32_t tpm_force_clear(void);
168 /**
169 * Issue a TPM_PhysicalEnable command.
170 *
171 * @return return code of the operation
172 */
173 uint32_t tpm_physical_enable(void);
175 /**
176 * Issue a TPM_PhysicalDisable command.
177 *
178 * @return return code of the operation
179 */
180 uint32_t tpm_physical_disable(void);
182 /**
183 * Issue a TPM_PhysicalSetDeactivated command.
184 *
185 * @param state boolean state of the deactivated flag
186 * @return return code of the operation
187 */
188 uint32_t tpm_physical_set_deactivated(uint8_t state);
190 /**
191 * Issue a TPM_GetCapability command. This implementation is limited
192 * to query sub_cap index that is 4-byte wide.
193 *
194 * @param cap_area partition of capabilities
195 * @param sub_cap further definition of capability, which is
196 * limited to be 4-byte wide
197 * @param cap output buffer for capability information
198 * @param count size of ouput buffer
199 * @return return code of the operation
200 */
201 uint32_t tpm_get_capability(uint32_t cap_area, uint32_t sub_cap,
202 void *cap, size_t count);
204 #endif /* __TPM_H */