ARM: DRA7xx: Lock DPLL_GMAC
[glsdk/glsdk-u-boot.git] / nand_spl / nand_boot_fsl_elbc.c
1 /*
2  * NAND boot for Freescale Enhanced Local Bus Controller, Flash Control Machine
3  *
4  * (C) Copyright 2006-2008
5  * Stefan Roese, DENX Software Engineering, sr@denx.de.
6  *
7  * Copyright (c) 2008 Freescale Semiconductor, Inc.
8  * Author: Scott Wood <scottwood@freescale.com>
9  *
10  * This program is free software; you can redistribute it and/or
11  * modify it under the terms of the GNU General Public License as
12  * published by the Free Software Foundation; either version 2 of
13  * the License, or (at your option) any later version.
14  *
15  * This program is distributed in the hope that it will be useful,
16  * but WITHOUT ANY WARRANTY; without even the implied warranty of
17  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
18  * GNU General Public License for more details.
19  *
20  * You should have received a copy of the GNU General Public License
21  * along with this program; if not, write to the Free Software
22  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23  * MA 02111-1307 USA
24  */
26 #include <common.h>
27 #include <asm/io.h>
28 #include <asm/fsl_lbc.h>
29 #include <linux/mtd/nand.h>
31 #define WINDOW_SIZE 8192
33 static void nand_wait(void)
34 {
35         fsl_lbc_t *regs = LBC_BASE_ADDR;
37         for (;;) {
38                 uint32_t status = in_be32(&regs->ltesr);
40                 if (status == 1)
41                         return;
43                 if (status & 1) {
44                         puts("read failed (ltesr)\n");
45                         for (;;);
46                 }
47         }
48 }
50 static void nand_load(unsigned int offs, int uboot_size, uchar *dst)
51 {
52         fsl_lbc_t *regs = LBC_BASE_ADDR;
53         uchar *buf = (uchar *)CONFIG_SYS_NAND_BASE;
54         const int large = CONFIG_SYS_NAND_OR_PRELIM & OR_FCM_PGS;
55         const int block_shift = large ? 17 : 14;
56         const int block_size = 1 << block_shift;
57         const int page_size = large ? 2048 : 512;
58         const int bad_marker = large ? page_size + 0 : page_size + 5;
59         int fmr = (15 << FMR_CWTO_SHIFT) | (2 << FMR_AL_SHIFT) | 2;
60         int pos = 0;
62         if (offs & (block_size - 1)) {
63                 puts("bad offset\n");
64                 for (;;);
65         }
67         if (large) {
68                 fmr |= FMR_ECCM;
69                 __raw_writel((NAND_CMD_READ0 << FCR_CMD0_SHIFT) |
70                         (NAND_CMD_READSTART << FCR_CMD1_SHIFT),
71                         &regs->fcr);
72                 __raw_writel(
73                         (FIR_OP_CW0 << FIR_OP0_SHIFT) |
74                         (FIR_OP_CA  << FIR_OP1_SHIFT) |
75                         (FIR_OP_PA  << FIR_OP2_SHIFT) |
76                         (FIR_OP_CW1 << FIR_OP3_SHIFT) |
77                         (FIR_OP_RBW << FIR_OP4_SHIFT),
78                         &regs->fir);
79         } else {
80                 __raw_writel(NAND_CMD_READ0 << FCR_CMD0_SHIFT, &regs->fcr);
81                 __raw_writel(
82                         (FIR_OP_CW0 << FIR_OP0_SHIFT) |
83                         (FIR_OP_CA  << FIR_OP1_SHIFT) |
84                         (FIR_OP_PA  << FIR_OP2_SHIFT) |
85                         (FIR_OP_RBW << FIR_OP3_SHIFT),
86                         &regs->fir);
87         }
89         __raw_writel(0, &regs->fbcr);
91         while (pos < uboot_size) {
92                 int i = 0;
93                 __raw_writel(offs >> block_shift, &regs->fbar);
95                 do {
96                         int j;
97                         unsigned int page_offs = (offs & (block_size - 1)) << 1;
99                         __raw_writel(~0, &regs->ltesr);
100                         __raw_writel(0, &regs->lteatr);
101                         __raw_writel(page_offs, &regs->fpar);
102                         __raw_writel(fmr, &regs->fmr);
103                         sync();
104                         __raw_writel(0, &regs->lsor);
105                         nand_wait();
107                         page_offs %= WINDOW_SIZE;
109                         /*
110                          * If either of the first two pages are marked bad,
111                          * continue to the next block.
112                          */
113                         if (i++ < 2 && buf[page_offs + bad_marker] != 0xff) {
114                                 puts("skipping\n");
115                                 offs = (offs + block_size) & ~(block_size - 1);
116                                 pos &= ~(block_size - 1);
117                                 break;
118                         }
120                         for (j = 0; j < page_size; j++)
121                                 dst[pos + j] = buf[page_offs + j];
123                         pos += page_size;
124                         offs += page_size;
125                 } while ((offs & (block_size - 1)) && (pos < uboot_size));
126         }
129 /*
130  * The main entry for NAND booting. It's necessary that SDRAM is already
131  * configured and available since this code loads the main U-Boot image
132  * from NAND into SDRAM and starts it from there.
133  */
134 void nand_boot(void)
136         __attribute__((noreturn)) void (*uboot)(void);
138         /*
139          * Load U-Boot image from NAND into RAM
140          */
141         nand_load(CONFIG_SYS_NAND_U_BOOT_OFFS, CONFIG_SYS_NAND_U_BOOT_SIZE,
142                   (uchar *)CONFIG_SYS_NAND_U_BOOT_DST);
144         /*
145          * Jump to U-Boot image
146          */
147         puts("transfering control\n");
148         /*
149          * Clean d-cache and invalidate i-cache, to
150          * make sure that no stale data is executed.
151          */
152         flush_cache(CONFIG_SYS_NAND_U_BOOT_DST, CONFIG_SYS_NAND_U_BOOT_SIZE);
153         uboot = (void *)CONFIG_SYS_NAND_U_BOOT_START;
154         uboot();