HACK: ARM: DRA7xx: Add Ethernet crossbar setting
[glsdk/glsdk-u-boot.git] / nand_spl / nand_boot_fsl_ifc.c
1 /*
2  * NAND boot for FSL Integrated Flash Controller, NAND Flash Control Machine
3  *
4  * Copyright 2011 Freescale Semiconductor, Inc.
5  * Author: Dipen Dudhat <dipen.dudhat@freescale.com>
6  *
7  * This program is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU General Public License as
9  * published by the Free Software Foundation; either version 2 of
10  * the License, or (at your option) any later version.
11  *
12  * This program is distributed in the hope that it will be useful,
13  * but WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.See the
15  * GNU General Public License for more details.
16  *
17  * You should have received a copy of the GNU General Public License
18  * along with this program; if not, write to the Free Software
19  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20  * MA 02111-1307 USA
21  */
23 #include <common.h>
24 #include <asm/io.h>
25 #include <asm/fsl_ifc.h>
26 #include <linux/mtd/nand.h>
28 static inline int is_blank(uchar *addr, int page_size)
29 {
30         int i;
32         for (i = 0; i < page_size; i++) {
33                 if (__raw_readb(&addr[i]) != 0xff)
34                         return 0;
35         }
37         /*
38          * For the SPL, don't worry about uncorrectable errors
39          * where the main area is all FFs but shouldn't be.
40          */
41         return 1;
42 }
44 /* returns nonzero if entire page is blank */
45 static inline int check_read_ecc(uchar *buf, u32 *eccstat,
46                                  unsigned int bufnum, int page_size)
47 {
48         u32 reg = eccstat[bufnum / 4];
49         int errors = (reg >> ((3 - bufnum % 4) * 8)) & 15;
51         if (errors == 15) { /* uncorrectable */
52                 /* Blank pages fail hw ECC checks */
53                 if (is_blank(buf, page_size))
54                         return 1;
56                 puts("ecc error\n");
57                 for (;;)
58                         ;
59         }
61         return 0;
62 }
64 static inline void nand_wait(uchar *buf, int bufnum, int page_size)
65 {
66         struct fsl_ifc *ifc = IFC_BASE_ADDR;
67         u32 status;
68         u32 eccstat[4];
69         int bufperpage = page_size / 512;
70         int bufnum_end, i;
72         bufnum *= bufperpage;
73         bufnum_end = bufnum + bufperpage - 1;
75         do {
76                 status = in_be32(&ifc->ifc_nand.nand_evter_stat);
77         } while (!(status & IFC_NAND_EVTER_STAT_OPC));
79         if (status & IFC_NAND_EVTER_STAT_FTOER) {
80                 puts("flash time out error\n");
81                 for (;;)
82                         ;
83         }
85         for (i = bufnum / 4; i <= bufnum_end / 4; i++)
86                 eccstat[i] = in_be32(&ifc->ifc_nand.nand_eccstat[i]);
88         for (i = bufnum; i <= bufnum_end; i++) {
89                 if (check_read_ecc(buf, eccstat, i, page_size))
90                         break;
91         }
93         out_be32(&ifc->ifc_nand.nand_evter_stat, status);
94 }
96 static inline int bad_block(uchar *marker, int port_size)
97 {
98         if (port_size == 8)
99                 return __raw_readb(marker) != 0xff;
100         else
101                 return __raw_readw((u16 *)marker) != 0xffff;
104 static void nand_load(unsigned int offs, int uboot_size, uchar *dst)
106         struct fsl_ifc *ifc = IFC_BASE_ADDR;
107         uchar *buf = (uchar *)CONFIG_SYS_NAND_BASE;
108         int page_size;
109         int port_size;
110         int pages_per_blk;
111         int blk_size;
112         int bad_marker = 0;
113         int bufnum_mask, bufnum;
115         int csor, cspr;
116         int pos = 0;
117         int j = 0;
119         int sram_addr;
120         int pg_no;
122         /* Get NAND Flash configuration */
123         csor = CONFIG_SYS_NAND_CSOR;
124         cspr = CONFIG_SYS_NAND_CSPR;
126         if (!(csor & CSOR_NAND_ECC_DEC_EN)) {
127                 /* soft ECC in SPL is unimplemented */
128                 puts("WARNING: soft ECC not checked in SPL\n");
129         } else {
130                 u32 hwcsor;
132                 /* make sure board is configured with ECC on boot */
133                 hwcsor = in_be32(&ifc->csor_cs[0].csor);
134                 if (!(hwcsor & CSOR_NAND_ECC_DEC_EN))
135                         puts("WARNING: ECC not checked in SPL, "
136                                 "check board cfg\n");
137         }
139         port_size = (cspr & CSPR_PORT_SIZE_16) ? 16 : 8;
141         if (csor & CSOR_NAND_PGS_4K) {
142                 page_size = 4096;
143                 bufnum_mask = 1;
144         } else if (csor & CSOR_NAND_PGS_2K) {
145                 page_size = 2048;
146                 bufnum_mask = 3;
147         } else {
148                 page_size = 512;
149                 bufnum_mask = 15;
151                 if (port_size == 8)
152                         bad_marker = 5;
153         }
155         pages_per_blk =
156                 32 << ((csor & CSOR_NAND_PB_MASK) >> CSOR_NAND_PB_SHIFT);
158         blk_size = pages_per_blk * page_size;
160         /* Open Full SRAM mapping for spare are access */
161         out_be32(&ifc->ifc_nand.ncfgr, 0x0);
163         /* Clear Boot events */
164         out_be32(&ifc->ifc_nand.nand_evter_stat, 0xffffffff);
166         /* Program FIR/FCR for Large/Small page */
167         if (page_size > 512) {
168                 out_be32(&ifc->ifc_nand.nand_fir0,
169                          (IFC_FIR_OP_CW0 << IFC_NAND_FIR0_OP0_SHIFT) |
170                          (IFC_FIR_OP_CA0 << IFC_NAND_FIR0_OP1_SHIFT) |
171                          (IFC_FIR_OP_RA0 << IFC_NAND_FIR0_OP2_SHIFT) |
172                          (IFC_FIR_OP_CMD1 << IFC_NAND_FIR0_OP3_SHIFT) |
173                          (IFC_FIR_OP_BTRD << IFC_NAND_FIR0_OP4_SHIFT));
174                 out_be32(&ifc->ifc_nand.nand_fir1, 0x0);
176                 out_be32(&ifc->ifc_nand.nand_fcr0,
177                         (NAND_CMD_READ0 << IFC_NAND_FCR0_CMD0_SHIFT) |
178                         (NAND_CMD_READSTART << IFC_NAND_FCR0_CMD1_SHIFT));
179         } else {
180                 out_be32(&ifc->ifc_nand.nand_fir0,
181                          (IFC_FIR_OP_CW0 << IFC_NAND_FIR0_OP0_SHIFT) |
182                          (IFC_FIR_OP_CA0 << IFC_NAND_FIR0_OP1_SHIFT) |
183                          (IFC_FIR_OP_RA0  << IFC_NAND_FIR0_OP2_SHIFT) |
184                          (IFC_FIR_OP_BTRD << IFC_NAND_FIR0_OP3_SHIFT));
185                 out_be32(&ifc->ifc_nand.nand_fir1, 0x0);
187                 out_be32(&ifc->ifc_nand.nand_fcr0,
188                         NAND_CMD_READ0 << IFC_NAND_FCR0_CMD0_SHIFT);
189         }
191         /* Program FBCR = 0 for full page read */
192         out_be32(&ifc->ifc_nand.nand_fbcr, 0);
194         /* Read and copy u-boot on SDRAM from NAND device, In parallel
195          * check for Bad block if found skip it and read continue to
196          * next Block
197          */
198         while (pos < uboot_size) {
199                 int i = 0;
200                 do {
201                         pg_no = offs / page_size;
202                         bufnum = pg_no & bufnum_mask;
203                         sram_addr = bufnum * page_size * 2;
205                         out_be32(&ifc->ifc_nand.row0, pg_no);
206                         out_be32(&ifc->ifc_nand.col0, 0);
207                         /* start read */
208                         out_be32(&ifc->ifc_nand.nandseq_strt,
209                                 IFC_NAND_SEQ_STRT_FIR_STRT);
211                         /* wait for read to complete */
212                         nand_wait(&buf[sram_addr], bufnum, page_size);
214                         /*
215                          * If either of the first two pages are marked bad,
216                          * continue to the next block.
217                          */
218                         if (i++ < 2 &&
219                             bad_block(&buf[sram_addr + page_size + bad_marker],
220                                       port_size)) {
221                                 puts("skipping\n");
222                                 offs = (offs + blk_size) & ~(blk_size - 1);
223                                 pos &= ~(blk_size - 1);
224                                 break;
225                         }
227                         for (j = 0; j < page_size; j++)
228                                 dst[pos + j] = __raw_readb(&buf[sram_addr + j]);
230                         pos += page_size;
231                         offs += page_size;
232                 } while ((offs & (blk_size - 1)) && (pos < uboot_size));
233         }
236 /*
237  * Main entrypoint for NAND Boot. It's necessary that SDRAM is already
238  * configured and available since this code loads the main U-boot image
239  * from NAND into SDRAM and starts from there.
240  */
241 void nand_boot(void)
243         __attribute__((noreturn)) void (*uboot)(void);
245         /*
246          * Load U-Boot image from NAND into RAM
247          */
248         nand_load(CONFIG_SYS_NAND_U_BOOT_OFFS, CONFIG_SYS_NAND_U_BOOT_SIZE,
249                   (uchar *)CONFIG_SYS_NAND_U_BOOT_DST);
251 #ifdef CONFIG_NAND_ENV_DST
252         nand_load(CONFIG_ENV_OFFSET, CONFIG_ENV_SIZE,
253                   (uchar *)CONFIG_NAND_ENV_DST);
255 #ifdef CONFIG_ENV_OFFSET_REDUND
256         nand_load(CONFIG_ENV_OFFSET_REDUND, CONFIG_ENV_SIZE,
257                   (uchar *)CONFIG_NAND_ENV_DST + CONFIG_ENV_SIZE);
258 #endif
259 #endif
261         /*
262          * Jump to U-Boot image
263          */
264         /*
265          * Clean d-cache and invalidate i-cache, to
266          * make sure that no stale data is executed.
267          */
268         flush_cache(CONFIG_SYS_NAND_U_BOOT_DST, CONFIG_SYS_NAND_U_BOOT_SIZE);
269         uboot = (void *)CONFIG_SYS_NAND_U_BOOT_START;
270         uboot();