ARM: DRA7xx: Lock DPLL_GMAC
[glsdk/glsdk-u-boot.git] / post / drivers / i2c.c
1 /*
2  * (C) Copyright 2002
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 /*
25  * I2C test
26  *
27  * For verifying the I2C bus, a full I2C bus scanning is performed.
28  *
29  * #ifdef CONFIG_SYS_POST_I2C_ADDRS
30  *   The test is considered as passed if all the devices and only the devices
31  *   in the list are found.
32  *   #ifdef CONFIG_SYS_POST_I2C_IGNORES
33  *     Ignore devices listed in CONFIG_SYS_POST_I2C_IGNORES.  These devices
34  *     are optional or not vital to board functionality.
35  *   #endif
36  * #else [ ! CONFIG_SYS_POST_I2C_ADDRS ]
37  *   The test is considered as passed if any I2C device is found.
38  * #endif
39  */
41 #include <common.h>
42 #include <post.h>
43 #include <i2c.h>
45 #if CONFIG_POST & CONFIG_SYS_POST_I2C
47 static int i2c_ignore_device(unsigned int chip)
48 {
49 #ifdef CONFIG_SYS_POST_I2C_IGNORES
50         const unsigned char i2c_ignore_list[] = CONFIG_SYS_POST_I2C_IGNORES;
51         int i;
53         for (i = 0; i < sizeof(i2c_ignore_list); i++)
54                 if (i2c_ignore_list[i] == chip)
55                         return 1;
56 #endif
58         return 0;
59 }
61 int i2c_post_test (int flags)
62 {
63         unsigned int i;
64 #ifndef CONFIG_SYS_POST_I2C_ADDRS
65         /* Start at address 1, address 0 is the general call address */
66         for (i = 1; i < 128; i++) {
67                 if (i2c_ignore_device(i))
68                         continue;
69                 if (i2c_probe (i) == 0)
70                         return 0;
71         }
73         /* No devices found */
74         return -1;
75 #else
76         unsigned int ret  = 0;
77         int j;
78         unsigned char i2c_addr_list[] = CONFIG_SYS_POST_I2C_ADDRS;
80         /* Start at address 1, address 0 is the general call address */
81         for (i = 1; i < 128; i++) {
82                 if (i2c_ignore_device(i))
83                         continue;
84                 if (i2c_probe(i) != 0)
85                         continue;
87                 for (j = 0; j < sizeof(i2c_addr_list); ++j) {
88                         if (i == i2c_addr_list[j]) {
89                                 i2c_addr_list[j] = 0xff;
90                                 break;
91                         }
92                 }
94                 if (j == sizeof(i2c_addr_list)) {
95                         ret = -1;
96                         post_log("I2C: addr %02x not expected\n", i);
97                 }
98         }
100         for (i = 0; i < sizeof(i2c_addr_list); ++i) {
101                 if (i2c_addr_list[i] == 0xff)
102                         continue;
103                 post_log("I2C: addr %02x did not respond\n", i2c_addr_list[i]);
104                 ret = -1;
105         }
107         return ret;
108 #endif
111 #endif /* CONFIG_POST & CONFIG_SYS_POST_I2C */