]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - post/drivers/i2c.c
Merge with /home/tur/git/u-boot#motionpro
[glsdk/glsdk-u-boot.git] / post / drivers / i2c.c
1 /*
2  * (C) Copyright 2002
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #include <common.h>
26 #ifdef CONFIG_POST
28 /*
29  * I2C test
30  *
31  * For verifying the I2C bus, a full I2C bus scanning is performed.
32  *
33  * #ifdef I2C_ADDR_LIST
34  *   The test is considered as passed if all the devices and
35  *   only the devices in the list are found.
36  * #else [ ! I2C_ADDR_LIST ]
37  *   The test is considered as passed if any I2C device is found.
38  * #endif
39  */
41 #include <post.h>
42 #include <i2c.h>
44 #if CONFIG_POST & CFG_POST_I2C
46 int i2c_post_test (int flags)
47 {
48         unsigned int i;
49         unsigned int good = 0;
50 #ifdef I2C_ADDR_LIST
51         unsigned int bad  = 0;
52         int j;
53         unsigned char i2c_addr_list[] = I2C_ADDR_LIST;
54         unsigned char i2c_miss_list[] = I2C_ADDR_LIST;
55 #endif
57         for (i = 0; i < 128; i++) {
58                 if (i2c_probe (i) == 0) {
59 #ifndef I2C_ADDR_LIST
60                         good++;
61 #else   /* I2C_ADDR_LIST */
62                         for (j=0; j<sizeof(i2c_addr_list); ++j) {
63                                 if (i == i2c_addr_list[j]) {
64                                         good++;
65                                         i2c_miss_list[j] = 0xFF;
66                                         break;
67                                 }
68                         }
69                         if (j == sizeof(i2c_addr_list)) {
70                                 bad++;
71                                 post_log ("I2C: addr %02X not expected\n",
72                                                 i);
73                         }
74 #endif  /* I2C_ADDR_LIST */
75                 }
76         }
78 #ifndef I2C_ADDR_LIST
79         return good > 0 ? 0 : -1;
80 #else   /* I2C_ADDR_LIST */
81         if (good != sizeof(i2c_addr_list)) {
82                 for (j=0; j<sizeof(i2c_miss_list); ++j) {
83                         if (i2c_miss_list[j] != 0xFF) {
84                                 post_log ("I2C: addr %02X did not respond\n",
85                                                 i2c_miss_list[j]);
86                         }
87                 }
88         }
89         return ((good == sizeof(i2c_addr_list)) && (bad == 0)) ? 0 : -1;
90 #endif
91 }
93 #endif /* CONFIG_POST & CFG_POST_I2C */
94 #endif /* CONFIG_POST */