1 /*
2 * (C) Copyright 2002
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #include <common.h>
26 /*
27 * CPU test
28 * Ternary instructions instr rA,rS,UIMM
29 *
30 * Logic instructions: ori, oris, xori, xoris
31 *
32 * The test contains a pre-built table of instructions, operands and
33 * expected results. For each table entry, the test will cyclically use
34 * different sets of operand registers and result registers.
35 */
37 #include <post.h>
38 #include "cpu_asm.h"
40 #if CONFIG_POST & CONFIG_SYS_POST_CPU
42 extern void cpu_post_exec_21 (ulong *code, ulong *cr, ulong *res, ulong op);
43 extern ulong cpu_post_makecr (long v);
45 static struct cpu_post_threei_s
46 {
47 ulong cmd;
48 ulong op1;
49 ushort op2;
50 ulong res;
51 } cpu_post_threei_table[] =
52 {
53 {
54 OP_ORI,
55 0x80000000,
56 0xffff,
57 0x8000ffff
58 },
59 {
60 OP_ORIS,
61 0x00008000,
62 0xffff,
63 0xffff8000
64 },
65 {
66 OP_XORI,
67 0x8000ffff,
68 0xffff,
69 0x80000000
70 },
71 {
72 OP_XORIS,
73 0x00008000,
74 0xffff,
75 0xffff8000
76 },
77 };
78 static unsigned int cpu_post_threei_size =
79 sizeof (cpu_post_threei_table) / sizeof (struct cpu_post_threei_s);
81 int cpu_post_test_threei (void)
82 {
83 int ret = 0;
84 unsigned int i, reg;
85 int flag = disable_interrupts();
87 for (i = 0; i < cpu_post_threei_size && ret == 0; i++)
88 {
89 struct cpu_post_threei_s *test = cpu_post_threei_table + i;
91 for (reg = 0; reg < 32 && ret == 0; reg++)
92 {
93 unsigned int reg0 = (reg + 0) % 32;
94 unsigned int reg1 = (reg + 1) % 32;
95 unsigned int stk = reg < 16 ? 31 : 15;
96 unsigned long code[] =
97 {
98 ASM_STW(stk, 1, -4),
99 ASM_ADDI(stk, 1, -16),
100 ASM_STW(3, stk, 8),
101 ASM_STW(reg0, stk, 4),
102 ASM_STW(reg1, stk, 0),
103 ASM_LWZ(reg0, stk, 8),
104 ASM_11IX(test->cmd, reg1, reg0, test->op2),
105 ASM_STW(reg1, stk, 8),
106 ASM_LWZ(reg1, stk, 0),
107 ASM_LWZ(reg0, stk, 4),
108 ASM_LWZ(3, stk, 8),
109 ASM_ADDI(1, stk, 16),
110 ASM_LWZ(stk, 1, -4),
111 ASM_BLR,
112 };
113 ulong res;
114 ulong cr;
116 cr = 0;
117 cpu_post_exec_21 (code, & cr, & res, test->op1);
119 ret = res == test->res && cr == 0 ? 0 : -1;
121 if (ret != 0)
122 {
123 post_log ("Error at threei test %d !\n", i);
124 }
125 }
126 }
128 if (flag)
129 enable_interrupts();
131 return ret;
132 }
134 #endif