1 /*
2 * (C) Copyright 2002
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 *
23 * Be sure to mark tests to be run before relocation as such with the
24 * CFG_POST_PREREL flag so that logging is done correctly if the
25 * logbuffer support is enabled.
26 */
28 #include <common.h>
30 #ifdef CONFIG_POST
32 #include <post.h>
34 extern int cache_post_test (int flags);
35 extern int watchdog_post_test (int flags);
36 extern int i2c_post_test (int flags);
37 extern int rtc_post_test (int flags);
38 extern int memory_post_test (int flags);
39 extern int cpu_post_test (int flags);
40 extern int uart_post_test (int flags);
41 extern int ether_post_test (int flags);
42 extern int spi_post_test (int flags);
43 extern int usb_post_test (int flags);
44 extern int spr_post_test (int flags);
45 extern int sysmon_post_test (int flags);
47 extern int sysmon_init_f (void);
49 extern void sysmon_reloc (void);
52 struct post_test post_list[] =
53 {
54 #if CONFIG_POST & CFG_POST_CACHE
55 {
56 "Cache test",
57 "cache",
58 "This test verifies the CPU cache operation.",
59 POST_RAM | POST_ALWAYS,
60 &cache_post_test,
61 NULL,
62 NULL,
63 CFG_POST_CACHE
64 },
65 #endif
66 #if CONFIG_POST & CFG_POST_WATCHDOG
67 {
68 "Watchdog timer test",
69 "watchdog",
70 "This test checks the watchdog timer.",
71 POST_RAM | POST_POWERON | POST_POWERFAIL | POST_MANUAL | POST_REBOOT,
72 &watchdog_post_test,
73 NULL,
74 NULL,
75 CFG_POST_WATCHDOG
76 },
77 #endif
78 #if CONFIG_POST & CFG_POST_I2C
79 {
80 "I2C test",
81 "i2c",
82 "This test verifies the I2C operation.",
83 POST_RAM | POST_ALWAYS,
84 &i2c_post_test,
85 NULL,
86 NULL,
87 CFG_POST_I2C
88 },
89 #endif
90 #if CONFIG_POST & CFG_POST_RTC
91 {
92 "RTC test",
93 "rtc",
94 "This test verifies the RTC operation.",
95 POST_RAM | POST_POWERFAIL | POST_MANUAL,
96 &rtc_post_test,
97 NULL,
98 NULL,
99 CFG_POST_RTC
100 },
101 #endif
102 #if CONFIG_POST & CFG_POST_MEMORY
103 {
104 "Memory test",
105 "memory",
106 "This test checks RAM.",
107 POST_ROM | POST_POWERON | POST_POWERFAIL | POST_PREREL,
108 &memory_post_test,
109 NULL,
110 NULL,
111 CFG_POST_MEMORY
112 },
113 #endif
114 #if CONFIG_POST & CFG_POST_CPU
115 {
116 "CPU test",
117 "cpu",
118 "This test verifies the arithmetic logic unit of"
119 " CPU.",
120 POST_RAM | POST_ALWAYS,
121 &cpu_post_test,
122 NULL,
123 NULL,
124 CFG_POST_CPU
125 },
126 #endif
127 #if CONFIG_POST & CFG_POST_UART
128 {
129 "UART test",
130 "uart",
131 "This test verifies the UART operation.",
132 POST_RAM | POST_POWERFAIL | POST_MANUAL,
133 &uart_post_test,
134 NULL,
135 NULL,
136 CFG_POST_UART
137 },
138 #endif
139 #if CONFIG_POST & CFG_POST_ETHER
140 {
141 "ETHERNET test",
142 "ethernet",
143 "This test verifies the ETHERNET operation.",
144 POST_RAM | POST_ALWAYS | POST_MANUAL,
145 ðer_post_test,
146 NULL,
147 NULL,
148 CFG_POST_ETHER
149 },
150 #endif
151 #if CONFIG_POST & CFG_POST_SPI
152 {
153 "SPI test",
154 "spi",
155 "This test verifies the SPI operation.",
156 POST_RAM | POST_ALWAYS | POST_MANUAL,
157 &spi_post_test,
158 NULL,
159 NULL,
160 CFG_POST_SPI
161 },
162 #endif
163 #if CONFIG_POST & CFG_POST_USB
164 {
165 "USB test",
166 "usb",
167 "This test verifies the USB operation.",
168 POST_RAM | POST_ALWAYS | POST_MANUAL,
169 &usb_post_test,
170 NULL,
171 NULL,
172 CFG_POST_USB
173 },
174 #endif
175 #if CONFIG_POST & CFG_POST_SPR
176 {
177 "SPR test",
178 "spr",
179 "This test checks SPR contents.",
180 POST_ROM | POST_ALWAYS | POST_PREREL,
181 &spr_post_test,
182 NULL,
183 NULL,
184 CFG_POST_SPR
185 },
186 #endif
187 #if CONFIG_POST & CFG_POST_SYSMON
188 {
189 "SYSMON test",
190 "sysmon",
191 "This test monitors system hardware.",
192 POST_RAM | POST_ALWAYS,
193 &sysmon_post_test,
194 &sysmon_init_f,
195 &sysmon_reloc,
196 CFG_POST_SYSMON
197 },
198 #endif
199 };
201 unsigned int post_list_size = sizeof (post_list) / sizeof (struct post_test);
203 #endif /* CONFIG_POST */