]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - post/tests.c
Merge branch 'master' of git://www.denx.de/git/u-boot-at91
[glsdk/glsdk-u-boot.git] / post / tests.c
1 /*
2  * (C) Copyright 2002
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  *
23  * Be sure to mark tests to be run before relocation as such with the
24  * CFG_POST_PREREL flag so that logging is done correctly if the
25  * logbuffer support is enabled.
26  */
28 #include <common.h>
30 #include <post.h>
32 extern int ocm_post_test (int flags);
33 extern int cache_post_test (int flags);
34 extern int watchdog_post_test (int flags);
35 extern int i2c_post_test (int flags);
36 extern int rtc_post_test (int flags);
37 extern int memory_post_test (int flags);
38 extern int cpu_post_test (int flags);
39 extern int fpu_post_test (int flags);
40 extern int uart_post_test (int flags);
41 extern int ether_post_test (int flags);
42 extern int spi_post_test (int flags);
43 extern int usb_post_test (int flags);
44 extern int spr_post_test (int flags);
45 extern int sysmon_post_test (int flags);
46 extern int dsp_post_test (int flags);
47 extern int codec_post_test (int flags);
48 extern int ecc_post_test (int flags);
50 extern int dspic_init_post_test (int flags);
51 extern int dspic_post_test (int flags);
52 extern int gdc_post_test (int flags);
53 extern int fpga_post_test (int flags);
54 extern int lwmon5_watchdog_post_test(int flags);
55 extern int sysmon1_post_test(int flags);
57 extern int sysmon_init_f (void);
59 extern void sysmon_reloc (void);
62 struct post_test post_list[] =
63 {
64 #if CONFIG_POST & CFG_POST_OCM
65     {
66         "OCM test",
67         "ocm",
68         "This test checks on chip memory (OCM).",
69         POST_ROM | POST_ALWAYS | POST_PREREL | POST_CRITICAL | POST_STOP,
70         &ocm_post_test,
71         NULL,
72         NULL,
73         CFG_POST_OCM
74     },
75 #endif
76 #if CONFIG_POST & CFG_POST_CACHE
77     {
78         "Cache test",
79         "cache",
80         "This test verifies the CPU cache operation.",
81         POST_RAM | POST_ALWAYS,
82         &cache_post_test,
83         NULL,
84         NULL,
85         CFG_POST_CACHE
86     },
87 #endif
88 #if CONFIG_POST & CFG_POST_WATCHDOG
89 #if defined(CONFIG_POST_WATCHDOG)
90         CONFIG_POST_WATCHDOG,
91 #else
92     {
93         "Watchdog timer test",
94         "watchdog",
95         "This test checks the watchdog timer.",
96         POST_RAM | POST_POWERON | POST_SLOWTEST | POST_MANUAL | POST_REBOOT,
97         &watchdog_post_test,
98         NULL,
99         NULL,
100         CFG_POST_WATCHDOG
101     },
102 #endif
103 #endif
104 #if CONFIG_POST & CFG_POST_I2C
105     {
106         "I2C test",
107         "i2c",
108         "This test verifies the I2C operation.",
109         POST_RAM | POST_ALWAYS,
110         &i2c_post_test,
111         NULL,
112         NULL,
113         CFG_POST_I2C
114     },
115 #endif
116 #if CONFIG_POST & CFG_POST_RTC
117     {
118         "RTC test",
119         "rtc",
120         "This test verifies the RTC operation.",
121         POST_RAM | POST_SLOWTEST | POST_MANUAL,
122         &rtc_post_test,
123         NULL,
124         NULL,
125         CFG_POST_RTC
126     },
127 #endif
128 #if CONFIG_POST & CFG_POST_MEMORY
129     {
130         "Memory test",
131         "memory",
132         "This test checks RAM.",
133         POST_ROM | POST_POWERON | POST_SLOWTEST | POST_PREREL,
134         &memory_post_test,
135         NULL,
136         NULL,
137         CFG_POST_MEMORY
138     },
139 #endif
140 #if CONFIG_POST & CFG_POST_CPU
141     {
142         "CPU test",
143         "cpu",
144         "This test verifies the arithmetic logic unit of"
145         " CPU.",
146         POST_RAM | POST_ALWAYS,
147         &cpu_post_test,
148         NULL,
149         NULL,
150         CFG_POST_CPU
151     },
152 #endif
153 #if CONFIG_POST & CFG_POST_FPU
154     {
155         "FPU test",
156         "fpu",
157         "This test verifies the arithmetic logic unit of"
158         " FPU.",
159         POST_RAM | POST_ALWAYS,
160         &fpu_post_test,
161         NULL,
162         NULL,
163         CFG_POST_FPU
164     },
165 #endif
166 #if CONFIG_POST & CFG_POST_UART
167     {
168         "UART test",
169         "uart",
170         "This test verifies the UART operation.",
171         POST_RAM | POST_SLOWTEST | POST_MANUAL,
172         &uart_post_test,
173         NULL,
174         NULL,
175         CFG_POST_UART
176     },
177 #endif
178 #if CONFIG_POST & CFG_POST_ETHER
179     {
180         "ETHERNET test",
181         "ethernet",
182         "This test verifies the ETHERNET operation.",
183         POST_RAM | POST_ALWAYS | POST_MANUAL,
184         &ether_post_test,
185         NULL,
186         NULL,
187         CFG_POST_ETHER
188     },
189 #endif
190 #if CONFIG_POST & CFG_POST_SPI
191     {
192         "SPI test",
193         "spi",
194         "This test verifies the SPI operation.",
195         POST_RAM | POST_ALWAYS | POST_MANUAL,
196         &spi_post_test,
197         NULL,
198         NULL,
199         CFG_POST_SPI
200     },
201 #endif
202 #if CONFIG_POST & CFG_POST_USB
203     {
204         "USB test",
205         "usb",
206         "This test verifies the USB operation.",
207         POST_RAM | POST_ALWAYS | POST_MANUAL,
208         &usb_post_test,
209         NULL,
210         NULL,
211         CFG_POST_USB
212     },
213 #endif
214 #if CONFIG_POST & CFG_POST_SPR
215     {
216         "SPR test",
217         "spr",
218         "This test checks SPR contents.",
219         POST_RAM | POST_ALWAYS,
220         &spr_post_test,
221         NULL,
222         NULL,
223         CFG_POST_SPR
224     },
225 #endif
226 #if CONFIG_POST & CFG_POST_SYSMON
227     {
228         "SYSMON test",
229         "sysmon",
230         "This test monitors system hardware.",
231         POST_RAM | POST_ALWAYS,
232         &sysmon_post_test,
233         &sysmon_init_f,
234         &sysmon_reloc,
235         CFG_POST_SYSMON
236     },
237 #endif
238 #if CONFIG_POST & CFG_POST_DSP
239     {
240         "DSP test",
241         "dsp",
242         "This test checks any connected DSP(s).",
243         POST_RAM | POST_ALWAYS | POST_MANUAL,
244         &dsp_post_test,
245         NULL,
246         NULL,
247         CFG_POST_DSP
248     },
249 #endif
250 #if CONFIG_POST & CFG_POST_CODEC
251     {
252         "CODEC test",
253         "codec",
254         "This test checks any connected codec(s).",
255         POST_RAM | POST_MANUAL,
256         &codec_post_test,
257         NULL,
258         NULL,
259         CFG_POST_CODEC
260     },
261 #endif
262 #if CONFIG_POST & CFG_POST_ECC
263     {
264         "ECC test",
265         "ecc",
266         "This test checks the ECC facility of memory.",
267         POST_ROM | POST_ALWAYS | POST_PREREL,
268         &ecc_post_test,
269         NULL,
270         NULL,
271         CFG_POST_ECC
272     },
273 #endif
274 #if CONFIG_POST & CFG_POST_BSPEC1
275         CONFIG_POST_BSPEC1,
276 #endif
277 #if CONFIG_POST & CFG_POST_BSPEC2
278         CONFIG_POST_BSPEC2,
279 #endif
280 #if CONFIG_POST & CFG_POST_BSPEC3
281         CONFIG_POST_BSPEC3,
282 #endif
283 #if CONFIG_POST & CFG_POST_BSPEC4
284         CONFIG_POST_BSPEC4,
285 #endif
286 #if CONFIG_POST & CFG_POST_BSPEC5
287         CONFIG_POST_BSPEC5,
288 #endif
289 };
291 unsigned int post_list_size = sizeof (post_list) / sizeof (struct post_test);