]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - post/tests.c
Merge branch 'master' of git://git.denx.de/u-boot-arm
[glsdk/glsdk-u-boot.git] / post / tests.c
1 /*
2  * (C) Copyright 2002
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  *
23  * Be sure to mark tests to be run before relocation as such with the
24  * CONFIG_SYS_POST_PREREL flag so that logging is done correctly if the
25  * logbuffer support is enabled.
26  */
28 #include <common.h>
30 #include <post.h>
32 extern int ocm_post_test (int flags);
33 extern int cache_post_test (int flags);
34 extern int watchdog_post_test (int flags);
35 extern int i2c_post_test (int flags);
36 extern int rtc_post_test (int flags);
37 extern int memory_post_test (int flags);
38 extern int cpu_post_test (int flags);
39 extern int fpu_post_test (int flags);
40 extern int uart_post_test (int flags);
41 extern int ether_post_test (int flags);
42 extern int spi_post_test (int flags);
43 extern int usb_post_test (int flags);
44 extern int spr_post_test (int flags);
45 extern int sysmon_post_test (int flags);
46 extern int dsp_post_test (int flags);
47 extern int codec_post_test (int flags);
48 extern int ecc_post_test (int flags);
50 extern int dspic_init_post_test (int flags);
51 extern int dspic_post_test (int flags);
52 extern int gdc_post_test (int flags);
53 extern int fpga_post_test (int flags);
54 extern int lwmon5_watchdog_post_test(int flags);
55 extern int sysmon1_post_test(int flags);
56 extern int coprocessor_post_test(int flags);
58 extern int sysmon_init_f (void);
60 extern void sysmon_reloc (void);
63 struct post_test post_list[] =
64 {
65 #if CONFIG_POST & CONFIG_SYS_POST_OCM
66     {
67         "OCM test",
68         "ocm",
69         "This test checks on chip memory (OCM).",
70         POST_ROM | POST_ALWAYS | POST_PREREL | POST_CRITICAL | POST_STOP,
71         &ocm_post_test,
72         NULL,
73         NULL,
74         CONFIG_SYS_POST_OCM
75     },
76 #endif
77 #if CONFIG_POST & CONFIG_SYS_POST_CACHE
78     {
79         "Cache test",
80         "cache",
81         "This test verifies the CPU cache operation.",
82         POST_RAM | POST_ALWAYS,
83         &cache_post_test,
84         NULL,
85         NULL,
86         CONFIG_SYS_POST_CACHE
87     },
88 #endif
89 #if CONFIG_POST & CONFIG_SYS_POST_WATCHDOG
90 #if defined(CONFIG_POST_WATCHDOG)
91         CONFIG_POST_WATCHDOG,
92 #else
93     {
94         "Watchdog timer test",
95         "watchdog",
96         "This test checks the watchdog timer.",
97         POST_RAM | POST_POWERON | POST_SLOWTEST | POST_MANUAL | POST_REBOOT,
98         &watchdog_post_test,
99         NULL,
100         NULL,
101         CONFIG_SYS_POST_WATCHDOG
102     },
103 #endif
104 #endif
105 #if CONFIG_POST & CONFIG_SYS_POST_I2C
106     {
107         "I2C test",
108         "i2c",
109         "This test verifies the I2C operation.",
110         POST_RAM | POST_ALWAYS,
111         &i2c_post_test,
112         NULL,
113         NULL,
114         CONFIG_SYS_POST_I2C
115     },
116 #endif
117 #if CONFIG_POST & CONFIG_SYS_POST_RTC
118     {
119         "RTC test",
120         "rtc",
121         "This test verifies the RTC operation.",
122         POST_RAM | POST_SLOWTEST | POST_MANUAL,
123         &rtc_post_test,
124         NULL,
125         NULL,
126         CONFIG_SYS_POST_RTC
127     },
128 #endif
129 #if CONFIG_POST & CONFIG_SYS_POST_MEMORY
130     {
131         "Memory test",
132         "memory",
133         "This test checks RAM.",
134         POST_ROM | POST_POWERON | POST_SLOWTEST | POST_PREREL,
135         &memory_post_test,
136         NULL,
137         NULL,
138         CONFIG_SYS_POST_MEMORY
139     },
140 #endif
141 #if CONFIG_POST & CONFIG_SYS_POST_CPU
142     {
143         "CPU test",
144         "cpu",
145         "This test verifies the arithmetic logic unit of"
146         " CPU.",
147         POST_RAM | POST_ALWAYS,
148         &cpu_post_test,
149         NULL,
150         NULL,
151         CONFIG_SYS_POST_CPU
152     },
153 #endif
154 #if CONFIG_POST & CONFIG_SYS_POST_FPU
155     {
156         "FPU test",
157         "fpu",
158         "This test verifies the arithmetic logic unit of"
159         " FPU.",
160         POST_RAM | POST_ALWAYS,
161         &fpu_post_test,
162         NULL,
163         NULL,
164         CONFIG_SYS_POST_FPU
165     },
166 #endif
167 #if CONFIG_POST & CONFIG_SYS_POST_UART
168     {
169         "UART test",
170         "uart",
171         "This test verifies the UART operation.",
172         POST_RAM | POST_SLOWTEST | POST_MANUAL,
173         &uart_post_test,
174         NULL,
175         NULL,
176         CONFIG_SYS_POST_UART
177     },
178 #endif
179 #if CONFIG_POST & CONFIG_SYS_POST_ETHER
180     {
181         "ETHERNET test",
182         "ethernet",
183         "This test verifies the ETHERNET operation.",
184         POST_RAM | POST_ALWAYS | POST_MANUAL,
185         &ether_post_test,
186         NULL,
187         NULL,
188         CONFIG_SYS_POST_ETHER
189     },
190 #endif
191 #if CONFIG_POST & CONFIG_SYS_POST_SPI
192     {
193         "SPI test",
194         "spi",
195         "This test verifies the SPI operation.",
196         POST_RAM | POST_ALWAYS | POST_MANUAL,
197         &spi_post_test,
198         NULL,
199         NULL,
200         CONFIG_SYS_POST_SPI
201     },
202 #endif
203 #if CONFIG_POST & CONFIG_SYS_POST_USB
204     {
205         "USB test",
206         "usb",
207         "This test verifies the USB operation.",
208         POST_RAM | POST_ALWAYS | POST_MANUAL,
209         &usb_post_test,
210         NULL,
211         NULL,
212         CONFIG_SYS_POST_USB
213     },
214 #endif
215 #if CONFIG_POST & CONFIG_SYS_POST_SPR
216     {
217         "SPR test",
218         "spr",
219         "This test checks SPR contents.",
220         POST_RAM | POST_ALWAYS,
221         &spr_post_test,
222         NULL,
223         NULL,
224         CONFIG_SYS_POST_SPR
225     },
226 #endif
227 #if CONFIG_POST & CONFIG_SYS_POST_SYSMON
228     {
229         "SYSMON test",
230         "sysmon",
231         "This test monitors system hardware.",
232         POST_RAM | POST_ALWAYS,
233         &sysmon_post_test,
234         &sysmon_init_f,
235         &sysmon_reloc,
236         CONFIG_SYS_POST_SYSMON
237     },
238 #endif
239 #if CONFIG_POST & CONFIG_SYS_POST_DSP
240     {
241         "DSP test",
242         "dsp",
243         "This test checks any connected DSP(s).",
244         POST_RAM | POST_ALWAYS | POST_MANUAL,
245         &dsp_post_test,
246         NULL,
247         NULL,
248         CONFIG_SYS_POST_DSP
249     },
250 #endif
251 #if CONFIG_POST & CONFIG_SYS_POST_CODEC
252     {
253         "CODEC test",
254         "codec",
255         "This test checks any connected codec(s).",
256         POST_RAM | POST_MANUAL,
257         &codec_post_test,
258         NULL,
259         NULL,
260         CONFIG_SYS_POST_CODEC
261     },
262 #endif
263 #if CONFIG_POST & CONFIG_SYS_POST_ECC
264     {
265         "ECC test",
266         "ecc",
267         "This test checks the ECC facility of memory.",
268         POST_ROM | POST_ALWAYS | POST_PREREL,
269         &ecc_post_test,
270         NULL,
271         NULL,
272         CONFIG_SYS_POST_ECC
273     },
274 #endif
275 #if CONFIG_POST & CONFIG_SYS_POST_BSPEC1
276         CONFIG_POST_BSPEC1,
277 #endif
278 #if CONFIG_POST & CONFIG_SYS_POST_BSPEC2
279         CONFIG_POST_BSPEC2,
280 #endif
281 #if CONFIG_POST & CONFIG_SYS_POST_BSPEC3
282         CONFIG_POST_BSPEC3,
283 #endif
284 #if CONFIG_POST & CONFIG_SYS_POST_BSPEC4
285         CONFIG_POST_BSPEC4,
286 #endif
287 #if CONFIG_POST & CONFIG_SYS_POST_BSPEC5
288         CONFIG_POST_BSPEC5,
289 #endif
290 #if CONFIG_POST & CONFIG_SYS_POST_COPROC
291     {
292         "Coprocessors communication test",
293         "coproc_com",
294         "This test checks communication with coprocessors.",
295         POST_RAM | POST_ALWAYS | POST_CRITICAL,
296         &coprocessor_post_test,
297         NULL,
298         NULL,
299         CONFIG_SYS_POST_COPROC
300     }
301 #endif
302 };
304 unsigned int post_list_size = sizeof (post_list) / sizeof (struct post_test);